1 //===- README_X86_64.txt - Notes for X86-64 code gen ----------------------===//
3 AMD64 Optimization Manual 8.2 has some nice information about optimizing integer
4 multiplication by a constant. How much of it applies to Intel's X86-64
5 implementation? There are definite trade-offs to consider: latency vs. register
6 pressure vs. code size.
8 //===---------------------------------------------------------------------===//
10 Are we better off using branches instead of cmove to implement FP to
11 unsigned i64?
13 _conv:
14 ucomiss LC0(%rip), %xmm0
15 cvttss2siq %xmm0, %rdx
16 jb L3
17 subss LC0(%rip), %xmm0
18 movabsq $-9223372036854775808, %rax
19 cvttss2siq %xmm0, %rdx
20 xorq %rax, %rdx
21 L3:
22 movq %rdx, %rax
23 ret
25 instead of
27 _conv:
28 movss LCPI1_0(%rip), %xmm1
29 cvttss2siq %xmm0, %rcx
30 movaps %xmm0, %xmm2
31 subss %xmm1, %xmm2
32 cvttss2siq %xmm2, %rax
33 movabsq $-9223372036854775808, %rdx
34 xorq %rdx, %rax
35 ucomiss %xmm1, %xmm0
36 cmovb %rcx, %rax
37 ret
39 Seems like the jb branch has high likelihood of being taken. It would have
40 saved a few instructions.
42 //===---------------------------------------------------------------------===//
44 It's not possible to reference AH, BH, CH, and DH registers in an instruction
45 requiring REX prefix. However, divb and mulb both produce results in AH. If isel
46 emits a CopyFromReg which gets turned into a movb and that can be allocated a
47 r8b - r15b.
49 To get around this, isel emits a CopyFromReg from AX and then right shift it
50 down by 8 and truncate it. It's not pretty but it works. We need some register
51 allocation magic to make the hack go away (e.g. putting additional constraints
52 on the result of the movb).
54 //===---------------------------------------------------------------------===//
56 The x86-64 ABI for hidden-argument struct returns requires that the
57 incoming value of %rdi be copied into %rax by the callee upon return.
59 The idea is that it saves callers from having to remember this value,
60 which would often require a callee-saved register. Callees usually
61 need to keep this value live for most of their body anyway, so it
62 doesn't add a significant burden on them.
64 We currently implement this in codegen, however this is suboptimal
65 because it means that it would be quite awkward to implement the
66 optimization for callers.
68 A better implementation would be to relax the LLVM IR rules for sret
69 arguments to allow a function with an sret argument to have a non-void
70 return type, and to have the front-end to set up the sret argument value
71 as the return value of the function. The front-end could more easily
72 emit uses of the returned struct value to be in terms of the function's
73 lowered return value, and it would free non-C frontends from a
74 complication only required by a C-based ABI.
76 //===---------------------------------------------------------------------===//
78 We get a redundant zero extension for code like this:
80 int mask[1000];
81 int foo(unsigned x) {
82 if (x < 10)
83 x = x * 45;
84 else
85 x = x * 78;
86 return mask[x];
87 }
89 _foo:
90 LBB1_0: ## entry
91 cmpl $9, %edi
92 jbe LBB1_3 ## bb
93 LBB1_1: ## bb1
94 imull $78, %edi, %eax
95 LBB1_2: ## bb2
96 movl %eax, %eax <----
97 movq _mask@GOTPCREL(%rip), %rcx
98 movl (%rcx,%rax,4), %eax
99 ret
100 LBB1_3: ## bb
101 imull $45, %edi, %eax
102 jmp LBB1_2 ## bb2
104 Before regalloc, we have:
106 %reg1025<def> = IMUL32rri8 %reg1024, 45, %EFLAGS<imp-def>
107 JMP mbb<bb2,0x203afb0>
108 Successors according to CFG: 0x203afb0 (#3)
110 bb1: 0x203af60, LLVM BB @0x1e02310, ID#2:
111 Predecessors according to CFG: 0x203aec0 (#0)
112 %reg1026<def> = IMUL32rri8 %reg1024, 78, %EFLAGS<imp-def>
113 Successors according to CFG: 0x203afb0 (#3)
115 bb2: 0x203afb0, LLVM BB @0x1e02340, ID#3:
116 Predecessors according to CFG: 0x203af10 (#1) 0x203af60 (#2)
117 %reg1027<def> = PHI %reg1025, mbb<bb,0x203af10>,
118 %reg1026, mbb<bb1,0x203af60>
119 %reg1029<def> = MOVZX64rr32 %reg1027
121 so we'd have to know that IMUL32rri8 leaves the high word zero extended and to
122 be able to recognize the zero extend. This could also presumably be implemented
123 if we have whole-function selectiondags.
125 //===---------------------------------------------------------------------===//
127 Take the following code
128 (from http://gcc.gnu.org/bugzilla/show_bug.cgi?id=34653):
129 extern unsigned long table[];
130 unsigned long foo(unsigned char *p) {
131 unsigned long tag = *p;
132 return table[tag >> 4] + table[tag & 0xf];
133 }
135 Current code generated:
136 movzbl (%rdi), %eax
137 movq %rax, %rcx
138 andq $240, %rcx
139 shrq %rcx
140 andq $15, %rax
141 movq table(,%rax,8), %rax
142 addq table(%rcx), %rax
143 ret
145 Issues:
146 1. First movq should be movl; saves a byte.
147 2. Both andq's should be andl; saves another two bytes. I think this was
148 implemented at one point, but subsequently regressed.
149 3. shrq should be shrl; saves another byte.
150 4. The first andq can be completely eliminated by using a slightly more
151 expensive addressing mode.
153 //===---------------------------------------------------------------------===//
155 Consider the following (contrived testcase, but contains common factors):
157 #include <stdarg.h>
158 int test(int x, ...) {
159 int sum, i;
160 va_list l;
161 va_start(l, x);
162 for (i = 0; i < x; i++)
163 sum += va_arg(l, int);
164 va_end(l);
165 return sum;
166 }
168 Testcase given in C because fixing it will likely involve changing the IR
169 generated for it. The primary issue with the result is that it doesn't do any
170 of the optimizations which are possible if we know the address of a va_list
171 in the current function is never taken:
172 1. We shouldn't spill the XMM registers because we only call va_arg with "int".
173 2. It would be nice if we could scalarrepl the va_list.
174 3. Probably overkill, but it'd be cool if we could peel off the first five
175 iterations of the loop.
177 Other optimizations involving functions which use va_arg on floats which don't
178 have the address of a va_list taken:
179 1. Conversely to the above, we shouldn't spill general registers if we only
180 call va_arg on "double".
181 2. If we know nothing more than 64 bits wide is read from the XMM registers,
182 we can change the spilling code to reduce the amount of stack used by half.
184 //===---------------------------------------------------------------------===//