1 //===-- X86TargetMachine.cpp - Define TargetMachine for the X86 -----------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file defines the X86 specific subclass of TargetMachine.
11 //
12 //===----------------------------------------------------------------------===//
14 #include "X86TargetMachine.h"
15 #include "X86.h"
16 #include "X86TargetObjectFile.h"
17 #include "llvm/CodeGen/Passes.h"
18 #include "llvm/IR/Function.h"
19 #include "llvm/PassManager.h"
20 #include "llvm/Support/CommandLine.h"
21 #include "llvm/Support/FormattedStream.h"
22 #include "llvm/Support/TargetRegistry.h"
23 #include "llvm/Target/TargetOptions.h"
24 using namespace llvm;
26 extern "C" void LLVMInitializeX86Target() {
27 // Register the target.
28 RegisterTargetMachine<X86TargetMachine> X(TheX86_32Target);
29 RegisterTargetMachine<X86TargetMachine> Y(TheX86_64Target);
30 }
32 static std::unique_ptr<TargetLoweringObjectFile> createTLOF(const Triple &TT) {
33 if (TT.isOSBinFormatMachO()) {
34 if (TT.getArch() == Triple::x86_64)
35 return make_unique<X86_64MachoTargetObjectFile>();
36 return make_unique<TargetLoweringObjectFileMachO>();
37 }
39 if (TT.isOSLinux())
40 return make_unique<X86LinuxTargetObjectFile>();
41 if (TT.isOSBinFormatELF())
42 return make_unique<TargetLoweringObjectFileELF>();
43 if (TT.isKnownWindowsMSVCEnvironment())
44 return make_unique<X86WindowsTargetObjectFile>();
45 if (TT.isOSBinFormatCOFF())
46 return make_unique<TargetLoweringObjectFileCOFF>();
47 llvm_unreachable("unknown subtarget type");
48 }
50 /// X86TargetMachine ctor - Create an X86 target.
51 ///
52 X86TargetMachine::X86TargetMachine(const Target &T, StringRef TT, StringRef CPU,
53 StringRef FS, const TargetOptions &Options,
54 Reloc::Model RM, CodeModel::Model CM,
55 CodeGenOpt::Level OL)
56 : LLVMTargetMachine(T, TT, CPU, FS, Options, RM, CM, OL),
57 TLOF(createTLOF(Triple(getTargetTriple()))),
58 Subtarget(TT, CPU, FS, *this, Options.StackAlignmentOverride) {
59 // default to hard float ABI
60 if (Options.FloatABIType == FloatABI::Default)
61 this->Options.FloatABIType = FloatABI::Hard;
63 // Windows stack unwinder gets confused when execution flow "falls through"
64 // after a call to 'noreturn' function.
65 // To prevent that, we emit a trap for 'unreachable' IR instructions.
66 // (which on X86, happens to be the 'ud2' instruction)
67 if (Subtarget.isTargetWin64())
68 this->Options.TrapUnreachable = true;
70 initAsmInfo();
71 }
73 X86TargetMachine::~X86TargetMachine() {}
75 const X86Subtarget *
76 X86TargetMachine::getSubtargetImpl(const Function &F) const {
77 AttributeSet FnAttrs = F.getAttributes();
78 Attribute CPUAttr =
79 FnAttrs.getAttribute(AttributeSet::FunctionIndex, "target-cpu");
80 Attribute FSAttr =
81 FnAttrs.getAttribute(AttributeSet::FunctionIndex, "target-features");
83 std::string CPU = !CPUAttr.hasAttribute(Attribute::None)
84 ? CPUAttr.getValueAsString().str()
85 : TargetCPU;
86 std::string FS = !FSAttr.hasAttribute(Attribute::None)
87 ? FSAttr.getValueAsString().str()
88 : TargetFS;
90 // FIXME: This is related to the code below to reset the target options,
91 // we need to know whether or not the soft float flag is set on the
92 // function before we can generate a subtarget. We also need to use
93 // it as a key for the subtarget since that can be the only difference
94 // between two functions.
95 Attribute SFAttr =
96 FnAttrs.getAttribute(AttributeSet::FunctionIndex, "use-soft-float");
97 bool SoftFloat = !SFAttr.hasAttribute(Attribute::None)
98 ? SFAttr.getValueAsString() == "true"
99 : Options.UseSoftFloat;
101 auto &I = SubtargetMap[CPU + FS + (SoftFloat ? "use-soft-float=true"
102 : "use-soft-float=false")];
103 if (!I) {
104 // This needs to be done before we create a new subtarget since any
105 // creation will depend on the TM and the code generation flags on the
106 // function that reside in TargetOptions.
107 resetTargetOptions(F);
108 I = llvm::make_unique<X86Subtarget>(TargetTriple, CPU, FS, *this,
109 Options.StackAlignmentOverride);
110 }
111 return I.get();
112 }
114 //===----------------------------------------------------------------------===//
115 // Command line options for x86
116 //===----------------------------------------------------------------------===//
117 static cl::opt<bool>
118 UseVZeroUpper("x86-use-vzeroupper", cl::Hidden,
119 cl::desc("Minimize AVX to SSE transition penalty"),
120 cl::init(true));
122 //===----------------------------------------------------------------------===//
123 // X86 Analysis Pass Setup
124 //===----------------------------------------------------------------------===//
126 void X86TargetMachine::addAnalysisPasses(PassManagerBase &PM) {
127 // Add first the target-independent BasicTTI pass, then our X86 pass. This
128 // allows the X86 pass to delegate to the target independent layer when
129 // appropriate.
130 PM.add(createBasicTargetTransformInfoPass(this));
131 PM.add(createX86TargetTransformInfoPass(this));
132 }
135 //===----------------------------------------------------------------------===//
136 // Pass Pipeline Configuration
137 //===----------------------------------------------------------------------===//
139 namespace {
140 /// X86 Code Generator Pass Configuration Options.
141 class X86PassConfig : public TargetPassConfig {
142 public:
143 X86PassConfig(X86TargetMachine *TM, PassManagerBase &PM)
144 : TargetPassConfig(TM, PM) {}
146 X86TargetMachine &getX86TargetMachine() const {
147 return getTM<X86TargetMachine>();
148 }
150 const X86Subtarget &getX86Subtarget() const {
151 return *getX86TargetMachine().getSubtargetImpl();
152 }
154 void addIRPasses() override;
155 bool addInstSelector() override;
156 bool addILPOpts() override;
157 void addPostRegAlloc() override;
158 void addPreEmitPass() override;
159 };
160 } // namespace
162 TargetPassConfig *X86TargetMachine::createPassConfig(PassManagerBase &PM) {
163 return new X86PassConfig(this, PM);
164 }
166 void X86PassConfig::addIRPasses() {
167 addPass(createAtomicExpandPass(&getX86TargetMachine()));
169 TargetPassConfig::addIRPasses();
170 }
172 bool X86PassConfig::addInstSelector() {
173 // Install an instruction selector.
174 addPass(createX86ISelDag(getX86TargetMachine(), getOptLevel()));
176 // For ELF, cleanup any local-dynamic TLS accesses.
177 if (getX86Subtarget().isTargetELF() && getOptLevel() != CodeGenOpt::None)
178 addPass(createCleanupLocalDynamicTLSPass());
180 addPass(createX86GlobalBaseRegPass());
182 return false;
183 }
185 bool X86PassConfig::addILPOpts() {
186 addPass(&EarlyIfConverterID);
187 return true;
188 }
190 void X86PassConfig::addPostRegAlloc() {
191 addPass(createX86FloatingPointStackifierPass());
192 }
194 void X86PassConfig::addPreEmitPass() {
195 if (getOptLevel() != CodeGenOpt::None && getX86Subtarget().hasSSE2())
196 addPass(createExecutionDependencyFixPass(&X86::VR128RegClass));
198 if (UseVZeroUpper)
199 addPass(createX86IssueVZeroUpperPass());
201 if (getOptLevel() != CodeGenOpt::None) {
202 addPass(createX86PadShortFunctions());
203 addPass(createX86FixupLEAs());
204 }
205 }