1 //===-- ArgumentPromotion.cpp - Promote by-reference arguments ------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This pass promotes "by reference" arguments to be "by value" arguments. In
11 // practice, this means looking for internal functions that have pointer
12 // arguments. If it can prove, through the use of alias analysis, that an
13 // argument is *only* loaded, then it can pass the value into the function
14 // instead of the address of the value. This can cause recursive simplification
15 // of code and lead to the elimination of allocas (especially in C++ template
16 // code like the STL).
17 //
18 // This pass also handles aggregate arguments that are passed into a function,
19 // scalarizing them if the elements of the aggregate are only loaded. Note that
20 // by default it refuses to scalarize aggregates which would require passing in
21 // more than three operands to the function, because passing thousands of
22 // operands for a large array or structure is unprofitable! This limit can be
23 // configured or disabled, however.
24 //
25 // Note that this transformation could also be done for arguments that are only
26 // stored to (returning the value instead), but does not currently. This case
27 // would be best handled when and if LLVM begins supporting multiple return
28 // values from functions.
29 //
30 //===----------------------------------------------------------------------===//
32 #define DEBUG_TYPE "argpromotion"
33 #include "llvm/Transforms/IPO.h"
34 #include "llvm/Constants.h"
35 #include "llvm/DerivedTypes.h"
36 #include "llvm/Module.h"
37 #include "llvm/CallGraphSCCPass.h"
38 #include "llvm/Instructions.h"
39 #include "llvm/LLVMContext.h"
40 #include "llvm/Analysis/AliasAnalysis.h"
41 #include "llvm/Analysis/CallGraph.h"
42 #include "llvm/Target/TargetData.h"
43 #include "llvm/Support/CallSite.h"
44 #include "llvm/Support/CFG.h"
45 #include "llvm/Support/Debug.h"
46 #include "llvm/Support/raw_ostream.h"
47 #include "llvm/ADT/DepthFirstIterator.h"
48 #include "llvm/ADT/Statistic.h"
49 #include "llvm/ADT/StringExtras.h"
50 #include <set>
51 using namespace llvm;
53 STATISTIC(NumArgumentsPromoted , "Number of pointer arguments promoted");
54 STATISTIC(NumAggregatesPromoted, "Number of aggregate arguments promoted");
55 STATISTIC(NumByValArgsPromoted , "Number of byval arguments promoted");
56 STATISTIC(NumArgumentsDead , "Number of dead pointer args eliminated");
58 namespace {
59 /// ArgPromotion - The 'by reference' to 'by value' argument promotion pass.
60 ///
61 struct ArgPromotion : public CallGraphSCCPass {
62 virtual void getAnalysisUsage(AnalysisUsage &AU) const {
63 AU.addRequired<AliasAnalysis>();
64 CallGraphSCCPass::getAnalysisUsage(AU);
65 }
67 virtual bool runOnSCC(std::vector<CallGraphNode *> &SCC);
68 static char ID; // Pass identification, replacement for typeid
69 explicit ArgPromotion(unsigned maxElements = 3)
70 : CallGraphSCCPass(&ID), maxElements(maxElements) {}
72 /// A vector used to hold the indices of a single GEP instruction
73 typedef std::vector<uint64_t> IndicesVector;
75 private:
76 CallGraphNode *PromoteArguments(CallGraphNode *CGN);
77 bool isSafeToPromoteArgument(Argument *Arg, bool isByVal) const;
78 CallGraphNode *DoPromotion(Function *F,
79 SmallPtrSet<Argument*, 8> &ArgsToPromote,
80 SmallPtrSet<Argument*, 8> &ByValArgsToTransform);
81 /// The maximum number of elements to expand, or 0 for unlimited.
82 unsigned maxElements;
83 };
84 }
86 char ArgPromotion::ID = 0;
87 static RegisterPass<ArgPromotion>
88 X("argpromotion", "Promote 'by reference' arguments to scalars");
90 Pass *llvm::createArgumentPromotionPass(unsigned maxElements) {
91 return new ArgPromotion(maxElements);
92 }
94 bool ArgPromotion::runOnSCC(std::vector<CallGraphNode *> &SCC) {
95 bool Changed = false, LocalChange;
97 do { // Iterate until we stop promoting from this SCC.
98 LocalChange = false;
99 // Attempt to promote arguments from all functions in this SCC.
100 for (unsigned i = 0, e = SCC.size(); i != e; ++i)
101 if (CallGraphNode *CGN = PromoteArguments(SCC[i])) {
102 LocalChange = true;
103 SCC[i] = CGN;
104 }
105 Changed |= LocalChange; // Remember that we changed something.
106 } while (LocalChange);
108 return Changed;
109 }
111 /// PromoteArguments - This method checks the specified function to see if there
112 /// are any promotable arguments and if it is safe to promote the function (for
113 /// example, all callers are direct). If safe to promote some arguments, it
114 /// calls the DoPromotion method.
115 ///
116 CallGraphNode *ArgPromotion::PromoteArguments(CallGraphNode *CGN) {
117 Function *F = CGN->getFunction();
119 // Make sure that it is local to this module.
120 if (!F || !F->hasLocalLinkage()) return 0;
122 // First check: see if there are any pointer arguments! If not, quick exit.
123 SmallVector<std::pair<Argument*, unsigned>, 16> PointerArgs;
124 unsigned ArgNo = 0;
125 for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end();
126 I != E; ++I, ++ArgNo)
127 if (I->getType()->isPointerTy())
128 PointerArgs.push_back(std::pair<Argument*, unsigned>(I, ArgNo));
129 if (PointerArgs.empty()) return 0;
131 // Second check: make sure that all callers are direct callers. We can't
132 // transform functions that have indirect callers.
133 if (F->hasAddressTaken())
134 return 0;
136 // Check to see which arguments are promotable. If an argument is promotable,
137 // add it to ArgsToPromote.
138 SmallPtrSet<Argument*, 8> ArgsToPromote;
139 SmallPtrSet<Argument*, 8> ByValArgsToTransform;
140 for (unsigned i = 0; i != PointerArgs.size(); ++i) {
141 bool isByVal = F->paramHasAttr(PointerArgs[i].second+1, Attribute::ByVal);
143 // If this is a byval argument, and if the aggregate type is small, just
144 // pass the elements, which is always safe.
145 Argument *PtrArg = PointerArgs[i].first;
146 if (isByVal) {
147 const Type *AgTy = cast<PointerType>(PtrArg->getType())->getElementType();
148 if (const StructType *STy = dyn_cast<StructType>(AgTy)) {
149 if (maxElements > 0 && STy->getNumElements() > maxElements) {
150 DEBUG(dbgs() << "argpromotion disable promoting argument '"
151 << PtrArg->getName() << "' because it would require adding more"
152 << " than " << maxElements << " arguments to the function.\n");
153 } else {
154 // If all the elements are single-value types, we can promote it.
155 bool AllSimple = true;
156 for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i)
157 if (!STy->getElementType(i)->isSingleValueType()) {
158 AllSimple = false;
159 break;
160 }
162 // Safe to transform, don't even bother trying to "promote" it.
163 // Passing the elements as a scalar will allow scalarrepl to hack on
164 // the new alloca we introduce.
165 if (AllSimple) {
166 ByValArgsToTransform.insert(PtrArg);
167 continue;
168 }
169 }
170 }
171 }
173 // Otherwise, see if we can promote the pointer to its value.
174 if (isSafeToPromoteArgument(PtrArg, isByVal))
175 ArgsToPromote.insert(PtrArg);
176 }
178 // No promotable pointer arguments.
179 if (ArgsToPromote.empty() && ByValArgsToTransform.empty())
180 return 0;
182 return DoPromotion(F, ArgsToPromote, ByValArgsToTransform);
183 }
185 /// IsAlwaysValidPointer - Return true if the specified pointer is always legal
186 /// to load.
187 static bool IsAlwaysValidPointer(Value *V) {
188 if (isa<AllocaInst>(V) || isa<GlobalVariable>(V)) return true;
189 if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(V))
190 return IsAlwaysValidPointer(GEP->getOperand(0));
191 if (ConstantExpr *CE = dyn_cast<ConstantExpr>(V))
192 if (CE->getOpcode() == Instruction::GetElementPtr)
193 return IsAlwaysValidPointer(CE->getOperand(0));
195 return false;
196 }
198 /// AllCalleesPassInValidPointerForArgument - Return true if we can prove that
199 /// all callees pass in a valid pointer for the specified function argument.
200 static bool AllCalleesPassInValidPointerForArgument(Argument *Arg) {
201 Function *Callee = Arg->getParent();
203 unsigned ArgNo = std::distance(Callee->arg_begin(),
204 Function::arg_iterator(Arg));
206 // Look at all call sites of the function. At this pointer we know we only
207 // have direct callees.
208 for (Value::use_iterator UI = Callee->use_begin(), E = Callee->use_end();
209 UI != E; ++UI) {
210 CallSite CS = CallSite::get(*UI);
211 assert(CS.getInstruction() && "Should only have direct calls!");
213 if (!IsAlwaysValidPointer(CS.getArgument(ArgNo)))
214 return false;
215 }
216 return true;
217 }
219 /// Returns true if Prefix is a prefix of longer. That means, Longer has a size
220 /// that is greater than or equal to the size of prefix, and each of the
221 /// elements in Prefix is the same as the corresponding elements in Longer.
222 ///
223 /// This means it also returns true when Prefix and Longer are equal!
224 static bool IsPrefix(const ArgPromotion::IndicesVector &Prefix,
225 const ArgPromotion::IndicesVector &Longer) {
226 if (Prefix.size() > Longer.size())
227 return false;
228 for (unsigned i = 0, e = Prefix.size(); i != e; ++i)
229 if (Prefix[i] != Longer[i])
230 return false;
231 return true;
232 }
235 /// Checks if Indices, or a prefix of Indices, is in Set.
236 static bool PrefixIn(const ArgPromotion::IndicesVector &Indices,
237 std::set<ArgPromotion::IndicesVector> &Set) {
238 std::set<ArgPromotion::IndicesVector>::iterator Low;
239 Low = Set.upper_bound(Indices);
240 if (Low != Set.begin())
241 Low--;
242 // Low is now the last element smaller than or equal to Indices. This means
243 // it points to a prefix of Indices (possibly Indices itself), if such
244 // prefix exists.
245 //
246 // This load is safe if any prefix of its operands is safe to load.
247 return Low != Set.end() && IsPrefix(*Low, Indices);
248 }
250 /// Mark the given indices (ToMark) as safe in the given set of indices
251 /// (Safe). Marking safe usually means adding ToMark to Safe. However, if there
252 /// is already a prefix of Indices in Safe, Indices are implicitely marked safe
253 /// already. Furthermore, any indices that Indices is itself a prefix of, are
254 /// removed from Safe (since they are implicitely safe because of Indices now).
255 static void MarkIndicesSafe(const ArgPromotion::IndicesVector &ToMark,
256 std::set<ArgPromotion::IndicesVector> &Safe) {
257 std::set<ArgPromotion::IndicesVector>::iterator Low;
258 Low = Safe.upper_bound(ToMark);
259 // Guard against the case where Safe is empty
260 if (Low != Safe.begin())
261 Low--;
262 // Low is now the last element smaller than or equal to Indices. This
263 // means it points to a prefix of Indices (possibly Indices itself), if
264 // such prefix exists.
265 if (Low != Safe.end()) {
266 if (IsPrefix(*Low, ToMark))
267 // If there is already a prefix of these indices (or exactly these
268 // indices) marked a safe, don't bother adding these indices
269 return;
271 // Increment Low, so we can use it as a "insert before" hint
272 ++Low;
273 }
274 // Insert
275 Low = Safe.insert(Low, ToMark);
276 ++Low;
277 // If there we're a prefix of longer index list(s), remove those
278 std::set<ArgPromotion::IndicesVector>::iterator End = Safe.end();
279 while (Low != End && IsPrefix(ToMark, *Low)) {
280 std::set<ArgPromotion::IndicesVector>::iterator Remove = Low;
281 ++Low;
282 Safe.erase(Remove);
283 }
284 }
286 /// isSafeToPromoteArgument - As you might guess from the name of this method,
287 /// it checks to see if it is both safe and useful to promote the argument.
288 /// This method limits promotion of aggregates to only promote up to three
289 /// elements of the aggregate in order to avoid exploding the number of
290 /// arguments passed in.
291 bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg, bool isByVal) const {
292 typedef std::set<IndicesVector> GEPIndicesSet;
294 // Quick exit for unused arguments
295 if (Arg->use_empty())
296 return true;
298 // We can only promote this argument if all of the uses are loads, or are GEP
299 // instructions (with constant indices) that are subsequently loaded.
300 //
301 // Promoting the argument causes it to be loaded in the caller
302 // unconditionally. This is only safe if we can prove that either the load
303 // would have happened in the callee anyway (ie, there is a load in the entry
304 // block) or the pointer passed in at every call site is guaranteed to be
305 // valid.
306 // In the former case, invalid loads can happen, but would have happened
307 // anyway, in the latter case, invalid loads won't happen. This prevents us
308 // from introducing an invalid load that wouldn't have happened in the
309 // original code.
310 //
311 // This set will contain all sets of indices that are loaded in the entry
312 // block, and thus are safe to unconditionally load in the caller.
313 GEPIndicesSet SafeToUnconditionallyLoad;
315 // This set contains all the sets of indices that we are planning to promote.
316 // This makes it possible to limit the number of arguments added.
317 GEPIndicesSet ToPromote;
319 // If the pointer is always valid, any load with first index 0 is valid.
320 if(isByVal || AllCalleesPassInValidPointerForArgument(Arg))
321 SafeToUnconditionallyLoad.insert(IndicesVector(1, 0));
323 // First, iterate the entry block and mark loads of (geps of) arguments as
324 // safe.
325 BasicBlock *EntryBlock = Arg->getParent()->begin();
326 // Declare this here so we can reuse it
327 IndicesVector Indices;
328 for (BasicBlock::iterator I = EntryBlock->begin(), E = EntryBlock->end();
329 I != E; ++I)
330 if (LoadInst *LI = dyn_cast<LoadInst>(I)) {
331 Value *V = LI->getPointerOperand();
332 if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(V)) {
333 V = GEP->getPointerOperand();
334 if (V == Arg) {
335 // This load actually loads (part of) Arg? Check the indices then.
336 Indices.reserve(GEP->getNumIndices());
337 for (User::op_iterator II = GEP->idx_begin(), IE = GEP->idx_end();
338 II != IE; ++II)
339 if (ConstantInt *CI = dyn_cast<ConstantInt>(*II))
340 Indices.push_back(CI->getSExtValue());
341 else
342 // We found a non-constant GEP index for this argument? Bail out
343 // right away, can't promote this argument at all.
344 return false;
346 // Indices checked out, mark them as safe
347 MarkIndicesSafe(Indices, SafeToUnconditionallyLoad);
348 Indices.clear();
349 }
350 } else if (V == Arg) {
351 // Direct loads are equivalent to a GEP with a single 0 index.
352 MarkIndicesSafe(IndicesVector(1, 0), SafeToUnconditionallyLoad);
353 }
354 }
356 // Now, iterate all uses of the argument to see if there are any uses that are
357 // not (GEP+)loads, or any (GEP+)loads that are not safe to promote.
358 SmallVector<LoadInst*, 16> Loads;
359 IndicesVector Operands;
360 for (Value::use_iterator UI = Arg->use_begin(), E = Arg->use_end();
361 UI != E; ++UI) {
362 Operands.clear();
363 if (LoadInst *LI = dyn_cast<LoadInst>(*UI)) {
364 if (LI->isVolatile()) return false; // Don't hack volatile loads
365 Loads.push_back(LI);
366 // Direct loads are equivalent to a GEP with a zero index and then a load.
367 Operands.push_back(0);
368 } else if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(*UI)) {
369 if (GEP->use_empty()) {
370 // Dead GEP's cause trouble later. Just remove them if we run into
371 // them.
372 getAnalysis<AliasAnalysis>().deleteValue(GEP);
373 GEP->eraseFromParent();
374 // TODO: This runs the above loop over and over again for dead GEPS
375 // Couldn't we just do increment the UI iterator earlier and erase the
376 // use?
377 return isSafeToPromoteArgument(Arg, isByVal);
378 }
380 // Ensure that all of the indices are constants.
381 for (User::op_iterator i = GEP->idx_begin(), e = GEP->idx_end();
382 i != e; ++i)
383 if (ConstantInt *C = dyn_cast<ConstantInt>(*i))
384 Operands.push_back(C->getSExtValue());
385 else
386 return false; // Not a constant operand GEP!
388 // Ensure that the only users of the GEP are load instructions.
389 for (Value::use_iterator UI = GEP->use_begin(), E = GEP->use_end();
390 UI != E; ++UI)
391 if (LoadInst *LI = dyn_cast<LoadInst>(*UI)) {
392 if (LI->isVolatile()) return false; // Don't hack volatile loads
393 Loads.push_back(LI);
394 } else {
395 // Other uses than load?
396 return false;
397 }
398 } else {
399 return false; // Not a load or a GEP.
400 }
402 // Now, see if it is safe to promote this load / loads of this GEP. Loading
403 // is safe if Operands, or a prefix of Operands, is marked as safe.
404 if (!PrefixIn(Operands, SafeToUnconditionallyLoad))
405 return false;
407 // See if we are already promoting a load with these indices. If not, check
408 // to make sure that we aren't promoting too many elements. If so, nothing
409 // to do.
410 if (ToPromote.find(Operands) == ToPromote.end()) {
411 if (maxElements > 0 && ToPromote.size() == maxElements) {
412 DEBUG(dbgs() << "argpromotion not promoting argument '"
413 << Arg->getName() << "' because it would require adding more "
414 << "than " << maxElements << " arguments to the function.\n");
415 // We limit aggregate promotion to only promoting up to a fixed number
416 // of elements of the aggregate.
417 return false;
418 }
419 ToPromote.insert(Operands);
420 }
421 }
423 if (Loads.empty()) return true; // No users, this is a dead argument.
425 // Okay, now we know that the argument is only used by load instructions and
426 // it is safe to unconditionally perform all of them. Use alias analysis to
427 // check to see if the pointer is guaranteed to not be modified from entry of
428 // the function to each of the load instructions.
430 // Because there could be several/many load instructions, remember which
431 // blocks we know to be transparent to the load.
432 SmallPtrSet<BasicBlock*, 16> TranspBlocks;
434 AliasAnalysis &AA = getAnalysis<AliasAnalysis>();
435 TargetData *TD = getAnalysisIfAvailable<TargetData>();
436 if (!TD) return false; // Without TargetData, assume the worst.
438 for (unsigned i = 0, e = Loads.size(); i != e; ++i) {
439 // Check to see if the load is invalidated from the start of the block to
440 // the load itself.
441 LoadInst *Load = Loads[i];
442 BasicBlock *BB = Load->getParent();
444 const PointerType *LoadTy =
445 cast<PointerType>(Load->getPointerOperand()->getType());
446 unsigned LoadSize =(unsigned)TD->getTypeStoreSize(LoadTy->getElementType());
448 if (AA.canInstructionRangeModify(BB->front(), *Load, Arg, LoadSize))
449 return false; // Pointer is invalidated!
451 // Now check every path from the entry block to the load for transparency.
452 // To do this, we perform a depth first search on the inverse CFG from the
453 // loading block.
454 for (pred_iterator PI = pred_begin(BB), E = pred_end(BB); PI != E; ++PI)
455 for (idf_ext_iterator<BasicBlock*, SmallPtrSet<BasicBlock*, 16> >
456 I = idf_ext_begin(*PI, TranspBlocks),
457 E = idf_ext_end(*PI, TranspBlocks); I != E; ++I)
458 if (AA.canBasicBlockModify(**I, Arg, LoadSize))
459 return false;
460 }
462 // If the path from the entry of the function to each load is free of
463 // instructions that potentially invalidate the load, we can make the
464 // transformation!
465 return true;
466 }
468 /// DoPromotion - This method actually performs the promotion of the specified
469 /// arguments, and returns the new function. At this point, we know that it's
470 /// safe to do so.
471 CallGraphNode *ArgPromotion::DoPromotion(Function *F,
472 SmallPtrSet<Argument*, 8> &ArgsToPromote,
473 SmallPtrSet<Argument*, 8> &ByValArgsToTransform) {
475 // Start by computing a new prototype for the function, which is the same as
476 // the old function, but has modified arguments.
477 const FunctionType *FTy = F->getFunctionType();
478 std::vector<const Type*> Params;
480 typedef std::set<IndicesVector> ScalarizeTable;
482 // ScalarizedElements - If we are promoting a pointer that has elements
483 // accessed out of it, keep track of which elements are accessed so that we
484 // can add one argument for each.
485 //
486 // Arguments that are directly loaded will have a zero element value here, to
487 // handle cases where there are both a direct load and GEP accesses.
488 //
489 std::map<Argument*, ScalarizeTable> ScalarizedElements;
491 // OriginalLoads - Keep track of a representative load instruction from the
492 // original function so that we can tell the alias analysis implementation
493 // what the new GEP/Load instructions we are inserting look like.
494 std::map<IndicesVector, LoadInst*> OriginalLoads;
496 // Attributes - Keep track of the parameter attributes for the arguments
497 // that we are *not* promoting. For the ones that we do promote, the parameter
498 // attributes are lost
499 SmallVector<AttributeWithIndex, 8> AttributesVec;
500 const AttrListPtr &PAL = F->getAttributes();
502 // Add any return attributes.
503 if (Attributes attrs = PAL.getRetAttributes())
504 AttributesVec.push_back(AttributeWithIndex::get(0, attrs));
506 // First, determine the new argument list
507 unsigned ArgIndex = 1;
508 for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end(); I != E;
509 ++I, ++ArgIndex) {
510 if (ByValArgsToTransform.count(I)) {
511 // Simple byval argument? Just add all the struct element types.
512 const Type *AgTy = cast<PointerType>(I->getType())->getElementType();
513 const StructType *STy = cast<StructType>(AgTy);
514 for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i)
515 Params.push_back(STy->getElementType(i));
516 ++NumByValArgsPromoted;
517 } else if (!ArgsToPromote.count(I)) {
518 // Unchanged argument
519 Params.push_back(I->getType());
520 if (Attributes attrs = PAL.getParamAttributes(ArgIndex))
521 AttributesVec.push_back(AttributeWithIndex::get(Params.size(), attrs));
522 } else if (I->use_empty()) {
523 // Dead argument (which are always marked as promotable)
524 ++NumArgumentsDead;
525 } else {
526 // Okay, this is being promoted. This means that the only uses are loads
527 // or GEPs which are only used by loads
529 // In this table, we will track which indices are loaded from the argument
530 // (where direct loads are tracked as no indices).
531 ScalarizeTable &ArgIndices = ScalarizedElements[I];
532 for (Value::use_iterator UI = I->use_begin(), E = I->use_end(); UI != E;
533 ++UI) {
534 Instruction *User = cast<Instruction>(*UI);
535 assert(isa<LoadInst>(User) || isa<GetElementPtrInst>(User));
536 IndicesVector Indices;
537 Indices.reserve(User->getNumOperands() - 1);
538 // Since loads will only have a single operand, and GEPs only a single
539 // non-index operand, this will record direct loads without any indices,
540 // and gep+loads with the GEP indices.
541 for (User::op_iterator II = User->op_begin() + 1, IE = User->op_end();
542 II != IE; ++II)
543 Indices.push_back(cast<ConstantInt>(*II)->getSExtValue());
544 // GEPs with a single 0 index can be merged with direct loads
545 if (Indices.size() == 1 && Indices.front() == 0)
546 Indices.clear();
547 ArgIndices.insert(Indices);
548 LoadInst *OrigLoad;
549 if (LoadInst *L = dyn_cast<LoadInst>(User))
550 OrigLoad = L;
551 else
552 // Take any load, we will use it only to update Alias Analysis
553 OrigLoad = cast<LoadInst>(User->use_back());
554 OriginalLoads[Indices] = OrigLoad;
555 }
557 // Add a parameter to the function for each element passed in.
558 for (ScalarizeTable::iterator SI = ArgIndices.begin(),
559 E = ArgIndices.end(); SI != E; ++SI) {
560 // not allowed to dereference ->begin() if size() is 0
561 Params.push_back(GetElementPtrInst::getIndexedType(I->getType(),
562 SI->begin(),
563 SI->end()));
564 assert(Params.back());
565 }
567 if (ArgIndices.size() == 1 && ArgIndices.begin()->empty())
568 ++NumArgumentsPromoted;
569 else
570 ++NumAggregatesPromoted;
571 }
572 }
574 // Add any function attributes.
575 if (Attributes attrs = PAL.getFnAttributes())
576 AttributesVec.push_back(AttributeWithIndex::get(~0, attrs));
578 const Type *RetTy = FTy->getReturnType();
580 // Work around LLVM bug PR56: the CWriter cannot emit varargs functions which
581 // have zero fixed arguments.
582 bool ExtraArgHack = false;
583 if (Params.empty() && FTy->isVarArg()) {
584 ExtraArgHack = true;
585 Params.push_back(Type::getInt32Ty(F->getContext()));
586 }
588 // Construct the new function type using the new arguments.
589 FunctionType *NFTy = FunctionType::get(RetTy, Params, FTy->isVarArg());
591 // Create the new function body and insert it into the module.
592 Function *NF = Function::Create(NFTy, F->getLinkage(), F->getName());
593 NF->copyAttributesFrom(F);
596 DEBUG(dbgs() << "ARG PROMOTION: Promoting to:" << *NF << "\n"
597 << "From: " << *F);
599 // Recompute the parameter attributes list based on the new arguments for
600 // the function.
601 NF->setAttributes(AttrListPtr::get(AttributesVec.begin(),
602 AttributesVec.end()));
603 AttributesVec.clear();
605 F->getParent()->getFunctionList().insert(F, NF);
606 NF->takeName(F);
608 // Get the alias analysis information that we need to update to reflect our
609 // changes.
610 AliasAnalysis &AA = getAnalysis<AliasAnalysis>();
612 // Get the callgraph information that we need to update to reflect our
613 // changes.
614 CallGraph &CG = getAnalysis<CallGraph>();
616 // Get a new callgraph node for NF.
617 CallGraphNode *NF_CGN = CG.getOrInsertFunction(NF);
620 // Loop over all of the callers of the function, transforming the call sites
621 // to pass in the loaded pointers.
622 //
623 SmallVector<Value*, 16> Args;
624 while (!F->use_empty()) {
625 CallSite CS = CallSite::get(F->use_back());
626 Instruction *Call = CS.getInstruction();
627 const AttrListPtr &CallPAL = CS.getAttributes();
629 // Add any return attributes.
630 if (Attributes attrs = CallPAL.getRetAttributes())
631 AttributesVec.push_back(AttributeWithIndex::get(0, attrs));
633 // Loop over the operands, inserting GEP and loads in the caller as
634 // appropriate.
635 CallSite::arg_iterator AI = CS.arg_begin();
636 ArgIndex = 1;
637 for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end();
638 I != E; ++I, ++AI, ++ArgIndex)
639 if (!ArgsToPromote.count(I) && !ByValArgsToTransform.count(I)) {
640 Args.push_back(*AI); // Unmodified argument
642 if (Attributes Attrs = CallPAL.getParamAttributes(ArgIndex))
643 AttributesVec.push_back(AttributeWithIndex::get(Args.size(), Attrs));
645 } else if (ByValArgsToTransform.count(I)) {
646 // Emit a GEP and load for each element of the struct.
647 const Type *AgTy = cast<PointerType>(I->getType())->getElementType();
648 const StructType *STy = cast<StructType>(AgTy);
649 Value *Idxs[2] = {
650 ConstantInt::get(Type::getInt32Ty(F->getContext()), 0), 0 };
651 for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
652 Idxs[1] = ConstantInt::get(Type::getInt32Ty(F->getContext()), i);
653 Value *Idx = GetElementPtrInst::Create(*AI, Idxs, Idxs+2,
654 (*AI)->getName()+"."+utostr(i),
655 Call);
656 // TODO: Tell AA about the new values?
657 Args.push_back(new LoadInst(Idx, Idx->getName()+".val", Call));
658 }
659 } else if (!I->use_empty()) {
660 // Non-dead argument: insert GEPs and loads as appropriate.
661 ScalarizeTable &ArgIndices = ScalarizedElements[I];
662 // Store the Value* version of the indices in here, but declare it now
663 // for reuse
664 std::vector<Value*> Ops;
665 for (ScalarizeTable::iterator SI = ArgIndices.begin(),
666 E = ArgIndices.end(); SI != E; ++SI) {
667 Value *V = *AI;
668 LoadInst *OrigLoad = OriginalLoads[*SI];
669 if (!SI->empty()) {
670 Ops.reserve(SI->size());
671 const Type *ElTy = V->getType();
672 for (IndicesVector::const_iterator II = SI->begin(),
673 IE = SI->end(); II != IE; ++II) {
674 // Use i32 to index structs, and i64 for others (pointers/arrays).
675 // This satisfies GEP constraints.
676 const Type *IdxTy = (ElTy->isStructTy() ?
677 Type::getInt32Ty(F->getContext()) :
678 Type::getInt64Ty(F->getContext()));
679 Ops.push_back(ConstantInt::get(IdxTy, *II));
680 // Keep track of the type we're currently indexing
681 ElTy = cast<CompositeType>(ElTy)->getTypeAtIndex(*II);
682 }
683 // And create a GEP to extract those indices
684 V = GetElementPtrInst::Create(V, Ops.begin(), Ops.end(),
685 V->getName()+".idx", Call);
686 Ops.clear();
687 AA.copyValue(OrigLoad->getOperand(0), V);
688 }
689 Args.push_back(new LoadInst(V, V->getName()+".val", Call));
690 AA.copyValue(OrigLoad, Args.back());
691 }
692 }
694 if (ExtraArgHack)
695 Args.push_back(Constant::getNullValue(Type::getInt32Ty(F->getContext())));
697 // Push any varargs arguments on the list
698 for (; AI != CS.arg_end(); ++AI, ++ArgIndex) {
699 Args.push_back(*AI);
700 if (Attributes Attrs = CallPAL.getParamAttributes(ArgIndex))
701 AttributesVec.push_back(AttributeWithIndex::get(Args.size(), Attrs));
702 }
704 // Add any function attributes.
705 if (Attributes attrs = CallPAL.getFnAttributes())
706 AttributesVec.push_back(AttributeWithIndex::get(~0, attrs));
708 Instruction *New;
709 if (InvokeInst *II = dyn_cast<InvokeInst>(Call)) {
710 New = InvokeInst::Create(NF, II->getNormalDest(), II->getUnwindDest(),
711 Args.begin(), Args.end(), "", Call);
712 cast<InvokeInst>(New)->setCallingConv(CS.getCallingConv());
713 cast<InvokeInst>(New)->setAttributes(AttrListPtr::get(AttributesVec.begin(),
714 AttributesVec.end()));
715 } else {
716 New = CallInst::Create(NF, Args.begin(), Args.end(), "", Call);
717 cast<CallInst>(New)->setCallingConv(CS.getCallingConv());
718 cast<CallInst>(New)->setAttributes(AttrListPtr::get(AttributesVec.begin(),
719 AttributesVec.end()));
720 if (cast<CallInst>(Call)->isTailCall())
721 cast<CallInst>(New)->setTailCall();
722 }
723 Args.clear();
724 AttributesVec.clear();
726 // Update the alias analysis implementation to know that we are replacing
727 // the old call with a new one.
728 AA.replaceWithNewValue(Call, New);
730 // Update the callgraph to know that the callsite has been transformed.
731 CallGraphNode *CalleeNode = CG[Call->getParent()->getParent()];
732 CalleeNode->replaceCallEdge(Call, New, NF_CGN);
734 if (!Call->use_empty()) {
735 Call->replaceAllUsesWith(New);
736 New->takeName(Call);
737 }
739 // Finally, remove the old call from the program, reducing the use-count of
740 // F.
741 Call->eraseFromParent();
742 }
744 // Since we have now created the new function, splice the body of the old
745 // function right into the new function, leaving the old rotting hulk of the
746 // function empty.
747 NF->getBasicBlockList().splice(NF->begin(), F->getBasicBlockList());
749 // Loop over the argument list, transfering uses of the old arguments over to
750 // the new arguments, also transfering over the names as well.
751 //
752 for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end(),
753 I2 = NF->arg_begin(); I != E; ++I) {
754 if (!ArgsToPromote.count(I) && !ByValArgsToTransform.count(I)) {
755 // If this is an unmodified argument, move the name and users over to the
756 // new version.
757 I->replaceAllUsesWith(I2);
758 I2->takeName(I);
759 AA.replaceWithNewValue(I, I2);
760 ++I2;
761 continue;
762 }
764 if (ByValArgsToTransform.count(I)) {
765 // In the callee, we create an alloca, and store each of the new incoming
766 // arguments into the alloca.
767 Instruction *InsertPt = NF->begin()->begin();
769 // Just add all the struct element types.
770 const Type *AgTy = cast<PointerType>(I->getType())->getElementType();
771 Value *TheAlloca = new AllocaInst(AgTy, 0, "", InsertPt);
772 const StructType *STy = cast<StructType>(AgTy);
773 Value *Idxs[2] = {
774 ConstantInt::get(Type::getInt32Ty(F->getContext()), 0), 0 };
776 for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
777 Idxs[1] = ConstantInt::get(Type::getInt32Ty(F->getContext()), i);
778 Value *Idx =
779 GetElementPtrInst::Create(TheAlloca, Idxs, Idxs+2,
780 TheAlloca->getName()+"."+Twine(i),
781 InsertPt);
782 I2->setName(I->getName()+"."+Twine(i));
783 new StoreInst(I2++, Idx, InsertPt);
784 }
786 // Anything that used the arg should now use the alloca.
787 I->replaceAllUsesWith(TheAlloca);
788 TheAlloca->takeName(I);
789 AA.replaceWithNewValue(I, TheAlloca);
790 continue;
791 }
793 if (I->use_empty()) {
794 AA.deleteValue(I);
795 continue;
796 }
798 // Otherwise, if we promoted this argument, then all users are load
799 // instructions (or GEPs with only load users), and all loads should be
800 // using the new argument that we added.
801 ScalarizeTable &ArgIndices = ScalarizedElements[I];
803 while (!I->use_empty()) {
804 if (LoadInst *LI = dyn_cast<LoadInst>(I->use_back())) {
805 assert(ArgIndices.begin()->empty() &&
806 "Load element should sort to front!");
807 I2->setName(I->getName()+".val");
808 LI->replaceAllUsesWith(I2);
809 AA.replaceWithNewValue(LI, I2);
810 LI->eraseFromParent();
811 DEBUG(dbgs() << "*** Promoted load of argument '" << I->getName()
812 << "' in function '" << F->getName() << "'\n");
813 } else {
814 GetElementPtrInst *GEP = cast<GetElementPtrInst>(I->use_back());
815 IndicesVector Operands;
816 Operands.reserve(GEP->getNumIndices());
817 for (User::op_iterator II = GEP->idx_begin(), IE = GEP->idx_end();
818 II != IE; ++II)
819 Operands.push_back(cast<ConstantInt>(*II)->getSExtValue());
821 // GEPs with a single 0 index can be merged with direct loads
822 if (Operands.size() == 1 && Operands.front() == 0)
823 Operands.clear();
825 Function::arg_iterator TheArg = I2;
826 for (ScalarizeTable::iterator It = ArgIndices.begin();
827 *It != Operands; ++It, ++TheArg) {
828 assert(It != ArgIndices.end() && "GEP not handled??");
829 }
831 std::string NewName = I->getName();
832 for (unsigned i = 0, e = Operands.size(); i != e; ++i) {
833 NewName += "." + utostr(Operands[i]);
834 }
835 NewName += ".val";
836 TheArg->setName(NewName);
838 DEBUG(dbgs() << "*** Promoted agg argument '" << TheArg->getName()
839 << "' of function '" << NF->getName() << "'\n");
841 // All of the uses must be load instructions. Replace them all with
842 // the argument specified by ArgNo.
843 while (!GEP->use_empty()) {
844 LoadInst *L = cast<LoadInst>(GEP->use_back());
845 L->replaceAllUsesWith(TheArg);
846 AA.replaceWithNewValue(L, TheArg);
847 L->eraseFromParent();
848 }
849 AA.deleteValue(GEP);
850 GEP->eraseFromParent();
851 }
852 }
854 // Increment I2 past all of the arguments added for this promoted pointer.
855 for (unsigned i = 0, e = ArgIndices.size(); i != e; ++i)
856 ++I2;
857 }
859 // Notify the alias analysis implementation that we inserted a new argument.
860 if (ExtraArgHack)
861 AA.copyValue(Constant::getNullValue(Type::getInt32Ty(F->getContext())),
862 NF->arg_begin());
865 // Tell the alias analysis that the old function is about to disappear.
866 AA.replaceWithNewValue(F, NF);
869 NF_CGN->stealCalledFunctionsFrom(CG[F]);
871 // Now that the old function is dead, delete it.
872 delete CG.removeFunctionFromModule(F);
874 return NF_CGN;
875 }