]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/Transforms/IPO/ArgumentPromotion.cpp
Use a safer iterator interface and get rid of std C++ library misuse.
[opencl/llvm.git] / lib / Transforms / IPO / ArgumentPromotion.cpp
1 //===-- ArgumentPromotion.cpp - Promote by-reference arguments ------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This pass promotes "by reference" arguments to be "by value" arguments.  In
11 // practice, this means looking for internal functions that have pointer
12 // arguments.  If it can prove, through the use of alias analysis, that an
13 // argument is *only* loaded, then it can pass the value into the function
14 // instead of the address of the value.  This can cause recursive simplification
15 // of code and lead to the elimination of allocas (especially in C++ template
16 // code like the STL).
17 //
18 // This pass also handles aggregate arguments that are passed into a function,
19 // scalarizing them if the elements of the aggregate are only loaded.  Note that
20 // by default it refuses to scalarize aggregates which would require passing in
21 // more than three operands to the function, because passing thousands of
22 // operands for a large array or structure is unprofitable! This limit can be
23 // configured or disabled, however.
24 //
25 // Note that this transformation could also be done for arguments that are only
26 // stored to (returning the value instead), but does not currently.  This case
27 // would be best handled when and if LLVM begins supporting multiple return
28 // values from functions.
29 //
30 //===----------------------------------------------------------------------===//
32 #define DEBUG_TYPE "argpromotion"
33 #include "llvm/Transforms/IPO.h"
34 #include "llvm/Constants.h"
35 #include "llvm/DerivedTypes.h"
36 #include "llvm/Module.h"
37 #include "llvm/CallGraphSCCPass.h"
38 #include "llvm/Instructions.h"
39 #include "llvm/Analysis/AliasAnalysis.h"
40 #include "llvm/Analysis/CallGraph.h"
41 #include "llvm/Target/TargetData.h"
42 #include "llvm/Support/CallSite.h"
43 #include "llvm/Support/CFG.h"
44 #include "llvm/Support/Debug.h"
45 #include "llvm/ADT/DepthFirstIterator.h"
46 #include "llvm/ADT/Statistic.h"
47 #include "llvm/ADT/StringExtras.h"
48 #include "llvm/Support/Compiler.h"
49 #include <set>
50 using namespace llvm;
52 STATISTIC(NumArgumentsPromoted , "Number of pointer arguments promoted");
53 STATISTIC(NumAggregatesPromoted, "Number of aggregate arguments promoted");
54 STATISTIC(NumByValArgsPromoted , "Number of byval arguments promoted");
55 STATISTIC(NumArgumentsDead     , "Number of dead pointer args eliminated");
57 namespace {
58   /// ArgPromotion - The 'by reference' to 'by value' argument promotion pass.
59   ///
60   struct VISIBILITY_HIDDEN ArgPromotion : public CallGraphSCCPass {
61     virtual void getAnalysisUsage(AnalysisUsage &AU) const {
62       AU.addRequired<AliasAnalysis>();
63       AU.addRequired<TargetData>();
64       CallGraphSCCPass::getAnalysisUsage(AU);
65     }
67     virtual bool runOnSCC(const std::vector<CallGraphNode *> &SCC);
68     static char ID; // Pass identification, replacement for typeid
69     explicit ArgPromotion(unsigned maxElements = 3)
70       : CallGraphSCCPass(&ID), maxElements(maxElements) {}
72     /// A vector used to hold the indices of a single GEP instruction
73     typedef std::vector<uint64_t> IndicesVector;
75   private:
76     bool PromoteArguments(CallGraphNode *CGN);
77     bool isSafeToPromoteArgument(Argument *Arg, bool isByVal) const;
78     Function *DoPromotion(Function *F,
79                           SmallPtrSet<Argument*, 8> &ArgsToPromote,
80                           SmallPtrSet<Argument*, 8> &ByValArgsToTransform);
81     /// The maximum number of elements to expand, or 0 for unlimited.
82     unsigned maxElements;
83   };
84 }
86 char ArgPromotion::ID = 0;
87 static RegisterPass<ArgPromotion>
88 X("argpromotion", "Promote 'by reference' arguments to scalars");
90 Pass *llvm::createArgumentPromotionPass(unsigned maxElements) {
91   return new ArgPromotion(maxElements);
92 }
94 bool ArgPromotion::runOnSCC(const std::vector<CallGraphNode *> &SCC) {
95   bool Changed = false, LocalChange;
97   do {  // Iterate until we stop promoting from this SCC.
98     LocalChange = false;
99     // Attempt to promote arguments from all functions in this SCC.
100     for (unsigned i = 0, e = SCC.size(); i != e; ++i)
101       LocalChange |= PromoteArguments(SCC[i]);
102     Changed |= LocalChange;               // Remember that we changed something.
103   } while (LocalChange);
105   return Changed;
108 /// PromoteArguments - This method checks the specified function to see if there
109 /// are any promotable arguments and if it is safe to promote the function (for
110 /// example, all callers are direct).  If safe to promote some arguments, it
111 /// calls the DoPromotion method.
112 ///
113 bool ArgPromotion::PromoteArguments(CallGraphNode *CGN) {
114   Function *F = CGN->getFunction();
116   // Make sure that it is local to this module.
117   if (!F || !F->hasLocalLinkage()) return false;
119   // First check: see if there are any pointer arguments!  If not, quick exit.
120   SmallVector<std::pair<Argument*, unsigned>, 16> PointerArgs;
121   unsigned ArgNo = 0;
122   for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end();
123        I != E; ++I, ++ArgNo)
124     if (isa<PointerType>(I->getType()))
125       PointerArgs.push_back(std::pair<Argument*, unsigned>(I, ArgNo));
126   if (PointerArgs.empty()) return false;
128   // Second check: make sure that all callers are direct callers.  We can't
129   // transform functions that have indirect callers.
130   for (Value::use_iterator UI = F->use_begin(), E = F->use_end();
131        UI != E; ++UI) {
132     CallSite CS = CallSite::get(*UI);
133     if (!CS.getInstruction())       // "Taking the address" of the function
134       return false;
136     // Ensure that this call site is CALLING the function, not passing it as
137     // an argument.
138     if (!CS.isCallee(UI))
139       return false;
140   }
142   // Check to see which arguments are promotable.  If an argument is promotable,
143   // add it to ArgsToPromote.
144   SmallPtrSet<Argument*, 8> ArgsToPromote;
145   SmallPtrSet<Argument*, 8> ByValArgsToTransform;
146   for (unsigned i = 0; i != PointerArgs.size(); ++i) {
147     bool isByVal = F->paramHasAttr(PointerArgs[i].second+1, Attribute::ByVal);
149     // If this is a byval argument, and if the aggregate type is small, just
150     // pass the elements, which is always safe.
151     Argument *PtrArg = PointerArgs[i].first;
152     if (isByVal) {
153       const Type *AgTy = cast<PointerType>(PtrArg->getType())->getElementType();
154       if (const StructType *STy = dyn_cast<StructType>(AgTy)) {
155         if (maxElements > 0 && STy->getNumElements() > maxElements) {
156           DOUT << "argpromotion disable promoting argument '"
157                << PtrArg->getName() << "' because it would require adding more "
158                << "than " << maxElements << " arguments to the function.\n";
159         } else {
160           // If all the elements are single-value types, we can promote it.
161           bool AllSimple = true;
162           for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i)
163             if (!STy->getElementType(i)->isSingleValueType()) {
164               AllSimple = false;
165               break;
166             }
168           // Safe to transform, don't even bother trying to "promote" it.
169           // Passing the elements as a scalar will allow scalarrepl to hack on
170           // the new alloca we introduce.
171           if (AllSimple) {
172             ByValArgsToTransform.insert(PtrArg);
173             continue;
174           }
175         }
176       }
177     }
179     // Otherwise, see if we can promote the pointer to its value.
180     if (isSafeToPromoteArgument(PtrArg, isByVal))
181       ArgsToPromote.insert(PtrArg);
182   }
184   // No promotable pointer arguments.
185   if (ArgsToPromote.empty() && ByValArgsToTransform.empty()) return false;
187   Function *NewF = DoPromotion(F, ArgsToPromote, ByValArgsToTransform);
189   // Update the call graph to know that the function has been transformed.
190   getAnalysis<CallGraph>().changeFunction(F, NewF);
191   return true;
194 /// IsAlwaysValidPointer - Return true if the specified pointer is always legal
195 /// to load.
196 static bool IsAlwaysValidPointer(Value *V) {
197   if (isa<AllocaInst>(V) || isa<GlobalVariable>(V)) return true;
198   if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(V))
199     return IsAlwaysValidPointer(GEP->getOperand(0));
200   if (ConstantExpr *CE = dyn_cast<ConstantExpr>(V))
201     if (CE->getOpcode() == Instruction::GetElementPtr)
202       return IsAlwaysValidPointer(CE->getOperand(0));
204   return false;
207 /// AllCalleesPassInValidPointerForArgument - Return true if we can prove that
208 /// all callees pass in a valid pointer for the specified function argument.
209 static bool AllCalleesPassInValidPointerForArgument(Argument *Arg) {
210   Function *Callee = Arg->getParent();
212   unsigned ArgNo = std::distance(Callee->arg_begin(),
213                                  Function::arg_iterator(Arg));
215   // Look at all call sites of the function.  At this pointer we know we only
216   // have direct callees.
217   for (Value::use_iterator UI = Callee->use_begin(), E = Callee->use_end();
218        UI != E; ++UI) {
219     CallSite CS = CallSite::get(*UI);
220     assert(CS.getInstruction() && "Should only have direct calls!");
222     if (!IsAlwaysValidPointer(CS.getArgument(ArgNo)))
223       return false;
224   }
225   return true;
228 /// Returns true if Prefix is a prefix of longer. That means, Longer has a size
229 /// that is greater than or equal to the size of prefix, and each of the
230 /// elements in Prefix is the same as the corresponding elements in Longer.
231 ///
232 /// This means it also returns true when Prefix and Longer are equal!
233 static bool IsPrefix(const ArgPromotion::IndicesVector &Prefix,
234                      const ArgPromotion::IndicesVector &Longer) {
235   if (Prefix.size() > Longer.size())
236     return false;
237   for (unsigned i = 0, e = Prefix.size(); i != e; ++i)
238     if (Prefix[i] != Longer[i])
239       return false;
240   return true;
244 /// Checks if Indices, or a prefix of Indices, is in Set.
245 static bool PrefixIn(const ArgPromotion::IndicesVector &Indices,
246                      std::set<ArgPromotion::IndicesVector> &Set) {
247     std::set<ArgPromotion::IndicesVector>::iterator Low;
248     Low = Set.upper_bound(Indices);
249     if (Low != Set.begin())
250       Low--;
251     // Low is now the last element smaller than or equal to Indices. This means
252     // it points to a prefix of Indices (possibly Indices itself), if such
253     // prefix exists.
254     //
255     // This load is safe if any prefix of its operands is safe to load.
256     return Low != Set.end() && IsPrefix(*Low, Indices);
259 /// Mark the given indices (ToMark) as safe in the the given set of indices
260 /// (Safe). Marking safe usually means adding ToMark to Safe. However, if there
261 /// is already a prefix of Indices in Safe, Indices are implicitely marked safe
262 /// already. Furthermore, any indices that Indices is itself a prefix of, are
263 /// removed from Safe (since they are implicitely safe because of Indices now).
264 static void MarkIndicesSafe(const ArgPromotion::IndicesVector &ToMark,
265                             std::set<ArgPromotion::IndicesVector> &Safe) {
266   std::set<ArgPromotion::IndicesVector>::iterator Low;
267   Low = Safe.upper_bound(ToMark);
268   // Guard against the case where Safe is empty
269   if (Low != Safe.begin())
270     Low--;
271   // Low is now the last element smaller than or equal to Indices. This
272   // means it points to a prefix of Indices (possibly Indices itself), if
273   // such prefix exists.
274   if (Low != Safe.end()) {
275     if (IsPrefix(*Low, ToMark))
276       // If there is already a prefix of these indices (or exactly these
277       // indices) marked a safe, don't bother adding these indices
278       return;
280     // Increment Low, so we can use it as a "insert before" hint
281     ++Low;
282   }
283   // Insert
284   Low = Safe.insert(Low, ToMark);
285   ++Low;
286   // If there we're a prefix of longer index list(s), remove those
287   std::set<ArgPromotion::IndicesVector>::iterator End = Safe.end();
288   while (Low != End && IsPrefix(ToMark, *Low)) {
289     std::set<ArgPromotion::IndicesVector>::iterator Remove = Low;
290     ++Low;
291     Safe.erase(Remove);
292   }
295 /// isSafeToPromoteArgument - As you might guess from the name of this method,
296 /// it checks to see if it is both safe and useful to promote the argument.
297 /// This method limits promotion of aggregates to only promote up to three
298 /// elements of the aggregate in order to avoid exploding the number of
299 /// arguments passed in.
300 bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg, bool isByVal) const {
301   typedef std::set<IndicesVector> GEPIndicesSet;
303   // Quick exit for unused arguments
304   if (Arg->use_empty())
305     return true;
307   // We can only promote this argument if all of the uses are loads, or are GEP
308   // instructions (with constant indices) that are subsequently loaded.
309   //
310   // Promoting the argument causes it to be loaded in the caller
311   // unconditionally. This is only safe if we can prove that either the load
312   // would have happened in the callee anyway (ie, there is a load in the entry
313   // block) or the pointer passed in at every call site is guaranteed to be
314   // valid.
315   // In the former case, invalid loads can happen, but would have happened
316   // anyway, in the latter case, invalid loads won't happen. This prevents us
317   // from introducing an invalid load that wouldn't have happened in the
318   // original code.
319   //
320   // This set will contain all sets of indices that are loaded in the entry
321   // block, and thus are safe to unconditionally load in the caller.
322   GEPIndicesSet SafeToUnconditionallyLoad;
324   // This set contains all the sets of indices that we are planning to promote.
325   // This makes it possible to limit the number of arguments added.
326   GEPIndicesSet ToPromote;
328   // If the pointer is always valid, any load with first index 0 is valid.
329   if(isByVal || AllCalleesPassInValidPointerForArgument(Arg))
330     SafeToUnconditionallyLoad.insert(IndicesVector(1, 0));
332   // First, iterate the entry block and mark loads of (geps of) arguments as
333   // safe.
334   BasicBlock *EntryBlock = Arg->getParent()->begin();
335   // Declare this here so we can reuse it
336   IndicesVector Indices;
337   for (BasicBlock::iterator I = EntryBlock->begin(), E = EntryBlock->end();
338        I != E; ++I)
339     if (LoadInst *LI = dyn_cast<LoadInst>(I)) {
340       Value *V = LI->getPointerOperand();
341       if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(V)) {
342         V = GEP->getPointerOperand();
343         if (V == Arg) {
344           // This load actually loads (part of) Arg? Check the indices then.
345           Indices.reserve(GEP->getNumIndices());
346           for (User::op_iterator II = GEP->idx_begin(), IE = GEP->idx_end();
347                II != IE; ++II)
348             if (ConstantInt *CI = dyn_cast<ConstantInt>(*II))
349               Indices.push_back(CI->getSExtValue());
350             else
351               // We found a non-constant GEP index for this argument? Bail out
352               // right away, can't promote this argument at all.
353               return false;
355           // Indices checked out, mark them as safe
356           MarkIndicesSafe(Indices, SafeToUnconditionallyLoad);
357           Indices.clear();
358         }
359       } else if (V == Arg) {
360         // Direct loads are equivalent to a GEP with a single 0 index.
361         MarkIndicesSafe(IndicesVector(1, 0), SafeToUnconditionallyLoad);
362       }
363     }
365   // Now, iterate all uses of the argument to see if there are any uses that are
366   // not (GEP+)loads, or any (GEP+)loads that are not safe to promote.
367   SmallVector<LoadInst*, 16> Loads;
368   IndicesVector Operands;
369   for (Value::use_iterator UI = Arg->use_begin(), E = Arg->use_end();
370        UI != E; ++UI) {
371     Operands.clear();
372     if (LoadInst *LI = dyn_cast<LoadInst>(*UI)) {
373       if (LI->isVolatile()) return false;  // Don't hack volatile loads
374       Loads.push_back(LI);
375       // Direct loads are equivalent to a GEP with a zero index and then a load.
376       Operands.push_back(0);
377     } else if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(*UI)) {
378       if (GEP->use_empty()) {
379         // Dead GEP's cause trouble later.  Just remove them if we run into
380         // them.
381         getAnalysis<AliasAnalysis>().deleteValue(GEP);
382         GEP->eraseFromParent();
383         // TODO: This runs the above loop over and over again for dead GEPS
384         // Couldn't we just do increment the UI iterator earlier and erase the
385         // use?
386         return isSafeToPromoteArgument(Arg, isByVal);
387       }
389       // Ensure that all of the indices are constants.
390       for (User::op_iterator i = GEP->idx_begin(), e = GEP->idx_end();
391         i != e; ++i)
392         if (ConstantInt *C = dyn_cast<ConstantInt>(*i))
393           Operands.push_back(C->getSExtValue());
394         else
395           return false;  // Not a constant operand GEP!
397       // Ensure that the only users of the GEP are load instructions.
398       for (Value::use_iterator UI = GEP->use_begin(), E = GEP->use_end();
399            UI != E; ++UI)
400         if (LoadInst *LI = dyn_cast<LoadInst>(*UI)) {
401           if (LI->isVolatile()) return false;  // Don't hack volatile loads
402           Loads.push_back(LI);
403         } else {
404           // Other uses than load?
405           return false;
406         }
407     } else {
408       return false;  // Not a load or a GEP.
409     }
411     // Now, see if it is safe to promote this load / loads of this GEP. Loading
412     // is safe if Operands, or a prefix of Operands, is marked as safe.
413     if (!PrefixIn(Operands, SafeToUnconditionallyLoad))
414       return false;
416     // See if we are already promoting a load with these indices. If not, check
417     // to make sure that we aren't promoting too many elements.  If so, nothing
418     // to do.
419     if (ToPromote.find(Operands) == ToPromote.end()) {
420       if (maxElements > 0 && ToPromote.size() == maxElements) {
421         DOUT << "argpromotion not promoting argument '"
422              << Arg->getName() << "' because it would require adding more "
423              << "than " << maxElements << " arguments to the function.\n";
424         // We limit aggregate promotion to only promoting up to a fixed number
425         // of elements of the aggregate.
426         return false;
427       }
428       ToPromote.insert(Operands);
429     }
430   }
432   if (Loads.empty()) return true;  // No users, this is a dead argument.
434   // Okay, now we know that the argument is only used by load instructions and
435   // it is safe to unconditionally perform all of them. Use alias analysis to
436   // check to see if the pointer is guaranteed to not be modified from entry of
437   // the function to each of the load instructions.
439   // Because there could be several/many load instructions, remember which
440   // blocks we know to be transparent to the load.
441   SmallPtrSet<BasicBlock*, 16> TranspBlocks;
443   AliasAnalysis &AA = getAnalysis<AliasAnalysis>();
444   TargetData &TD = getAnalysis<TargetData>();
446   for (unsigned i = 0, e = Loads.size(); i != e; ++i) {
447     // Check to see if the load is invalidated from the start of the block to
448     // the load itself.
449     LoadInst *Load = Loads[i];
450     BasicBlock *BB = Load->getParent();
452     const PointerType *LoadTy =
453       cast<PointerType>(Load->getPointerOperand()->getType());
454     unsigned LoadSize = (unsigned)TD.getTypeStoreSize(LoadTy->getElementType());
456     if (AA.canInstructionRangeModify(BB->front(), *Load, Arg, LoadSize))
457       return false;  // Pointer is invalidated!
459     // Now check every path from the entry block to the load for transparency.
460     // To do this, we perform a depth first search on the inverse CFG from the
461     // loading block.
462     for (pred_iterator PI = pred_begin(BB), E = pred_end(BB); PI != E; ++PI)
463       for (idf_ext_iterator<BasicBlock*, SmallPtrSet<BasicBlock*, 16> >
464              I = idf_ext_begin(*PI, TranspBlocks),
465              E = idf_ext_end(*PI, TranspBlocks); I != E; ++I)
466         if (AA.canBasicBlockModify(**I, Arg, LoadSize))
467           return false;
468   }
470   // If the path from the entry of the function to each load is free of
471   // instructions that potentially invalidate the load, we can make the
472   // transformation!
473   return true;
476 /// DoPromotion - This method actually performs the promotion of the specified
477 /// arguments, and returns the new function.  At this point, we know that it's
478 /// safe to do so.
479 Function *ArgPromotion::DoPromotion(Function *F,
480                                     SmallPtrSet<Argument*, 8> &ArgsToPromote,
481                               SmallPtrSet<Argument*, 8> &ByValArgsToTransform) {
483   // Start by computing a new prototype for the function, which is the same as
484   // the old function, but has modified arguments.
485   const FunctionType *FTy = F->getFunctionType();
486   std::vector<const Type*> Params;
488   typedef std::set<IndicesVector> ScalarizeTable;
490   // ScalarizedElements - If we are promoting a pointer that has elements
491   // accessed out of it, keep track of which elements are accessed so that we
492   // can add one argument for each.
493   //
494   // Arguments that are directly loaded will have a zero element value here, to
495   // handle cases where there are both a direct load and GEP accesses.
496   //
497   std::map<Argument*, ScalarizeTable> ScalarizedElements;
499   // OriginalLoads - Keep track of a representative load instruction from the
500   // original function so that we can tell the alias analysis implementation
501   // what the new GEP/Load instructions we are inserting look like.
502   std::map<IndicesVector, LoadInst*> OriginalLoads;
504   // Attributes - Keep track of the parameter attributes for the arguments
505   // that we are *not* promoting. For the ones that we do promote, the parameter
506   // attributes are lost
507   SmallVector<AttributeWithIndex, 8> AttributesVec;
508   const AttrListPtr &PAL = F->getAttributes();
510   // Add any return attributes.
511   if (Attributes attrs = PAL.getRetAttributes())
512     AttributesVec.push_back(AttributeWithIndex::get(0, attrs));
514   // First, determine the new argument list
515   unsigned ArgIndex = 1;
516   for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end(); I != E;
517        ++I, ++ArgIndex) {
518     if (ByValArgsToTransform.count(I)) {
519       // Simple byval argument? Just add all the struct element types.
520       const Type *AgTy = cast<PointerType>(I->getType())->getElementType();
521       const StructType *STy = cast<StructType>(AgTy);
522       for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i)
523         Params.push_back(STy->getElementType(i));
524       ++NumByValArgsPromoted;
525     } else if (!ArgsToPromote.count(I)) {
526       // Unchanged argument
527       Params.push_back(I->getType());
528       if (Attributes attrs = PAL.getParamAttributes(ArgIndex))
529         AttributesVec.push_back(AttributeWithIndex::get(Params.size(), attrs));
530     } else if (I->use_empty()) {
531       // Dead argument (which are always marked as promotable)
532       ++NumArgumentsDead;
533     } else {
534       // Okay, this is being promoted. This means that the only uses are loads
535       // or GEPs which are only used by loads
537       // In this table, we will track which indices are loaded from the argument
538       // (where direct loads are tracked as no indices).
539       ScalarizeTable &ArgIndices = ScalarizedElements[I];
540       for (Value::use_iterator UI = I->use_begin(), E = I->use_end(); UI != E;
541            ++UI) {
542         Instruction *User = cast<Instruction>(*UI);
543         assert(isa<LoadInst>(User) || isa<GetElementPtrInst>(User));
544         IndicesVector Indices;
545         Indices.reserve(User->getNumOperands() - 1);
546         // Since loads will only have a single operand, and GEPs only a single
547         // non-index operand, this will record direct loads without any indices,
548         // and gep+loads with the GEP indices.
549         for (User::op_iterator II = User->op_begin() + 1, IE = User->op_end();
550              II != IE; ++II)
551           Indices.push_back(cast<ConstantInt>(*II)->getSExtValue());
552         // GEPs with a single 0 index can be merged with direct loads
553         if (Indices.size() == 1 && Indices.front() == 0)
554           Indices.clear();
555         ArgIndices.insert(Indices);
556         LoadInst *OrigLoad;
557         if (LoadInst *L = dyn_cast<LoadInst>(User))
558           OrigLoad = L;
559         else
560           // Take any load, we will use it only to update Alias Analysis
561           OrigLoad = cast<LoadInst>(User->use_back());
562         OriginalLoads[Indices] = OrigLoad;
563       }
565       // Add a parameter to the function for each element passed in.
566       for (ScalarizeTable::iterator SI = ArgIndices.begin(),
567              E = ArgIndices.end(); SI != E; ++SI) {
568         // not allowed to dereference ->begin() if size() is 0
569         Params.push_back(GetElementPtrInst::getIndexedType(I->getType(),
570                                                            SI->begin(),
571                                                            SI->end()));
572         assert(Params.back());
573       }
575       if (ArgIndices.size() == 1 && ArgIndices.begin()->empty())
576         ++NumArgumentsPromoted;
577       else
578         ++NumAggregatesPromoted;
579     }
580   }
582   // Add any function attributes.
583   if (Attributes attrs = PAL.getFnAttributes())
584     AttributesVec.push_back(AttributeWithIndex::get(~0, attrs));
586   const Type *RetTy = FTy->getReturnType();
588   // Work around LLVM bug PR56: the CWriter cannot emit varargs functions which
589   // have zero fixed arguments.
590   bool ExtraArgHack = false;
591   if (Params.empty() && FTy->isVarArg()) {
592     ExtraArgHack = true;
593     Params.push_back(Type::Int32Ty);
594   }
596   // Construct the new function type using the new arguments.
597   FunctionType *NFTy = FunctionType::get(RetTy, Params, FTy->isVarArg());
599   // Create the new function body and insert it into the module...
600   Function *NF = Function::Create(NFTy, F->getLinkage(), F->getName());
601   NF->copyAttributesFrom(F);
603   // Recompute the parameter attributes list based on the new arguments for
604   // the function.
605   NF->setAttributes(AttrListPtr::get(AttributesVec.begin(), AttributesVec.end()));
606   AttributesVec.clear();
608   F->getParent()->getFunctionList().insert(F, NF);
609   NF->takeName(F);
611   // Get the alias analysis information that we need to update to reflect our
612   // changes.
613   AliasAnalysis &AA = getAnalysis<AliasAnalysis>();
615   // Get the callgraph information that we need to update to reflect our
616   // changes.
617   CallGraph &CG = getAnalysis<CallGraph>();
619   // Loop over all of the callers of the function, transforming the call sites
620   // to pass in the loaded pointers.
621   //
622   SmallVector<Value*, 16> Args;
623   while (!F->use_empty()) {
624     CallSite CS = CallSite::get(F->use_back());
625     Instruction *Call = CS.getInstruction();
626     const AttrListPtr &CallPAL = CS.getAttributes();
628     // Add any return attributes.
629     if (Attributes attrs = CallPAL.getRetAttributes())
630       AttributesVec.push_back(AttributeWithIndex::get(0, attrs));
632     // Loop over the operands, inserting GEP and loads in the caller as
633     // appropriate.
634     CallSite::arg_iterator AI = CS.arg_begin();
635     ArgIndex = 1;
636     for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end();
637          I != E; ++I, ++AI, ++ArgIndex)
638       if (!ArgsToPromote.count(I) && !ByValArgsToTransform.count(I)) {
639         Args.push_back(*AI);          // Unmodified argument
641         if (Attributes Attrs = CallPAL.getParamAttributes(ArgIndex))
642           AttributesVec.push_back(AttributeWithIndex::get(Args.size(), Attrs));
644       } else if (ByValArgsToTransform.count(I)) {
645         // Emit a GEP and load for each element of the struct.
646         const Type *AgTy = cast<PointerType>(I->getType())->getElementType();
647         const StructType *STy = cast<StructType>(AgTy);
648         Value *Idxs[2] = { ConstantInt::get(Type::Int32Ty, 0), 0 };
649         for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
650           Idxs[1] = ConstantInt::get(Type::Int32Ty, i);
651           Value *Idx = GetElementPtrInst::Create(*AI, Idxs, Idxs+2,
652                                                  (*AI)->getName()+"."+utostr(i),
653                                                  Call);
654           // TODO: Tell AA about the new values?
655           Args.push_back(new LoadInst(Idx, Idx->getName()+".val", Call));
656         }
657       } else if (!I->use_empty()) {
658         // Non-dead argument: insert GEPs and loads as appropriate.
659         ScalarizeTable &ArgIndices = ScalarizedElements[I];
660         // Store the Value* version of the indices in here, but declare it now
661         // for reuse
662         std::vector<Value*> Ops;
663         for (ScalarizeTable::iterator SI = ArgIndices.begin(),
664                E = ArgIndices.end(); SI != E; ++SI) {
665           Value *V = *AI;
666           LoadInst *OrigLoad = OriginalLoads[*SI];
667           if (!SI->empty()) {
668             Ops.reserve(SI->size());
669             const Type *ElTy = V->getType();
670             for (IndicesVector::const_iterator II = SI->begin(),
671                  IE = SI->end(); II != IE; ++II) {
672               // Use i32 to index structs, and i64 for others (pointers/arrays).
673               // This satisfies GEP constraints.
674               const Type *IdxTy = (isa<StructType>(ElTy) ? Type::Int32Ty : Type::Int64Ty);
675               Ops.push_back(ConstantInt::get(IdxTy, *II));
676               // Keep track of the type we're currently indexing
677               ElTy = cast<CompositeType>(ElTy)->getTypeAtIndex(*II);
678             }
679             // And create a GEP to extract those indices
680             V = GetElementPtrInst::Create(V, Ops.begin(), Ops.end(),
681                                           V->getName()+".idx", Call);
682             Ops.clear();
683             AA.copyValue(OrigLoad->getOperand(0), V);
684           }
685           Args.push_back(new LoadInst(V, V->getName()+".val", Call));
686           AA.copyValue(OrigLoad, Args.back());
687         }
688       }
690     if (ExtraArgHack)
691       Args.push_back(Constant::getNullValue(Type::Int32Ty));
693     // Push any varargs arguments on the list
694     for (; AI != CS.arg_end(); ++AI, ++ArgIndex) {
695       Args.push_back(*AI);
696       if (Attributes Attrs = CallPAL.getParamAttributes(ArgIndex))
697         AttributesVec.push_back(AttributeWithIndex::get(Args.size(), Attrs));
698     }
700     // Add any function attributes.
701     if (Attributes attrs = CallPAL.getFnAttributes())
702       AttributesVec.push_back(AttributeWithIndex::get(~0, attrs));
704     Instruction *New;
705     if (InvokeInst *II = dyn_cast<InvokeInst>(Call)) {
706       New = InvokeInst::Create(NF, II->getNormalDest(), II->getUnwindDest(),
707                                Args.begin(), Args.end(), "", Call);
708       cast<InvokeInst>(New)->setCallingConv(CS.getCallingConv());
709       cast<InvokeInst>(New)->setAttributes(AttrListPtr::get(AttributesVec.begin(),
710                                                           AttributesVec.end()));
711     } else {
712       New = CallInst::Create(NF, Args.begin(), Args.end(), "", Call);
713       cast<CallInst>(New)->setCallingConv(CS.getCallingConv());
714       cast<CallInst>(New)->setAttributes(AttrListPtr::get(AttributesVec.begin(),
715                                                         AttributesVec.end()));
716       if (cast<CallInst>(Call)->isTailCall())
717         cast<CallInst>(New)->setTailCall();
718     }
719     Args.clear();
720     AttributesVec.clear();
722     // Update the alias analysis implementation to know that we are replacing
723     // the old call with a new one.
724     AA.replaceWithNewValue(Call, New);
726     // Update the callgraph to know that the callsite has been transformed.
727     CG[Call->getParent()->getParent()]->replaceCallSite(Call, New);
729     if (!Call->use_empty()) {
730       Call->replaceAllUsesWith(New);
731       New->takeName(Call);
732     }
734     // Finally, remove the old call from the program, reducing the use-count of
735     // F.
736     Call->eraseFromParent();
737   }
739   // Since we have now created the new function, splice the body of the old
740   // function right into the new function, leaving the old rotting hulk of the
741   // function empty.
742   NF->getBasicBlockList().splice(NF->begin(), F->getBasicBlockList());
744   // Loop over the argument list, transfering uses of the old arguments over to
745   // the new arguments, also transfering over the names as well.
746   //
747   for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end(),
748        I2 = NF->arg_begin(); I != E; ++I) {
749     if (!ArgsToPromote.count(I) && !ByValArgsToTransform.count(I)) {
750       // If this is an unmodified argument, move the name and users over to the
751       // new version.
752       I->replaceAllUsesWith(I2);
753       I2->takeName(I);
754       AA.replaceWithNewValue(I, I2);
755       ++I2;
756       continue;
757     }
759     if (ByValArgsToTransform.count(I)) {
760       // In the callee, we create an alloca, and store each of the new incoming
761       // arguments into the alloca.
762       Instruction *InsertPt = NF->begin()->begin();
764       // Just add all the struct element types.
765       const Type *AgTy = cast<PointerType>(I->getType())->getElementType();
766       Value *TheAlloca = new AllocaInst(AgTy, 0, "", InsertPt);
767       const StructType *STy = cast<StructType>(AgTy);
768       Value *Idxs[2] = { ConstantInt::get(Type::Int32Ty, 0), 0 };
770       for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
771         Idxs[1] = ConstantInt::get(Type::Int32Ty, i);
772         std::string Name = TheAlloca->getName()+"."+utostr(i);
773         Value *Idx = GetElementPtrInst::Create(TheAlloca, Idxs, Idxs+2,
774                                                Name, InsertPt);
775         I2->setName(I->getName()+"."+utostr(i));
776         new StoreInst(I2++, Idx, InsertPt);
777       }
779       // Anything that used the arg should now use the alloca.
780       I->replaceAllUsesWith(TheAlloca);
781       TheAlloca->takeName(I);
782       AA.replaceWithNewValue(I, TheAlloca);
783       continue;
784     }
786     if (I->use_empty()) {
787       AA.deleteValue(I);
788       continue;
789     }
791     // Otherwise, if we promoted this argument, then all users are load
792     // instructions (or GEPs with only load users), and all loads should be
793     // using the new argument that we added.
794     ScalarizeTable &ArgIndices = ScalarizedElements[I];
796     while (!I->use_empty()) {
797       if (LoadInst *LI = dyn_cast<LoadInst>(I->use_back())) {
798         assert(ArgIndices.begin()->empty() &&
799                "Load element should sort to front!");
800         I2->setName(I->getName()+".val");
801         LI->replaceAllUsesWith(I2);
802         AA.replaceWithNewValue(LI, I2);
803         LI->eraseFromParent();
804         DOUT << "*** Promoted load of argument '" << I->getName()
805              << "' in function '" << F->getName() << "'\n";
806       } else {
807         GetElementPtrInst *GEP = cast<GetElementPtrInst>(I->use_back());
808         IndicesVector Operands;
809         Operands.reserve(GEP->getNumIndices());
810         for (User::op_iterator II = GEP->idx_begin(), IE = GEP->idx_end();
811              II != IE; ++II)
812           Operands.push_back(cast<ConstantInt>(*II)->getSExtValue());
814         // GEPs with a single 0 index can be merged with direct loads
815         if (Operands.size() == 1 && Operands.front() == 0)
816           Operands.clear();
818         Function::arg_iterator TheArg = I2;
819         for (ScalarizeTable::iterator It = ArgIndices.begin();
820              *It != Operands; ++It, ++TheArg) {
821           assert(It != ArgIndices.end() && "GEP not handled??");
822         }
824         std::string NewName = I->getName();
825         for (unsigned i = 0, e = Operands.size(); i != e; ++i) {
826             NewName += "." + utostr(Operands[i]);
827         }
828         NewName += ".val";
829         TheArg->setName(NewName);
831         DOUT << "*** Promoted agg argument '" << TheArg->getName()
832              << "' of function '" << NF->getName() << "'\n";
834         // All of the uses must be load instructions.  Replace them all with
835         // the argument specified by ArgNo.
836         while (!GEP->use_empty()) {
837           LoadInst *L = cast<LoadInst>(GEP->use_back());
838           L->replaceAllUsesWith(TheArg);
839           AA.replaceWithNewValue(L, TheArg);
840           L->eraseFromParent();
841         }
842         AA.deleteValue(GEP);
843         GEP->eraseFromParent();
844       }
845     }
847     // Increment I2 past all of the arguments added for this promoted pointer.
848     for (unsigned i = 0, e = ArgIndices.size(); i != e; ++i)
849       ++I2;
850   }
852   // Notify the alias analysis implementation that we inserted a new argument.
853   if (ExtraArgHack)
854     AA.copyValue(Constant::getNullValue(Type::Int32Ty), NF->arg_begin());
857   // Tell the alias analysis that the old function is about to disappear.
858   AA.replaceWithNewValue(F, NF);
860   // Now that the old function is dead, delete it.
861   F->eraseFromParent();
862   return NF;