]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/Transforms/IPO/ArgumentPromotion.cpp
ArgumentPromotion: Propagate debug locations on calls for which arguments are promoted.
[opencl/llvm.git] / lib / Transforms / IPO / ArgumentPromotion.cpp
1 //===-- ArgumentPromotion.cpp - Promote by-reference arguments ------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This pass promotes "by reference" arguments to be "by value" arguments.  In
11 // practice, this means looking for internal functions that have pointer
12 // arguments.  If it can prove, through the use of alias analysis, that an
13 // argument is *only* loaded, then it can pass the value into the function
14 // instead of the address of the value.  This can cause recursive simplification
15 // of code and lead to the elimination of allocas (especially in C++ template
16 // code like the STL).
17 //
18 // This pass also handles aggregate arguments that are passed into a function,
19 // scalarizing them if the elements of the aggregate are only loaded.  Note that
20 // by default it refuses to scalarize aggregates which would require passing in
21 // more than three operands to the function, because passing thousands of
22 // operands for a large array or structure is unprofitable! This limit can be
23 // configured or disabled, however.
24 //
25 // Note that this transformation could also be done for arguments that are only
26 // stored to (returning the value instead), but does not currently.  This case
27 // would be best handled when and if LLVM begins supporting multiple return
28 // values from functions.
29 //
30 //===----------------------------------------------------------------------===//
32 #include "llvm/Transforms/IPO.h"
33 #include "llvm/ADT/DepthFirstIterator.h"
34 #include "llvm/ADT/Statistic.h"
35 #include "llvm/ADT/StringExtras.h"
36 #include "llvm/Analysis/AliasAnalysis.h"
37 #include "llvm/Analysis/CallGraph.h"
38 #include "llvm/Analysis/CallGraphSCCPass.h"
39 #include "llvm/IR/CFG.h"
40 #include "llvm/IR/CallSite.h"
41 #include "llvm/IR/Constants.h"
42 #include "llvm/IR/DerivedTypes.h"
43 #include "llvm/IR/Instructions.h"
44 #include "llvm/IR/LLVMContext.h"
45 #include "llvm/IR/Module.h"
46 #include "llvm/Support/Debug.h"
47 #include "llvm/Support/raw_ostream.h"
48 #include <set>
49 using namespace llvm;
51 #define DEBUG_TYPE "argpromotion"
53 STATISTIC(NumArgumentsPromoted , "Number of pointer arguments promoted");
54 STATISTIC(NumAggregatesPromoted, "Number of aggregate arguments promoted");
55 STATISTIC(NumByValArgsPromoted , "Number of byval arguments promoted");
56 STATISTIC(NumArgumentsDead     , "Number of dead pointer args eliminated");
58 namespace {
59   /// ArgPromotion - The 'by reference' to 'by value' argument promotion pass.
60   ///
61   struct ArgPromotion : public CallGraphSCCPass {
62     void getAnalysisUsage(AnalysisUsage &AU) const override {
63       AU.addRequired<AliasAnalysis>();
64       CallGraphSCCPass::getAnalysisUsage(AU);
65     }
67     bool runOnSCC(CallGraphSCC &SCC) override;
68     static char ID; // Pass identification, replacement for typeid
69     explicit ArgPromotion(unsigned maxElements = 3)
70         : CallGraphSCCPass(ID), maxElements(maxElements) {
71       initializeArgPromotionPass(*PassRegistry::getPassRegistry());
72     }
74     /// A vector used to hold the indices of a single GEP instruction
75     typedef std::vector<uint64_t> IndicesVector;
77   private:
78     CallGraphNode *PromoteArguments(CallGraphNode *CGN);
79     bool isSafeToPromoteArgument(Argument *Arg, bool isByVal) const;
80     CallGraphNode *DoPromotion(Function *F,
81                                SmallPtrSet<Argument*, 8> &ArgsToPromote,
82                                SmallPtrSet<Argument*, 8> &ByValArgsToTransform);
83     /// The maximum number of elements to expand, or 0 for unlimited.
84     unsigned maxElements;
85   };
86 }
88 char ArgPromotion::ID = 0;
89 INITIALIZE_PASS_BEGIN(ArgPromotion, "argpromotion",
90                 "Promote 'by reference' arguments to scalars", false, false)
91 INITIALIZE_AG_DEPENDENCY(AliasAnalysis)
92 INITIALIZE_PASS_DEPENDENCY(CallGraphWrapperPass)
93 INITIALIZE_PASS_END(ArgPromotion, "argpromotion",
94                 "Promote 'by reference' arguments to scalars", false, false)
96 Pass *llvm::createArgumentPromotionPass(unsigned maxElements) {
97   return new ArgPromotion(maxElements);
98 }
100 bool ArgPromotion::runOnSCC(CallGraphSCC &SCC) {
101   bool Changed = false, LocalChange;
103   do {  // Iterate until we stop promoting from this SCC.
104     LocalChange = false;
105     // Attempt to promote arguments from all functions in this SCC.
106     for (CallGraphSCC::iterator I = SCC.begin(), E = SCC.end(); I != E; ++I) {
107       if (CallGraphNode *CGN = PromoteArguments(*I)) {
108         LocalChange = true;
109         SCC.ReplaceNode(*I, CGN);
110       }
111     }
112     Changed |= LocalChange;               // Remember that we changed something.
113   } while (LocalChange);
114   
115   return Changed;
118 /// PromoteArguments - This method checks the specified function to see if there
119 /// are any promotable arguments and if it is safe to promote the function (for
120 /// example, all callers are direct).  If safe to promote some arguments, it
121 /// calls the DoPromotion method.
122 ///
123 CallGraphNode *ArgPromotion::PromoteArguments(CallGraphNode *CGN) {
124   Function *F = CGN->getFunction();
126   // Make sure that it is local to this module.
127   if (!F || !F->hasLocalLinkage()) return nullptr;
129   // First check: see if there are any pointer arguments!  If not, quick exit.
130   SmallVector<Argument*, 16> PointerArgs;
131   for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end(); I != E; ++I)
132     if (I->getType()->isPointerTy())
133       PointerArgs.push_back(I);
134   if (PointerArgs.empty()) return nullptr;
136   // Second check: make sure that all callers are direct callers.  We can't
137   // transform functions that have indirect callers.  Also see if the function
138   // is self-recursive.
139   bool isSelfRecursive = false;
140   for (Use &U : F->uses()) {
141     CallSite CS(U.getUser());
142     // Must be a direct call.
143     if (CS.getInstruction() == nullptr || !CS.isCallee(&U)) return nullptr;
144     
145     if (CS.getInstruction()->getParent()->getParent() == F)
146       isSelfRecursive = true;
147   }
148   
149   // Check to see which arguments are promotable.  If an argument is promotable,
150   // add it to ArgsToPromote.
151   SmallPtrSet<Argument*, 8> ArgsToPromote;
152   SmallPtrSet<Argument*, 8> ByValArgsToTransform;
153   for (unsigned i = 0, e = PointerArgs.size(); i != e; ++i) {
154     Argument *PtrArg = PointerArgs[i];
155     Type *AgTy = cast<PointerType>(PtrArg->getType())->getElementType();
157     // If this is a byval argument, and if the aggregate type is small, just
158     // pass the elements, which is always safe.  This does not apply to
159     // inalloca.
160     if (PtrArg->hasByValAttr()) {
161       if (StructType *STy = dyn_cast<StructType>(AgTy)) {
162         if (maxElements > 0 && STy->getNumElements() > maxElements) {
163           DEBUG(dbgs() << "argpromotion disable promoting argument '"
164                 << PtrArg->getName() << "' because it would require adding more"
165                 << " than " << maxElements << " arguments to the function.\n");
166           continue;
167         }
168         
169         // If all the elements are single-value types, we can promote it.
170         bool AllSimple = true;
171         for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
172           if (!STy->getElementType(i)->isSingleValueType()) {
173             AllSimple = false;
174             break;
175           }
176         }
178         // Safe to transform, don't even bother trying to "promote" it.
179         // Passing the elements as a scalar will allow scalarrepl to hack on
180         // the new alloca we introduce.
181         if (AllSimple) {
182           ByValArgsToTransform.insert(PtrArg);
183           continue;
184         }
185       }
186     }
188     // If the argument is a recursive type and we're in a recursive
189     // function, we could end up infinitely peeling the function argument.
190     if (isSelfRecursive) {
191       if (StructType *STy = dyn_cast<StructType>(AgTy)) {
192         bool RecursiveType = false;
193         for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
194           if (STy->getElementType(i) == PtrArg->getType()) {
195             RecursiveType = true;
196             break;
197           }
198         }
199         if (RecursiveType)
200           continue;
201       }
202     }
203     
204     // Otherwise, see if we can promote the pointer to its value.
205     if (isSafeToPromoteArgument(PtrArg, PtrArg->hasByValOrInAllocaAttr()))
206       ArgsToPromote.insert(PtrArg);
207   }
209   // No promotable pointer arguments.
210   if (ArgsToPromote.empty() && ByValArgsToTransform.empty()) 
211     return nullptr;
213   return DoPromotion(F, ArgsToPromote, ByValArgsToTransform);
216 /// AllCallersPassInValidPointerForArgument - Return true if we can prove that
217 /// all callees pass in a valid pointer for the specified function argument.
218 static bool AllCallersPassInValidPointerForArgument(Argument *Arg) {
219   Function *Callee = Arg->getParent();
221   unsigned ArgNo = Arg->getArgNo();
223   // Look at all call sites of the function.  At this pointer we know we only
224   // have direct callees.
225   for (User *U : Callee->users()) {
226     CallSite CS(U);
227     assert(CS && "Should only have direct calls!");
229     if (!CS.getArgument(ArgNo)->isDereferenceablePointer())
230       return false;
231   }
232   return true;
235 /// Returns true if Prefix is a prefix of longer. That means, Longer has a size
236 /// that is greater than or equal to the size of prefix, and each of the
237 /// elements in Prefix is the same as the corresponding elements in Longer.
238 ///
239 /// This means it also returns true when Prefix and Longer are equal!
240 static bool IsPrefix(const ArgPromotion::IndicesVector &Prefix,
241                      const ArgPromotion::IndicesVector &Longer) {
242   if (Prefix.size() > Longer.size())
243     return false;
244   return std::equal(Prefix.begin(), Prefix.end(), Longer.begin());
248 /// Checks if Indices, or a prefix of Indices, is in Set.
249 static bool PrefixIn(const ArgPromotion::IndicesVector &Indices,
250                      std::set<ArgPromotion::IndicesVector> &Set) {
251     std::set<ArgPromotion::IndicesVector>::iterator Low;
252     Low = Set.upper_bound(Indices);
253     if (Low != Set.begin())
254       Low--;
255     // Low is now the last element smaller than or equal to Indices. This means
256     // it points to a prefix of Indices (possibly Indices itself), if such
257     // prefix exists.
258     //
259     // This load is safe if any prefix of its operands is safe to load.
260     return Low != Set.end() && IsPrefix(*Low, Indices);
263 /// Mark the given indices (ToMark) as safe in the given set of indices
264 /// (Safe). Marking safe usually means adding ToMark to Safe. However, if there
265 /// is already a prefix of Indices in Safe, Indices are implicitely marked safe
266 /// already. Furthermore, any indices that Indices is itself a prefix of, are
267 /// removed from Safe (since they are implicitely safe because of Indices now).
268 static void MarkIndicesSafe(const ArgPromotion::IndicesVector &ToMark,
269                             std::set<ArgPromotion::IndicesVector> &Safe) {
270   std::set<ArgPromotion::IndicesVector>::iterator Low;
271   Low = Safe.upper_bound(ToMark);
272   // Guard against the case where Safe is empty
273   if (Low != Safe.begin())
274     Low--;
275   // Low is now the last element smaller than or equal to Indices. This
276   // means it points to a prefix of Indices (possibly Indices itself), if
277   // such prefix exists.
278   if (Low != Safe.end()) {
279     if (IsPrefix(*Low, ToMark))
280       // If there is already a prefix of these indices (or exactly these
281       // indices) marked a safe, don't bother adding these indices
282       return;
284     // Increment Low, so we can use it as a "insert before" hint
285     ++Low;
286   }
287   // Insert
288   Low = Safe.insert(Low, ToMark);
289   ++Low;
290   // If there we're a prefix of longer index list(s), remove those
291   std::set<ArgPromotion::IndicesVector>::iterator End = Safe.end();
292   while (Low != End && IsPrefix(ToMark, *Low)) {
293     std::set<ArgPromotion::IndicesVector>::iterator Remove = Low;
294     ++Low;
295     Safe.erase(Remove);
296   }
299 /// isSafeToPromoteArgument - As you might guess from the name of this method,
300 /// it checks to see if it is both safe and useful to promote the argument.
301 /// This method limits promotion of aggregates to only promote up to three
302 /// elements of the aggregate in order to avoid exploding the number of
303 /// arguments passed in.
304 bool ArgPromotion::isSafeToPromoteArgument(Argument *Arg,
305                                            bool isByValOrInAlloca) const {
306   typedef std::set<IndicesVector> GEPIndicesSet;
308   // Quick exit for unused arguments
309   if (Arg->use_empty())
310     return true;
312   // We can only promote this argument if all of the uses are loads, or are GEP
313   // instructions (with constant indices) that are subsequently loaded.
314   //
315   // Promoting the argument causes it to be loaded in the caller
316   // unconditionally. This is only safe if we can prove that either the load
317   // would have happened in the callee anyway (ie, there is a load in the entry
318   // block) or the pointer passed in at every call site is guaranteed to be
319   // valid.
320   // In the former case, invalid loads can happen, but would have happened
321   // anyway, in the latter case, invalid loads won't happen. This prevents us
322   // from introducing an invalid load that wouldn't have happened in the
323   // original code.
324   //
325   // This set will contain all sets of indices that are loaded in the entry
326   // block, and thus are safe to unconditionally load in the caller.
327   //
328   // This optimization is also safe for InAlloca parameters, because it verifies
329   // that the address isn't captured.
330   GEPIndicesSet SafeToUnconditionallyLoad;
332   // This set contains all the sets of indices that we are planning to promote.
333   // This makes it possible to limit the number of arguments added.
334   GEPIndicesSet ToPromote;
336   // If the pointer is always valid, any load with first index 0 is valid.
337   if (isByValOrInAlloca || AllCallersPassInValidPointerForArgument(Arg))
338     SafeToUnconditionallyLoad.insert(IndicesVector(1, 0));
340   // First, iterate the entry block and mark loads of (geps of) arguments as
341   // safe.
342   BasicBlock *EntryBlock = Arg->getParent()->begin();
343   // Declare this here so we can reuse it
344   IndicesVector Indices;
345   for (BasicBlock::iterator I = EntryBlock->begin(), E = EntryBlock->end();
346        I != E; ++I)
347     if (LoadInst *LI = dyn_cast<LoadInst>(I)) {
348       Value *V = LI->getPointerOperand();
349       if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(V)) {
350         V = GEP->getPointerOperand();
351         if (V == Arg) {
352           // This load actually loads (part of) Arg? Check the indices then.
353           Indices.reserve(GEP->getNumIndices());
354           for (User::op_iterator II = GEP->idx_begin(), IE = GEP->idx_end();
355                II != IE; ++II)
356             if (ConstantInt *CI = dyn_cast<ConstantInt>(*II))
357               Indices.push_back(CI->getSExtValue());
358             else
359               // We found a non-constant GEP index for this argument? Bail out
360               // right away, can't promote this argument at all.
361               return false;
363           // Indices checked out, mark them as safe
364           MarkIndicesSafe(Indices, SafeToUnconditionallyLoad);
365           Indices.clear();
366         }
367       } else if (V == Arg) {
368         // Direct loads are equivalent to a GEP with a single 0 index.
369         MarkIndicesSafe(IndicesVector(1, 0), SafeToUnconditionallyLoad);
370       }
371     }
373   // Now, iterate all uses of the argument to see if there are any uses that are
374   // not (GEP+)loads, or any (GEP+)loads that are not safe to promote.
375   SmallVector<LoadInst*, 16> Loads;
376   IndicesVector Operands;
377   for (Use &U : Arg->uses()) {
378     User *UR = U.getUser();
379     Operands.clear();
380     if (LoadInst *LI = dyn_cast<LoadInst>(UR)) {
381       // Don't hack volatile/atomic loads
382       if (!LI->isSimple()) return false;
383       Loads.push_back(LI);
384       // Direct loads are equivalent to a GEP with a zero index and then a load.
385       Operands.push_back(0);
386     } else if (GetElementPtrInst *GEP = dyn_cast<GetElementPtrInst>(UR)) {
387       if (GEP->use_empty()) {
388         // Dead GEP's cause trouble later.  Just remove them if we run into
389         // them.
390         getAnalysis<AliasAnalysis>().deleteValue(GEP);
391         GEP->eraseFromParent();
392         // TODO: This runs the above loop over and over again for dead GEPs
393         // Couldn't we just do increment the UI iterator earlier and erase the
394         // use?
395         return isSafeToPromoteArgument(Arg, isByValOrInAlloca);
396       }
398       // Ensure that all of the indices are constants.
399       for (User::op_iterator i = GEP->idx_begin(), e = GEP->idx_end();
400         i != e; ++i)
401         if (ConstantInt *C = dyn_cast<ConstantInt>(*i))
402           Operands.push_back(C->getSExtValue());
403         else
404           return false;  // Not a constant operand GEP!
406       // Ensure that the only users of the GEP are load instructions.
407       for (User *GEPU : GEP->users())
408         if (LoadInst *LI = dyn_cast<LoadInst>(GEPU)) {
409           // Don't hack volatile/atomic loads
410           if (!LI->isSimple()) return false;
411           Loads.push_back(LI);
412         } else {
413           // Other uses than load?
414           return false;
415         }
416     } else {
417       return false;  // Not a load or a GEP.
418     }
420     // Now, see if it is safe to promote this load / loads of this GEP. Loading
421     // is safe if Operands, or a prefix of Operands, is marked as safe.
422     if (!PrefixIn(Operands, SafeToUnconditionallyLoad))
423       return false;
425     // See if we are already promoting a load with these indices. If not, check
426     // to make sure that we aren't promoting too many elements.  If so, nothing
427     // to do.
428     if (ToPromote.find(Operands) == ToPromote.end()) {
429       if (maxElements > 0 && ToPromote.size() == maxElements) {
430         DEBUG(dbgs() << "argpromotion not promoting argument '"
431               << Arg->getName() << "' because it would require adding more "
432               << "than " << maxElements << " arguments to the function.\n");
433         // We limit aggregate promotion to only promoting up to a fixed number
434         // of elements of the aggregate.
435         return false;
436       }
437       ToPromote.insert(Operands);
438     }
439   }
441   if (Loads.empty()) return true;  // No users, this is a dead argument.
443   // Okay, now we know that the argument is only used by load instructions and
444   // it is safe to unconditionally perform all of them. Use alias analysis to
445   // check to see if the pointer is guaranteed to not be modified from entry of
446   // the function to each of the load instructions.
448   // Because there could be several/many load instructions, remember which
449   // blocks we know to be transparent to the load.
450   SmallPtrSet<BasicBlock*, 16> TranspBlocks;
452   AliasAnalysis &AA = getAnalysis<AliasAnalysis>();
454   for (unsigned i = 0, e = Loads.size(); i != e; ++i) {
455     // Check to see if the load is invalidated from the start of the block to
456     // the load itself.
457     LoadInst *Load = Loads[i];
458     BasicBlock *BB = Load->getParent();
460     AliasAnalysis::Location Loc = AA.getLocation(Load);
461     if (AA.canInstructionRangeModify(BB->front(), *Load, Loc))
462       return false;  // Pointer is invalidated!
464     // Now check every path from the entry block to the load for transparency.
465     // To do this, we perform a depth first search on the inverse CFG from the
466     // loading block.
467     for (pred_iterator PI = pred_begin(BB), E = pred_end(BB); PI != E; ++PI) {
468       BasicBlock *P = *PI;
469       for (idf_ext_iterator<BasicBlock*, SmallPtrSet<BasicBlock*, 16> >
470              I = idf_ext_begin(P, TranspBlocks),
471              E = idf_ext_end(P, TranspBlocks); I != E; ++I)
472         if (AA.canBasicBlockModify(**I, Loc))
473           return false;
474     }
475   }
477   // If the path from the entry of the function to each load is free of
478   // instructions that potentially invalidate the load, we can make the
479   // transformation!
480   return true;
483 /// DoPromotion - This method actually performs the promotion of the specified
484 /// arguments, and returns the new function.  At this point, we know that it's
485 /// safe to do so.
486 CallGraphNode *ArgPromotion::DoPromotion(Function *F,
487                                SmallPtrSet<Argument*, 8> &ArgsToPromote,
488                               SmallPtrSet<Argument*, 8> &ByValArgsToTransform) {
490   // Start by computing a new prototype for the function, which is the same as
491   // the old function, but has modified arguments.
492   FunctionType *FTy = F->getFunctionType();
493   std::vector<Type*> Params;
495   typedef std::set<IndicesVector> ScalarizeTable;
497   // ScalarizedElements - If we are promoting a pointer that has elements
498   // accessed out of it, keep track of which elements are accessed so that we
499   // can add one argument for each.
500   //
501   // Arguments that are directly loaded will have a zero element value here, to
502   // handle cases where there are both a direct load and GEP accesses.
503   //
504   std::map<Argument*, ScalarizeTable> ScalarizedElements;
506   // OriginalLoads - Keep track of a representative load instruction from the
507   // original function so that we can tell the alias analysis implementation
508   // what the new GEP/Load instructions we are inserting look like.
509   // We need to keep the original loads for each argument and the elements
510   // of the argument that are accessed.
511   std::map<std::pair<Argument*, IndicesVector>, LoadInst*> OriginalLoads;
513   // Attribute - Keep track of the parameter attributes for the arguments
514   // that we are *not* promoting. For the ones that we do promote, the parameter
515   // attributes are lost
516   SmallVector<AttributeSet, 8> AttributesVec;
517   const AttributeSet &PAL = F->getAttributes();
519   // Add any return attributes.
520   if (PAL.hasAttributes(AttributeSet::ReturnIndex))
521     AttributesVec.push_back(AttributeSet::get(F->getContext(),
522                                               PAL.getRetAttributes()));
524   // First, determine the new argument list
525   unsigned ArgIndex = 1;
526   for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end(); I != E;
527        ++I, ++ArgIndex) {
528     if (ByValArgsToTransform.count(I)) {
529       // Simple byval argument? Just add all the struct element types.
530       Type *AgTy = cast<PointerType>(I->getType())->getElementType();
531       StructType *STy = cast<StructType>(AgTy);
532       for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i)
533         Params.push_back(STy->getElementType(i));
534       ++NumByValArgsPromoted;
535     } else if (!ArgsToPromote.count(I)) {
536       // Unchanged argument
537       Params.push_back(I->getType());
538       AttributeSet attrs = PAL.getParamAttributes(ArgIndex);
539       if (attrs.hasAttributes(ArgIndex)) {
540         AttrBuilder B(attrs, ArgIndex);
541         AttributesVec.
542           push_back(AttributeSet::get(F->getContext(), Params.size(), B));
543       }
544     } else if (I->use_empty()) {
545       // Dead argument (which are always marked as promotable)
546       ++NumArgumentsDead;
547     } else {
548       // Okay, this is being promoted. This means that the only uses are loads
549       // or GEPs which are only used by loads
551       // In this table, we will track which indices are loaded from the argument
552       // (where direct loads are tracked as no indices).
553       ScalarizeTable &ArgIndices = ScalarizedElements[I];
554       for (User *U : I->users()) {
555         Instruction *UI = cast<Instruction>(U);
556         assert(isa<LoadInst>(UI) || isa<GetElementPtrInst>(UI));
557         IndicesVector Indices;
558         Indices.reserve(UI->getNumOperands() - 1);
559         // Since loads will only have a single operand, and GEPs only a single
560         // non-index operand, this will record direct loads without any indices,
561         // and gep+loads with the GEP indices.
562         for (User::op_iterator II = UI->op_begin() + 1, IE = UI->op_end();
563              II != IE; ++II)
564           Indices.push_back(cast<ConstantInt>(*II)->getSExtValue());
565         // GEPs with a single 0 index can be merged with direct loads
566         if (Indices.size() == 1 && Indices.front() == 0)
567           Indices.clear();
568         ArgIndices.insert(Indices);
569         LoadInst *OrigLoad;
570         if (LoadInst *L = dyn_cast<LoadInst>(UI))
571           OrigLoad = L;
572         else
573           // Take any load, we will use it only to update Alias Analysis
574           OrigLoad = cast<LoadInst>(UI->user_back());
575         OriginalLoads[std::make_pair(I, Indices)] = OrigLoad;
576       }
578       // Add a parameter to the function for each element passed in.
579       for (ScalarizeTable::iterator SI = ArgIndices.begin(),
580              E = ArgIndices.end(); SI != E; ++SI) {
581         // not allowed to dereference ->begin() if size() is 0
582         Params.push_back(GetElementPtrInst::getIndexedType(I->getType(), *SI));
583         assert(Params.back());
584       }
586       if (ArgIndices.size() == 1 && ArgIndices.begin()->empty())
587         ++NumArgumentsPromoted;
588       else
589         ++NumAggregatesPromoted;
590     }
591   }
593   // Add any function attributes.
594   if (PAL.hasAttributes(AttributeSet::FunctionIndex))
595     AttributesVec.push_back(AttributeSet::get(FTy->getContext(),
596                                               PAL.getFnAttributes()));
598   Type *RetTy = FTy->getReturnType();
600   // Construct the new function type using the new arguments.
601   FunctionType *NFTy = FunctionType::get(RetTy, Params, FTy->isVarArg());
603   // Create the new function body and insert it into the module.
604   Function *NF = Function::Create(NFTy, F->getLinkage(), F->getName());
605   NF->copyAttributesFrom(F);
607   
608   DEBUG(dbgs() << "ARG PROMOTION:  Promoting to:" << *NF << "\n"
609         << "From: " << *F);
610   
611   // Recompute the parameter attributes list based on the new arguments for
612   // the function.
613   NF->setAttributes(AttributeSet::get(F->getContext(), AttributesVec));
614   AttributesVec.clear();
616   F->getParent()->getFunctionList().insert(F, NF);
617   NF->takeName(F);
619   // Get the alias analysis information that we need to update to reflect our
620   // changes.
621   AliasAnalysis &AA = getAnalysis<AliasAnalysis>();
623   // Get the callgraph information that we need to update to reflect our
624   // changes.
625   CallGraph &CG = getAnalysis<CallGraphWrapperPass>().getCallGraph();
627   // Get a new callgraph node for NF.
628   CallGraphNode *NF_CGN = CG.getOrInsertFunction(NF);
630   // Loop over all of the callers of the function, transforming the call sites
631   // to pass in the loaded pointers.
632   //
633   SmallVector<Value*, 16> Args;
634   while (!F->use_empty()) {
635     CallSite CS(F->user_back());
636     assert(CS.getCalledFunction() == F);
637     Instruction *Call = CS.getInstruction();
638     const AttributeSet &CallPAL = CS.getAttributes();
640     // Add any return attributes.
641     if (CallPAL.hasAttributes(AttributeSet::ReturnIndex))
642       AttributesVec.push_back(AttributeSet::get(F->getContext(),
643                                                 CallPAL.getRetAttributes()));
645     // Loop over the operands, inserting GEP and loads in the caller as
646     // appropriate.
647     CallSite::arg_iterator AI = CS.arg_begin();
648     ArgIndex = 1;
649     for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end();
650          I != E; ++I, ++AI, ++ArgIndex)
651       if (!ArgsToPromote.count(I) && !ByValArgsToTransform.count(I)) {
652         Args.push_back(*AI);          // Unmodified argument
654         if (CallPAL.hasAttributes(ArgIndex)) {
655           AttrBuilder B(CallPAL, ArgIndex);
656           AttributesVec.
657             push_back(AttributeSet::get(F->getContext(), Args.size(), B));
658         }
659       } else if (ByValArgsToTransform.count(I)) {
660         // Emit a GEP and load for each element of the struct.
661         Type *AgTy = cast<PointerType>(I->getType())->getElementType();
662         StructType *STy = cast<StructType>(AgTy);
663         Value *Idxs[2] = {
664               ConstantInt::get(Type::getInt32Ty(F->getContext()), 0), nullptr };
665         for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
666           Idxs[1] = ConstantInt::get(Type::getInt32Ty(F->getContext()), i);
667           Value *Idx = GetElementPtrInst::Create(*AI, Idxs,
668                                                  (*AI)->getName()+"."+utostr(i),
669                                                  Call);
670           // TODO: Tell AA about the new values?
671           Args.push_back(new LoadInst(Idx, Idx->getName()+".val", Call));
672         }
673       } else if (!I->use_empty()) {
674         // Non-dead argument: insert GEPs and loads as appropriate.
675         ScalarizeTable &ArgIndices = ScalarizedElements[I];
676         // Store the Value* version of the indices in here, but declare it now
677         // for reuse.
678         std::vector<Value*> Ops;
679         for (ScalarizeTable::iterator SI = ArgIndices.begin(),
680                E = ArgIndices.end(); SI != E; ++SI) {
681           Value *V = *AI;
682           LoadInst *OrigLoad = OriginalLoads[std::make_pair(I, *SI)];
683           if (!SI->empty()) {
684             Ops.reserve(SI->size());
685             Type *ElTy = V->getType();
686             for (IndicesVector::const_iterator II = SI->begin(),
687                  IE = SI->end(); II != IE; ++II) {
688               // Use i32 to index structs, and i64 for others (pointers/arrays).
689               // This satisfies GEP constraints.
690               Type *IdxTy = (ElTy->isStructTy() ?
691                     Type::getInt32Ty(F->getContext()) : 
692                     Type::getInt64Ty(F->getContext()));
693               Ops.push_back(ConstantInt::get(IdxTy, *II));
694               // Keep track of the type we're currently indexing.
695               ElTy = cast<CompositeType>(ElTy)->getTypeAtIndex(*II);
696             }
697             // And create a GEP to extract those indices.
698             V = GetElementPtrInst::Create(V, Ops, V->getName()+".idx", Call);
699             Ops.clear();
700             AA.copyValue(OrigLoad->getOperand(0), V);
701           }
702           // Since we're replacing a load make sure we take the alignment
703           // of the previous load.
704           LoadInst *newLoad = new LoadInst(V, V->getName()+".val", Call);
705           newLoad->setAlignment(OrigLoad->getAlignment());
706           // Transfer the TBAA info too.
707           newLoad->setMetadata(LLVMContext::MD_tbaa,
708                                OrigLoad->getMetadata(LLVMContext::MD_tbaa));
709           Args.push_back(newLoad);
710           AA.copyValue(OrigLoad, Args.back());
711         }
712       }
714     // Push any varargs arguments on the list.
715     for (; AI != CS.arg_end(); ++AI, ++ArgIndex) {
716       Args.push_back(*AI);
717       if (CallPAL.hasAttributes(ArgIndex)) {
718         AttrBuilder B(CallPAL, ArgIndex);
719         AttributesVec.
720           push_back(AttributeSet::get(F->getContext(), Args.size(), B));
721       }
722     }
724     // Add any function attributes.
725     if (CallPAL.hasAttributes(AttributeSet::FunctionIndex))
726       AttributesVec.push_back(AttributeSet::get(Call->getContext(),
727                                                 CallPAL.getFnAttributes()));
729     Instruction *New;
730     if (InvokeInst *II = dyn_cast<InvokeInst>(Call)) {
731       New = InvokeInst::Create(NF, II->getNormalDest(), II->getUnwindDest(),
732                                Args, "", Call);
733       cast<InvokeInst>(New)->setCallingConv(CS.getCallingConv());
734       cast<InvokeInst>(New)->setAttributes(AttributeSet::get(II->getContext(),
735                                                             AttributesVec));
736     } else {
737       New = CallInst::Create(NF, Args, "", Call);
738       cast<CallInst>(New)->setCallingConv(CS.getCallingConv());
739       cast<CallInst>(New)->setAttributes(AttributeSet::get(New->getContext(),
740                                                           AttributesVec));
741       if (cast<CallInst>(Call)->isTailCall())
742         cast<CallInst>(New)->setTailCall();
743     }
744     New->setDebugLoc(Call->getDebugLoc());
745     Args.clear();
746     AttributesVec.clear();
748     // Update the alias analysis implementation to know that we are replacing
749     // the old call with a new one.
750     AA.replaceWithNewValue(Call, New);
752     // Update the callgraph to know that the callsite has been transformed.
753     CallGraphNode *CalleeNode = CG[Call->getParent()->getParent()];
754     CalleeNode->replaceCallEdge(Call, New, NF_CGN);
756     if (!Call->use_empty()) {
757       Call->replaceAllUsesWith(New);
758       New->takeName(Call);
759     }
761     // Finally, remove the old call from the program, reducing the use-count of
762     // F.
763     Call->eraseFromParent();
764   }
766   // Since we have now created the new function, splice the body of the old
767   // function right into the new function, leaving the old rotting hulk of the
768   // function empty.
769   NF->getBasicBlockList().splice(NF->begin(), F->getBasicBlockList());
771   // Loop over the argument list, transferring uses of the old arguments over to
772   // the new arguments, also transferring over the names as well.
773   //
774   for (Function::arg_iterator I = F->arg_begin(), E = F->arg_end(),
775        I2 = NF->arg_begin(); I != E; ++I) {
776     if (!ArgsToPromote.count(I) && !ByValArgsToTransform.count(I)) {
777       // If this is an unmodified argument, move the name and users over to the
778       // new version.
779       I->replaceAllUsesWith(I2);
780       I2->takeName(I);
781       AA.replaceWithNewValue(I, I2);
782       ++I2;
783       continue;
784     }
786     if (ByValArgsToTransform.count(I)) {
787       // In the callee, we create an alloca, and store each of the new incoming
788       // arguments into the alloca.
789       Instruction *InsertPt = NF->begin()->begin();
791       // Just add all the struct element types.
792       Type *AgTy = cast<PointerType>(I->getType())->getElementType();
793       Value *TheAlloca = new AllocaInst(AgTy, nullptr, "", InsertPt);
794       StructType *STy = cast<StructType>(AgTy);
795       Value *Idxs[2] = {
796             ConstantInt::get(Type::getInt32Ty(F->getContext()), 0), nullptr };
798       for (unsigned i = 0, e = STy->getNumElements(); i != e; ++i) {
799         Idxs[1] = ConstantInt::get(Type::getInt32Ty(F->getContext()), i);
800         Value *Idx = 
801           GetElementPtrInst::Create(TheAlloca, Idxs,
802                                     TheAlloca->getName()+"."+Twine(i), 
803                                     InsertPt);
804         I2->setName(I->getName()+"."+Twine(i));
805         new StoreInst(I2++, Idx, InsertPt);
806       }
808       // Anything that used the arg should now use the alloca.
809       I->replaceAllUsesWith(TheAlloca);
810       TheAlloca->takeName(I);
811       AA.replaceWithNewValue(I, TheAlloca);
813       // If the alloca is used in a call, we must clear the tail flag since
814       // the callee now uses an alloca from the caller.
815       for (User *U : TheAlloca->users()) {
816         CallInst *Call = dyn_cast<CallInst>(U);
817         if (!Call)
818           continue;
819         Call->setTailCall(false);
820       }
821       continue;
822     }
824     if (I->use_empty()) {
825       AA.deleteValue(I);
826       continue;
827     }
829     // Otherwise, if we promoted this argument, then all users are load
830     // instructions (or GEPs with only load users), and all loads should be
831     // using the new argument that we added.
832     ScalarizeTable &ArgIndices = ScalarizedElements[I];
834     while (!I->use_empty()) {
835       if (LoadInst *LI = dyn_cast<LoadInst>(I->user_back())) {
836         assert(ArgIndices.begin()->empty() &&
837                "Load element should sort to front!");
838         I2->setName(I->getName()+".val");
839         LI->replaceAllUsesWith(I2);
840         AA.replaceWithNewValue(LI, I2);
841         LI->eraseFromParent();
842         DEBUG(dbgs() << "*** Promoted load of argument '" << I->getName()
843               << "' in function '" << F->getName() << "'\n");
844       } else {
845         GetElementPtrInst *GEP = cast<GetElementPtrInst>(I->user_back());
846         IndicesVector Operands;
847         Operands.reserve(GEP->getNumIndices());
848         for (User::op_iterator II = GEP->idx_begin(), IE = GEP->idx_end();
849              II != IE; ++II)
850           Operands.push_back(cast<ConstantInt>(*II)->getSExtValue());
852         // GEPs with a single 0 index can be merged with direct loads
853         if (Operands.size() == 1 && Operands.front() == 0)
854           Operands.clear();
856         Function::arg_iterator TheArg = I2;
857         for (ScalarizeTable::iterator It = ArgIndices.begin();
858              *It != Operands; ++It, ++TheArg) {
859           assert(It != ArgIndices.end() && "GEP not handled??");
860         }
862         std::string NewName = I->getName();
863         for (unsigned i = 0, e = Operands.size(); i != e; ++i) {
864             NewName += "." + utostr(Operands[i]);
865         }
866         NewName += ".val";
867         TheArg->setName(NewName);
869         DEBUG(dbgs() << "*** Promoted agg argument '" << TheArg->getName()
870               << "' of function '" << NF->getName() << "'\n");
872         // All of the uses must be load instructions.  Replace them all with
873         // the argument specified by ArgNo.
874         while (!GEP->use_empty()) {
875           LoadInst *L = cast<LoadInst>(GEP->user_back());
876           L->replaceAllUsesWith(TheArg);
877           AA.replaceWithNewValue(L, TheArg);
878           L->eraseFromParent();
879         }
880         AA.deleteValue(GEP);
881         GEP->eraseFromParent();
882       }
883     }
885     // Increment I2 past all of the arguments added for this promoted pointer.
886     std::advance(I2, ArgIndices.size());
887   }
889   // Tell the alias analysis that the old function is about to disappear.
890   AA.replaceWithNewValue(F, NF);
892   
893   NF_CGN->stealCalledFunctionsFrom(CG[F]);
894   
895   // Now that the old function is dead, delete it.  If there is a dangling
896   // reference to the CallgraphNode, just leave the dead function around for
897   // someone else to nuke.
898   CallGraphNode *CGN = CG[F];
899   if (CGN->getNumReferences() == 0)
900     delete CG.removeFunctionFromModule(CGN);
901   else
902     F->setLinkage(Function::ExternalLinkage);
903   
904   return NF_CGN;