Standardize {pred,succ,use,user}_empty()
[opencl/llvm.git] / lib / Transforms / IPO / PruneEH.cpp
1 //===- PruneEH.cpp - Pass which deletes unused exception handlers ---------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements a simple interprocedural pass which walks the
11 // call-graph, turning invoke instructions into calls, iff the callee cannot
12 // throw an exception, and marking functions 'nounwind' if they cannot throw.
13 // It implements this as a bottom-up traversal of the call-graph.
14 //
15 //===----------------------------------------------------------------------===//
17 #include "llvm/Transforms/IPO.h"
18 #include "llvm/ADT/SmallPtrSet.h"
19 #include "llvm/ADT/SmallVector.h"
20 #include "llvm/ADT/Statistic.h"
21 #include "llvm/Analysis/CallGraph.h"
22 #include "llvm/Analysis/CallGraphSCCPass.h"
23 #include "llvm/IR/CFG.h"
24 #include "llvm/IR/Constants.h"
25 #include "llvm/IR/Function.h"
26 #include "llvm/IR/Instructions.h"
27 #include "llvm/IR/IntrinsicInst.h"
28 #include "llvm/IR/LLVMContext.h"
29 #include <algorithm>
30 using namespace llvm;
32 #define DEBUG_TYPE "prune-eh"
34 STATISTIC(NumRemoved, "Number of invokes removed");
35 STATISTIC(NumUnreach, "Number of noreturn calls optimized");
37 namespace {
38   struct PruneEH : public CallGraphSCCPass {
39     static char ID; // Pass identification, replacement for typeid
40     PruneEH() : CallGraphSCCPass(ID) {
41       initializePruneEHPass(*PassRegistry::getPassRegistry());
42     }
44     // runOnSCC - Analyze the SCC, performing the transformation if possible.
45     bool runOnSCC(CallGraphSCC &SCC) override;
47     bool SimplifyFunction(Function *F);
48     void DeleteBasicBlock(BasicBlock *BB);
49   };
50 }
52 char PruneEH::ID = 0;
53 INITIALIZE_PASS_BEGIN(PruneEH, "prune-eh",
54                 "Remove unused exception handling info", false, false)
55 INITIALIZE_PASS_DEPENDENCY(CallGraphWrapperPass)
56 INITIALIZE_PASS_END(PruneEH, "prune-eh",
57                 "Remove unused exception handling info", false, false)
59 Pass *llvm::createPruneEHPass() { return new PruneEH(); }
62 bool PruneEH::runOnSCC(CallGraphSCC &SCC) {
63   SmallPtrSet<CallGraphNode *, 8> SCCNodes;
64   CallGraph &CG = getAnalysis<CallGraphWrapperPass>().getCallGraph();
65   bool MadeChange = false;
67   // Fill SCCNodes with the elements of the SCC.  Used for quickly
68   // looking up whether a given CallGraphNode is in this SCC.
69   for (CallGraphSCC::iterator I = SCC.begin(), E = SCC.end(); I != E; ++I)
70     SCCNodes.insert(*I);
72   // First pass, scan all of the functions in the SCC, simplifying them
73   // according to what we know.
74   for (CallGraphSCC::iterator I = SCC.begin(), E = SCC.end(); I != E; ++I)
75     if (Function *F = (*I)->getFunction())
76       MadeChange |= SimplifyFunction(F);
78   // Next, check to see if any callees might throw or if there are any external
79   // functions in this SCC: if so, we cannot prune any functions in this SCC.
80   // Definitions that are weak and not declared non-throwing might be 
81   // overridden at linktime with something that throws, so assume that.
82   // If this SCC includes the unwind instruction, we KNOW it throws, so
83   // obviously the SCC might throw.
84   //
85   bool SCCMightUnwind = false, SCCMightReturn = false;
86   for (CallGraphSCC::iterator I = SCC.begin(), E = SCC.end(); 
87        (!SCCMightUnwind || !SCCMightReturn) && I != E; ++I) {
88     Function *F = (*I)->getFunction();
89     if (!F) {
90       SCCMightUnwind = true;
91       SCCMightReturn = true;
92     } else if (F->isDeclaration() || F->mayBeOverridden()) {
93       SCCMightUnwind |= !F->doesNotThrow();
94       SCCMightReturn |= !F->doesNotReturn();
95     } else {
96       bool CheckUnwind = !SCCMightUnwind && !F->doesNotThrow();
97       bool CheckReturn = !SCCMightReturn && !F->doesNotReturn();
99       if (!CheckUnwind && !CheckReturn)
100         continue;
102       // Check to see if this function performs an unwind or calls an
103       // unwinding function.
104       for (Function::iterator BB = F->begin(), E = F->end(); BB != E; ++BB) {
105         if (CheckUnwind && isa<ResumeInst>(BB->getTerminator())) {
106           // Uses unwind / resume!
107           SCCMightUnwind = true;
108         } else if (CheckReturn && isa<ReturnInst>(BB->getTerminator())) {
109           SCCMightReturn = true;
110         }
112         // Invoke instructions don't allow unwinding to continue, so we are
113         // only interested in call instructions.
114         if (CheckUnwind && !SCCMightUnwind)
115           for (BasicBlock::iterator I = BB->begin(), E = BB->end(); I != E; ++I)
116             if (CallInst *CI = dyn_cast<CallInst>(I)) {
117               if (CI->doesNotThrow()) {
118                 // This call cannot throw.
119               } else if (Function *Callee = CI->getCalledFunction()) {
120                 CallGraphNode *CalleeNode = CG[Callee];
121                 // If the callee is outside our current SCC then we may
122                 // throw because it might.
123                 if (!SCCNodes.count(CalleeNode)) {
124                   SCCMightUnwind = true;
125                   break;
126                 }
127               } else {
128                 // Indirect call, it might throw.
129                 SCCMightUnwind = true;
130                 break;
131               }
132             }
133         if (SCCMightUnwind && SCCMightReturn) break;
134       }
135     }
136   }
138   // If the SCC doesn't unwind or doesn't throw, note this fact.
139   if (!SCCMightUnwind || !SCCMightReturn)
140     for (CallGraphSCC::iterator I = SCC.begin(), E = SCC.end(); I != E; ++I) {
141       AttrBuilder NewAttributes;
143       if (!SCCMightUnwind)
144         NewAttributes.addAttribute(Attribute::NoUnwind);
145       if (!SCCMightReturn)
146         NewAttributes.addAttribute(Attribute::NoReturn);
148       Function *F = (*I)->getFunction();
149       const AttributeSet &PAL = F->getAttributes().getFnAttributes();
150       const AttributeSet &NPAL = AttributeSet::get(
151           F->getContext(), AttributeSet::FunctionIndex, NewAttributes);
153       if (PAL != NPAL) {
154         MadeChange = true;
155         F->addAttributes(AttributeSet::FunctionIndex, NPAL);
156       }
157     }
159   for (CallGraphSCC::iterator I = SCC.begin(), E = SCC.end(); I != E; ++I) {
160     // Convert any invoke instructions to non-throwing functions in this node
161     // into call instructions with a branch.  This makes the exception blocks
162     // dead.
163     if (Function *F = (*I)->getFunction())
164       MadeChange |= SimplifyFunction(F);
165   }
167   return MadeChange;
171 // SimplifyFunction - Given information about callees, simplify the specified
172 // function if we have invokes to non-unwinding functions or code after calls to
173 // no-return functions.
174 bool PruneEH::SimplifyFunction(Function *F) {
175   bool MadeChange = false;
176   for (Function::iterator BB = F->begin(), E = F->end(); BB != E; ++BB) {
177     if (InvokeInst *II = dyn_cast<InvokeInst>(BB->getTerminator()))
178       if (II->doesNotThrow()) {
179         SmallVector<Value*, 8> Args(II->op_begin(), II->op_end() - 3);
180         // Insert a call instruction before the invoke.
181         CallInst *Call = CallInst::Create(II->getCalledValue(), Args, "", II);
182         Call->takeName(II);
183         Call->setCallingConv(II->getCallingConv());
184         Call->setAttributes(II->getAttributes());
185         Call->setDebugLoc(II->getDebugLoc());
187         // Anything that used the value produced by the invoke instruction
188         // now uses the value produced by the call instruction.  Note that we
189         // do this even for void functions and calls with no uses so that the
190         // callgraph edge is updated.
191         II->replaceAllUsesWith(Call);
192         BasicBlock *UnwindBlock = II->getUnwindDest();
193         UnwindBlock->removePredecessor(II->getParent());
195         // Insert a branch to the normal destination right before the
196         // invoke.
197         BranchInst::Create(II->getNormalDest(), II);
199         // Finally, delete the invoke instruction!
200         BB->getInstList().pop_back();
202         // If the unwind block is now dead, nuke it.
203         if (pred_empty(UnwindBlock))
204           DeleteBasicBlock(UnwindBlock);  // Delete the new BB.
206         ++NumRemoved;
207         MadeChange = true;
208       }
210     for (BasicBlock::iterator I = BB->begin(), E = BB->end(); I != E; )
211       if (CallInst *CI = dyn_cast<CallInst>(I++))
212         if (CI->doesNotReturn() && !isa<UnreachableInst>(I)) {
213           // This call calls a function that cannot return.  Insert an
214           // unreachable instruction after it and simplify the code.  Do this
215           // by splitting the BB, adding the unreachable, then deleting the
216           // new BB.
217           BasicBlock *New = BB->splitBasicBlock(I);
219           // Remove the uncond branch and add an unreachable.
220           BB->getInstList().pop_back();
221           new UnreachableInst(BB->getContext(), BB);
223           DeleteBasicBlock(New);  // Delete the new BB.
224           MadeChange = true;
225           ++NumUnreach;
226           break;
227         }
228   }
230   return MadeChange;
233 /// DeleteBasicBlock - remove the specified basic block from the program,
234 /// updating the callgraph to reflect any now-obsolete edges due to calls that
235 /// exist in the BB.
236 void PruneEH::DeleteBasicBlock(BasicBlock *BB) {
237   assert(pred_empty(BB) && "BB is not dead!");
238   CallGraph &CG = getAnalysis<CallGraphWrapperPass>().getCallGraph();
240   CallGraphNode *CGN = CG[BB->getParent()];
241   for (BasicBlock::iterator I = BB->end(), E = BB->begin(); I != E; ) {
242     --I;
243     if (CallInst *CI = dyn_cast<CallInst>(I)) {
244       if (!isa<IntrinsicInst>(I))
245         CGN->removeCallEdgeFor(CI);
246     } else if (InvokeInst *II = dyn_cast<InvokeInst>(I))
247       CGN->removeCallEdgeFor(II);
248     if (!I->use_empty())
249       I->replaceAllUsesWith(UndefValue::get(I->getType()));
250   }
252   // Get the list of successors of this block.
253   std::vector<BasicBlock*> Succs(succ_begin(BB), succ_end(BB));
255   for (unsigned i = 0, e = Succs.size(); i != e; ++i)
256     Succs[i]->removePredecessor(BB);
258   BB->eraseFromParent();