]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/Transforms/Instrumentation/AddressSanitizer.cpp
[asan] Fix compiler warnings.
[opencl/llvm.git] / lib / Transforms / Instrumentation / AddressSanitizer.cpp
1 //===-- AddressSanitizer.cpp - memory error detector ------------*- C++ -*-===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file is a part of AddressSanitizer, an address sanity checker.
11 // Details of the algorithm:
12 //  http://code.google.com/p/address-sanitizer/wiki/AddressSanitizerAlgorithm
13 //
14 //===----------------------------------------------------------------------===//
16 #include "llvm/Transforms/Instrumentation.h"
17 #include "llvm/ADT/ArrayRef.h"
18 #include "llvm/ADT/DenseMap.h"
19 #include "llvm/ADT/DepthFirstIterator.h"
20 #include "llvm/ADT/SmallSet.h"
21 #include "llvm/ADT/SmallString.h"
22 #include "llvm/ADT/SmallVector.h"
23 #include "llvm/ADT/Statistic.h"
24 #include "llvm/ADT/StringExtras.h"
25 #include "llvm/ADT/Triple.h"
26 #include "llvm/IR/CallSite.h"
27 #include "llvm/IR/DIBuilder.h"
28 #include "llvm/IR/DataLayout.h"
29 #include "llvm/IR/Function.h"
30 #include "llvm/IR/IRBuilder.h"
31 #include "llvm/IR/InlineAsm.h"
32 #include "llvm/IR/InstVisitor.h"
33 #include "llvm/IR/IntrinsicInst.h"
34 #include "llvm/IR/LLVMContext.h"
35 #include "llvm/IR/MDBuilder.h"
36 #include "llvm/IR/Module.h"
37 #include "llvm/IR/Type.h"
38 #include "llvm/Support/CommandLine.h"
39 #include "llvm/Support/DataTypes.h"
40 #include "llvm/Support/Debug.h"
41 #include "llvm/Support/Endian.h"
42 #include "llvm/Support/system_error.h"
43 #include "llvm/Transforms/Utils/ASanStackFrameLayout.h"
44 #include "llvm/Transforms/Utils/BasicBlockUtils.h"
45 #include "llvm/Transforms/Utils/Cloning.h"
46 #include "llvm/Transforms/Utils/Local.h"
47 #include "llvm/Transforms/Utils/ModuleUtils.h"
48 #include "llvm/Transforms/Utils/SpecialCaseList.h"
49 #include <algorithm>
50 #include <string>
52 using namespace llvm;
54 #define DEBUG_TYPE "asan"
56 static const uint64_t kDefaultShadowScale = 3;
57 static const uint64_t kDefaultShadowOffset32 = 1ULL << 29;
58 static const uint64_t kIOSShadowOffset32 = 1ULL << 30;
59 static const uint64_t kDefaultShadowOffset64 = 1ULL << 44;
60 static const uint64_t kSmallX86_64ShadowOffset = 0x7FFF8000;  // < 2G.
61 static const uint64_t kPPC64_ShadowOffset64 = 1ULL << 41;
62 static const uint64_t kMIPS32_ShadowOffset32 = 0x0aaa8000;
63 static const uint64_t kFreeBSD_ShadowOffset32 = 1ULL << 30;
64 static const uint64_t kFreeBSD_ShadowOffset64 = 1ULL << 46;
66 static const size_t kMinStackMallocSize = 1 << 6;  // 64B
67 static const size_t kMaxStackMallocSize = 1 << 16;  // 64K
68 static const uintptr_t kCurrentStackFrameMagic = 0x41B58AB3;
69 static const uintptr_t kRetiredStackFrameMagic = 0x45E0360E;
71 static const char *const kAsanModuleCtorName = "asan.module_ctor";
72 static const char *const kAsanModuleDtorName = "asan.module_dtor";
73 static const int         kAsanCtorAndCtorPriority = 1;
74 static const char *const kAsanReportErrorTemplate = "__asan_report_";
75 static const char *const kAsanReportLoadN = "__asan_report_load_n";
76 static const char *const kAsanReportStoreN = "__asan_report_store_n";
77 static const char *const kAsanRegisterGlobalsName = "__asan_register_globals";
78 static const char *const kAsanUnregisterGlobalsName =
79     "__asan_unregister_globals";
80 static const char *const kAsanPoisonGlobalsName = "__asan_before_dynamic_init";
81 static const char *const kAsanUnpoisonGlobalsName = "__asan_after_dynamic_init";
82 static const char *const kAsanInitName = "__asan_init_v3";
83 static const char *const kAsanCovName = "__sanitizer_cov";
84 static const char *const kAsanPtrCmp = "__sanitizer_ptr_cmp";
85 static const char *const kAsanPtrSub = "__sanitizer_ptr_sub";
86 static const char *const kAsanHandleNoReturnName = "__asan_handle_no_return";
87 static const int         kMaxAsanStackMallocSizeClass = 10;
88 static const char *const kAsanStackMallocNameTemplate = "__asan_stack_malloc_";
89 static const char *const kAsanStackFreeNameTemplate = "__asan_stack_free_";
90 static const char *const kAsanGenPrefix = "__asan_gen_";
91 static const char *const kAsanPoisonStackMemoryName =
92     "__asan_poison_stack_memory";
93 static const char *const kAsanUnpoisonStackMemoryName =
94     "__asan_unpoison_stack_memory";
96 static const char *const kAsanOptionDetectUAR =
97     "__asan_option_detect_stack_use_after_return";
99 #ifndef NDEBUG
100 static const int kAsanStackAfterReturnMagic = 0xf5;
101 #endif
103 // Accesses sizes are powers of two: 1, 2, 4, 8, 16.
104 static const size_t kNumberOfAccessSizes = 5;
106 // Command-line flags.
108 // This flag may need to be replaced with -f[no-]asan-reads.
109 static cl::opt<bool> ClInstrumentReads("asan-instrument-reads",
110        cl::desc("instrument read instructions"), cl::Hidden, cl::init(true));
111 static cl::opt<bool> ClInstrumentWrites("asan-instrument-writes",
112        cl::desc("instrument write instructions"), cl::Hidden, cl::init(true));
113 static cl::opt<bool> ClInstrumentAtomics("asan-instrument-atomics",
114        cl::desc("instrument atomic instructions (rmw, cmpxchg)"),
115        cl::Hidden, cl::init(true));
116 static cl::opt<bool> ClAlwaysSlowPath("asan-always-slow-path",
117        cl::desc("use instrumentation with slow path for all accesses"),
118        cl::Hidden, cl::init(false));
119 // This flag limits the number of instructions to be instrumented
120 // in any given BB. Normally, this should be set to unlimited (INT_MAX),
121 // but due to http://llvm.org/bugs/show_bug.cgi?id=12652 we temporary
122 // set it to 10000.
123 static cl::opt<int> ClMaxInsnsToInstrumentPerBB("asan-max-ins-per-bb",
124        cl::init(10000),
125        cl::desc("maximal number of instructions to instrument in any given BB"),
126        cl::Hidden);
127 // This flag may need to be replaced with -f[no]asan-stack.
128 static cl::opt<bool> ClStack("asan-stack",
129        cl::desc("Handle stack memory"), cl::Hidden, cl::init(true));
130 // This flag may need to be replaced with -f[no]asan-use-after-return.
131 static cl::opt<bool> ClUseAfterReturn("asan-use-after-return",
132        cl::desc("Check return-after-free"), cl::Hidden, cl::init(false));
133 // This flag may need to be replaced with -f[no]asan-globals.
134 static cl::opt<bool> ClGlobals("asan-globals",
135        cl::desc("Handle global objects"), cl::Hidden, cl::init(true));
136 static cl::opt<int> ClCoverage("asan-coverage",
137        cl::desc("ASan coverage. 0: none, 1: entry block, 2: all blocks"),
138        cl::Hidden, cl::init(false));
139 static cl::opt<int> ClCoverageBlockThreshold("asan-coverage-block-threshold",
140        cl::desc("Add coverage instrumentation only to the entry block if there "
141                 "are more than this number of blocks."),
142        cl::Hidden, cl::init(1500));
143 static cl::opt<bool> ClInitializers("asan-initialization-order",
144        cl::desc("Handle C++ initializer order"), cl::Hidden, cl::init(false));
145 static cl::opt<bool> ClInvalidPointerPairs("asan-detect-invalid-pointer-pair",
146        cl::desc("Instrument <, <=, >, >=, - with pointer operands"),
147        cl::Hidden, cl::init(false));
148 static cl::opt<unsigned> ClRealignStack("asan-realign-stack",
149        cl::desc("Realign stack to the value of this flag (power of two)"),
150        cl::Hidden, cl::init(32));
151 static cl::opt<std::string> ClBlacklistFile("asan-blacklist",
152        cl::desc("File containing the list of objects to ignore "
153                 "during instrumentation"), cl::Hidden);
154 static cl::opt<int> ClInstrumentationWithCallsThreshold(
155     "asan-instrumentation-with-call-threshold",
156        cl::desc("If the function being instrumented contains more than "
157                 "this number of memory accesses, use callbacks instead of "
158                 "inline checks (-1 means never use callbacks)."),
159        cl::Hidden, cl::init(10000));
160 static cl::opt<std::string> ClMemoryAccessCallbackPrefix(
161        "asan-memory-access-callback-prefix",
162        cl::desc("Prefix for memory access callbacks"), cl::Hidden,
163        cl::init("__asan_"));
165 // This is an experimental feature that will allow to choose between
166 // instrumented and non-instrumented code at link-time.
167 // If this option is on, just before instrumenting a function we create its
168 // clone; if the function is not changed by asan the clone is deleted.
169 // If we end up with a clone, we put the instrumented function into a section
170 // called "ASAN" and the uninstrumented function into a section called "NOASAN".
171 //
172 // This is still a prototype, we need to figure out a way to keep two copies of
173 // a function so that the linker can easily choose one of them.
174 static cl::opt<bool> ClKeepUninstrumented("asan-keep-uninstrumented-functions",
175        cl::desc("Keep uninstrumented copies of functions"),
176        cl::Hidden, cl::init(false));
178 // These flags allow to change the shadow mapping.
179 // The shadow mapping looks like
180 //    Shadow = (Mem >> scale) + (1 << offset_log)
181 static cl::opt<int> ClMappingScale("asan-mapping-scale",
182        cl::desc("scale of asan shadow mapping"), cl::Hidden, cl::init(0));
184 // Optimization flags. Not user visible, used mostly for testing
185 // and benchmarking the tool.
186 static cl::opt<bool> ClOpt("asan-opt",
187        cl::desc("Optimize instrumentation"), cl::Hidden, cl::init(true));
188 static cl::opt<bool> ClOptSameTemp("asan-opt-same-temp",
189        cl::desc("Instrument the same temp just once"), cl::Hidden,
190        cl::init(true));
191 static cl::opt<bool> ClOptGlobals("asan-opt-globals",
192        cl::desc("Don't instrument scalar globals"), cl::Hidden, cl::init(true));
194 static cl::opt<bool> ClCheckLifetime("asan-check-lifetime",
195        cl::desc("Use llvm.lifetime intrinsics to insert extra checks"),
196        cl::Hidden, cl::init(false));
198 // Debug flags.
199 static cl::opt<int> ClDebug("asan-debug", cl::desc("debug"), cl::Hidden,
200                             cl::init(0));
201 static cl::opt<int> ClDebugStack("asan-debug-stack", cl::desc("debug stack"),
202                                  cl::Hidden, cl::init(0));
203 static cl::opt<std::string> ClDebugFunc("asan-debug-func",
204                                         cl::Hidden, cl::desc("Debug func"));
205 static cl::opt<int> ClDebugMin("asan-debug-min", cl::desc("Debug min inst"),
206                                cl::Hidden, cl::init(-1));
207 static cl::opt<int> ClDebugMax("asan-debug-max", cl::desc("Debug man inst"),
208                                cl::Hidden, cl::init(-1));
210 STATISTIC(NumInstrumentedReads, "Number of instrumented reads");
211 STATISTIC(NumInstrumentedWrites, "Number of instrumented writes");
212 STATISTIC(NumOptimizedAccessesToGlobalArray,
213           "Number of optimized accesses to global arrays");
214 STATISTIC(NumOptimizedAccessesToGlobalVar,
215           "Number of optimized accesses to global vars");
217 namespace {
218 /// A set of dynamically initialized globals extracted from metadata.
219 class SetOfDynamicallyInitializedGlobals {
220  public:
221   void Init(Module& M) {
222     // Clang generates metadata identifying all dynamically initialized globals.
223     NamedMDNode *DynamicGlobals =
224         M.getNamedMetadata("llvm.asan.dynamically_initialized_globals");
225     if (!DynamicGlobals)
226       return;
227     for (int i = 0, n = DynamicGlobals->getNumOperands(); i < n; ++i) {
228       MDNode *MDN = DynamicGlobals->getOperand(i);
229       assert(MDN->getNumOperands() == 1);
230       Value *VG = MDN->getOperand(0);
231       // The optimizer may optimize away a global entirely, in which case we
232       // cannot instrument access to it.
233       if (!VG)
234         continue;
235       DynInitGlobals.insert(cast<GlobalVariable>(VG));
236     }
237   }
238   bool Contains(GlobalVariable *G) { return DynInitGlobals.count(G) != 0; }
239  private:
240   SmallSet<GlobalValue*, 32> DynInitGlobals;
241 };
243 /// This struct defines the shadow mapping using the rule:
244 ///   shadow = (mem >> Scale) ADD-or-OR Offset.
245 struct ShadowMapping {
246   int Scale;
247   uint64_t Offset;
248   bool OrShadowOffset;
249 };
251 static ShadowMapping getShadowMapping(const Module &M, int LongSize) {
252   llvm::Triple TargetTriple(M.getTargetTriple());
253   bool IsAndroid = TargetTriple.getEnvironment() == llvm::Triple::Android;
254   bool IsIOS = TargetTriple.getOS() == llvm::Triple::IOS;
255   bool IsFreeBSD = TargetTriple.getOS() == llvm::Triple::FreeBSD;
256   bool IsLinux = TargetTriple.getOS() == llvm::Triple::Linux;
257   bool IsPPC64 = TargetTriple.getArch() == llvm::Triple::ppc64 ||
258                  TargetTriple.getArch() == llvm::Triple::ppc64le;
259   bool IsX86_64 = TargetTriple.getArch() == llvm::Triple::x86_64;
260   bool IsMIPS32 = TargetTriple.getArch() == llvm::Triple::mips ||
261                   TargetTriple.getArch() == llvm::Triple::mipsel;
263   ShadowMapping Mapping;
265   if (LongSize == 32) {
266     if (IsAndroid)
267       Mapping.Offset = 0;
268     else if (IsMIPS32)
269       Mapping.Offset = kMIPS32_ShadowOffset32;
270     else if (IsFreeBSD)
271       Mapping.Offset = kFreeBSD_ShadowOffset32;
272     else if (IsIOS)
273       Mapping.Offset = kIOSShadowOffset32;
274     else
275       Mapping.Offset = kDefaultShadowOffset32;
276   } else {  // LongSize == 64
277     if (IsPPC64)
278       Mapping.Offset = kPPC64_ShadowOffset64;
279     else if (IsFreeBSD)
280       Mapping.Offset = kFreeBSD_ShadowOffset64;
281     else if (IsLinux && IsX86_64)
282       Mapping.Offset = kSmallX86_64ShadowOffset;
283     else
284       Mapping.Offset = kDefaultShadowOffset64;
285   }
287   Mapping.Scale = kDefaultShadowScale;
288   if (ClMappingScale) {
289     Mapping.Scale = ClMappingScale;
290   }
292   // OR-ing shadow offset if more efficient (at least on x86) if the offset
293   // is a power of two, but on ppc64 we have to use add since the shadow
294   // offset is not necessary 1/8-th of the address space.
295   Mapping.OrShadowOffset = !IsPPC64 && !(Mapping.Offset & (Mapping.Offset - 1));
297   return Mapping;
300 static size_t RedzoneSizeForScale(int MappingScale) {
301   // Redzone used for stack and globals is at least 32 bytes.
302   // For scales 6 and 7, the redzone has to be 64 and 128 bytes respectively.
303   return std::max(32U, 1U << MappingScale);
306 /// AddressSanitizer: instrument the code in module to find memory bugs.
307 struct AddressSanitizer : public FunctionPass {
308   AddressSanitizer(bool CheckInitOrder = true,
309                    bool CheckUseAfterReturn = false,
310                    bool CheckLifetime = false,
311                    StringRef BlacklistFile = StringRef())
312       : FunctionPass(ID),
313         CheckInitOrder(CheckInitOrder || ClInitializers),
314         CheckUseAfterReturn(CheckUseAfterReturn || ClUseAfterReturn),
315         CheckLifetime(CheckLifetime || ClCheckLifetime),
316         BlacklistFile(BlacklistFile.empty() ? ClBlacklistFile
317                                             : BlacklistFile) {}
318   const char *getPassName() const override {
319     return "AddressSanitizerFunctionPass";
320   }
321   void instrumentMop(Instruction *I, bool UseCalls);
322   void instrumentPointerComparisonOrSubtraction(Instruction *I);
323   void instrumentAddress(Instruction *OrigIns, Instruction *InsertBefore,
324                          Value *Addr, uint32_t TypeSize, bool IsWrite,
325                          Value *SizeArgument, bool UseCalls);
326   Value *createSlowPathCmp(IRBuilder<> &IRB, Value *AddrLong,
327                            Value *ShadowValue, uint32_t TypeSize);
328   Instruction *generateCrashCode(Instruction *InsertBefore, Value *Addr,
329                                  bool IsWrite, size_t AccessSizeIndex,
330                                  Value *SizeArgument);
331   void instrumentMemIntrinsic(MemIntrinsic *MI);
332   Value *memToShadow(Value *Shadow, IRBuilder<> &IRB);
333   bool runOnFunction(Function &F) override;
334   bool maybeInsertAsanInitAtFunctionEntry(Function &F);
335   bool doInitialization(Module &M) override;
336   static char ID;  // Pass identification, replacement for typeid
338  private:
339   void initializeCallbacks(Module &M);
341   bool LooksLikeCodeInBug11395(Instruction *I);
342   bool GlobalIsLinkerInitialized(GlobalVariable *G);
343   bool InjectCoverage(Function &F, const ArrayRef<BasicBlock*> AllBlocks);
344   void InjectCoverageAtBlock(Function &F, BasicBlock &BB);
346   bool CheckInitOrder;
347   bool CheckUseAfterReturn;
348   bool CheckLifetime;
349   SmallString<64> BlacklistFile;
351   LLVMContext *C;
352   const DataLayout *DL;
353   int LongSize;
354   Type *IntptrTy;
355   ShadowMapping Mapping;
356   Function *AsanCtorFunction;
357   Function *AsanInitFunction;
358   Function *AsanHandleNoReturnFunc;
359   Function *AsanCovFunction;
360   Function *AsanPtrCmpFunction, *AsanPtrSubFunction;
361   std::unique_ptr<SpecialCaseList> BL;
362   // This array is indexed by AccessIsWrite and log2(AccessSize).
363   Function *AsanErrorCallback[2][kNumberOfAccessSizes];
364   Function *AsanMemoryAccessCallback[2][kNumberOfAccessSizes];
365   // This array is indexed by AccessIsWrite.
366   Function *AsanErrorCallbackSized[2],
367            *AsanMemoryAccessCallbackSized[2];
368   Function *AsanMemmove, *AsanMemcpy, *AsanMemset;
369   InlineAsm *EmptyAsm;
370   SetOfDynamicallyInitializedGlobals DynamicallyInitializedGlobals;
372   friend struct FunctionStackPoisoner;
373 };
375 class AddressSanitizerModule : public ModulePass {
376  public:
377   AddressSanitizerModule(bool CheckInitOrder = true,
378                          StringRef BlacklistFile = StringRef())
379       : ModulePass(ID),
380         CheckInitOrder(CheckInitOrder || ClInitializers),
381         BlacklistFile(BlacklistFile.empty() ? ClBlacklistFile
382                                             : BlacklistFile) {}
383   bool runOnModule(Module &M) override;
384   static char ID;  // Pass identification, replacement for typeid
385   const char *getPassName() const override {
386     return "AddressSanitizerModule";
387   }
389  private:
390   void initializeCallbacks(Module &M);
392   bool ShouldInstrumentGlobal(GlobalVariable *G);
393   void createInitializerPoisonCalls(Module &M, GlobalValue *ModuleName);
394   size_t MinRedzoneSizeForGlobal() const {
395     return RedzoneSizeForScale(Mapping.Scale);
396   }
398   bool CheckInitOrder;
399   SmallString<64> BlacklistFile;
401   std::unique_ptr<SpecialCaseList> BL;
402   SetOfDynamicallyInitializedGlobals DynamicallyInitializedGlobals;
403   Type *IntptrTy;
404   LLVMContext *C;
405   const DataLayout *DL;
406   ShadowMapping Mapping;
407   Function *AsanPoisonGlobals;
408   Function *AsanUnpoisonGlobals;
409   Function *AsanRegisterGlobals;
410   Function *AsanUnregisterGlobals;
411 };
413 // Stack poisoning does not play well with exception handling.
414 // When an exception is thrown, we essentially bypass the code
415 // that unpoisones the stack. This is why the run-time library has
416 // to intercept __cxa_throw (as well as longjmp, etc) and unpoison the entire
417 // stack in the interceptor. This however does not work inside the
418 // actual function which catches the exception. Most likely because the
419 // compiler hoists the load of the shadow value somewhere too high.
420 // This causes asan to report a non-existing bug on 453.povray.
421 // It sounds like an LLVM bug.
422 struct FunctionStackPoisoner : public InstVisitor<FunctionStackPoisoner> {
423   Function &F;
424   AddressSanitizer &ASan;
425   DIBuilder DIB;
426   LLVMContext *C;
427   Type *IntptrTy;
428   Type *IntptrPtrTy;
429   ShadowMapping Mapping;
431   SmallVector<AllocaInst*, 16> AllocaVec;
432   SmallVector<Instruction*, 8> RetVec;
433   unsigned StackAlignment;
435   Function *AsanStackMallocFunc[kMaxAsanStackMallocSizeClass + 1],
436            *AsanStackFreeFunc[kMaxAsanStackMallocSizeClass + 1];
437   Function *AsanPoisonStackMemoryFunc, *AsanUnpoisonStackMemoryFunc;
439   // Stores a place and arguments of poisoning/unpoisoning call for alloca.
440   struct AllocaPoisonCall {
441     IntrinsicInst *InsBefore;
442     AllocaInst *AI;
443     uint64_t Size;
444     bool DoPoison;
445   };
446   SmallVector<AllocaPoisonCall, 8> AllocaPoisonCallVec;
448   // Maps Value to an AllocaInst from which the Value is originated.
449   typedef DenseMap<Value*, AllocaInst*> AllocaForValueMapTy;
450   AllocaForValueMapTy AllocaForValue;
452   FunctionStackPoisoner(Function &F, AddressSanitizer &ASan)
453       : F(F), ASan(ASan), DIB(*F.getParent()), C(ASan.C),
454         IntptrTy(ASan.IntptrTy), IntptrPtrTy(PointerType::get(IntptrTy, 0)),
455         Mapping(ASan.Mapping),
456         StackAlignment(1 << Mapping.Scale) {}
458   bool runOnFunction() {
459     if (!ClStack) return false;
460     // Collect alloca, ret, lifetime instructions etc.
461     for (BasicBlock *BB : depth_first(&F.getEntryBlock()))
462       visit(*BB);
464     if (AllocaVec.empty()) return false;
466     initializeCallbacks(*F.getParent());
468     poisonStack();
470     if (ClDebugStack) {
471       DEBUG(dbgs() << F);
472     }
473     return true;
474   }
476   // Finds all static Alloca instructions and puts
477   // poisoned red zones around all of them.
478   // Then unpoison everything back before the function returns.
479   void poisonStack();
481   // ----------------------- Visitors.
482   /// \brief Collect all Ret instructions.
483   void visitReturnInst(ReturnInst &RI) {
484     RetVec.push_back(&RI);
485   }
487   /// \brief Collect Alloca instructions we want (and can) handle.
488   void visitAllocaInst(AllocaInst &AI) {
489     if (!isInterestingAlloca(AI)) return;
491     StackAlignment = std::max(StackAlignment, AI.getAlignment());
492     AllocaVec.push_back(&AI);
493   }
495   /// \brief Collect lifetime intrinsic calls to check for use-after-scope
496   /// errors.
497   void visitIntrinsicInst(IntrinsicInst &II) {
498     if (!ASan.CheckLifetime) return;
499     Intrinsic::ID ID = II.getIntrinsicID();
500     if (ID != Intrinsic::lifetime_start &&
501         ID != Intrinsic::lifetime_end)
502       return;
503     // Found lifetime intrinsic, add ASan instrumentation if necessary.
504     ConstantInt *Size = dyn_cast<ConstantInt>(II.getArgOperand(0));
505     // If size argument is undefined, don't do anything.
506     if (Size->isMinusOne()) return;
507     // Check that size doesn't saturate uint64_t and can
508     // be stored in IntptrTy.
509     const uint64_t SizeValue = Size->getValue().getLimitedValue();
510     if (SizeValue == ~0ULL ||
511         !ConstantInt::isValueValidForType(IntptrTy, SizeValue))
512       return;
513     // Find alloca instruction that corresponds to llvm.lifetime argument.
514     AllocaInst *AI = findAllocaForValue(II.getArgOperand(1));
515     if (!AI) return;
516     bool DoPoison = (ID == Intrinsic::lifetime_end);
517     AllocaPoisonCall APC = {&II, AI, SizeValue, DoPoison};
518     AllocaPoisonCallVec.push_back(APC);
519   }
521   // ---------------------- Helpers.
522   void initializeCallbacks(Module &M);
524   // Check if we want (and can) handle this alloca.
525   bool isInterestingAlloca(AllocaInst &AI) const {
526     return (!AI.isArrayAllocation() && AI.isStaticAlloca() &&
527             AI.getAllocatedType()->isSized() &&
528             // alloca() may be called with 0 size, ignore it.
529             getAllocaSizeInBytes(&AI) > 0);
530   }
532   uint64_t getAllocaSizeInBytes(AllocaInst *AI) const {
533     Type *Ty = AI->getAllocatedType();
534     uint64_t SizeInBytes = ASan.DL->getTypeAllocSize(Ty);
535     return SizeInBytes;
536   }
537   /// Finds alloca where the value comes from.
538   AllocaInst *findAllocaForValue(Value *V);
539   void poisonRedZones(const ArrayRef<uint8_t> ShadowBytes, IRBuilder<> &IRB,
540                       Value *ShadowBase, bool DoPoison);
541   void poisonAlloca(Value *V, uint64_t Size, IRBuilder<> &IRB, bool DoPoison);
543   void SetShadowToStackAfterReturnInlined(IRBuilder<> &IRB, Value *ShadowBase,
544                                           int Size);
545 };
547 }  // namespace
549 char AddressSanitizer::ID = 0;
550 INITIALIZE_PASS(AddressSanitizer, "asan",
551     "AddressSanitizer: detects use-after-free and out-of-bounds bugs.",
552     false, false)
553 FunctionPass *llvm::createAddressSanitizerFunctionPass(
554     bool CheckInitOrder, bool CheckUseAfterReturn, bool CheckLifetime,
555     StringRef BlacklistFile) {
556   return new AddressSanitizer(CheckInitOrder, CheckUseAfterReturn,
557                               CheckLifetime, BlacklistFile);
560 char AddressSanitizerModule::ID = 0;
561 INITIALIZE_PASS(AddressSanitizerModule, "asan-module",
562     "AddressSanitizer: detects use-after-free and out-of-bounds bugs."
563     "ModulePass", false, false)
564 ModulePass *llvm::createAddressSanitizerModulePass(
565     bool CheckInitOrder, StringRef BlacklistFile) {
566   return new AddressSanitizerModule(CheckInitOrder, BlacklistFile);
569 static size_t TypeSizeToSizeIndex(uint32_t TypeSize) {
570   size_t Res = countTrailingZeros(TypeSize / 8);
571   assert(Res < kNumberOfAccessSizes);
572   return Res;
575 // \brief Create a constant for Str so that we can pass it to the run-time lib.
576 static GlobalVariable *createPrivateGlobalForString(
577     Module &M, StringRef Str, bool AllowMerging) {
578   Constant *StrConst = ConstantDataArray::getString(M.getContext(), Str);
579   // We use private linkage for module-local strings. If they can be merged
580   // with another one, we set the unnamed_addr attribute.
581   GlobalVariable *GV =
582       new GlobalVariable(M, StrConst->getType(), true,
583                          GlobalValue::PrivateLinkage, StrConst, kAsanGenPrefix);
584   if (AllowMerging)
585     GV->setUnnamedAddr(true);
586   GV->setAlignment(1);  // Strings may not be merged w/o setting align 1.
587   return GV;
590 static bool GlobalWasGeneratedByAsan(GlobalVariable *G) {
591   return G->getName().find(kAsanGenPrefix) == 0;
594 Value *AddressSanitizer::memToShadow(Value *Shadow, IRBuilder<> &IRB) {
595   // Shadow >> scale
596   Shadow = IRB.CreateLShr(Shadow, Mapping.Scale);
597   if (Mapping.Offset == 0)
598     return Shadow;
599   // (Shadow >> scale) | offset
600   if (Mapping.OrShadowOffset)
601     return IRB.CreateOr(Shadow, ConstantInt::get(IntptrTy, Mapping.Offset));
602   else
603     return IRB.CreateAdd(Shadow, ConstantInt::get(IntptrTy, Mapping.Offset));
606 // Instrument memset/memmove/memcpy
607 void AddressSanitizer::instrumentMemIntrinsic(MemIntrinsic *MI) {
608   IRBuilder<> IRB(MI);
609   if (isa<MemTransferInst>(MI)) {
610     IRB.CreateCall3(
611         isa<MemMoveInst>(MI) ? AsanMemmove : AsanMemcpy,
612         IRB.CreatePointerCast(MI->getOperand(0), IRB.getInt8PtrTy()),
613         IRB.CreatePointerCast(MI->getOperand(1), IRB.getInt8PtrTy()),
614         IRB.CreateIntCast(MI->getOperand(2), IntptrTy, false));
615   } else if (isa<MemSetInst>(MI)) {
616     IRB.CreateCall3(
617         AsanMemset,
618         IRB.CreatePointerCast(MI->getOperand(0), IRB.getInt8PtrTy()),
619         IRB.CreateIntCast(MI->getOperand(1), IRB.getInt32Ty(), false),
620         IRB.CreateIntCast(MI->getOperand(2), IntptrTy, false));
621   }
622   MI->eraseFromParent();
625 // If I is an interesting memory access, return the PointerOperand
626 // and set IsWrite. Otherwise return NULL.
627 static Value *isInterestingMemoryAccess(Instruction *I, bool *IsWrite) {
628   if (LoadInst *LI = dyn_cast<LoadInst>(I)) {
629     if (!ClInstrumentReads) return nullptr;
630     *IsWrite = false;
631     return LI->getPointerOperand();
632   }
633   if (StoreInst *SI = dyn_cast<StoreInst>(I)) {
634     if (!ClInstrumentWrites) return nullptr;
635     *IsWrite = true;
636     return SI->getPointerOperand();
637   }
638   if (AtomicRMWInst *RMW = dyn_cast<AtomicRMWInst>(I)) {
639     if (!ClInstrumentAtomics) return nullptr;
640     *IsWrite = true;
641     return RMW->getPointerOperand();
642   }
643   if (AtomicCmpXchgInst *XCHG = dyn_cast<AtomicCmpXchgInst>(I)) {
644     if (!ClInstrumentAtomics) return nullptr;
645     *IsWrite = true;
646     return XCHG->getPointerOperand();
647   }
648   return nullptr;
651 static bool isPointerOperand(Value *V) {
652   return V->getType()->isPointerTy() || isa<PtrToIntInst>(V);
655 // This is a rough heuristic; it may cause both false positives and
656 // false negatives. The proper implementation requires cooperation with
657 // the frontend.
658 static bool isInterestingPointerComparisonOrSubtraction(Instruction *I) {
659   if (ICmpInst *Cmp = dyn_cast<ICmpInst>(I)) {
660     if (!Cmp->isRelational())
661       return false;
662   } else if (BinaryOperator *BO = dyn_cast<BinaryOperator>(I)) {
663     if (BO->getOpcode() != Instruction::Sub)
664       return false;
665   } else {
666     return false;
667   }
668   if (!isPointerOperand(I->getOperand(0)) ||
669       !isPointerOperand(I->getOperand(1)))
670       return false;
671   return true;
674 bool AddressSanitizer::GlobalIsLinkerInitialized(GlobalVariable *G) {
675   // If a global variable does not have dynamic initialization we don't
676   // have to instrument it.  However, if a global does not have initializer
677   // at all, we assume it has dynamic initializer (in other TU).
678   return G->hasInitializer() && !DynamicallyInitializedGlobals.Contains(G);
681 void
682 AddressSanitizer::instrumentPointerComparisonOrSubtraction(Instruction *I) {
683   IRBuilder<> IRB(I);
684   Function *F = isa<ICmpInst>(I) ? AsanPtrCmpFunction : AsanPtrSubFunction;
685   Value *Param[2] = {I->getOperand(0), I->getOperand(1)};
686   for (int i = 0; i < 2; i++) {
687     if (Param[i]->getType()->isPointerTy())
688       Param[i] = IRB.CreatePointerCast(Param[i], IntptrTy);
689   }
690   IRB.CreateCall2(F, Param[0], Param[1]);
693 void AddressSanitizer::instrumentMop(Instruction *I, bool UseCalls) {
694   bool IsWrite = false;
695   Value *Addr = isInterestingMemoryAccess(I, &IsWrite);
696   assert(Addr);
697   if (ClOpt && ClOptGlobals) {
698     if (GlobalVariable *G = dyn_cast<GlobalVariable>(Addr)) {
699       // If initialization order checking is disabled, a simple access to a
700       // dynamically initialized global is always valid.
701       if (!CheckInitOrder || GlobalIsLinkerInitialized(G)) {
702         NumOptimizedAccessesToGlobalVar++;
703         return;
704       }
705     }
706     ConstantExpr *CE = dyn_cast<ConstantExpr>(Addr);
707     if (CE && CE->isGEPWithNoNotionalOverIndexing()) {
708       if (GlobalVariable *G = dyn_cast<GlobalVariable>(CE->getOperand(0))) {
709         if (CE->getOperand(1)->isNullValue() && GlobalIsLinkerInitialized(G)) {
710           NumOptimizedAccessesToGlobalArray++;
711           return;
712         }
713       }
714     }
715   }
717   Type *OrigPtrTy = Addr->getType();
718   Type *OrigTy = cast<PointerType>(OrigPtrTy)->getElementType();
720   assert(OrigTy->isSized());
721   uint32_t TypeSize = DL->getTypeStoreSizeInBits(OrigTy);
723   assert((TypeSize % 8) == 0);
725   if (IsWrite)
726     NumInstrumentedWrites++;
727   else
728     NumInstrumentedReads++;
730   // Instrument a 1-, 2-, 4-, 8-, or 16- byte access with one check.
731   if (TypeSize == 8  || TypeSize == 16 ||
732       TypeSize == 32 || TypeSize == 64 || TypeSize == 128)
733     return instrumentAddress(I, I, Addr, TypeSize, IsWrite, nullptr, UseCalls);
734   // Instrument unusual size (but still multiple of 8).
735   // We can not do it with a single check, so we do 1-byte check for the first
736   // and the last bytes. We call __asan_report_*_n(addr, real_size) to be able
737   // to report the actual access size.
738   IRBuilder<> IRB(I);
739   Value *Size = ConstantInt::get(IntptrTy, TypeSize / 8);
740   Value *AddrLong = IRB.CreatePointerCast(Addr, IntptrTy);
741   if (UseCalls) {
742     IRB.CreateCall2(AsanMemoryAccessCallbackSized[IsWrite], AddrLong, Size);
743   } else {
744     Value *LastByte = IRB.CreateIntToPtr(
745         IRB.CreateAdd(AddrLong, ConstantInt::get(IntptrTy, TypeSize / 8 - 1)),
746         OrigPtrTy);
747     instrumentAddress(I, I, Addr, 8, IsWrite, Size, false);
748     instrumentAddress(I, I, LastByte, 8, IsWrite, Size, false);
749   }
752 // Validate the result of Module::getOrInsertFunction called for an interface
753 // function of AddressSanitizer. If the instrumented module defines a function
754 // with the same name, their prototypes must match, otherwise
755 // getOrInsertFunction returns a bitcast.
756 static Function *checkInterfaceFunction(Constant *FuncOrBitcast) {
757   if (isa<Function>(FuncOrBitcast)) return cast<Function>(FuncOrBitcast);
758   FuncOrBitcast->dump();
759   report_fatal_error("trying to redefine an AddressSanitizer "
760                      "interface function");
763 Instruction *AddressSanitizer::generateCrashCode(
764     Instruction *InsertBefore, Value *Addr,
765     bool IsWrite, size_t AccessSizeIndex, Value *SizeArgument) {
766   IRBuilder<> IRB(InsertBefore);
767   CallInst *Call = SizeArgument
768     ? IRB.CreateCall2(AsanErrorCallbackSized[IsWrite], Addr, SizeArgument)
769     : IRB.CreateCall(AsanErrorCallback[IsWrite][AccessSizeIndex], Addr);
771   // We don't do Call->setDoesNotReturn() because the BB already has
772   // UnreachableInst at the end.
773   // This EmptyAsm is required to avoid callback merge.
774   IRB.CreateCall(EmptyAsm);
775   return Call;
778 Value *AddressSanitizer::createSlowPathCmp(IRBuilder<> &IRB, Value *AddrLong,
779                                             Value *ShadowValue,
780                                             uint32_t TypeSize) {
781   size_t Granularity = 1 << Mapping.Scale;
782   // Addr & (Granularity - 1)
783   Value *LastAccessedByte = IRB.CreateAnd(
784       AddrLong, ConstantInt::get(IntptrTy, Granularity - 1));
785   // (Addr & (Granularity - 1)) + size - 1
786   if (TypeSize / 8 > 1)
787     LastAccessedByte = IRB.CreateAdd(
788         LastAccessedByte, ConstantInt::get(IntptrTy, TypeSize / 8 - 1));
789   // (uint8_t) ((Addr & (Granularity-1)) + size - 1)
790   LastAccessedByte = IRB.CreateIntCast(
791       LastAccessedByte, ShadowValue->getType(), false);
792   // ((uint8_t) ((Addr & (Granularity-1)) + size - 1)) >= ShadowValue
793   return IRB.CreateICmpSGE(LastAccessedByte, ShadowValue);
796 void AddressSanitizer::instrumentAddress(Instruction *OrigIns,
797                                          Instruction *InsertBefore, Value *Addr,
798                                          uint32_t TypeSize, bool IsWrite,
799                                          Value *SizeArgument, bool UseCalls) {
800   IRBuilder<> IRB(InsertBefore);
801   Value *AddrLong = IRB.CreatePointerCast(Addr, IntptrTy);
802   size_t AccessSizeIndex = TypeSizeToSizeIndex(TypeSize);
804   if (UseCalls) {
805     IRB.CreateCall(AsanMemoryAccessCallback[IsWrite][AccessSizeIndex],
806                    AddrLong);
807     return;
808   }
810   Type *ShadowTy  = IntegerType::get(
811       *C, std::max(8U, TypeSize >> Mapping.Scale));
812   Type *ShadowPtrTy = PointerType::get(ShadowTy, 0);
813   Value *ShadowPtr = memToShadow(AddrLong, IRB);
814   Value *CmpVal = Constant::getNullValue(ShadowTy);
815   Value *ShadowValue = IRB.CreateLoad(
816       IRB.CreateIntToPtr(ShadowPtr, ShadowPtrTy));
818   Value *Cmp = IRB.CreateICmpNE(ShadowValue, CmpVal);
819   size_t Granularity = 1 << Mapping.Scale;
820   TerminatorInst *CrashTerm = nullptr;
822   if (ClAlwaysSlowPath || (TypeSize < 8 * Granularity)) {
823     TerminatorInst *CheckTerm =
824         SplitBlockAndInsertIfThen(Cmp, InsertBefore, false);
825     assert(dyn_cast<BranchInst>(CheckTerm)->isUnconditional());
826     BasicBlock *NextBB = CheckTerm->getSuccessor(0);
827     IRB.SetInsertPoint(CheckTerm);
828     Value *Cmp2 = createSlowPathCmp(IRB, AddrLong, ShadowValue, TypeSize);
829     BasicBlock *CrashBlock =
830         BasicBlock::Create(*C, "", NextBB->getParent(), NextBB);
831     CrashTerm = new UnreachableInst(*C, CrashBlock);
832     BranchInst *NewTerm = BranchInst::Create(CrashBlock, NextBB, Cmp2);
833     ReplaceInstWithInst(CheckTerm, NewTerm);
834   } else {
835     CrashTerm = SplitBlockAndInsertIfThen(Cmp, InsertBefore, true);
836   }
838   Instruction *Crash = generateCrashCode(
839       CrashTerm, AddrLong, IsWrite, AccessSizeIndex, SizeArgument);
840   Crash->setDebugLoc(OrigIns->getDebugLoc());
843 void AddressSanitizerModule::createInitializerPoisonCalls(
844     Module &M, GlobalValue *ModuleName) {
845   // We do all of our poisoning and unpoisoning within a global constructor.
846   // These are called _GLOBAL__(sub_)?I_.*.
847   // TODO: Consider looking through the functions in
848   // M.getGlobalVariable("llvm.global_ctors") instead of using this stringly
849   // typed approach.
850   Function *GlobalInit = nullptr;
851   for (auto &F : M.getFunctionList()) {
852     StringRef FName = F.getName();
854     const char kGlobalPrefix[] = "_GLOBAL__";
855     if (!FName.startswith(kGlobalPrefix))
856       continue;
857     FName = FName.substr(strlen(kGlobalPrefix));
859     const char kOptionalSub[] = "sub_";
860     if (FName.startswith(kOptionalSub))
861       FName = FName.substr(strlen(kOptionalSub));
863     if (FName.startswith("I_")) {
864       GlobalInit = &F;
865       break;
866     }
867   }
868   // If that function is not present, this TU contains no globals, or they have
869   // all been optimized away
870   if (!GlobalInit)
871     return;
873   // Set up the arguments to our poison/unpoison functions.
874   IRBuilder<> IRB(GlobalInit->begin()->getFirstInsertionPt());
876   // Add a call to poison all external globals before the given function starts.
877   Value *ModuleNameAddr = ConstantExpr::getPointerCast(ModuleName, IntptrTy);
878   IRB.CreateCall(AsanPoisonGlobals, ModuleNameAddr);
880   // Add calls to unpoison all globals before each return instruction.
881   for (Function::iterator I = GlobalInit->begin(), E = GlobalInit->end();
882        I != E; ++I) {
883     if (ReturnInst *RI = dyn_cast<ReturnInst>(I->getTerminator())) {
884       CallInst::Create(AsanUnpoisonGlobals, "", RI);
885     }
886   }
889 bool AddressSanitizerModule::ShouldInstrumentGlobal(GlobalVariable *G) {
890   Type *Ty = cast<PointerType>(G->getType())->getElementType();
891   DEBUG(dbgs() << "GLOBAL: " << *G << "\n");
893   if (BL->isIn(*G)) return false;
894   if (!Ty->isSized()) return false;
895   if (!G->hasInitializer()) return false;
896   if (GlobalWasGeneratedByAsan(G)) return false;  // Our own global.
897   // Touch only those globals that will not be defined in other modules.
898   // Don't handle ODR type linkages since other modules may be built w/o asan.
899   if (G->getLinkage() != GlobalVariable::ExternalLinkage &&
900       G->getLinkage() != GlobalVariable::PrivateLinkage &&
901       G->getLinkage() != GlobalVariable::InternalLinkage)
902     return false;
903   // Two problems with thread-locals:
904   //   - The address of the main thread's copy can't be computed at link-time.
905   //   - Need to poison all copies, not just the main thread's one.
906   if (G->isThreadLocal())
907     return false;
908   // For now, just ignore this Global if the alignment is large.
909   if (G->getAlignment() > MinRedzoneSizeForGlobal()) return false;
911   // Ignore all the globals with the names starting with "\01L_OBJC_".
912   // Many of those are put into the .cstring section. The linker compresses
913   // that section by removing the spare \0s after the string terminator, so
914   // our redzones get broken.
915   if ((G->getName().find("\01L_OBJC_") == 0) ||
916       (G->getName().find("\01l_OBJC_") == 0)) {
917     DEBUG(dbgs() << "Ignoring \\01L_OBJC_* global: " << *G << "\n");
918     return false;
919   }
921   if (G->hasSection()) {
922     StringRef Section(G->getSection());
923     // Ignore the globals from the __OBJC section. The ObjC runtime assumes
924     // those conform to /usr/lib/objc/runtime.h, so we can't add redzones to
925     // them.
926     if (Section.startswith("__OBJC,") ||
927         Section.startswith("__DATA, __objc_")) {
928       DEBUG(dbgs() << "Ignoring ObjC runtime global: " << *G << "\n");
929       return false;
930     }
931     // See http://code.google.com/p/address-sanitizer/issues/detail?id=32
932     // Constant CFString instances are compiled in the following way:
933     //  -- the string buffer is emitted into
934     //     __TEXT,__cstring,cstring_literals
935     //  -- the constant NSConstantString structure referencing that buffer
936     //     is placed into __DATA,__cfstring
937     // Therefore there's no point in placing redzones into __DATA,__cfstring.
938     // Moreover, it causes the linker to crash on OS X 10.7
939     if (Section.startswith("__DATA,__cfstring")) {
940       DEBUG(dbgs() << "Ignoring CFString: " << *G << "\n");
941       return false;
942     }
943     // The linker merges the contents of cstring_literals and removes the
944     // trailing zeroes.
945     if (Section.startswith("__TEXT,__cstring,cstring_literals")) {
946       DEBUG(dbgs() << "Ignoring a cstring literal: " << *G << "\n");
947       return false;
948     }
950     // Callbacks put into the CRT initializer/terminator sections
951     // should not be instrumented.
952     // See https://code.google.com/p/address-sanitizer/issues/detail?id=305
953     // and http://msdn.microsoft.com/en-US/en-en/library/bb918180(v=vs.120).aspx
954     if (Section.startswith(".CRT")) {
955       DEBUG(dbgs() << "Ignoring a global initializer callback: " << *G << "\n");
956       return false;
957     }
959     // Globals from llvm.metadata aren't emitted, do not instrument them.
960     if (Section == "llvm.metadata") return false;
961   }
963   return true;
966 void AddressSanitizerModule::initializeCallbacks(Module &M) {
967   IRBuilder<> IRB(*C);
968   // Declare our poisoning and unpoisoning functions.
969   AsanPoisonGlobals = checkInterfaceFunction(M.getOrInsertFunction(
970       kAsanPoisonGlobalsName, IRB.getVoidTy(), IntptrTy, NULL));
971   AsanPoisonGlobals->setLinkage(Function::ExternalLinkage);
972   AsanUnpoisonGlobals = checkInterfaceFunction(M.getOrInsertFunction(
973       kAsanUnpoisonGlobalsName, IRB.getVoidTy(), NULL));
974   AsanUnpoisonGlobals->setLinkage(Function::ExternalLinkage);
975   // Declare functions that register/unregister globals.
976   AsanRegisterGlobals = checkInterfaceFunction(M.getOrInsertFunction(
977       kAsanRegisterGlobalsName, IRB.getVoidTy(),
978       IntptrTy, IntptrTy, NULL));
979   AsanRegisterGlobals->setLinkage(Function::ExternalLinkage);
980   AsanUnregisterGlobals = checkInterfaceFunction(M.getOrInsertFunction(
981       kAsanUnregisterGlobalsName,
982       IRB.getVoidTy(), IntptrTy, IntptrTy, NULL));
983   AsanUnregisterGlobals->setLinkage(Function::ExternalLinkage);
986 // This function replaces all global variables with new variables that have
987 // trailing redzones. It also creates a function that poisons
988 // redzones and inserts this function into llvm.global_ctors.
989 bool AddressSanitizerModule::runOnModule(Module &M) {
990   if (!ClGlobals) return false;
992   DataLayoutPass *DLP = getAnalysisIfAvailable<DataLayoutPass>();
993   if (!DLP)
994     return false;
995   DL = &DLP->getDataLayout();
997   BL.reset(SpecialCaseList::createOrDie(BlacklistFile));
998   if (BL->isIn(M)) return false;
999   C = &(M.getContext());
1000   int LongSize = DL->getPointerSizeInBits();
1001   IntptrTy = Type::getIntNTy(*C, LongSize);
1002   Mapping = getShadowMapping(M, LongSize);
1003   initializeCallbacks(M);
1004   DynamicallyInitializedGlobals.Init(M);
1006   SmallVector<GlobalVariable *, 16> GlobalsToChange;
1008   for (Module::GlobalListType::iterator G = M.global_begin(),
1009        E = M.global_end(); G != E; ++G) {
1010     if (ShouldInstrumentGlobal(G))
1011       GlobalsToChange.push_back(G);
1012   }
1014   size_t n = GlobalsToChange.size();
1015   if (n == 0) return false;
1017   // A global is described by a structure
1018   //   size_t beg;
1019   //   size_t size;
1020   //   size_t size_with_redzone;
1021   //   const char *name;
1022   //   const char *module_name;
1023   //   size_t has_dynamic_init;
1024   // We initialize an array of such structures and pass it to a run-time call.
1025   StructType *GlobalStructTy = StructType::get(IntptrTy, IntptrTy,
1026                                                IntptrTy, IntptrTy,
1027                                                IntptrTy, IntptrTy, NULL);
1028   SmallVector<Constant *, 16> Initializers(n);
1030   Function *CtorFunc = M.getFunction(kAsanModuleCtorName);
1031   assert(CtorFunc);
1032   IRBuilder<> IRB(CtorFunc->getEntryBlock().getTerminator());
1034   bool HasDynamicallyInitializedGlobals = false;
1036   // We shouldn't merge same module names, as this string serves as unique
1037   // module ID in runtime.
1038   GlobalVariable *ModuleName = createPrivateGlobalForString(
1039       M, M.getModuleIdentifier(), /*AllowMerging*/false);
1041   for (size_t i = 0; i < n; i++) {
1042     static const uint64_t kMaxGlobalRedzone = 1 << 18;
1043     GlobalVariable *G = GlobalsToChange[i];
1044     PointerType *PtrTy = cast<PointerType>(G->getType());
1045     Type *Ty = PtrTy->getElementType();
1046     uint64_t SizeInBytes = DL->getTypeAllocSize(Ty);
1047     uint64_t MinRZ = MinRedzoneSizeForGlobal();
1048     // MinRZ <= RZ <= kMaxGlobalRedzone
1049     // and trying to make RZ to be ~ 1/4 of SizeInBytes.
1050     uint64_t RZ = std::max(MinRZ,
1051                          std::min(kMaxGlobalRedzone,
1052                                   (SizeInBytes / MinRZ / 4) * MinRZ));
1053     uint64_t RightRedzoneSize = RZ;
1054     // Round up to MinRZ
1055     if (SizeInBytes % MinRZ)
1056       RightRedzoneSize += MinRZ - (SizeInBytes % MinRZ);
1057     assert(((RightRedzoneSize + SizeInBytes) % MinRZ) == 0);
1058     Type *RightRedZoneTy = ArrayType::get(IRB.getInt8Ty(), RightRedzoneSize);
1059     // Determine whether this global should be poisoned in initialization.
1060     bool GlobalHasDynamicInitializer =
1061         DynamicallyInitializedGlobals.Contains(G);
1062     // Don't check initialization order if this global is blacklisted.
1063     GlobalHasDynamicInitializer &= !BL->isIn(*G, "init");
1065     StructType *NewTy = StructType::get(Ty, RightRedZoneTy, NULL);
1066     Constant *NewInitializer = ConstantStruct::get(
1067         NewTy, G->getInitializer(),
1068         Constant::getNullValue(RightRedZoneTy), NULL);
1070     GlobalVariable *Name =
1071         createPrivateGlobalForString(M, G->getName(), /*AllowMerging*/true);
1073     // Create a new global variable with enough space for a redzone.
1074     GlobalValue::LinkageTypes Linkage = G->getLinkage();
1075     if (G->isConstant() && Linkage == GlobalValue::PrivateLinkage)
1076       Linkage = GlobalValue::InternalLinkage;
1077     GlobalVariable *NewGlobal = new GlobalVariable(
1078         M, NewTy, G->isConstant(), Linkage,
1079         NewInitializer, "", G, G->getThreadLocalMode());
1080     NewGlobal->copyAttributesFrom(G);
1081     NewGlobal->setAlignment(MinRZ);
1083     Value *Indices2[2];
1084     Indices2[0] = IRB.getInt32(0);
1085     Indices2[1] = IRB.getInt32(0);
1087     G->replaceAllUsesWith(
1088         ConstantExpr::getGetElementPtr(NewGlobal, Indices2, true));
1089     NewGlobal->takeName(G);
1090     G->eraseFromParent();
1092     Initializers[i] = ConstantStruct::get(
1093         GlobalStructTy,
1094         ConstantExpr::getPointerCast(NewGlobal, IntptrTy),
1095         ConstantInt::get(IntptrTy, SizeInBytes),
1096         ConstantInt::get(IntptrTy, SizeInBytes + RightRedzoneSize),
1097         ConstantExpr::getPointerCast(Name, IntptrTy),
1098         ConstantExpr::getPointerCast(ModuleName, IntptrTy),
1099         ConstantInt::get(IntptrTy, GlobalHasDynamicInitializer),
1100         NULL);
1102     // Populate the first and last globals declared in this TU.
1103     if (CheckInitOrder && GlobalHasDynamicInitializer)
1104       HasDynamicallyInitializedGlobals = true;
1106     DEBUG(dbgs() << "NEW GLOBAL: " << *NewGlobal << "\n");
1107   }
1109   ArrayType *ArrayOfGlobalStructTy = ArrayType::get(GlobalStructTy, n);
1110   GlobalVariable *AllGlobals = new GlobalVariable(
1111       M, ArrayOfGlobalStructTy, false, GlobalVariable::InternalLinkage,
1112       ConstantArray::get(ArrayOfGlobalStructTy, Initializers), "");
1114   // Create calls for poisoning before initializers run and unpoisoning after.
1115   if (CheckInitOrder && HasDynamicallyInitializedGlobals)
1116     createInitializerPoisonCalls(M, ModuleName);
1117   IRB.CreateCall2(AsanRegisterGlobals,
1118                   IRB.CreatePointerCast(AllGlobals, IntptrTy),
1119                   ConstantInt::get(IntptrTy, n));
1121   // We also need to unregister globals at the end, e.g. when a shared library
1122   // gets closed.
1123   Function *AsanDtorFunction = Function::Create(
1124       FunctionType::get(Type::getVoidTy(*C), false),
1125       GlobalValue::InternalLinkage, kAsanModuleDtorName, &M);
1126   BasicBlock *AsanDtorBB = BasicBlock::Create(*C, "", AsanDtorFunction);
1127   IRBuilder<> IRB_Dtor(ReturnInst::Create(*C, AsanDtorBB));
1128   IRB_Dtor.CreateCall2(AsanUnregisterGlobals,
1129                        IRB.CreatePointerCast(AllGlobals, IntptrTy),
1130                        ConstantInt::get(IntptrTy, n));
1131   appendToGlobalDtors(M, AsanDtorFunction, kAsanCtorAndCtorPriority);
1133   DEBUG(dbgs() << M);
1134   return true;
1137 void AddressSanitizer::initializeCallbacks(Module &M) {
1138   IRBuilder<> IRB(*C);
1139   // Create __asan_report* callbacks.
1140   for (size_t AccessIsWrite = 0; AccessIsWrite <= 1; AccessIsWrite++) {
1141     for (size_t AccessSizeIndex = 0; AccessSizeIndex < kNumberOfAccessSizes;
1142          AccessSizeIndex++) {
1143       // IsWrite and TypeSize are encoded in the function name.
1144       std::string Suffix =
1145           (AccessIsWrite ? "store" : "load") + itostr(1 << AccessSizeIndex);
1146       AsanErrorCallback[AccessIsWrite][AccessSizeIndex] =
1147           checkInterfaceFunction(
1148               M.getOrInsertFunction(kAsanReportErrorTemplate + Suffix,
1149                                     IRB.getVoidTy(), IntptrTy, NULL));
1150       AsanMemoryAccessCallback[AccessIsWrite][AccessSizeIndex] =
1151           checkInterfaceFunction(
1152               M.getOrInsertFunction(ClMemoryAccessCallbackPrefix + Suffix,
1153                                     IRB.getVoidTy(), IntptrTy, NULL));
1154     }
1155   }
1156   AsanErrorCallbackSized[0] = checkInterfaceFunction(M.getOrInsertFunction(
1157               kAsanReportLoadN, IRB.getVoidTy(), IntptrTy, IntptrTy, NULL));
1158   AsanErrorCallbackSized[1] = checkInterfaceFunction(M.getOrInsertFunction(
1159               kAsanReportStoreN, IRB.getVoidTy(), IntptrTy, IntptrTy, NULL));
1161   AsanMemoryAccessCallbackSized[0] = checkInterfaceFunction(
1162       M.getOrInsertFunction(ClMemoryAccessCallbackPrefix + "loadN",
1163                             IRB.getVoidTy(), IntptrTy, IntptrTy, NULL));
1164   AsanMemoryAccessCallbackSized[1] = checkInterfaceFunction(
1165       M.getOrInsertFunction(ClMemoryAccessCallbackPrefix + "storeN",
1166                             IRB.getVoidTy(), IntptrTy, IntptrTy, NULL));
1168   AsanMemmove = checkInterfaceFunction(M.getOrInsertFunction(
1169       ClMemoryAccessCallbackPrefix + "memmove", IRB.getInt8PtrTy(),
1170       IRB.getInt8PtrTy(), IRB.getInt8PtrTy(), IntptrTy, NULL));
1171   AsanMemcpy = checkInterfaceFunction(M.getOrInsertFunction(
1172       ClMemoryAccessCallbackPrefix + "memcpy", IRB.getInt8PtrTy(),
1173       IRB.getInt8PtrTy(), IRB.getInt8PtrTy(), IntptrTy, NULL));
1174   AsanMemset = checkInterfaceFunction(M.getOrInsertFunction(
1175       ClMemoryAccessCallbackPrefix + "memset", IRB.getInt8PtrTy(),
1176       IRB.getInt8PtrTy(), IRB.getInt32Ty(), IntptrTy, NULL));
1178   AsanHandleNoReturnFunc = checkInterfaceFunction(
1179       M.getOrInsertFunction(kAsanHandleNoReturnName, IRB.getVoidTy(), NULL));
1180   AsanCovFunction = checkInterfaceFunction(M.getOrInsertFunction(
1181       kAsanCovName, IRB.getVoidTy(), NULL));
1182   AsanPtrCmpFunction = checkInterfaceFunction(M.getOrInsertFunction(
1183       kAsanPtrCmp, IRB.getVoidTy(), IntptrTy, IntptrTy, NULL));
1184   AsanPtrSubFunction = checkInterfaceFunction(M.getOrInsertFunction(
1185       kAsanPtrSub, IRB.getVoidTy(), IntptrTy, IntptrTy, NULL));
1186   // We insert an empty inline asm after __asan_report* to avoid callback merge.
1187   EmptyAsm = InlineAsm::get(FunctionType::get(IRB.getVoidTy(), false),
1188                             StringRef(""), StringRef(""),
1189                             /*hasSideEffects=*/true);
1192 // virtual
1193 bool AddressSanitizer::doInitialization(Module &M) {
1194   // Initialize the private fields. No one has accessed them before.
1195   DataLayoutPass *DLP = getAnalysisIfAvailable<DataLayoutPass>();
1196   if (!DLP)
1197     report_fatal_error("data layout missing");
1198   DL = &DLP->getDataLayout();
1200   BL.reset(SpecialCaseList::createOrDie(BlacklistFile));
1201   DynamicallyInitializedGlobals.Init(M);
1203   C = &(M.getContext());
1204   LongSize = DL->getPointerSizeInBits();
1205   IntptrTy = Type::getIntNTy(*C, LongSize);
1207   AsanCtorFunction = Function::Create(
1208       FunctionType::get(Type::getVoidTy(*C), false),
1209       GlobalValue::InternalLinkage, kAsanModuleCtorName, &M);
1210   BasicBlock *AsanCtorBB = BasicBlock::Create(*C, "", AsanCtorFunction);
1211   // call __asan_init in the module ctor.
1212   IRBuilder<> IRB(ReturnInst::Create(*C, AsanCtorBB));
1213   AsanInitFunction = checkInterfaceFunction(
1214       M.getOrInsertFunction(kAsanInitName, IRB.getVoidTy(), NULL));
1215   AsanInitFunction->setLinkage(Function::ExternalLinkage);
1216   IRB.CreateCall(AsanInitFunction);
1218   Mapping = getShadowMapping(M, LongSize);
1220   appendToGlobalCtors(M, AsanCtorFunction, kAsanCtorAndCtorPriority);
1221   return true;
1224 bool AddressSanitizer::maybeInsertAsanInitAtFunctionEntry(Function &F) {
1225   // For each NSObject descendant having a +load method, this method is invoked
1226   // by the ObjC runtime before any of the static constructors is called.
1227   // Therefore we need to instrument such methods with a call to __asan_init
1228   // at the beginning in order to initialize our runtime before any access to
1229   // the shadow memory.
1230   // We cannot just ignore these methods, because they may call other
1231   // instrumented functions.
1232   if (F.getName().find(" load]") != std::string::npos) {
1233     IRBuilder<> IRB(F.begin()->begin());
1234     IRB.CreateCall(AsanInitFunction);
1235     return true;
1236   }
1237   return false;
1240 void AddressSanitizer::InjectCoverageAtBlock(Function &F, BasicBlock &BB) {
1241   BasicBlock::iterator IP = BB.getFirstInsertionPt(), BE = BB.end();
1242   // Skip static allocas at the top of the entry block so they don't become
1243   // dynamic when we split the block.  If we used our optimized stack layout,
1244   // then there will only be one alloca and it will come first.
1245   for (; IP != BE; ++IP) {
1246     AllocaInst *AI = dyn_cast<AllocaInst>(IP);
1247     if (!AI || !AI->isStaticAlloca())
1248       break;
1249   }
1251   IRBuilder<> IRB(IP);
1252   Type *Int8Ty = IRB.getInt8Ty();
1253   GlobalVariable *Guard = new GlobalVariable(
1254       *F.getParent(), Int8Ty, false, GlobalValue::PrivateLinkage,
1255       Constant::getNullValue(Int8Ty), "__asan_gen_cov_" + F.getName());
1256   LoadInst *Load = IRB.CreateLoad(Guard);
1257   Load->setAtomic(Monotonic);
1258   Load->setAlignment(1);
1259   Value *Cmp = IRB.CreateICmpEQ(Constant::getNullValue(Int8Ty), Load);
1260   Instruction *Ins = SplitBlockAndInsertIfThen(
1261       Cmp, IP, false, MDBuilder(*C).createBranchWeights(1, 100000));
1262   IRB.SetInsertPoint(Ins);
1263   // We pass &F to __sanitizer_cov. We could avoid this and rely on
1264   // GET_CALLER_PC, but having the PC of the first instruction is just nice.
1265   Instruction *Call = IRB.CreateCall(AsanCovFunction);
1266   Call->setDebugLoc(IP->getDebugLoc());
1267   StoreInst *Store = IRB.CreateStore(ConstantInt::get(Int8Ty, 1), Guard);
1268   Store->setAtomic(Monotonic);
1269   Store->setAlignment(1);
1272 // Poor man's coverage that works with ASan.
1273 // We create a Guard boolean variable with the same linkage
1274 // as the function and inject this code into the entry block (-asan-coverage=1)
1275 // or all blocks (-asan-coverage=2):
1276 // if (*Guard) {
1277 //    __sanitizer_cov(&F);
1278 //    *Guard = 1;
1279 // }
1280 // The accesses to Guard are atomic. The rest of the logic is
1281 // in __sanitizer_cov (it's fine to call it more than once).
1282 //
1283 // This coverage implementation provides very limited data:
1284 // it only tells if a given function (block) was ever executed.
1285 // No counters, no per-edge data.
1286 // But for many use cases this is what we need and the added slowdown
1287 // is negligible. This simple implementation will probably be obsoleted
1288 // by the upcoming Clang-based coverage implementation.
1289 // By having it here and now we hope to
1290 //  a) get the functionality to users earlier and
1291 //  b) collect usage statistics to help improve Clang coverage design.
1292 bool AddressSanitizer::InjectCoverage(Function &F,
1293                                       const ArrayRef<BasicBlock *> AllBlocks) {
1294   if (!ClCoverage) return false;
1296   if (ClCoverage == 1 ||
1297       (unsigned)ClCoverageBlockThreshold < AllBlocks.size()) {
1298     InjectCoverageAtBlock(F, F.getEntryBlock());
1299   } else {
1300     for (size_t i = 0, n = AllBlocks.size(); i < n; i++)
1301       InjectCoverageAtBlock(F, *AllBlocks[i]);
1302   }
1303   return true;
1306 bool AddressSanitizer::runOnFunction(Function &F) {
1307   if (BL->isIn(F)) return false;
1308   if (&F == AsanCtorFunction) return false;
1309   if (F.getLinkage() == GlobalValue::AvailableExternallyLinkage) return false;
1310   DEBUG(dbgs() << "ASAN instrumenting:\n" << F << "\n");
1311   initializeCallbacks(*F.getParent());
1313   // If needed, insert __asan_init before checking for SanitizeAddress attr.
1314   maybeInsertAsanInitAtFunctionEntry(F);
1316   if (!F.hasFnAttribute(Attribute::SanitizeAddress))
1317     return false;
1319   if (!ClDebugFunc.empty() && ClDebugFunc != F.getName())
1320     return false;
1322   // We want to instrument every address only once per basic block (unless there
1323   // are calls between uses).
1324   SmallSet<Value*, 16> TempsToInstrument;
1325   SmallVector<Instruction*, 16> ToInstrument;
1326   SmallVector<Instruction*, 8> NoReturnCalls;
1327   SmallVector<BasicBlock*, 16> AllBlocks;
1328   SmallVector<Instruction*, 16> PointerComparisonsOrSubtracts;
1329   int NumAllocas = 0;
1330   bool IsWrite;
1332   // Fill the set of memory operations to instrument.
1333   for (Function::iterator FI = F.begin(), FE = F.end();
1334        FI != FE; ++FI) {
1335     AllBlocks.push_back(FI);
1336     TempsToInstrument.clear();
1337     int NumInsnsPerBB = 0;
1338     for (BasicBlock::iterator BI = FI->begin(), BE = FI->end();
1339          BI != BE; ++BI) {
1340       if (LooksLikeCodeInBug11395(BI)) return false;
1341       if (Value *Addr = isInterestingMemoryAccess(BI, &IsWrite)) {
1342         if (ClOpt && ClOptSameTemp) {
1343           if (!TempsToInstrument.insert(Addr))
1344             continue;  // We've seen this temp in the current BB.
1345         }
1346       } else if (ClInvalidPointerPairs &&
1347                  isInterestingPointerComparisonOrSubtraction(BI)) {
1348         PointerComparisonsOrSubtracts.push_back(BI);
1349         continue;
1350       } else if (isa<MemIntrinsic>(BI)) {
1351         // ok, take it.
1352       } else {
1353         if (isa<AllocaInst>(BI))
1354           NumAllocas++;
1355         CallSite CS(BI);
1356         if (CS) {
1357           // A call inside BB.
1358           TempsToInstrument.clear();
1359           if (CS.doesNotReturn())
1360             NoReturnCalls.push_back(CS.getInstruction());
1361         }
1362         continue;
1363       }
1364       ToInstrument.push_back(BI);
1365       NumInsnsPerBB++;
1366       if (NumInsnsPerBB >= ClMaxInsnsToInstrumentPerBB)
1367         break;
1368     }
1369   }
1371   Function *UninstrumentedDuplicate = nullptr;
1372   bool LikelyToInstrument =
1373       !NoReturnCalls.empty() || !ToInstrument.empty() || (NumAllocas > 0);
1374   if (ClKeepUninstrumented && LikelyToInstrument) {
1375     ValueToValueMapTy VMap;
1376     UninstrumentedDuplicate = CloneFunction(&F, VMap, false);
1377     UninstrumentedDuplicate->removeFnAttr(Attribute::SanitizeAddress);
1378     UninstrumentedDuplicate->setName("NOASAN_" + F.getName());
1379     F.getParent()->getFunctionList().push_back(UninstrumentedDuplicate);
1380   }
1382   bool UseCalls = false;
1383   if (ClInstrumentationWithCallsThreshold >= 0 &&
1384       ToInstrument.size() > (unsigned)ClInstrumentationWithCallsThreshold)
1385     UseCalls = true;
1387   // Instrument.
1388   int NumInstrumented = 0;
1389   for (size_t i = 0, n = ToInstrument.size(); i != n; i++) {
1390     Instruction *Inst = ToInstrument[i];
1391     if (ClDebugMin < 0 || ClDebugMax < 0 ||
1392         (NumInstrumented >= ClDebugMin && NumInstrumented <= ClDebugMax)) {
1393       if (isInterestingMemoryAccess(Inst, &IsWrite))
1394         instrumentMop(Inst, UseCalls);
1395       else
1396         instrumentMemIntrinsic(cast<MemIntrinsic>(Inst));
1397     }
1398     NumInstrumented++;
1399   }
1401   FunctionStackPoisoner FSP(F, *this);
1402   bool ChangedStack = FSP.runOnFunction();
1404   // We must unpoison the stack before every NoReturn call (throw, _exit, etc).
1405   // See e.g. http://code.google.com/p/address-sanitizer/issues/detail?id=37
1406   for (size_t i = 0, n = NoReturnCalls.size(); i != n; i++) {
1407     Instruction *CI = NoReturnCalls[i];
1408     IRBuilder<> IRB(CI);
1409     IRB.CreateCall(AsanHandleNoReturnFunc);
1410   }
1412   for (size_t i = 0, n = PointerComparisonsOrSubtracts.size(); i != n; i++) {
1413     instrumentPointerComparisonOrSubtraction(PointerComparisonsOrSubtracts[i]);
1414     NumInstrumented++;
1415   }
1417   bool res = NumInstrumented > 0 || ChangedStack || !NoReturnCalls.empty();
1419   if (InjectCoverage(F, AllBlocks))
1420     res = true;
1422   DEBUG(dbgs() << "ASAN done instrumenting: " << res << " " << F << "\n");
1424   if (ClKeepUninstrumented) {
1425     if (!res) {
1426       // No instrumentation is done, no need for the duplicate.
1427       if (UninstrumentedDuplicate)
1428         UninstrumentedDuplicate->eraseFromParent();
1429     } else {
1430       // The function was instrumented. We must have the duplicate.
1431       assert(UninstrumentedDuplicate);
1432       UninstrumentedDuplicate->setSection("NOASAN");
1433       assert(!F.hasSection());
1434       F.setSection("ASAN");
1435     }
1436   }
1438   return res;
1441 // Workaround for bug 11395: we don't want to instrument stack in functions
1442 // with large assembly blobs (32-bit only), otherwise reg alloc may crash.
1443 // FIXME: remove once the bug 11395 is fixed.
1444 bool AddressSanitizer::LooksLikeCodeInBug11395(Instruction *I) {
1445   if (LongSize != 32) return false;
1446   CallInst *CI = dyn_cast<CallInst>(I);
1447   if (!CI || !CI->isInlineAsm()) return false;
1448   if (CI->getNumArgOperands() <= 5) return false;
1449   // We have inline assembly with quite a few arguments.
1450   return true;
1453 void FunctionStackPoisoner::initializeCallbacks(Module &M) {
1454   IRBuilder<> IRB(*C);
1455   for (int i = 0; i <= kMaxAsanStackMallocSizeClass; i++) {
1456     std::string Suffix = itostr(i);
1457     AsanStackMallocFunc[i] = checkInterfaceFunction(
1458         M.getOrInsertFunction(kAsanStackMallocNameTemplate + Suffix, IntptrTy,
1459                               IntptrTy, IntptrTy, NULL));
1460     AsanStackFreeFunc[i] = checkInterfaceFunction(M.getOrInsertFunction(
1461         kAsanStackFreeNameTemplate + Suffix, IRB.getVoidTy(), IntptrTy,
1462         IntptrTy, IntptrTy, NULL));
1463   }
1464   AsanPoisonStackMemoryFunc = checkInterfaceFunction(M.getOrInsertFunction(
1465       kAsanPoisonStackMemoryName, IRB.getVoidTy(), IntptrTy, IntptrTy, NULL));
1466   AsanUnpoisonStackMemoryFunc = checkInterfaceFunction(M.getOrInsertFunction(
1467       kAsanUnpoisonStackMemoryName, IRB.getVoidTy(), IntptrTy, IntptrTy, NULL));
1470 void
1471 FunctionStackPoisoner::poisonRedZones(const ArrayRef<uint8_t> ShadowBytes,
1472                                       IRBuilder<> &IRB, Value *ShadowBase,
1473                                       bool DoPoison) {
1474   size_t n = ShadowBytes.size();
1475   size_t i = 0;
1476   // We need to (un)poison n bytes of stack shadow. Poison as many as we can
1477   // using 64-bit stores (if we are on 64-bit arch), then poison the rest
1478   // with 32-bit stores, then with 16-byte stores, then with 8-byte stores.
1479   for (size_t LargeStoreSizeInBytes = ASan.LongSize / 8;
1480        LargeStoreSizeInBytes != 0; LargeStoreSizeInBytes /= 2) {
1481     for (; i + LargeStoreSizeInBytes - 1 < n; i += LargeStoreSizeInBytes) {
1482       uint64_t Val = 0;
1483       for (size_t j = 0; j < LargeStoreSizeInBytes; j++) {
1484         if (ASan.DL->isLittleEndian())
1485           Val |= (uint64_t)ShadowBytes[i + j] << (8 * j);
1486         else
1487           Val = (Val << 8) | ShadowBytes[i + j];
1488       }
1489       if (!Val) continue;
1490       Value *Ptr = IRB.CreateAdd(ShadowBase, ConstantInt::get(IntptrTy, i));
1491       Type *StoreTy = Type::getIntNTy(*C, LargeStoreSizeInBytes * 8);
1492       Value *Poison = ConstantInt::get(StoreTy, DoPoison ? Val : 0);
1493       IRB.CreateStore(Poison, IRB.CreateIntToPtr(Ptr, StoreTy->getPointerTo()));
1494     }
1495   }
1498 // Fake stack allocator (asan_fake_stack.h) has 11 size classes
1499 // for every power of 2 from kMinStackMallocSize to kMaxAsanStackMallocSizeClass
1500 static int StackMallocSizeClass(uint64_t LocalStackSize) {
1501   assert(LocalStackSize <= kMaxStackMallocSize);
1502   uint64_t MaxSize = kMinStackMallocSize;
1503   for (int i = 0; ; i++, MaxSize *= 2)
1504     if (LocalStackSize <= MaxSize)
1505       return i;
1506   llvm_unreachable("impossible LocalStackSize");
1509 // Set Size bytes starting from ShadowBase to kAsanStackAfterReturnMagic.
1510 // We can not use MemSet intrinsic because it may end up calling the actual
1511 // memset. Size is a multiple of 8.
1512 // Currently this generates 8-byte stores on x86_64; it may be better to
1513 // generate wider stores.
1514 void FunctionStackPoisoner::SetShadowToStackAfterReturnInlined(
1515     IRBuilder<> &IRB, Value *ShadowBase, int Size) {
1516   assert(!(Size % 8));
1517   assert(kAsanStackAfterReturnMagic == 0xf5);
1518   for (int i = 0; i < Size; i += 8) {
1519     Value *p = IRB.CreateAdd(ShadowBase, ConstantInt::get(IntptrTy, i));
1520     IRB.CreateStore(ConstantInt::get(IRB.getInt64Ty(), 0xf5f5f5f5f5f5f5f5ULL),
1521                     IRB.CreateIntToPtr(p, IRB.getInt64Ty()->getPointerTo()));
1522   }
1525 static DebugLoc getFunctionEntryDebugLocation(Function &F) {
1526   BasicBlock::iterator I = F.getEntryBlock().begin(),
1527                        E = F.getEntryBlock().end();
1528   for (; I != E; ++I)
1529     if (!isa<AllocaInst>(I))
1530       break;
1531   return I->getDebugLoc();
1534 void FunctionStackPoisoner::poisonStack() {
1535   int StackMallocIdx = -1;
1536   DebugLoc EntryDebugLocation = getFunctionEntryDebugLocation(F);
1538   assert(AllocaVec.size() > 0);
1539   Instruction *InsBefore = AllocaVec[0];
1540   IRBuilder<> IRB(InsBefore);
1541   IRB.SetCurrentDebugLocation(EntryDebugLocation);
1543   SmallVector<ASanStackVariableDescription, 16> SVD;
1544   SVD.reserve(AllocaVec.size());
1545   for (size_t i = 0, n = AllocaVec.size(); i < n; i++) {
1546     AllocaInst *AI = AllocaVec[i];
1547     ASanStackVariableDescription D = { AI->getName().data(),
1548                                    getAllocaSizeInBytes(AI),
1549                                    AI->getAlignment(), AI, 0};
1550     SVD.push_back(D);
1551   }
1552   // Minimal header size (left redzone) is 4 pointers,
1553   // i.e. 32 bytes on 64-bit platforms and 16 bytes in 32-bit platforms.
1554   size_t MinHeaderSize = ASan.LongSize / 2;
1555   ASanStackFrameLayout L;
1556   ComputeASanStackFrameLayout(SVD, 1UL << Mapping.Scale, MinHeaderSize, &L);
1557   DEBUG(dbgs() << L.DescriptionString << " --- " << L.FrameSize << "\n");
1558   uint64_t LocalStackSize = L.FrameSize;
1559   bool DoStackMalloc =
1560       ASan.CheckUseAfterReturn && LocalStackSize <= kMaxStackMallocSize;
1562   Type *ByteArrayTy = ArrayType::get(IRB.getInt8Ty(), LocalStackSize);
1563   AllocaInst *MyAlloca =
1564       new AllocaInst(ByteArrayTy, "MyAlloca", InsBefore);
1565   MyAlloca->setDebugLoc(EntryDebugLocation);
1566   assert((ClRealignStack & (ClRealignStack - 1)) == 0);
1567   size_t FrameAlignment = std::max(L.FrameAlignment, (size_t)ClRealignStack);
1568   MyAlloca->setAlignment(FrameAlignment);
1569   assert(MyAlloca->isStaticAlloca());
1570   Value *OrigStackBase = IRB.CreatePointerCast(MyAlloca, IntptrTy);
1571   Value *LocalStackBase = OrigStackBase;
1573   if (DoStackMalloc) {
1574     // LocalStackBase = OrigStackBase
1575     // if (__asan_option_detect_stack_use_after_return)
1576     //   LocalStackBase = __asan_stack_malloc_N(LocalStackBase, OrigStackBase);
1577     StackMallocIdx = StackMallocSizeClass(LocalStackSize);
1578     assert(StackMallocIdx <= kMaxAsanStackMallocSizeClass);
1579     Constant *OptionDetectUAR = F.getParent()->getOrInsertGlobal(
1580         kAsanOptionDetectUAR, IRB.getInt32Ty());
1581     Value *Cmp = IRB.CreateICmpNE(IRB.CreateLoad(OptionDetectUAR),
1582                                   Constant::getNullValue(IRB.getInt32Ty()));
1583     Instruction *Term = SplitBlockAndInsertIfThen(Cmp, InsBefore, false);
1584     BasicBlock *CmpBlock = cast<Instruction>(Cmp)->getParent();
1585     IRBuilder<> IRBIf(Term);
1586     IRBIf.SetCurrentDebugLocation(EntryDebugLocation);
1587     LocalStackBase = IRBIf.CreateCall2(
1588         AsanStackMallocFunc[StackMallocIdx],
1589         ConstantInt::get(IntptrTy, LocalStackSize), OrigStackBase);
1590     BasicBlock *SetBlock = cast<Instruction>(LocalStackBase)->getParent();
1591     IRB.SetInsertPoint(InsBefore);
1592     IRB.SetCurrentDebugLocation(EntryDebugLocation);
1593     PHINode *Phi = IRB.CreatePHI(IntptrTy, 2);
1594     Phi->addIncoming(OrigStackBase, CmpBlock);
1595     Phi->addIncoming(LocalStackBase, SetBlock);
1596     LocalStackBase = Phi;
1597   }
1599   // Insert poison calls for lifetime intrinsics for alloca.
1600   bool HavePoisonedAllocas = false;
1601   for (size_t i = 0, n = AllocaPoisonCallVec.size(); i < n; i++) {
1602     const AllocaPoisonCall &APC = AllocaPoisonCallVec[i];
1603     assert(APC.InsBefore);
1604     assert(APC.AI);
1605     IRBuilder<> IRB(APC.InsBefore);
1606     poisonAlloca(APC.AI, APC.Size, IRB, APC.DoPoison);
1607     HavePoisonedAllocas |= APC.DoPoison;
1608   }
1610   // Replace Alloca instructions with base+offset.
1611   for (size_t i = 0, n = SVD.size(); i < n; i++) {
1612     AllocaInst *AI = SVD[i].AI;
1613     Value *NewAllocaPtr = IRB.CreateIntToPtr(
1614         IRB.CreateAdd(LocalStackBase,
1615                       ConstantInt::get(IntptrTy, SVD[i].Offset)),
1616         AI->getType());
1617     replaceDbgDeclareForAlloca(AI, NewAllocaPtr, DIB);
1618     AI->replaceAllUsesWith(NewAllocaPtr);
1619   }
1621   // The left-most redzone has enough space for at least 4 pointers.
1622   // Write the Magic value to redzone[0].
1623   Value *BasePlus0 = IRB.CreateIntToPtr(LocalStackBase, IntptrPtrTy);
1624   IRB.CreateStore(ConstantInt::get(IntptrTy, kCurrentStackFrameMagic),
1625                   BasePlus0);
1626   // Write the frame description constant to redzone[1].
1627   Value *BasePlus1 = IRB.CreateIntToPtr(
1628     IRB.CreateAdd(LocalStackBase, ConstantInt::get(IntptrTy, ASan.LongSize/8)),
1629     IntptrPtrTy);
1630   GlobalVariable *StackDescriptionGlobal =
1631       createPrivateGlobalForString(*F.getParent(), L.DescriptionString,
1632                                    /*AllowMerging*/true);
1633   Value *Description = IRB.CreatePointerCast(StackDescriptionGlobal,
1634                                              IntptrTy);
1635   IRB.CreateStore(Description, BasePlus1);
1636   // Write the PC to redzone[2].
1637   Value *BasePlus2 = IRB.CreateIntToPtr(
1638     IRB.CreateAdd(LocalStackBase, ConstantInt::get(IntptrTy,
1639                                                    2 * ASan.LongSize/8)),
1640     IntptrPtrTy);
1641   IRB.CreateStore(IRB.CreatePointerCast(&F, IntptrTy), BasePlus2);
1643   // Poison the stack redzones at the entry.
1644   Value *ShadowBase = ASan.memToShadow(LocalStackBase, IRB);
1645   poisonRedZones(L.ShadowBytes, IRB, ShadowBase, true);
1647   // (Un)poison the stack before all ret instructions.
1648   for (size_t i = 0, n = RetVec.size(); i < n; i++) {
1649     Instruction *Ret = RetVec[i];
1650     IRBuilder<> IRBRet(Ret);
1651     // Mark the current frame as retired.
1652     IRBRet.CreateStore(ConstantInt::get(IntptrTy, kRetiredStackFrameMagic),
1653                        BasePlus0);
1654     if (DoStackMalloc) {
1655       assert(StackMallocIdx >= 0);
1656       // if LocalStackBase != OrigStackBase:
1657       //     // In use-after-return mode, poison the whole stack frame.
1658       //     if StackMallocIdx <= 4
1659       //         // For small sizes inline the whole thing:
1660       //         memset(ShadowBase, kAsanStackAfterReturnMagic, ShadowSize);
1661       //         **SavedFlagPtr(LocalStackBase) = 0
1662       //     else
1663       //         __asan_stack_free_N(LocalStackBase, OrigStackBase)
1664       // else
1665       //     <This is not a fake stack; unpoison the redzones>
1666       Value *Cmp = IRBRet.CreateICmpNE(LocalStackBase, OrigStackBase);
1667       TerminatorInst *ThenTerm, *ElseTerm;
1668       SplitBlockAndInsertIfThenElse(Cmp, Ret, &ThenTerm, &ElseTerm);
1670       IRBuilder<> IRBPoison(ThenTerm);
1671       if (StackMallocIdx <= 4) {
1672         int ClassSize = kMinStackMallocSize << StackMallocIdx;
1673         SetShadowToStackAfterReturnInlined(IRBPoison, ShadowBase,
1674                                            ClassSize >> Mapping.Scale);
1675         Value *SavedFlagPtrPtr = IRBPoison.CreateAdd(
1676             LocalStackBase,
1677             ConstantInt::get(IntptrTy, ClassSize - ASan.LongSize / 8));
1678         Value *SavedFlagPtr = IRBPoison.CreateLoad(
1679             IRBPoison.CreateIntToPtr(SavedFlagPtrPtr, IntptrPtrTy));
1680         IRBPoison.CreateStore(
1681             Constant::getNullValue(IRBPoison.getInt8Ty()),
1682             IRBPoison.CreateIntToPtr(SavedFlagPtr, IRBPoison.getInt8PtrTy()));
1683       } else {
1684         // For larger frames call __asan_stack_free_*.
1685         IRBPoison.CreateCall3(AsanStackFreeFunc[StackMallocIdx], LocalStackBase,
1686                               ConstantInt::get(IntptrTy, LocalStackSize),
1687                               OrigStackBase);
1688       }
1690       IRBuilder<> IRBElse(ElseTerm);
1691       poisonRedZones(L.ShadowBytes, IRBElse, ShadowBase, false);
1692     } else if (HavePoisonedAllocas) {
1693       // If we poisoned some allocas in llvm.lifetime analysis,
1694       // unpoison whole stack frame now.
1695       assert(LocalStackBase == OrigStackBase);
1696       poisonAlloca(LocalStackBase, LocalStackSize, IRBRet, false);
1697     } else {
1698       poisonRedZones(L.ShadowBytes, IRBRet, ShadowBase, false);
1699     }
1700   }
1702   // We are done. Remove the old unused alloca instructions.
1703   for (size_t i = 0, n = AllocaVec.size(); i < n; i++)
1704     AllocaVec[i]->eraseFromParent();
1707 void FunctionStackPoisoner::poisonAlloca(Value *V, uint64_t Size,
1708                                          IRBuilder<> &IRB, bool DoPoison) {
1709   // For now just insert the call to ASan runtime.
1710   Value *AddrArg = IRB.CreatePointerCast(V, IntptrTy);
1711   Value *SizeArg = ConstantInt::get(IntptrTy, Size);
1712   IRB.CreateCall2(DoPoison ? AsanPoisonStackMemoryFunc
1713                            : AsanUnpoisonStackMemoryFunc,
1714                   AddrArg, SizeArg);
1717 // Handling llvm.lifetime intrinsics for a given %alloca:
1718 // (1) collect all llvm.lifetime.xxx(%size, %value) describing the alloca.
1719 // (2) if %size is constant, poison memory for llvm.lifetime.end (to detect
1720 //     invalid accesses) and unpoison it for llvm.lifetime.start (the memory
1721 //     could be poisoned by previous llvm.lifetime.end instruction, as the
1722 //     variable may go in and out of scope several times, e.g. in loops).
1723 // (3) if we poisoned at least one %alloca in a function,
1724 //     unpoison the whole stack frame at function exit.
1726 AllocaInst *FunctionStackPoisoner::findAllocaForValue(Value *V) {
1727   if (AllocaInst *AI = dyn_cast<AllocaInst>(V))
1728     // We're intested only in allocas we can handle.
1729     return isInterestingAlloca(*AI) ? AI : nullptr;
1730   // See if we've already calculated (or started to calculate) alloca for a
1731   // given value.
1732   AllocaForValueMapTy::iterator I = AllocaForValue.find(V);
1733   if (I != AllocaForValue.end())
1734     return I->second;
1735   // Store 0 while we're calculating alloca for value V to avoid
1736   // infinite recursion if the value references itself.
1737   AllocaForValue[V] = nullptr;
1738   AllocaInst *Res = nullptr;
1739   if (CastInst *CI = dyn_cast<CastInst>(V))
1740     Res = findAllocaForValue(CI->getOperand(0));
1741   else if (PHINode *PN = dyn_cast<PHINode>(V)) {
1742     for (unsigned i = 0, e = PN->getNumIncomingValues(); i != e; ++i) {
1743       Value *IncValue = PN->getIncomingValue(i);
1744       // Allow self-referencing phi-nodes.
1745       if (IncValue == PN) continue;
1746       AllocaInst *IncValueAI = findAllocaForValue(IncValue);
1747       // AI for incoming values should exist and should all be equal.
1748       if (IncValueAI == nullptr || (Res != nullptr && IncValueAI != Res))
1749         return nullptr;
1750       Res = IncValueAI;
1751     }
1752   }
1753   if (Res)
1754     AllocaForValue[V] = Res;
1755   return Res;