b6023e2ce7897fcc9232b1ce53eef1e3626cdbf4
[opencl/llvm.git] / lib / Transforms / Scalar / Reg2Mem.cpp
1 //===- Reg2Mem.cpp - Convert registers to allocas -------------------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file demotes all registers to memory references.  It is intended to be
11 // the inverse of PromoteMemoryToRegister.  By converting to loads, the only
12 // values live across basic blocks are allocas and loads before phi nodes.
13 // It is intended that this should make CFG hacking much easier.
14 // To make later hacking easier, the entry block is split into two, such that
15 // all introduced allocas and nothing else are in the entry block.
16 //
17 //===----------------------------------------------------------------------===//
19 #include "llvm/Transforms/Scalar.h"
20 #include "llvm/ADT/Statistic.h"
21 #include "llvm/IR/BasicBlock.h"
22 #include "llvm/IR/CFG.h"
23 #include "llvm/IR/Function.h"
24 #include "llvm/IR/Instructions.h"
25 #include "llvm/IR/LLVMContext.h"
26 #include "llvm/IR/Module.h"
27 #include "llvm/Pass.h"
28 #include "llvm/Transforms/Utils/Local.h"
29 #include <list>
30 using namespace llvm;
32 #define DEBUG_TYPE "reg2mem"
34 STATISTIC(NumRegsDemoted, "Number of registers demoted");
35 STATISTIC(NumPhisDemoted, "Number of phi-nodes demoted");
37 namespace {
38   struct RegToMem : public FunctionPass {
39     static char ID; // Pass identification, replacement for typeid
40     RegToMem() : FunctionPass(ID) {
41       initializeRegToMemPass(*PassRegistry::getPassRegistry());
42     }
44     void getAnalysisUsage(AnalysisUsage &AU) const override {
45       AU.addRequiredID(BreakCriticalEdgesID);
46       AU.addPreservedID(BreakCriticalEdgesID);
47     }
49     bool valueEscapes(const Instruction *Inst) const {
50       const BasicBlock *BB = Inst->getParent();
51       for (const User *U : Inst->users()) {
52         const Instruction *UI = cast<Instruction>(U);
53         if (UI->getParent() != BB || isa<PHINode>(UI))
54           return true;
55       }
56       return false;
57     }
59     bool runOnFunction(Function &F) override;
60   };
61 }
63 char RegToMem::ID = 0;
64 INITIALIZE_PASS_BEGIN(RegToMem, "reg2mem", "Demote all values to stack slots",
65                 false, false)
66 INITIALIZE_PASS_DEPENDENCY(BreakCriticalEdges)
67 INITIALIZE_PASS_END(RegToMem, "reg2mem", "Demote all values to stack slots",
68                 false, false)
70 bool RegToMem::runOnFunction(Function &F) {
71   if (F.isDeclaration())
72     return false;
74   // Insert all new allocas into entry block.
75   BasicBlock *BBEntry = &F.getEntryBlock();
76   assert(pred_begin(BBEntry) == pred_end(BBEntry) &&
77          "Entry block to function must not have predecessors!");
79   // Find first non-alloca instruction and create insertion point. This is
80   // safe if block is well-formed: it always have terminator, otherwise
81   // we'll get and assertion.
82   BasicBlock::iterator I = BBEntry->begin();
83   while (isa<AllocaInst>(I)) ++I;
85   CastInst *AllocaInsertionPoint =
86     new BitCastInst(Constant::getNullValue(Type::getInt32Ty(F.getContext())),
87                     Type::getInt32Ty(F.getContext()),
88                     "reg2mem alloca point", I);
90   // Find the escaped instructions. But don't create stack slots for
91   // allocas in entry block.
92   std::list<Instruction*> WorkList;
93   for (Function::iterator ibb = F.begin(), ibe = F.end();
94        ibb != ibe; ++ibb)
95     for (BasicBlock::iterator iib = ibb->begin(), iie = ibb->end();
96          iib != iie; ++iib) {
97       if (!(isa<AllocaInst>(iib) && iib->getParent() == BBEntry) &&
98           valueEscapes(iib)) {
99         WorkList.push_front(&*iib);
100       }
101     }
103   // Demote escaped instructions
104   NumRegsDemoted += WorkList.size();
105   for (std::list<Instruction*>::iterator ilb = WorkList.begin(),
106        ile = WorkList.end(); ilb != ile; ++ilb)
107     DemoteRegToStack(**ilb, false, AllocaInsertionPoint);
109   WorkList.clear();
111   // Find all phi's
112   for (Function::iterator ibb = F.begin(), ibe = F.end();
113        ibb != ibe; ++ibb)
114     for (BasicBlock::iterator iib = ibb->begin(), iie = ibb->end();
115          iib != iie; ++iib)
116       if (isa<PHINode>(iib))
117         WorkList.push_front(&*iib);
119   // Demote phi nodes
120   NumPhisDemoted += WorkList.size();
121   for (std::list<Instruction*>::iterator ilb = WorkList.begin(),
122        ile = WorkList.end(); ilb != ile; ++ilb)
123     DemotePHIToStack(cast<PHINode>(*ilb), AllocaInsertionPoint);
125   return true;
129 // createDemoteRegisterToMemory - Provide an entry point to create this pass.
130 char &llvm::DemoteRegisterToMemoryID = RegToMem::ID;
131 FunctionPass *llvm::createDemoteRegisterToMemoryPass() {
132   return new RegToMem();