]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - lib/Transforms/Utils/InlineFunction.cpp
Refuse to inline two functions which use different personality functions.
[opencl/llvm.git] / lib / Transforms / Utils / InlineFunction.cpp
1 //===- InlineFunction.cpp - Code to perform function inlining -------------===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements inlining of a function into a call site, resolving
11 // parameters and the return value as appropriate.
12 //
13 // The code in this file for handling inlines through invoke
14 // instructions preserves semantics only under some assumptions about
15 // the behavior of unwinders which correspond to gcc-style libUnwind
16 // exception personality functions.  Eventually the IR will be
17 // improved to make this unnecessary, but until then, this code is
18 // marked [LIBUNWIND].
19 //
20 //===----------------------------------------------------------------------===//
22 #include "llvm/Transforms/Utils/Cloning.h"
23 #include "llvm/Constants.h"
24 #include "llvm/DerivedTypes.h"
25 #include "llvm/Module.h"
26 #include "llvm/Instructions.h"
27 #include "llvm/IntrinsicInst.h"
28 #include "llvm/Intrinsics.h"
29 #include "llvm/Attributes.h"
30 #include "llvm/Analysis/CallGraph.h"
31 #include "llvm/Analysis/DebugInfo.h"
32 #include "llvm/Analysis/InstructionSimplify.h"
33 #include "llvm/Target/TargetData.h"
34 #include "llvm/Transforms/Utils/Local.h"
35 #include "llvm/ADT/SmallVector.h"
36 #include "llvm/ADT/StringExtras.h"
37 #include "llvm/Support/CallSite.h"
38 #include "llvm/Support/IRBuilder.h"
39 using namespace llvm;
41 bool llvm::InlineFunction(CallInst *CI, InlineFunctionInfo &IFI) {
42   return InlineFunction(CallSite(CI), IFI);
43 }
44 bool llvm::InlineFunction(InvokeInst *II, InlineFunctionInfo &IFI) {
45   return InlineFunction(CallSite(II), IFI);
46 }
48 /// [LIBUNWIND] Look for an llvm.eh.exception call in the given block.
49 static EHExceptionInst *findExceptionInBlock(BasicBlock *bb) {
50   for (BasicBlock::iterator i = bb->begin(), e = bb->end(); i != e; i++) {
51     EHExceptionInst *exn = dyn_cast<EHExceptionInst>(i);
52     if (exn) return exn;
53   }
55   return 0;
56 }
58 /// [LIBUNWIND] Look for the 'best' llvm.eh.selector instruction for
59 /// the given llvm.eh.exception call.
60 static EHSelectorInst *findSelectorForException(EHExceptionInst *exn) {
61   BasicBlock *exnBlock = exn->getParent();
63   EHSelectorInst *outOfBlockSelector = 0;
64   for (Instruction::use_iterator
65          ui = exn->use_begin(), ue = exn->use_end(); ui != ue; ++ui) {
66     EHSelectorInst *sel = dyn_cast<EHSelectorInst>(*ui);
67     if (!sel) continue;
69     // Immediately accept an eh.selector in the same block as the
70     // excepton call.
71     if (sel->getParent() == exnBlock) return sel;
73     // Otherwise, use the first selector we see.
74     if (!outOfBlockSelector) outOfBlockSelector = sel;
75   }
77   return outOfBlockSelector;
78 }
80 /// [LIBUNWIND] Find the (possibly absent) call to @llvm.eh.selector
81 /// in the given landing pad.  In principle, llvm.eh.exception is
82 /// required to be in the landing pad; in practice, SplitCriticalEdge
83 /// can break that invariant, and then inlining can break it further.
84 /// There's a real need for a reliable solution here, but until that
85 /// happens, we have some fragile workarounds here.
86 static EHSelectorInst *findSelectorForLandingPad(BasicBlock *lpad) {
87   // Look for an exception call in the actual landing pad.
88   EHExceptionInst *exn = findExceptionInBlock(lpad);
89   if (exn) return findSelectorForException(exn);
91   // Okay, if that failed, look for one in an obvious successor.  If
92   // we find one, we'll fix the IR by moving things back to the
93   // landing pad.
95   bool dominates = true; // does the lpad dominate the exn call
96   BasicBlock *nonDominated = 0; // if not, the first non-dominated block
97   BasicBlock *lastDominated = 0; // and the block which branched to it
99   BasicBlock *exnBlock = lpad;
101   // We need to protect against lpads that lead into infinite loops.
102   SmallPtrSet<BasicBlock*,4> visited;
103   visited.insert(exnBlock);
105   do {
106     // We're not going to apply this hack to anything more complicated
107     // than a series of unconditional branches, so if the block
108     // doesn't terminate in an unconditional branch, just fail.  More
109     // complicated cases can arise when, say, sinking a call into a
110     // split unwind edge and then inlining it; but that can do almost
111     // *anything* to the CFG, including leaving the selector
112     // completely unreachable.  The only way to fix that properly is
113     // to (1) prohibit transforms which move the exception or selector
114     // values away from the landing pad, e.g. by producing them with
115     // instructions that are pinned to an edge like a phi, or
116     // producing them with not-really-instructions, and (2) making
117     // transforms which split edges deal with that.
118     BranchInst *branch = dyn_cast<BranchInst>(&exnBlock->back());
119     if (!branch || branch->isConditional()) return 0;
121     BasicBlock *successor = branch->getSuccessor(0);
123     // Fail if we found an infinite loop.
124     if (!visited.insert(successor)) return 0;
126     // If the successor isn't dominated by exnBlock:
127     if (!successor->getSinglePredecessor()) {
128       // We don't want to have to deal with threading the exception
129       // through multiple levels of phi, so give up if we've already
130       // followed a non-dominating edge.
131       if (!dominates) return 0;
133       // Otherwise, remember this as a non-dominating edge.
134       dominates = false;
135       nonDominated = successor;
136       lastDominated = exnBlock;
137     }
139     exnBlock = successor;
141     // Can we stop here?
142     exn = findExceptionInBlock(exnBlock);
143   } while (!exn);
145   // Look for a selector call for the exception we found.
146   EHSelectorInst *selector = findSelectorForException(exn);
147   if (!selector) return 0;
149   // The easy case is when the landing pad still dominates the
150   // exception call, in which case we can just move both calls back to
151   // the landing pad.
152   if (dominates) {
153     selector->moveBefore(lpad->getFirstNonPHI());
154     exn->moveBefore(selector);
155     return selector;
156   }
158   // Otherwise, we have to split at the first non-dominating block.
159   // The CFG looks basically like this:
160   //    lpad:
161   //      phis_0
162   //      insnsAndBranches_1
163   //      br label %nonDominated
164   //    nonDominated:
165   //      phis_2
166   //      insns_3
167   //      %exn = call i8* @llvm.eh.exception()
168   //      insnsAndBranches_4
169   //      %selector = call @llvm.eh.selector(i8* %exn, ...
170   // We need to turn this into:
171   //    lpad:
172   //      phis_0
173   //      %exn0 = call i8* @llvm.eh.exception()
174   //      %selector0 = call @llvm.eh.selector(i8* %exn0, ...
175   //      insnsAndBranches_1
176   //      br label %split // from lastDominated
177   //    nonDominated:
178   //      phis_2 (without edge from lastDominated)
179   //      %exn1 = call i8* @llvm.eh.exception()
180   //      %selector1 = call i8* @llvm.eh.selector(i8* %exn1, ...
181   //      br label %split
182   //    split:
183   //      phis_2 (edge from lastDominated, edge from split)
184   //      %exn = phi ...
185   //      %selector = phi ...
186   //      insns_3
187   //      insnsAndBranches_4
189   assert(nonDominated);
190   assert(lastDominated);
192   // First, make clones of the intrinsics to go in lpad.
193   EHExceptionInst *lpadExn = cast<EHExceptionInst>(exn->clone());
194   EHSelectorInst *lpadSelector = cast<EHSelectorInst>(selector->clone());
195   lpadSelector->setArgOperand(0, lpadExn);
196   lpadSelector->insertBefore(lpad->getFirstNonPHI());
197   lpadExn->insertBefore(lpadSelector);
199   // Split the non-dominated block.
200   BasicBlock *split =
201     nonDominated->splitBasicBlock(nonDominated->getFirstNonPHI(),
202                                   nonDominated->getName() + ".lpad-fix");
204   // Redirect the last dominated branch there.
205   cast<BranchInst>(lastDominated->back()).setSuccessor(0, split);
207   // Move the existing intrinsics to the end of the old block.
208   selector->moveBefore(&nonDominated->back());
209   exn->moveBefore(selector);
211   Instruction *splitIP = &split->front();
213   // For all the phis in nonDominated, make a new phi in split to join
214   // that phi with the edge from lastDominated.
215   for (BasicBlock::iterator
216          i = nonDominated->begin(), e = nonDominated->end(); i != e; ++i) {
217     PHINode *phi = dyn_cast<PHINode>(i);
218     if (!phi) break;
220     PHINode *splitPhi = PHINode::Create(phi->getType(), 2, phi->getName(),
221                                         splitIP);
222     phi->replaceAllUsesWith(splitPhi);
223     splitPhi->addIncoming(phi, nonDominated);
224     splitPhi->addIncoming(phi->removeIncomingValue(lastDominated),
225                           lastDominated);
226   }
228   // Make new phis for the exception and selector.
229   PHINode *exnPhi = PHINode::Create(exn->getType(), 2, "", splitIP);
230   exn->replaceAllUsesWith(exnPhi);
231   selector->setArgOperand(0, exn); // except for this use
232   exnPhi->addIncoming(exn, nonDominated);
233   exnPhi->addIncoming(lpadExn, lastDominated);
235   PHINode *selectorPhi = PHINode::Create(selector->getType(), 2, "", splitIP);
236   selector->replaceAllUsesWith(selectorPhi);
237   selectorPhi->addIncoming(selector, nonDominated);
238   selectorPhi->addIncoming(lpadSelector, lastDominated);
240   return lpadSelector;
243 namespace {
244   /// A class for recording information about inlining through an invoke.
245   class InvokeInliningInfo {
246     BasicBlock *OuterUnwindDest;
247     EHSelectorInst *OuterSelector;
248     BasicBlock *InnerUnwindDest;
249     PHINode *InnerExceptionPHI;
250     PHINode *InnerSelectorPHI;
251     SmallVector<Value*, 8> UnwindDestPHIValues;
253   public:
254     InvokeInliningInfo(InvokeInst *II) :
255       OuterUnwindDest(II->getUnwindDest()), OuterSelector(0),
256       InnerUnwindDest(0), InnerExceptionPHI(0), InnerSelectorPHI(0) {
258       // If there are PHI nodes in the unwind destination block, we
259       // need to keep track of which values came into them from the
260       // invoke before removing the edge from this block.
261       llvm::BasicBlock *invokeBB = II->getParent();
262       for (BasicBlock::iterator I = OuterUnwindDest->begin();
263              isa<PHINode>(I); ++I) {
264         // Save the value to use for this edge.
265         PHINode *phi = cast<PHINode>(I);
266         UnwindDestPHIValues.push_back(phi->getIncomingValueForBlock(invokeBB));
267       }
268     }
270     /// The outer unwind destination is the target of unwind edges
271     /// introduced for calls within the inlined function.
272     BasicBlock *getOuterUnwindDest() const {
273       return OuterUnwindDest;
274     }
276     EHSelectorInst *getOuterSelector() {
277       if (!OuterSelector)
278         OuterSelector = findSelectorForLandingPad(OuterUnwindDest);
279       return OuterSelector;
280     }
282     BasicBlock *getInnerUnwindDest();
284     bool forwardEHResume(CallInst *call, BasicBlock *src);
286     /// Add incoming-PHI values to the unwind destination block for
287     /// the given basic block, using the values for the original
288     /// invoke's source block.
289     void addIncomingPHIValuesFor(BasicBlock *BB) const {
290       addIncomingPHIValuesForInto(BB, OuterUnwindDest);
291     }
293     void addIncomingPHIValuesForInto(BasicBlock *src, BasicBlock *dest) const {
294       BasicBlock::iterator I = dest->begin();
295       for (unsigned i = 0, e = UnwindDestPHIValues.size(); i != e; ++i, ++I) {
296         PHINode *phi = cast<PHINode>(I);
297         phi->addIncoming(UnwindDestPHIValues[i], src);
298       }
299     }
300   };
303 /// Get or create a target for the branch out of rewritten calls to
304 /// llvm.eh.resume.
305 BasicBlock *InvokeInliningInfo::getInnerUnwindDest() {
306   if (InnerUnwindDest) return InnerUnwindDest;
308   // Find and hoist the llvm.eh.exception and llvm.eh.selector calls
309   // in the outer landing pad to immediately following the phis.
310   EHSelectorInst *selector = getOuterSelector();
311   if (!selector) return 0;
313   // The call to llvm.eh.exception *must* be in the landing pad.
314   Instruction *exn = cast<Instruction>(selector->getArgOperand(0));
315   assert(exn->getParent() == OuterUnwindDest);
317   // TODO: recognize when we've already done this, so that we don't
318   // get a linear number of these when inlining calls into lots of
319   // invokes with the same landing pad.
321   // Do the hoisting.
322   Instruction *splitPoint = exn->getParent()->getFirstNonPHI();
323   assert(splitPoint != selector && "selector-on-exception dominance broken!");
324   if (splitPoint == exn) {
325     selector->removeFromParent();
326     selector->insertAfter(exn);
327     splitPoint = selector->getNextNode();
328   } else {
329     exn->moveBefore(splitPoint);
330     selector->moveBefore(splitPoint);
331   }
333   // Split the landing pad.
334   InnerUnwindDest = OuterUnwindDest->splitBasicBlock(splitPoint,
335                                         OuterUnwindDest->getName() + ".body");
337   // The number of incoming edges we expect to the inner landing pad.
338   const unsigned phiCapacity = 2;
340   // Create corresponding new phis for all the phis in the outer landing pad.
341   BasicBlock::iterator insertPoint = InnerUnwindDest->begin();
342   BasicBlock::iterator I = OuterUnwindDest->begin();
343   for (unsigned i = 0, e = UnwindDestPHIValues.size(); i != e; ++i, ++I) {
344     PHINode *outerPhi = cast<PHINode>(I);
345     PHINode *innerPhi = PHINode::Create(outerPhi->getType(), phiCapacity,
346                                         outerPhi->getName() + ".lpad-body",
347                                         insertPoint);
348     outerPhi->replaceAllUsesWith(innerPhi);
349     innerPhi->addIncoming(outerPhi, OuterUnwindDest);
350   }
352   // Create a phi for the exception value...
353   InnerExceptionPHI = PHINode::Create(exn->getType(), phiCapacity,
354                                       "exn.lpad-body", insertPoint);
355   exn->replaceAllUsesWith(InnerExceptionPHI);
356   selector->setArgOperand(0, exn); // restore this use
357   InnerExceptionPHI->addIncoming(exn, OuterUnwindDest);
359   // ...and the selector.
360   InnerSelectorPHI = PHINode::Create(selector->getType(), phiCapacity,
361                                      "selector.lpad-body", insertPoint);
362   selector->replaceAllUsesWith(InnerSelectorPHI);
363   InnerSelectorPHI->addIncoming(selector, OuterUnwindDest);
365   // All done.
366   return InnerUnwindDest;
369 /// [LIBUNWIND] Try to forward the given call, which logically occurs
370 /// at the end of the given block, as a branch to the inner unwind
371 /// block.  Returns true if the call was forwarded.
372 bool InvokeInliningInfo::forwardEHResume(CallInst *call, BasicBlock *src) {
373   // First, check whether this is a call to the intrinsic.
374   Function *fn = dyn_cast<Function>(call->getCalledValue());
375   if (!fn || fn->getName() != "llvm.eh.resume")
376     return false;
377   
378   // At this point, we need to return true on all paths, because
379   // otherwise we'll construct an invoke of the intrinsic, which is
380   // not well-formed.
382   // Try to find or make an inner unwind dest, which will fail if we
383   // can't find a selector call for the outer unwind dest.
384   BasicBlock *dest = getInnerUnwindDest();
385   bool hasSelector = (dest != 0);
387   // If we failed, just use the outer unwind dest, dropping the
388   // exception and selector on the floor.
389   if (!hasSelector)
390     dest = OuterUnwindDest;
392   // Make a branch.
393   BranchInst::Create(dest, src);
395   // Update the phis in the destination.  They were inserted in an
396   // order which makes this work.
397   addIncomingPHIValuesForInto(src, dest);
399   if (hasSelector) {
400     InnerExceptionPHI->addIncoming(call->getArgOperand(0), src);
401     InnerSelectorPHI->addIncoming(call->getArgOperand(1), src);
402   }
404   return true;
407 /// [LIBUNWIND] Check whether this selector is "only cleanups":
408 ///   call i32 @llvm.eh.selector(blah, blah, i32 0)
409 static bool isCleanupOnlySelector(EHSelectorInst *selector) {
410   if (selector->getNumArgOperands() != 3) return false;
411   ConstantInt *val = dyn_cast<ConstantInt>(selector->getArgOperand(2));
412   return (val && val->isZero());
415 /// HandleCallsInBlockInlinedThroughInvoke - When we inline a basic block into
416 /// an invoke, we have to turn all of the calls that can throw into
417 /// invokes.  This function analyze BB to see if there are any calls, and if so,
418 /// it rewrites them to be invokes that jump to InvokeDest and fills in the PHI
419 /// nodes in that block with the values specified in InvokeDestPHIValues.
420 ///
421 /// Returns true to indicate that the next block should be skipped.
422 static bool HandleCallsInBlockInlinedThroughInvoke(BasicBlock *BB,
423                                                    InvokeInliningInfo &Invoke) {
424   for (BasicBlock::iterator BBI = BB->begin(), E = BB->end(); BBI != E; ) {
425     Instruction *I = BBI++;
426     
427     // We only need to check for function calls: inlined invoke
428     // instructions require no special handling.
429     CallInst *CI = dyn_cast<CallInst>(I);
430     if (CI == 0) continue;
432     // LIBUNWIND: merge selector instructions.
433     if (EHSelectorInst *Inner = dyn_cast<EHSelectorInst>(CI)) {
434       EHSelectorInst *Outer = Invoke.getOuterSelector();
435       if (!Outer) continue;
437       bool innerIsOnlyCleanup = isCleanupOnlySelector(Inner);
438       bool outerIsOnlyCleanup = isCleanupOnlySelector(Outer);
440       // If both selectors contain only cleanups, we don't need to do
441       // anything.  TODO: this is really just a very specific instance
442       // of a much more general optimization.
443       if (innerIsOnlyCleanup && outerIsOnlyCleanup) continue;
445       // Otherwise, we just append the outer selector to the inner selector.
446       SmallVector<Value*, 16> NewSelector;
447       for (unsigned i = 0, e = Inner->getNumArgOperands(); i != e; ++i)
448         NewSelector.push_back(Inner->getArgOperand(i));
449       for (unsigned i = 2, e = Outer->getNumArgOperands(); i != e; ++i)
450         NewSelector.push_back(Outer->getArgOperand(i));
452       CallInst *NewInner =
453         IRBuilder<>(Inner).CreateCall(Inner->getCalledValue(), NewSelector);
454       // No need to copy attributes, calling convention, etc.
455       NewInner->takeName(Inner);
456       Inner->replaceAllUsesWith(NewInner);
457       Inner->eraseFromParent();
458       continue;
459     }
460     
461     // If this call cannot unwind, don't convert it to an invoke.
462     if (CI->doesNotThrow())
463       continue;
464     
465     // Convert this function call into an invoke instruction.
466     // First, split the basic block.
467     BasicBlock *Split = BB->splitBasicBlock(CI, CI->getName()+".noexc");
469     // Delete the unconditional branch inserted by splitBasicBlock
470     BB->getInstList().pop_back();
472     // LIBUNWIND: If this is a call to @llvm.eh.resume, just branch
473     // directly to the new landing pad.
474     if (Invoke.forwardEHResume(CI, BB)) {
475       // TODO: 'Split' is now unreachable; clean it up.
477       // We want to leave the original call intact so that the call
478       // graph and other structures won't get misled.  We also have to
479       // avoid processing the next block, or we'll iterate here forever.
480       return true;
481     }
483     // Otherwise, create the new invoke instruction.
484     ImmutableCallSite CS(CI);
485     SmallVector<Value*, 8> InvokeArgs(CS.arg_begin(), CS.arg_end());
486     InvokeInst *II =
487       InvokeInst::Create(CI->getCalledValue(), Split,
488                          Invoke.getOuterUnwindDest(),
489                          InvokeArgs, CI->getName(), BB);
490     II->setCallingConv(CI->getCallingConv());
491     II->setAttributes(CI->getAttributes());
492     
493     // Make sure that anything using the call now uses the invoke!  This also
494     // updates the CallGraph if present, because it uses a WeakVH.
495     CI->replaceAllUsesWith(II);
497     Split->getInstList().pop_front();  // Delete the original call
499     // Update any PHI nodes in the exceptional block to indicate that
500     // there is now a new entry in them.
501     Invoke.addIncomingPHIValuesFor(BB);
502     return false;
503   }
505   return false;
507   
509 /// HandleInlinedInvoke - If we inlined an invoke site, we need to convert calls
510 /// in the body of the inlined function into invokes and turn unwind
511 /// instructions into branches to the invoke unwind dest.
512 ///
513 /// II is the invoke instruction being inlined.  FirstNewBlock is the first
514 /// block of the inlined code (the last block is the end of the function),
515 /// and InlineCodeInfo is information about the code that got inlined.
516 static void HandleInlinedInvoke(InvokeInst *II, BasicBlock *FirstNewBlock,
517                                 ClonedCodeInfo &InlinedCodeInfo) {
518   BasicBlock *InvokeDest = II->getUnwindDest();
520   Function *Caller = FirstNewBlock->getParent();
522   // The inlined code is currently at the end of the function, scan from the
523   // start of the inlined code to its end, checking for stuff we need to
524   // rewrite.  If the code doesn't have calls or unwinds, we know there is
525   // nothing to rewrite.
526   if (!InlinedCodeInfo.ContainsCalls && !InlinedCodeInfo.ContainsUnwinds) {
527     // Now that everything is happy, we have one final detail.  The PHI nodes in
528     // the exception destination block still have entries due to the original
529     // invoke instruction.  Eliminate these entries (which might even delete the
530     // PHI node) now.
531     InvokeDest->removePredecessor(II->getParent());
532     return;
533   }
535   InvokeInliningInfo Invoke(II);
536   
537   for (Function::iterator BB = FirstNewBlock, E = Caller->end(); BB != E; ++BB){
538     if (InlinedCodeInfo.ContainsCalls)
539       if (HandleCallsInBlockInlinedThroughInvoke(BB, Invoke)) {
540         // Honor a request to skip the next block.  We don't need to
541         // consider UnwindInsts in this case either.
542         ++BB;
543         continue;
544       }
546     if (UnwindInst *UI = dyn_cast<UnwindInst>(BB->getTerminator())) {
547       // An UnwindInst requires special handling when it gets inlined into an
548       // invoke site.  Once this happens, we know that the unwind would cause
549       // a control transfer to the invoke exception destination, so we can
550       // transform it into a direct branch to the exception destination.
551       BranchInst::Create(InvokeDest, UI);
553       // Delete the unwind instruction!
554       UI->eraseFromParent();
556       // Update any PHI nodes in the exceptional block to indicate that
557       // there is now a new entry in them.
558       Invoke.addIncomingPHIValuesFor(BB);
559     }
560   }
562   // Now that everything is happy, we have one final detail.  The PHI nodes in
563   // the exception destination block still have entries due to the original
564   // invoke instruction.  Eliminate these entries (which might even delete the
565   // PHI node) now.
566   InvokeDest->removePredecessor(II->getParent());
569 /// UpdateCallGraphAfterInlining - Once we have cloned code over from a callee
570 /// into the caller, update the specified callgraph to reflect the changes we
571 /// made.  Note that it's possible that not all code was copied over, so only
572 /// some edges of the callgraph may remain.
573 static void UpdateCallGraphAfterInlining(CallSite CS,
574                                          Function::iterator FirstNewBlock,
575                                          ValueToValueMapTy &VMap,
576                                          InlineFunctionInfo &IFI) {
577   CallGraph &CG = *IFI.CG;
578   const Function *Caller = CS.getInstruction()->getParent()->getParent();
579   const Function *Callee = CS.getCalledFunction();
580   CallGraphNode *CalleeNode = CG[Callee];
581   CallGraphNode *CallerNode = CG[Caller];
583   // Since we inlined some uninlined call sites in the callee into the caller,
584   // add edges from the caller to all of the callees of the callee.
585   CallGraphNode::iterator I = CalleeNode->begin(), E = CalleeNode->end();
587   // Consider the case where CalleeNode == CallerNode.
588   CallGraphNode::CalledFunctionsVector CallCache;
589   if (CalleeNode == CallerNode) {
590     CallCache.assign(I, E);
591     I = CallCache.begin();
592     E = CallCache.end();
593   }
595   for (; I != E; ++I) {
596     const Value *OrigCall = I->first;
598     ValueToValueMapTy::iterator VMI = VMap.find(OrigCall);
599     // Only copy the edge if the call was inlined!
600     if (VMI == VMap.end() || VMI->second == 0)
601       continue;
602     
603     // If the call was inlined, but then constant folded, there is no edge to
604     // add.  Check for this case.
605     Instruction *NewCall = dyn_cast<Instruction>(VMI->second);
606     if (NewCall == 0) continue;
608     // Remember that this call site got inlined for the client of
609     // InlineFunction.
610     IFI.InlinedCalls.push_back(NewCall);
612     // It's possible that inlining the callsite will cause it to go from an
613     // indirect to a direct call by resolving a function pointer.  If this
614     // happens, set the callee of the new call site to a more precise
615     // destination.  This can also happen if the call graph node of the caller
616     // was just unnecessarily imprecise.
617     if (I->second->getFunction() == 0)
618       if (Function *F = CallSite(NewCall).getCalledFunction()) {
619         // Indirect call site resolved to direct call.
620         CallerNode->addCalledFunction(CallSite(NewCall), CG[F]);
622         continue;
623       }
625     CallerNode->addCalledFunction(CallSite(NewCall), I->second);
626   }
627   
628   // Update the call graph by deleting the edge from Callee to Caller.  We must
629   // do this after the loop above in case Caller and Callee are the same.
630   CallerNode->removeCallEdgeFor(CS);
633 /// HandleByValArgument - When inlining a call site that has a byval argument,
634 /// we have to make the implicit memcpy explicit by adding it.
635 static Value *HandleByValArgument(Value *Arg, Instruction *TheCall,
636                                   const Function *CalledFunc,
637                                   InlineFunctionInfo &IFI,
638                                   unsigned ByValAlignment) {
639   Type *AggTy = cast<PointerType>(Arg->getType())->getElementType();
641   // If the called function is readonly, then it could not mutate the caller's
642   // copy of the byval'd memory.  In this case, it is safe to elide the copy and
643   // temporary.
644   if (CalledFunc->onlyReadsMemory()) {
645     // If the byval argument has a specified alignment that is greater than the
646     // passed in pointer, then we either have to round up the input pointer or
647     // give up on this transformation.
648     if (ByValAlignment <= 1)  // 0 = unspecified, 1 = no particular alignment.
649       return Arg;
651     // If the pointer is already known to be sufficiently aligned, or if we can
652     // round it up to a larger alignment, then we don't need a temporary.
653     if (getOrEnforceKnownAlignment(Arg, ByValAlignment,
654                                    IFI.TD) >= ByValAlignment)
655       return Arg;
656     
657     // Otherwise, we have to make a memcpy to get a safe alignment.  This is bad
658     // for code quality, but rarely happens and is required for correctness.
659   }
660   
661   LLVMContext &Context = Arg->getContext();
663   Type *VoidPtrTy = Type::getInt8PtrTy(Context);
664   
665   // Create the alloca.  If we have TargetData, use nice alignment.
666   unsigned Align = 1;
667   if (IFI.TD)
668     Align = IFI.TD->getPrefTypeAlignment(AggTy);
669   
670   // If the byval had an alignment specified, we *must* use at least that
671   // alignment, as it is required by the byval argument (and uses of the
672   // pointer inside the callee).
673   Align = std::max(Align, ByValAlignment);
674   
675   Function *Caller = TheCall->getParent()->getParent(); 
676   
677   Value *NewAlloca = new AllocaInst(AggTy, 0, Align, Arg->getName(), 
678                                     &*Caller->begin()->begin());
679   // Emit a memcpy.
680   Type *Tys[3] = {VoidPtrTy, VoidPtrTy, Type::getInt64Ty(Context)};
681   Function *MemCpyFn = Intrinsic::getDeclaration(Caller->getParent(),
682                                                  Intrinsic::memcpy, 
683                                                  Tys);
684   Value *DestCast = new BitCastInst(NewAlloca, VoidPtrTy, "tmp", TheCall);
685   Value *SrcCast = new BitCastInst(Arg, VoidPtrTy, "tmp", TheCall);
686   
687   Value *Size;
688   if (IFI.TD == 0)
689     Size = ConstantExpr::getSizeOf(AggTy);
690   else
691     Size = ConstantInt::get(Type::getInt64Ty(Context),
692                             IFI.TD->getTypeStoreSize(AggTy));
693   
694   // Always generate a memcpy of alignment 1 here because we don't know
695   // the alignment of the src pointer.  Other optimizations can infer
696   // better alignment.
697   Value *CallArgs[] = {
698     DestCast, SrcCast, Size,
699     ConstantInt::get(Type::getInt32Ty(Context), 1),
700     ConstantInt::getFalse(Context) // isVolatile
701   };
702   IRBuilder<>(TheCall).CreateCall(MemCpyFn, CallArgs);
703   
704   // Uses of the argument in the function should use our new alloca
705   // instead.
706   return NewAlloca;
709 // isUsedByLifetimeMarker - Check whether this Value is used by a lifetime
710 // intrinsic.
711 static bool isUsedByLifetimeMarker(Value *V) {
712   for (Value::use_iterator UI = V->use_begin(), UE = V->use_end(); UI != UE;
713        ++UI) {
714     if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(*UI)) {
715       switch (II->getIntrinsicID()) {
716       default: break;
717       case Intrinsic::lifetime_start:
718       case Intrinsic::lifetime_end:
719         return true;
720       }
721     }
722   }
723   return false;
726 // hasLifetimeMarkers - Check whether the given alloca already has
727 // lifetime.start or lifetime.end intrinsics.
728 static bool hasLifetimeMarkers(AllocaInst *AI) {
729   Type *Int8PtrTy = Type::getInt8PtrTy(AI->getType()->getContext());
730   if (AI->getType() == Int8PtrTy)
731     return isUsedByLifetimeMarker(AI);
733   // Do a scan to find all the casts to i8*.
734   for (Value::use_iterator I = AI->use_begin(), E = AI->use_end(); I != E;
735        ++I) {
736     if (I->getType() != Int8PtrTy) continue;
737     if (I->stripPointerCasts() != AI) continue;
738     if (isUsedByLifetimeMarker(*I))
739       return true;
740   }
741   return false;
744 /// updateInlinedAtInfo - Helper function used by fixupLineNumbers to recursively
745 /// update InlinedAtEntry of a DebugLoc.
746 static DebugLoc updateInlinedAtInfo(const DebugLoc &DL, 
747                                     const DebugLoc &InlinedAtDL,
748                                     LLVMContext &Ctx) {
749   if (MDNode *IA = DL.getInlinedAt(Ctx)) {
750     DebugLoc NewInlinedAtDL 
751       = updateInlinedAtInfo(DebugLoc::getFromDILocation(IA), InlinedAtDL, Ctx);
752     return DebugLoc::get(DL.getLine(), DL.getCol(), DL.getScope(Ctx),
753                          NewInlinedAtDL.getAsMDNode(Ctx));
754   }
755                                              
756   return DebugLoc::get(DL.getLine(), DL.getCol(), DL.getScope(Ctx),
757                        InlinedAtDL.getAsMDNode(Ctx));
761 /// fixupLineNumbers - Update inlined instructions' line numbers to 
762 /// to encode location where these instructions are inlined.
763 static void fixupLineNumbers(Function *Fn, Function::iterator FI,
764                               Instruction *TheCall) {
765   DebugLoc TheCallDL = TheCall->getDebugLoc();
766   if (TheCallDL.isUnknown())
767     return;
769   for (; FI != Fn->end(); ++FI) {
770     for (BasicBlock::iterator BI = FI->begin(), BE = FI->end();
771          BI != BE; ++BI) {
772       DebugLoc DL = BI->getDebugLoc();
773       if (!DL.isUnknown()) {
774         BI->setDebugLoc(updateInlinedAtInfo(DL, TheCallDL, BI->getContext()));
775         if (DbgValueInst *DVI = dyn_cast<DbgValueInst>(BI)) {
776           LLVMContext &Ctx = BI->getContext();
777           MDNode *InlinedAt = BI->getDebugLoc().getInlinedAt(Ctx);
778           DVI->setOperand(2, createInlinedVariable(DVI->getVariable(), 
779                                                    InlinedAt, Ctx));
780         }
781       }
782     }
783   }
786 // InlineFunction - This function inlines the called function into the basic
787 // block of the caller.  This returns false if it is not possible to inline this
788 // call.  The program is still in a well defined state if this occurs though.
789 //
790 // Note that this only does one level of inlining.  For example, if the
791 // instruction 'call B' is inlined, and 'B' calls 'C', then the call to 'C' now
792 // exists in the instruction stream.  Similarly this will inline a recursive
793 // function by one level.
794 //
795 bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
796   Instruction *TheCall = CS.getInstruction();
797   LLVMContext &Context = TheCall->getContext();
798   assert(TheCall->getParent() && TheCall->getParent()->getParent() &&
799          "Instruction not in function!");
801   // If IFI has any state in it, zap it before we fill it in.
802   IFI.reset();
803   
804   const Function *CalledFunc = CS.getCalledFunction();
805   if (CalledFunc == 0 ||          // Can't inline external function or indirect
806       CalledFunc->isDeclaration() || // call, or call to a vararg function!
807       CalledFunc->getFunctionType()->isVarArg()) return false;
809   // If the call to the callee is not a tail call, we must clear the 'tail'
810   // flags on any calls that we inline.
811   bool MustClearTailCallFlags =
812     !(isa<CallInst>(TheCall) && cast<CallInst>(TheCall)->isTailCall());
814   // If the call to the callee cannot throw, set the 'nounwind' flag on any
815   // calls that we inline.
816   bool MarkNoUnwind = CS.doesNotThrow();
818   BasicBlock *OrigBB = TheCall->getParent();
819   Function *Caller = OrigBB->getParent();
821   // GC poses two hazards to inlining, which only occur when the callee has GC:
822   //  1. If the caller has no GC, then the callee's GC must be propagated to the
823   //     caller.
824   //  2. If the caller has a differing GC, it is invalid to inline.
825   if (CalledFunc->hasGC()) {
826     if (!Caller->hasGC())
827       Caller->setGC(CalledFunc->getGC());
828     else if (CalledFunc->getGC() != Caller->getGC())
829       return false;
830   }
832   // Find the personality function used by the landing pads of the caller. If it
833   // exists, then check to see that it matches the personality function used in
834   // the callee.
835   for (Function::const_iterator
836          I = Caller->begin(), E = Caller->end(); I != E; ++I)
837     if (const InvokeInst *II = dyn_cast<InvokeInst>(I->getTerminator())) {
838       const BasicBlock *BB = II->getUnwindDest();
839       // FIXME: This 'isa' here should become go away once the new EH system is
840       // in place.
841       if (!isa<LandingPadInst>(BB->getFirstNonPHI()))
842         continue;
843       const LandingPadInst *LP = cast<LandingPadInst>(BB->getFirstNonPHI());
844       const Value *CallerPersFn = LP->getPersonalityFn();
846       // If the personality functions match, then we can perform the
847       // inlining. Otherwise, we can't inline.
848       // TODO: This isn't 100% true. Some personality functions are proper
849       //       supersets of others and can be used in place of the other.
850       for (Function::const_iterator
851              I = CalledFunc->begin(), E = CalledFunc->end(); I != E; ++I)
852         if (const InvokeInst *II = dyn_cast<InvokeInst>(I->getTerminator())) {
853           const BasicBlock *BB = II->getUnwindDest();
854           // FIXME: This 'if/dyn_cast' here should become a normal 'cast' once
855           // the new EH system is in place.
856           if (const LandingPadInst *LP =
857               dyn_cast<LandingPadInst>(BB->getFirstNonPHI()))
858             if (CallerPersFn != LP->getPersonalityFn())
859               return false;
860           break;
861         }
863       break;
864     }
866   // Get an iterator to the last basic block in the function, which will have
867   // the new function inlined after it.
868   //
869   Function::iterator LastBlock = &Caller->back();
871   // Make sure to capture all of the return instructions from the cloned
872   // function.
873   SmallVector<ReturnInst*, 8> Returns;
874   ClonedCodeInfo InlinedFunctionInfo;
875   Function::iterator FirstNewBlock;
877   { // Scope to destroy VMap after cloning.
878     ValueToValueMapTy VMap;
880     assert(CalledFunc->arg_size() == CS.arg_size() &&
881            "No varargs calls can be inlined!");
883     // Calculate the vector of arguments to pass into the function cloner, which
884     // matches up the formal to the actual argument values.
885     CallSite::arg_iterator AI = CS.arg_begin();
886     unsigned ArgNo = 0;
887     for (Function::const_arg_iterator I = CalledFunc->arg_begin(),
888          E = CalledFunc->arg_end(); I != E; ++I, ++AI, ++ArgNo) {
889       Value *ActualArg = *AI;
891       // When byval arguments actually inlined, we need to make the copy implied
892       // by them explicit.  However, we don't do this if the callee is readonly
893       // or readnone, because the copy would be unneeded: the callee doesn't
894       // modify the struct.
895       if (CalledFunc->paramHasAttr(ArgNo+1, Attribute::ByVal)) {
896         ActualArg = HandleByValArgument(ActualArg, TheCall, CalledFunc, IFI,
897                                         CalledFunc->getParamAlignment(ArgNo+1));
898  
899         // Calls that we inline may use the new alloca, so we need to clear
900         // their 'tail' flags if HandleByValArgument introduced a new alloca and
901         // the callee has calls.
902         MustClearTailCallFlags |= ActualArg != *AI;
903       }
905       VMap[I] = ActualArg;
906     }
908     // We want the inliner to prune the code as it copies.  We would LOVE to
909     // have no dead or constant instructions leftover after inlining occurs
910     // (which can happen, e.g., because an argument was constant), but we'll be
911     // happy with whatever the cloner can do.
912     CloneAndPruneFunctionInto(Caller, CalledFunc, VMap, 
913                               /*ModuleLevelChanges=*/false, Returns, ".i",
914                               &InlinedFunctionInfo, IFI.TD, TheCall);
916     // Remember the first block that is newly cloned over.
917     FirstNewBlock = LastBlock; ++FirstNewBlock;
919     // Update the callgraph if requested.
920     if (IFI.CG)
921       UpdateCallGraphAfterInlining(CS, FirstNewBlock, VMap, IFI);
923     // Update inlined instructions' line number information.
924     fixupLineNumbers(Caller, FirstNewBlock, TheCall);
925   }
927   // If there are any alloca instructions in the block that used to be the entry
928   // block for the callee, move them to the entry block of the caller.  First
929   // calculate which instruction they should be inserted before.  We insert the
930   // instructions at the end of the current alloca list.
931   //
932   {
933     BasicBlock::iterator InsertPoint = Caller->begin()->begin();
934     for (BasicBlock::iterator I = FirstNewBlock->begin(),
935          E = FirstNewBlock->end(); I != E; ) {
936       AllocaInst *AI = dyn_cast<AllocaInst>(I++);
937       if (AI == 0) continue;
938       
939       // If the alloca is now dead, remove it.  This often occurs due to code
940       // specialization.
941       if (AI->use_empty()) {
942         AI->eraseFromParent();
943         continue;
944       }
946       if (!isa<Constant>(AI->getArraySize()))
947         continue;
948       
949       // Keep track of the static allocas that we inline into the caller.
950       IFI.StaticAllocas.push_back(AI);
951       
952       // Scan for the block of allocas that we can move over, and move them
953       // all at once.
954       while (isa<AllocaInst>(I) &&
955              isa<Constant>(cast<AllocaInst>(I)->getArraySize())) {
956         IFI.StaticAllocas.push_back(cast<AllocaInst>(I));
957         ++I;
958       }
960       // Transfer all of the allocas over in a block.  Using splice means
961       // that the instructions aren't removed from the symbol table, then
962       // reinserted.
963       Caller->getEntryBlock().getInstList().splice(InsertPoint,
964                                                    FirstNewBlock->getInstList(),
965                                                    AI, I);
966     }
967   }
969   // Leave lifetime markers for the static alloca's, scoping them to the
970   // function we just inlined.
971   if (!IFI.StaticAllocas.empty()) {
972     IRBuilder<> builder(FirstNewBlock->begin());
973     for (unsigned ai = 0, ae = IFI.StaticAllocas.size(); ai != ae; ++ai) {
974       AllocaInst *AI = IFI.StaticAllocas[ai];
976       // If the alloca is already scoped to something smaller than the whole
977       // function then there's no need to add redundant, less accurate markers.
978       if (hasLifetimeMarkers(AI))
979         continue;
981       builder.CreateLifetimeStart(AI);
982       for (unsigned ri = 0, re = Returns.size(); ri != re; ++ri) {
983         IRBuilder<> builder(Returns[ri]);
984         builder.CreateLifetimeEnd(AI);
985       }
986     }
987   }
989   // If the inlined code contained dynamic alloca instructions, wrap the inlined
990   // code with llvm.stacksave/llvm.stackrestore intrinsics.
991   if (InlinedFunctionInfo.ContainsDynamicAllocas) {
992     Module *M = Caller->getParent();
993     // Get the two intrinsics we care about.
994     Function *StackSave = Intrinsic::getDeclaration(M, Intrinsic::stacksave);
995     Function *StackRestore=Intrinsic::getDeclaration(M,Intrinsic::stackrestore);
997     // Insert the llvm.stacksave.
998     CallInst *SavedPtr = IRBuilder<>(FirstNewBlock, FirstNewBlock->begin())
999       .CreateCall(StackSave, "savedstack");
1001     // Insert a call to llvm.stackrestore before any return instructions in the
1002     // inlined function.
1003     for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
1004       IRBuilder<>(Returns[i]).CreateCall(StackRestore, SavedPtr);
1005     }
1007     // Count the number of StackRestore calls we insert.
1008     unsigned NumStackRestores = Returns.size();
1010     // If we are inlining an invoke instruction, insert restores before each
1011     // unwind.  These unwinds will be rewritten into branches later.
1012     if (InlinedFunctionInfo.ContainsUnwinds && isa<InvokeInst>(TheCall)) {
1013       for (Function::iterator BB = FirstNewBlock, E = Caller->end();
1014            BB != E; ++BB)
1015         if (UnwindInst *UI = dyn_cast<UnwindInst>(BB->getTerminator())) {
1016           IRBuilder<>(UI).CreateCall(StackRestore, SavedPtr);
1017           ++NumStackRestores;
1018         }
1019     }
1020   }
1022   // If we are inlining tail call instruction through a call site that isn't
1023   // marked 'tail', we must remove the tail marker for any calls in the inlined
1024   // code.  Also, calls inlined through a 'nounwind' call site should be marked
1025   // 'nounwind'.
1026   if (InlinedFunctionInfo.ContainsCalls &&
1027       (MustClearTailCallFlags || MarkNoUnwind)) {
1028     for (Function::iterator BB = FirstNewBlock, E = Caller->end();
1029          BB != E; ++BB)
1030       for (BasicBlock::iterator I = BB->begin(), E = BB->end(); I != E; ++I)
1031         if (CallInst *CI = dyn_cast<CallInst>(I)) {
1032           if (MustClearTailCallFlags)
1033             CI->setTailCall(false);
1034           if (MarkNoUnwind)
1035             CI->setDoesNotThrow();
1036         }
1037   }
1039   // If we are inlining through a 'nounwind' call site then any inlined 'unwind'
1040   // instructions are unreachable.
1041   if (InlinedFunctionInfo.ContainsUnwinds && MarkNoUnwind)
1042     for (Function::iterator BB = FirstNewBlock, E = Caller->end();
1043          BB != E; ++BB) {
1044       TerminatorInst *Term = BB->getTerminator();
1045       if (isa<UnwindInst>(Term)) {
1046         new UnreachableInst(Context, Term);
1047         BB->getInstList().erase(Term);
1048       }
1049     }
1051   // If we are inlining for an invoke instruction, we must make sure to rewrite
1052   // any inlined 'unwind' instructions into branches to the invoke exception
1053   // destination, and call instructions into invoke instructions.
1054   if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
1055     HandleInlinedInvoke(II, FirstNewBlock, InlinedFunctionInfo);
1057   // If we cloned in _exactly one_ basic block, and if that block ends in a
1058   // return instruction, we splice the body of the inlined callee directly into
1059   // the calling basic block.
1060   if (Returns.size() == 1 && std::distance(FirstNewBlock, Caller->end()) == 1) {
1061     // Move all of the instructions right before the call.
1062     OrigBB->getInstList().splice(TheCall, FirstNewBlock->getInstList(),
1063                                  FirstNewBlock->begin(), FirstNewBlock->end());
1064     // Remove the cloned basic block.
1065     Caller->getBasicBlockList().pop_back();
1067     // If the call site was an invoke instruction, add a branch to the normal
1068     // destination.
1069     if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
1070       BranchInst::Create(II->getNormalDest(), TheCall);
1072     // If the return instruction returned a value, replace uses of the call with
1073     // uses of the returned value.
1074     if (!TheCall->use_empty()) {
1075       ReturnInst *R = Returns[0];
1076       if (TheCall == R->getReturnValue())
1077         TheCall->replaceAllUsesWith(UndefValue::get(TheCall->getType()));
1078       else
1079         TheCall->replaceAllUsesWith(R->getReturnValue());
1080     }
1081     // Since we are now done with the Call/Invoke, we can delete it.
1082     TheCall->eraseFromParent();
1084     // Since we are now done with the return instruction, delete it also.
1085     Returns[0]->eraseFromParent();
1087     // We are now done with the inlining.
1088     return true;
1089   }
1091   // Otherwise, we have the normal case, of more than one block to inline or
1092   // multiple return sites.
1094   // We want to clone the entire callee function into the hole between the
1095   // "starter" and "ender" blocks.  How we accomplish this depends on whether
1096   // this is an invoke instruction or a call instruction.
1097   BasicBlock *AfterCallBB;
1098   if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall)) {
1100     // Add an unconditional branch to make this look like the CallInst case...
1101     BranchInst *NewBr = BranchInst::Create(II->getNormalDest(), TheCall);
1103     // Split the basic block.  This guarantees that no PHI nodes will have to be
1104     // updated due to new incoming edges, and make the invoke case more
1105     // symmetric to the call case.
1106     AfterCallBB = OrigBB->splitBasicBlock(NewBr,
1107                                           CalledFunc->getName()+".exit");
1109   } else {  // It's a call
1110     // If this is a call instruction, we need to split the basic block that
1111     // the call lives in.
1112     //
1113     AfterCallBB = OrigBB->splitBasicBlock(TheCall,
1114                                           CalledFunc->getName()+".exit");
1115   }
1117   // Change the branch that used to go to AfterCallBB to branch to the first
1118   // basic block of the inlined function.
1119   //
1120   TerminatorInst *Br = OrigBB->getTerminator();
1121   assert(Br && Br->getOpcode() == Instruction::Br &&
1122          "splitBasicBlock broken!");
1123   Br->setOperand(0, FirstNewBlock);
1126   // Now that the function is correct, make it a little bit nicer.  In
1127   // particular, move the basic blocks inserted from the end of the function
1128   // into the space made by splitting the source basic block.
1129   Caller->getBasicBlockList().splice(AfterCallBB, Caller->getBasicBlockList(),
1130                                      FirstNewBlock, Caller->end());
1132   // Handle all of the return instructions that we just cloned in, and eliminate
1133   // any users of the original call/invoke instruction.
1134   Type *RTy = CalledFunc->getReturnType();
1136   PHINode *PHI = 0;
1137   if (Returns.size() > 1) {
1138     // The PHI node should go at the front of the new basic block to merge all
1139     // possible incoming values.
1140     if (!TheCall->use_empty()) {
1141       PHI = PHINode::Create(RTy, Returns.size(), TheCall->getName(),
1142                             AfterCallBB->begin());
1143       // Anything that used the result of the function call should now use the
1144       // PHI node as their operand.
1145       TheCall->replaceAllUsesWith(PHI);
1146     }
1148     // Loop over all of the return instructions adding entries to the PHI node
1149     // as appropriate.
1150     if (PHI) {
1151       for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
1152         ReturnInst *RI = Returns[i];
1153         assert(RI->getReturnValue()->getType() == PHI->getType() &&
1154                "Ret value not consistent in function!");
1155         PHI->addIncoming(RI->getReturnValue(), RI->getParent());
1156       }
1157     }
1160     // Add a branch to the merge points and remove return instructions.
1161     for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
1162       ReturnInst *RI = Returns[i];
1163       BranchInst::Create(AfterCallBB, RI);
1164       RI->eraseFromParent();
1165     }
1166   } else if (!Returns.empty()) {
1167     // Otherwise, if there is exactly one return value, just replace anything
1168     // using the return value of the call with the computed value.
1169     if (!TheCall->use_empty()) {
1170       if (TheCall == Returns[0]->getReturnValue())
1171         TheCall->replaceAllUsesWith(UndefValue::get(TheCall->getType()));
1172       else
1173         TheCall->replaceAllUsesWith(Returns[0]->getReturnValue());
1174     }
1176     // Update PHI nodes that use the ReturnBB to use the AfterCallBB.
1177     BasicBlock *ReturnBB = Returns[0]->getParent();
1178     ReturnBB->replaceAllUsesWith(AfterCallBB);
1180     // Splice the code from the return block into the block that it will return
1181     // to, which contains the code that was after the call.
1182     AfterCallBB->getInstList().splice(AfterCallBB->begin(),
1183                                       ReturnBB->getInstList());
1185     // Delete the return instruction now and empty ReturnBB now.
1186     Returns[0]->eraseFromParent();
1187     ReturnBB->eraseFromParent();
1188   } else if (!TheCall->use_empty()) {
1189     // No returns, but something is using the return value of the call.  Just
1190     // nuke the result.
1191     TheCall->replaceAllUsesWith(UndefValue::get(TheCall->getType()));
1192   }
1194   // Since we are now done with the Call/Invoke, we can delete it.
1195   TheCall->eraseFromParent();
1197   // We should always be able to fold the entry block of the function into the
1198   // single predecessor of the block...
1199   assert(cast<BranchInst>(Br)->isUnconditional() && "splitBasicBlock broken!");
1200   BasicBlock *CalleeEntry = cast<BranchInst>(Br)->getSuccessor(0);
1202   // Splice the code entry block into calling block, right before the
1203   // unconditional branch.
1204   CalleeEntry->replaceAllUsesWith(OrigBB);  // Update PHI nodes
1205   OrigBB->getInstList().splice(Br, CalleeEntry->getInstList());
1207   // Remove the unconditional branch.
1208   OrigBB->getInstList().erase(Br);
1210   // Now we can remove the CalleeEntry block, which is now empty.
1211   Caller->getBasicBlockList().erase(CalleeEntry);
1213   // If we inserted a phi node, check to see if it has a single value (e.g. all
1214   // the entries are the same or undef).  If so, remove the PHI so it doesn't
1215   // block other optimizations.
1216   if (PHI)
1217     if (Value *V = SimplifyInstruction(PHI, IFI.TD)) {
1218       PHI->replaceAllUsesWith(V);
1219       PHI->eraseFromParent();
1220     }
1222   return true;