1 //===- InlineFunction.cpp - Code to perform function inlining -------------===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // This file implements inlining of a function into a call site, resolving
11 // parameters and the return value as appropriate.
12 //
13 // The code in this file for handling inlines through invoke
14 // instructions preserves semantics only under some assumptions about
15 // the behavior of unwinders which correspond to gcc-style libUnwind
16 // exception personality functions. Eventually the IR will be
17 // improved to make this unnecessary, but until then, this code is
18 // marked [LIBUNWIND].
19 //
20 //===----------------------------------------------------------------------===//
22 #include "llvm/Transforms/Utils/Cloning.h"
23 #include "llvm/Constants.h"
24 #include "llvm/DerivedTypes.h"
25 #include "llvm/Module.h"
26 #include "llvm/Instructions.h"
27 #include "llvm/IntrinsicInst.h"
28 #include "llvm/Intrinsics.h"
29 #include "llvm/Attributes.h"
30 #include "llvm/Analysis/CallGraph.h"
31 #include "llvm/Analysis/DebugInfo.h"
32 #include "llvm/Analysis/InstructionSimplify.h"
33 #include "llvm/Target/TargetData.h"
34 #include "llvm/Transforms/Utils/Local.h"
35 #include "llvm/ADT/SmallVector.h"
36 #include "llvm/ADT/StringExtras.h"
37 #include "llvm/Support/CallSite.h"
38 #include "llvm/Support/IRBuilder.h"
39 using namespace llvm;
41 bool llvm::InlineFunction(CallInst *CI, InlineFunctionInfo &IFI) {
42 return InlineFunction(CallSite(CI), IFI);
43 }
44 bool llvm::InlineFunction(InvokeInst *II, InlineFunctionInfo &IFI) {
45 return InlineFunction(CallSite(II), IFI);
46 }
48 /// [LIBUNWIND] Look for an llvm.eh.exception call in the given block.
49 static EHExceptionInst *findExceptionInBlock(BasicBlock *bb) {
50 for (BasicBlock::iterator i = bb->begin(), e = bb->end(); i != e; i++) {
51 EHExceptionInst *exn = dyn_cast<EHExceptionInst>(i);
52 if (exn) return exn;
53 }
55 return 0;
56 }
58 /// [LIBUNWIND] Look for the 'best' llvm.eh.selector instruction for
59 /// the given llvm.eh.exception call.
60 static EHSelectorInst *findSelectorForException(EHExceptionInst *exn) {
61 BasicBlock *exnBlock = exn->getParent();
63 EHSelectorInst *outOfBlockSelector = 0;
64 for (Instruction::use_iterator
65 ui = exn->use_begin(), ue = exn->use_end(); ui != ue; ++ui) {
66 EHSelectorInst *sel = dyn_cast<EHSelectorInst>(*ui);
67 if (!sel) continue;
69 // Immediately accept an eh.selector in the same block as the
70 // excepton call.
71 if (sel->getParent() == exnBlock) return sel;
73 // Otherwise, use the first selector we see.
74 if (!outOfBlockSelector) outOfBlockSelector = sel;
75 }
77 return outOfBlockSelector;
78 }
80 /// [LIBUNWIND] Find the (possibly absent) call to @llvm.eh.selector
81 /// in the given landing pad. In principle, llvm.eh.exception is
82 /// required to be in the landing pad; in practice, SplitCriticalEdge
83 /// can break that invariant, and then inlining can break it further.
84 /// There's a real need for a reliable solution here, but until that
85 /// happens, we have some fragile workarounds here.
86 static EHSelectorInst *findSelectorForLandingPad(BasicBlock *lpad) {
87 // Look for an exception call in the actual landing pad.
88 EHExceptionInst *exn = findExceptionInBlock(lpad);
89 if (exn) return findSelectorForException(exn);
91 // Okay, if that failed, look for one in an obvious successor. If
92 // we find one, we'll fix the IR by moving things back to the
93 // landing pad.
95 bool dominates = true; // does the lpad dominate the exn call
96 BasicBlock *nonDominated = 0; // if not, the first non-dominated block
97 BasicBlock *lastDominated = 0; // and the block which branched to it
99 BasicBlock *exnBlock = lpad;
101 // We need to protect against lpads that lead into infinite loops.
102 SmallPtrSet<BasicBlock*,4> visited;
103 visited.insert(exnBlock);
105 do {
106 // We're not going to apply this hack to anything more complicated
107 // than a series of unconditional branches, so if the block
108 // doesn't terminate in an unconditional branch, just fail. More
109 // complicated cases can arise when, say, sinking a call into a
110 // split unwind edge and then inlining it; but that can do almost
111 // *anything* to the CFG, including leaving the selector
112 // completely unreachable. The only way to fix that properly is
113 // to (1) prohibit transforms which move the exception or selector
114 // values away from the landing pad, e.g. by producing them with
115 // instructions that are pinned to an edge like a phi, or
116 // producing them with not-really-instructions, and (2) making
117 // transforms which split edges deal with that.
118 BranchInst *branch = dyn_cast<BranchInst>(&exnBlock->back());
119 if (!branch || branch->isConditional()) return 0;
121 BasicBlock *successor = branch->getSuccessor(0);
123 // Fail if we found an infinite loop.
124 if (!visited.insert(successor)) return 0;
126 // If the successor isn't dominated by exnBlock:
127 if (!successor->getSinglePredecessor()) {
128 // We don't want to have to deal with threading the exception
129 // through multiple levels of phi, so give up if we've already
130 // followed a non-dominating edge.
131 if (!dominates) return 0;
133 // Otherwise, remember this as a non-dominating edge.
134 dominates = false;
135 nonDominated = successor;
136 lastDominated = exnBlock;
137 }
139 exnBlock = successor;
141 // Can we stop here?
142 exn = findExceptionInBlock(exnBlock);
143 } while (!exn);
145 // Look for a selector call for the exception we found.
146 EHSelectorInst *selector = findSelectorForException(exn);
147 if (!selector) return 0;
149 // The easy case is when the landing pad still dominates the
150 // exception call, in which case we can just move both calls back to
151 // the landing pad.
152 if (dominates) {
153 selector->moveBefore(lpad->getFirstNonPHI());
154 exn->moveBefore(selector);
155 return selector;
156 }
158 // Otherwise, we have to split at the first non-dominating block.
159 // The CFG looks basically like this:
160 // lpad:
161 // phis_0
162 // insnsAndBranches_1
163 // br label %nonDominated
164 // nonDominated:
165 // phis_2
166 // insns_3
167 // %exn = call i8* @llvm.eh.exception()
168 // insnsAndBranches_4
169 // %selector = call @llvm.eh.selector(i8* %exn, ...
170 // We need to turn this into:
171 // lpad:
172 // phis_0
173 // %exn0 = call i8* @llvm.eh.exception()
174 // %selector0 = call @llvm.eh.selector(i8* %exn0, ...
175 // insnsAndBranches_1
176 // br label %split // from lastDominated
177 // nonDominated:
178 // phis_2 (without edge from lastDominated)
179 // %exn1 = call i8* @llvm.eh.exception()
180 // %selector1 = call i8* @llvm.eh.selector(i8* %exn1, ...
181 // br label %split
182 // split:
183 // phis_2 (edge from lastDominated, edge from split)
184 // %exn = phi ...
185 // %selector = phi ...
186 // insns_3
187 // insnsAndBranches_4
189 assert(nonDominated);
190 assert(lastDominated);
192 // First, make clones of the intrinsics to go in lpad.
193 EHExceptionInst *lpadExn = cast<EHExceptionInst>(exn->clone());
194 EHSelectorInst *lpadSelector = cast<EHSelectorInst>(selector->clone());
195 lpadSelector->setArgOperand(0, lpadExn);
196 lpadSelector->insertBefore(lpad->getFirstNonPHI());
197 lpadExn->insertBefore(lpadSelector);
199 // Split the non-dominated block.
200 BasicBlock *split =
201 nonDominated->splitBasicBlock(nonDominated->getFirstNonPHI(),
202 nonDominated->getName() + ".lpad-fix");
204 // Redirect the last dominated branch there.
205 cast<BranchInst>(lastDominated->back()).setSuccessor(0, split);
207 // Move the existing intrinsics to the end of the old block.
208 selector->moveBefore(&nonDominated->back());
209 exn->moveBefore(selector);
211 Instruction *splitIP = &split->front();
213 // For all the phis in nonDominated, make a new phi in split to join
214 // that phi with the edge from lastDominated.
215 for (BasicBlock::iterator
216 i = nonDominated->begin(), e = nonDominated->end(); i != e; ++i) {
217 PHINode *phi = dyn_cast<PHINode>(i);
218 if (!phi) break;
220 PHINode *splitPhi = PHINode::Create(phi->getType(), 2, phi->getName(),
221 splitIP);
222 phi->replaceAllUsesWith(splitPhi);
223 splitPhi->addIncoming(phi, nonDominated);
224 splitPhi->addIncoming(phi->removeIncomingValue(lastDominated),
225 lastDominated);
226 }
228 // Make new phis for the exception and selector.
229 PHINode *exnPhi = PHINode::Create(exn->getType(), 2, "", splitIP);
230 exn->replaceAllUsesWith(exnPhi);
231 selector->setArgOperand(0, exn); // except for this use
232 exnPhi->addIncoming(exn, nonDominated);
233 exnPhi->addIncoming(lpadExn, lastDominated);
235 PHINode *selectorPhi = PHINode::Create(selector->getType(), 2, "", splitIP);
236 selector->replaceAllUsesWith(selectorPhi);
237 selectorPhi->addIncoming(selector, nonDominated);
238 selectorPhi->addIncoming(lpadSelector, lastDominated);
240 return lpadSelector;
241 }
243 namespace {
244 /// A class for recording information about inlining through an invoke.
245 class InvokeInliningInfo {
246 BasicBlock *OuterUnwindDest;
247 EHSelectorInst *OuterSelector;
248 BasicBlock *InnerUnwindDest;
249 PHINode *InnerExceptionPHI;
250 PHINode *InnerSelectorPHI;
251 SmallVector<Value*, 8> UnwindDestPHIValues;
253 public:
254 InvokeInliningInfo(InvokeInst *II) :
255 OuterUnwindDest(II->getUnwindDest()), OuterSelector(0),
256 InnerUnwindDest(0), InnerExceptionPHI(0), InnerSelectorPHI(0) {
258 // If there are PHI nodes in the unwind destination block, we
259 // need to keep track of which values came into them from the
260 // invoke before removing the edge from this block.
261 llvm::BasicBlock *invokeBB = II->getParent();
262 for (BasicBlock::iterator I = OuterUnwindDest->begin();
263 isa<PHINode>(I); ++I) {
264 // Save the value to use for this edge.
265 PHINode *phi = cast<PHINode>(I);
266 UnwindDestPHIValues.push_back(phi->getIncomingValueForBlock(invokeBB));
267 }
268 }
270 /// The outer unwind destination is the target of unwind edges
271 /// introduced for calls within the inlined function.
272 BasicBlock *getOuterUnwindDest() const {
273 return OuterUnwindDest;
274 }
276 EHSelectorInst *getOuterSelector() {
277 if (!OuterSelector)
278 OuterSelector = findSelectorForLandingPad(OuterUnwindDest);
279 return OuterSelector;
280 }
282 BasicBlock *getInnerUnwindDest();
284 bool forwardEHResume(CallInst *call, BasicBlock *src);
286 /// Add incoming-PHI values to the unwind destination block for
287 /// the given basic block, using the values for the original
288 /// invoke's source block.
289 void addIncomingPHIValuesFor(BasicBlock *BB) const {
290 addIncomingPHIValuesForInto(BB, OuterUnwindDest);
291 }
293 void addIncomingPHIValuesForInto(BasicBlock *src, BasicBlock *dest) const {
294 BasicBlock::iterator I = dest->begin();
295 for (unsigned i = 0, e = UnwindDestPHIValues.size(); i != e; ++i, ++I) {
296 PHINode *phi = cast<PHINode>(I);
297 phi->addIncoming(UnwindDestPHIValues[i], src);
298 }
299 }
300 };
301 }
303 /// Get or create a target for the branch out of rewritten calls to
304 /// llvm.eh.resume.
305 BasicBlock *InvokeInliningInfo::getInnerUnwindDest() {
306 if (InnerUnwindDest) return InnerUnwindDest;
308 // Find and hoist the llvm.eh.exception and llvm.eh.selector calls
309 // in the outer landing pad to immediately following the phis.
310 EHSelectorInst *selector = getOuterSelector();
311 if (!selector) return 0;
313 // The call to llvm.eh.exception *must* be in the landing pad.
314 Instruction *exn = cast<Instruction>(selector->getArgOperand(0));
315 assert(exn->getParent() == OuterUnwindDest);
317 // TODO: recognize when we've already done this, so that we don't
318 // get a linear number of these when inlining calls into lots of
319 // invokes with the same landing pad.
321 // Do the hoisting.
322 Instruction *splitPoint = exn->getParent()->getFirstNonPHI();
323 assert(splitPoint != selector && "selector-on-exception dominance broken!");
324 if (splitPoint == exn) {
325 selector->removeFromParent();
326 selector->insertAfter(exn);
327 splitPoint = selector->getNextNode();
328 } else {
329 exn->moveBefore(splitPoint);
330 selector->moveBefore(splitPoint);
331 }
333 // Split the landing pad.
334 InnerUnwindDest = OuterUnwindDest->splitBasicBlock(splitPoint,
335 OuterUnwindDest->getName() + ".body");
337 // The number of incoming edges we expect to the inner landing pad.
338 const unsigned phiCapacity = 2;
340 // Create corresponding new phis for all the phis in the outer landing pad.
341 BasicBlock::iterator insertPoint = InnerUnwindDest->begin();
342 BasicBlock::iterator I = OuterUnwindDest->begin();
343 for (unsigned i = 0, e = UnwindDestPHIValues.size(); i != e; ++i, ++I) {
344 PHINode *outerPhi = cast<PHINode>(I);
345 PHINode *innerPhi = PHINode::Create(outerPhi->getType(), phiCapacity,
346 outerPhi->getName() + ".lpad-body",
347 insertPoint);
348 outerPhi->replaceAllUsesWith(innerPhi);
349 innerPhi->addIncoming(outerPhi, OuterUnwindDest);
350 }
352 // Create a phi for the exception value...
353 InnerExceptionPHI = PHINode::Create(exn->getType(), phiCapacity,
354 "exn.lpad-body", insertPoint);
355 exn->replaceAllUsesWith(InnerExceptionPHI);
356 selector->setArgOperand(0, exn); // restore this use
357 InnerExceptionPHI->addIncoming(exn, OuterUnwindDest);
359 // ...and the selector.
360 InnerSelectorPHI = PHINode::Create(selector->getType(), phiCapacity,
361 "selector.lpad-body", insertPoint);
362 selector->replaceAllUsesWith(InnerSelectorPHI);
363 InnerSelectorPHI->addIncoming(selector, OuterUnwindDest);
365 // All done.
366 return InnerUnwindDest;
367 }
369 /// [LIBUNWIND] Try to forward the given call, which logically occurs
370 /// at the end of the given block, as a branch to the inner unwind
371 /// block. Returns true if the call was forwarded.
372 bool InvokeInliningInfo::forwardEHResume(CallInst *call, BasicBlock *src) {
373 // First, check whether this is a call to the intrinsic.
374 Function *fn = dyn_cast<Function>(call->getCalledValue());
375 if (!fn || fn->getName() != "llvm.eh.resume")
376 return false;
378 // At this point, we need to return true on all paths, because
379 // otherwise we'll construct an invoke of the intrinsic, which is
380 // not well-formed.
382 // Try to find or make an inner unwind dest, which will fail if we
383 // can't find a selector call for the outer unwind dest.
384 BasicBlock *dest = getInnerUnwindDest();
385 bool hasSelector = (dest != 0);
387 // If we failed, just use the outer unwind dest, dropping the
388 // exception and selector on the floor.
389 if (!hasSelector)
390 dest = OuterUnwindDest;
392 // Make a branch.
393 BranchInst::Create(dest, src);
395 // Update the phis in the destination. They were inserted in an
396 // order which makes this work.
397 addIncomingPHIValuesForInto(src, dest);
399 if (hasSelector) {
400 InnerExceptionPHI->addIncoming(call->getArgOperand(0), src);
401 InnerSelectorPHI->addIncoming(call->getArgOperand(1), src);
402 }
404 return true;
405 }
407 /// [LIBUNWIND] Check whether this selector is "only cleanups":
408 /// call i32 @llvm.eh.selector(blah, blah, i32 0)
409 static bool isCleanupOnlySelector(EHSelectorInst *selector) {
410 if (selector->getNumArgOperands() != 3) return false;
411 ConstantInt *val = dyn_cast<ConstantInt>(selector->getArgOperand(2));
412 return (val && val->isZero());
413 }
415 /// HandleCallsInBlockInlinedThroughInvoke - When we inline a basic block into
416 /// an invoke, we have to turn all of the calls that can throw into
417 /// invokes. This function analyze BB to see if there are any calls, and if so,
418 /// it rewrites them to be invokes that jump to InvokeDest and fills in the PHI
419 /// nodes in that block with the values specified in InvokeDestPHIValues.
420 ///
421 /// Returns true to indicate that the next block should be skipped.
422 static bool HandleCallsInBlockInlinedThroughInvoke(BasicBlock *BB,
423 InvokeInliningInfo &Invoke) {
424 for (BasicBlock::iterator BBI = BB->begin(), E = BB->end(); BBI != E; ) {
425 Instruction *I = BBI++;
427 // We only need to check for function calls: inlined invoke
428 // instructions require no special handling.
429 CallInst *CI = dyn_cast<CallInst>(I);
430 if (CI == 0) continue;
432 // LIBUNWIND: merge selector instructions.
433 if (EHSelectorInst *Inner = dyn_cast<EHSelectorInst>(CI)) {
434 EHSelectorInst *Outer = Invoke.getOuterSelector();
435 if (!Outer) continue;
437 bool innerIsOnlyCleanup = isCleanupOnlySelector(Inner);
438 bool outerIsOnlyCleanup = isCleanupOnlySelector(Outer);
440 // If both selectors contain only cleanups, we don't need to do
441 // anything. TODO: this is really just a very specific instance
442 // of a much more general optimization.
443 if (innerIsOnlyCleanup && outerIsOnlyCleanup) continue;
445 // Otherwise, we just append the outer selector to the inner selector.
446 SmallVector<Value*, 16> NewSelector;
447 for (unsigned i = 0, e = Inner->getNumArgOperands(); i != e; ++i)
448 NewSelector.push_back(Inner->getArgOperand(i));
449 for (unsigned i = 2, e = Outer->getNumArgOperands(); i != e; ++i)
450 NewSelector.push_back(Outer->getArgOperand(i));
452 CallInst *NewInner =
453 IRBuilder<>(Inner).CreateCall(Inner->getCalledValue(),
454 NewSelector.begin(),
455 NewSelector.end());
456 // No need to copy attributes, calling convention, etc.
457 NewInner->takeName(Inner);
458 Inner->replaceAllUsesWith(NewInner);
459 Inner->eraseFromParent();
460 continue;
461 }
463 // If this call cannot unwind, don't convert it to an invoke.
464 if (CI->doesNotThrow())
465 continue;
467 // Convert this function call into an invoke instruction.
468 // First, split the basic block.
469 BasicBlock *Split = BB->splitBasicBlock(CI, CI->getName()+".noexc");
471 // Delete the unconditional branch inserted by splitBasicBlock
472 BB->getInstList().pop_back();
474 // LIBUNWIND: If this is a call to @llvm.eh.resume, just branch
475 // directly to the new landing pad.
476 if (Invoke.forwardEHResume(CI, BB)) {
477 // TODO: 'Split' is now unreachable; clean it up.
479 // We want to leave the original call intact so that the call
480 // graph and other structures won't get misled. We also have to
481 // avoid processing the next block, or we'll iterate here forever.
482 return true;
483 }
485 // Otherwise, create the new invoke instruction.
486 ImmutableCallSite CS(CI);
487 SmallVector<Value*, 8> InvokeArgs(CS.arg_begin(), CS.arg_end());
488 InvokeInst *II =
489 InvokeInst::Create(CI->getCalledValue(), Split,
490 Invoke.getOuterUnwindDest(),
491 InvokeArgs.begin(), InvokeArgs.end(),
492 CI->getName(), BB);
493 II->setCallingConv(CI->getCallingConv());
494 II->setAttributes(CI->getAttributes());
496 // Make sure that anything using the call now uses the invoke! This also
497 // updates the CallGraph if present, because it uses a WeakVH.
498 CI->replaceAllUsesWith(II);
500 Split->getInstList().pop_front(); // Delete the original call
502 // Update any PHI nodes in the exceptional block to indicate that
503 // there is now a new entry in them.
504 Invoke.addIncomingPHIValuesFor(BB);
505 return false;
506 }
508 return false;
509 }
512 /// HandleInlinedInvoke - If we inlined an invoke site, we need to convert calls
513 /// in the body of the inlined function into invokes and turn unwind
514 /// instructions into branches to the invoke unwind dest.
515 ///
516 /// II is the invoke instruction being inlined. FirstNewBlock is the first
517 /// block of the inlined code (the last block is the end of the function),
518 /// and InlineCodeInfo is information about the code that got inlined.
519 static void HandleInlinedInvoke(InvokeInst *II, BasicBlock *FirstNewBlock,
520 ClonedCodeInfo &InlinedCodeInfo) {
521 BasicBlock *InvokeDest = II->getUnwindDest();
523 Function *Caller = FirstNewBlock->getParent();
525 // The inlined code is currently at the end of the function, scan from the
526 // start of the inlined code to its end, checking for stuff we need to
527 // rewrite. If the code doesn't have calls or unwinds, we know there is
528 // nothing to rewrite.
529 if (!InlinedCodeInfo.ContainsCalls && !InlinedCodeInfo.ContainsUnwinds) {
530 // Now that everything is happy, we have one final detail. The PHI nodes in
531 // the exception destination block still have entries due to the original
532 // invoke instruction. Eliminate these entries (which might even delete the
533 // PHI node) now.
534 InvokeDest->removePredecessor(II->getParent());
535 return;
536 }
538 InvokeInliningInfo Invoke(II);
540 for (Function::iterator BB = FirstNewBlock, E = Caller->end(); BB != E; ++BB){
541 if (InlinedCodeInfo.ContainsCalls)
542 if (HandleCallsInBlockInlinedThroughInvoke(BB, Invoke)) {
543 // Honor a request to skip the next block. We don't need to
544 // consider UnwindInsts in this case either.
545 ++BB;
546 continue;
547 }
549 if (UnwindInst *UI = dyn_cast<UnwindInst>(BB->getTerminator())) {
550 // An UnwindInst requires special handling when it gets inlined into an
551 // invoke site. Once this happens, we know that the unwind would cause
552 // a control transfer to the invoke exception destination, so we can
553 // transform it into a direct branch to the exception destination.
554 BranchInst::Create(InvokeDest, UI);
556 // Delete the unwind instruction!
557 UI->eraseFromParent();
559 // Update any PHI nodes in the exceptional block to indicate that
560 // there is now a new entry in them.
561 Invoke.addIncomingPHIValuesFor(BB);
562 }
563 }
565 // Now that everything is happy, we have one final detail. The PHI nodes in
566 // the exception destination block still have entries due to the original
567 // invoke instruction. Eliminate these entries (which might even delete the
568 // PHI node) now.
569 InvokeDest->removePredecessor(II->getParent());
570 }
572 /// UpdateCallGraphAfterInlining - Once we have cloned code over from a callee
573 /// into the caller, update the specified callgraph to reflect the changes we
574 /// made. Note that it's possible that not all code was copied over, so only
575 /// some edges of the callgraph may remain.
576 static void UpdateCallGraphAfterInlining(CallSite CS,
577 Function::iterator FirstNewBlock,
578 ValueToValueMapTy &VMap,
579 InlineFunctionInfo &IFI) {
580 CallGraph &CG = *IFI.CG;
581 const Function *Caller = CS.getInstruction()->getParent()->getParent();
582 const Function *Callee = CS.getCalledFunction();
583 CallGraphNode *CalleeNode = CG[Callee];
584 CallGraphNode *CallerNode = CG[Caller];
586 // Since we inlined some uninlined call sites in the callee into the caller,
587 // add edges from the caller to all of the callees of the callee.
588 CallGraphNode::iterator I = CalleeNode->begin(), E = CalleeNode->end();
590 // Consider the case where CalleeNode == CallerNode.
591 CallGraphNode::CalledFunctionsVector CallCache;
592 if (CalleeNode == CallerNode) {
593 CallCache.assign(I, E);
594 I = CallCache.begin();
595 E = CallCache.end();
596 }
598 for (; I != E; ++I) {
599 const Value *OrigCall = I->first;
601 ValueToValueMapTy::iterator VMI = VMap.find(OrigCall);
602 // Only copy the edge if the call was inlined!
603 if (VMI == VMap.end() || VMI->second == 0)
604 continue;
606 // If the call was inlined, but then constant folded, there is no edge to
607 // add. Check for this case.
608 Instruction *NewCall = dyn_cast<Instruction>(VMI->second);
609 if (NewCall == 0) continue;
611 // Remember that this call site got inlined for the client of
612 // InlineFunction.
613 IFI.InlinedCalls.push_back(NewCall);
615 // It's possible that inlining the callsite will cause it to go from an
616 // indirect to a direct call by resolving a function pointer. If this
617 // happens, set the callee of the new call site to a more precise
618 // destination. This can also happen if the call graph node of the caller
619 // was just unnecessarily imprecise.
620 if (I->second->getFunction() == 0)
621 if (Function *F = CallSite(NewCall).getCalledFunction()) {
622 // Indirect call site resolved to direct call.
623 CallerNode->addCalledFunction(CallSite(NewCall), CG[F]);
625 continue;
626 }
628 CallerNode->addCalledFunction(CallSite(NewCall), I->second);
629 }
631 // Update the call graph by deleting the edge from Callee to Caller. We must
632 // do this after the loop above in case Caller and Callee are the same.
633 CallerNode->removeCallEdgeFor(CS);
634 }
636 /// HandleByValArgument - When inlining a call site that has a byval argument,
637 /// we have to make the implicit memcpy explicit by adding it.
638 static Value *HandleByValArgument(Value *Arg, Instruction *TheCall,
639 const Function *CalledFunc,
640 InlineFunctionInfo &IFI,
641 unsigned ByValAlignment) {
642 const Type *AggTy = cast<PointerType>(Arg->getType())->getElementType();
644 // If the called function is readonly, then it could not mutate the caller's
645 // copy of the byval'd memory. In this case, it is safe to elide the copy and
646 // temporary.
647 if (CalledFunc->onlyReadsMemory()) {
648 // If the byval argument has a specified alignment that is greater than the
649 // passed in pointer, then we either have to round up the input pointer or
650 // give up on this transformation.
651 if (ByValAlignment <= 1) // 0 = unspecified, 1 = no particular alignment.
652 return Arg;
654 // If the pointer is already known to be sufficiently aligned, or if we can
655 // round it up to a larger alignment, then we don't need a temporary.
656 if (getOrEnforceKnownAlignment(Arg, ByValAlignment,
657 IFI.TD) >= ByValAlignment)
658 return Arg;
660 // Otherwise, we have to make a memcpy to get a safe alignment. This is bad
661 // for code quality, but rarely happens and is required for correctness.
662 }
664 LLVMContext &Context = Arg->getContext();
666 const Type *VoidPtrTy = Type::getInt8PtrTy(Context);
668 // Create the alloca. If we have TargetData, use nice alignment.
669 unsigned Align = 1;
670 if (IFI.TD)
671 Align = IFI.TD->getPrefTypeAlignment(AggTy);
673 // If the byval had an alignment specified, we *must* use at least that
674 // alignment, as it is required by the byval argument (and uses of the
675 // pointer inside the callee).
676 Align = std::max(Align, ByValAlignment);
678 Function *Caller = TheCall->getParent()->getParent();
680 Value *NewAlloca = new AllocaInst(AggTy, 0, Align, Arg->getName(),
681 &*Caller->begin()->begin());
682 // Emit a memcpy.
683 const Type *Tys[3] = {VoidPtrTy, VoidPtrTy, Type::getInt64Ty(Context)};
684 Function *MemCpyFn = Intrinsic::getDeclaration(Caller->getParent(),
685 Intrinsic::memcpy,
686 Tys, 3);
687 Value *DestCast = new BitCastInst(NewAlloca, VoidPtrTy, "tmp", TheCall);
688 Value *SrcCast = new BitCastInst(Arg, VoidPtrTy, "tmp", TheCall);
690 Value *Size;
691 if (IFI.TD == 0)
692 Size = ConstantExpr::getSizeOf(AggTy);
693 else
694 Size = ConstantInt::get(Type::getInt64Ty(Context),
695 IFI.TD->getTypeStoreSize(AggTy));
697 // Always generate a memcpy of alignment 1 here because we don't know
698 // the alignment of the src pointer. Other optimizations can infer
699 // better alignment.
700 Value *CallArgs[] = {
701 DestCast, SrcCast, Size,
702 ConstantInt::get(Type::getInt32Ty(Context), 1),
703 ConstantInt::getFalse(Context) // isVolatile
704 };
705 IRBuilder<>(TheCall).CreateCall(MemCpyFn, CallArgs, CallArgs+5);
707 // Uses of the argument in the function should use our new alloca
708 // instead.
709 return NewAlloca;
710 }
712 // isUsedByLifetimeMarker - Check whether this Value is used by a lifetime
713 // intrinsic.
714 static bool isUsedByLifetimeMarker(Value *V) {
715 for (Value::use_iterator UI = V->use_begin(), UE = V->use_end(); UI != UE;
716 ++UI) {
717 if (IntrinsicInst *II = dyn_cast<IntrinsicInst>(*UI)) {
718 switch (II->getIntrinsicID()) {
719 default: break;
720 case Intrinsic::lifetime_start:
721 case Intrinsic::lifetime_end:
722 return true;
723 }
724 }
725 }
726 return false;
727 }
729 // hasLifetimeMarkers - Check whether the given alloca already has
730 // lifetime.start or lifetime.end intrinsics.
731 static bool hasLifetimeMarkers(AllocaInst *AI) {
732 const Type *Int8PtrTy = Type::getInt8PtrTy(AI->getType()->getContext());
733 if (AI->getType() == Int8PtrTy)
734 return isUsedByLifetimeMarker(AI);
736 // Do a scan to find all the casts to i8*.
737 for (Value::use_iterator I = AI->use_begin(), E = AI->use_end(); I != E;
738 ++I) {
739 if (I->getType() != Int8PtrTy) continue;
740 if (I->stripPointerCasts() != AI) continue;
741 if (isUsedByLifetimeMarker(*I))
742 return true;
743 }
744 return false;
745 }
747 // InlineFunction - This function inlines the called function into the basic
748 // block of the caller. This returns false if it is not possible to inline this
749 // call. The program is still in a well defined state if this occurs though.
750 //
751 // Note that this only does one level of inlining. For example, if the
752 // instruction 'call B' is inlined, and 'B' calls 'C', then the call to 'C' now
753 // exists in the instruction stream. Similarly this will inline a recursive
754 // function by one level.
755 //
756 bool llvm::InlineFunction(CallSite CS, InlineFunctionInfo &IFI) {
757 Instruction *TheCall = CS.getInstruction();
758 LLVMContext &Context = TheCall->getContext();
759 assert(TheCall->getParent() && TheCall->getParent()->getParent() &&
760 "Instruction not in function!");
762 // If IFI has any state in it, zap it before we fill it in.
763 IFI.reset();
765 const Function *CalledFunc = CS.getCalledFunction();
766 if (CalledFunc == 0 || // Can't inline external function or indirect
767 CalledFunc->isDeclaration() || // call, or call to a vararg function!
768 CalledFunc->getFunctionType()->isVarArg()) return false;
770 // If the call to the callee is not a tail call, we must clear the 'tail'
771 // flags on any calls that we inline.
772 bool MustClearTailCallFlags =
773 !(isa<CallInst>(TheCall) && cast<CallInst>(TheCall)->isTailCall());
775 // If the call to the callee cannot throw, set the 'nounwind' flag on any
776 // calls that we inline.
777 bool MarkNoUnwind = CS.doesNotThrow();
779 BasicBlock *OrigBB = TheCall->getParent();
780 Function *Caller = OrigBB->getParent();
782 // GC poses two hazards to inlining, which only occur when the callee has GC:
783 // 1. If the caller has no GC, then the callee's GC must be propagated to the
784 // caller.
785 // 2. If the caller has a differing GC, it is invalid to inline.
786 if (CalledFunc->hasGC()) {
787 if (!Caller->hasGC())
788 Caller->setGC(CalledFunc->getGC());
789 else if (CalledFunc->getGC() != Caller->getGC())
790 return false;
791 }
793 // Get an iterator to the last basic block in the function, which will have
794 // the new function inlined after it.
795 //
796 Function::iterator LastBlock = &Caller->back();
798 // Make sure to capture all of the return instructions from the cloned
799 // function.
800 SmallVector<ReturnInst*, 8> Returns;
801 ClonedCodeInfo InlinedFunctionInfo;
802 Function::iterator FirstNewBlock;
804 { // Scope to destroy VMap after cloning.
805 ValueToValueMapTy VMap;
807 assert(CalledFunc->arg_size() == CS.arg_size() &&
808 "No varargs calls can be inlined!");
810 // Calculate the vector of arguments to pass into the function cloner, which
811 // matches up the formal to the actual argument values.
812 CallSite::arg_iterator AI = CS.arg_begin();
813 unsigned ArgNo = 0;
814 for (Function::const_arg_iterator I = CalledFunc->arg_begin(),
815 E = CalledFunc->arg_end(); I != E; ++I, ++AI, ++ArgNo) {
816 Value *ActualArg = *AI;
818 // When byval arguments actually inlined, we need to make the copy implied
819 // by them explicit. However, we don't do this if the callee is readonly
820 // or readnone, because the copy would be unneeded: the callee doesn't
821 // modify the struct.
822 if (CalledFunc->paramHasAttr(ArgNo+1, Attribute::ByVal)) {
823 ActualArg = HandleByValArgument(ActualArg, TheCall, CalledFunc, IFI,
824 CalledFunc->getParamAlignment(ArgNo+1));
826 // Calls that we inline may use the new alloca, so we need to clear
827 // their 'tail' flags if HandleByValArgument introduced a new alloca and
828 // the callee has calls.
829 MustClearTailCallFlags |= ActualArg != *AI;
830 }
832 VMap[I] = ActualArg;
833 }
835 // We want the inliner to prune the code as it copies. We would LOVE to
836 // have no dead or constant instructions leftover after inlining occurs
837 // (which can happen, e.g., because an argument was constant), but we'll be
838 // happy with whatever the cloner can do.
839 CloneAndPruneFunctionInto(Caller, CalledFunc, VMap,
840 /*ModuleLevelChanges=*/false, Returns, ".i",
841 &InlinedFunctionInfo, IFI.TD, TheCall);
843 // Remember the first block that is newly cloned over.
844 FirstNewBlock = LastBlock; ++FirstNewBlock;
846 // Update the callgraph if requested.
847 if (IFI.CG)
848 UpdateCallGraphAfterInlining(CS, FirstNewBlock, VMap, IFI);
849 }
851 // If there are any alloca instructions in the block that used to be the entry
852 // block for the callee, move them to the entry block of the caller. First
853 // calculate which instruction they should be inserted before. We insert the
854 // instructions at the end of the current alloca list.
855 //
856 {
857 BasicBlock::iterator InsertPoint = Caller->begin()->begin();
858 for (BasicBlock::iterator I = FirstNewBlock->begin(),
859 E = FirstNewBlock->end(); I != E; ) {
860 AllocaInst *AI = dyn_cast<AllocaInst>(I++);
861 if (AI == 0) continue;
863 // If the alloca is now dead, remove it. This often occurs due to code
864 // specialization.
865 if (AI->use_empty()) {
866 AI->eraseFromParent();
867 continue;
868 }
870 if (!isa<Constant>(AI->getArraySize()))
871 continue;
873 // Keep track of the static allocas that we inline into the caller.
874 IFI.StaticAllocas.push_back(AI);
876 // Scan for the block of allocas that we can move over, and move them
877 // all at once.
878 while (isa<AllocaInst>(I) &&
879 isa<Constant>(cast<AllocaInst>(I)->getArraySize())) {
880 IFI.StaticAllocas.push_back(cast<AllocaInst>(I));
881 ++I;
882 }
884 // Transfer all of the allocas over in a block. Using splice means
885 // that the instructions aren't removed from the symbol table, then
886 // reinserted.
887 Caller->getEntryBlock().getInstList().splice(InsertPoint,
888 FirstNewBlock->getInstList(),
889 AI, I);
890 }
891 }
893 // Leave lifetime markers for the static alloca's, scoping them to the
894 // function we just inlined.
895 if (!IFI.StaticAllocas.empty()) {
896 IRBuilder<> builder(FirstNewBlock->begin());
897 for (unsigned ai = 0, ae = IFI.StaticAllocas.size(); ai != ae; ++ai) {
898 AllocaInst *AI = IFI.StaticAllocas[ai];
900 // If the alloca is already scoped to something smaller than the whole
901 // function then there's no need to add redundant, less accurate markers.
902 if (hasLifetimeMarkers(AI))
903 continue;
905 builder.CreateLifetimeStart(AI);
906 for (unsigned ri = 0, re = Returns.size(); ri != re; ++ri) {
907 IRBuilder<> builder(Returns[ri]);
908 builder.CreateLifetimeEnd(AI);
909 }
910 }
911 }
913 // If the inlined code contained dynamic alloca instructions, wrap the inlined
914 // code with llvm.stacksave/llvm.stackrestore intrinsics.
915 if (InlinedFunctionInfo.ContainsDynamicAllocas) {
916 Module *M = Caller->getParent();
917 // Get the two intrinsics we care about.
918 Function *StackSave = Intrinsic::getDeclaration(M, Intrinsic::stacksave);
919 Function *StackRestore=Intrinsic::getDeclaration(M,Intrinsic::stackrestore);
921 // Insert the llvm.stacksave.
922 CallInst *SavedPtr = IRBuilder<>(FirstNewBlock, FirstNewBlock->begin())
923 .CreateCall(StackSave, "savedstack");
925 // Insert a call to llvm.stackrestore before any return instructions in the
926 // inlined function.
927 for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
928 IRBuilder<>(Returns[i]).CreateCall(StackRestore, SavedPtr);
929 }
931 // Count the number of StackRestore calls we insert.
932 unsigned NumStackRestores = Returns.size();
934 // If we are inlining an invoke instruction, insert restores before each
935 // unwind. These unwinds will be rewritten into branches later.
936 if (InlinedFunctionInfo.ContainsUnwinds && isa<InvokeInst>(TheCall)) {
937 for (Function::iterator BB = FirstNewBlock, E = Caller->end();
938 BB != E; ++BB)
939 if (UnwindInst *UI = dyn_cast<UnwindInst>(BB->getTerminator())) {
940 IRBuilder<>(UI).CreateCall(StackRestore, SavedPtr);
941 ++NumStackRestores;
942 }
943 }
944 }
946 // If we are inlining tail call instruction through a call site that isn't
947 // marked 'tail', we must remove the tail marker for any calls in the inlined
948 // code. Also, calls inlined through a 'nounwind' call site should be marked
949 // 'nounwind'.
950 if (InlinedFunctionInfo.ContainsCalls &&
951 (MustClearTailCallFlags || MarkNoUnwind)) {
952 for (Function::iterator BB = FirstNewBlock, E = Caller->end();
953 BB != E; ++BB)
954 for (BasicBlock::iterator I = BB->begin(), E = BB->end(); I != E; ++I)
955 if (CallInst *CI = dyn_cast<CallInst>(I)) {
956 if (MustClearTailCallFlags)
957 CI->setTailCall(false);
958 if (MarkNoUnwind)
959 CI->setDoesNotThrow();
960 }
961 }
963 // If we are inlining through a 'nounwind' call site then any inlined 'unwind'
964 // instructions are unreachable.
965 if (InlinedFunctionInfo.ContainsUnwinds && MarkNoUnwind)
966 for (Function::iterator BB = FirstNewBlock, E = Caller->end();
967 BB != E; ++BB) {
968 TerminatorInst *Term = BB->getTerminator();
969 if (isa<UnwindInst>(Term)) {
970 new UnreachableInst(Context, Term);
971 BB->getInstList().erase(Term);
972 }
973 }
975 // If we are inlining for an invoke instruction, we must make sure to rewrite
976 // any inlined 'unwind' instructions into branches to the invoke exception
977 // destination, and call instructions into invoke instructions.
978 if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
979 HandleInlinedInvoke(II, FirstNewBlock, InlinedFunctionInfo);
981 // If we cloned in _exactly one_ basic block, and if that block ends in a
982 // return instruction, we splice the body of the inlined callee directly into
983 // the calling basic block.
984 if (Returns.size() == 1 && std::distance(FirstNewBlock, Caller->end()) == 1) {
985 // Move all of the instructions right before the call.
986 OrigBB->getInstList().splice(TheCall, FirstNewBlock->getInstList(),
987 FirstNewBlock->begin(), FirstNewBlock->end());
988 // Remove the cloned basic block.
989 Caller->getBasicBlockList().pop_back();
991 // If the call site was an invoke instruction, add a branch to the normal
992 // destination.
993 if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall))
994 BranchInst::Create(II->getNormalDest(), TheCall);
996 // If the return instruction returned a value, replace uses of the call with
997 // uses of the returned value.
998 if (!TheCall->use_empty()) {
999 ReturnInst *R = Returns[0];
1000 if (TheCall == R->getReturnValue())
1001 TheCall->replaceAllUsesWith(UndefValue::get(TheCall->getType()));
1002 else
1003 TheCall->replaceAllUsesWith(R->getReturnValue());
1004 }
1005 // Since we are now done with the Call/Invoke, we can delete it.
1006 TheCall->eraseFromParent();
1008 // Since we are now done with the return instruction, delete it also.
1009 Returns[0]->eraseFromParent();
1011 // We are now done with the inlining.
1012 return true;
1013 }
1015 // Otherwise, we have the normal case, of more than one block to inline or
1016 // multiple return sites.
1018 // We want to clone the entire callee function into the hole between the
1019 // "starter" and "ender" blocks. How we accomplish this depends on whether
1020 // this is an invoke instruction or a call instruction.
1021 BasicBlock *AfterCallBB;
1022 if (InvokeInst *II = dyn_cast<InvokeInst>(TheCall)) {
1024 // Add an unconditional branch to make this look like the CallInst case...
1025 BranchInst *NewBr = BranchInst::Create(II->getNormalDest(), TheCall);
1027 // Split the basic block. This guarantees that no PHI nodes will have to be
1028 // updated due to new incoming edges, and make the invoke case more
1029 // symmetric to the call case.
1030 AfterCallBB = OrigBB->splitBasicBlock(NewBr,
1031 CalledFunc->getName()+".exit");
1033 } else { // It's a call
1034 // If this is a call instruction, we need to split the basic block that
1035 // the call lives in.
1036 //
1037 AfterCallBB = OrigBB->splitBasicBlock(TheCall,
1038 CalledFunc->getName()+".exit");
1039 }
1041 // Change the branch that used to go to AfterCallBB to branch to the first
1042 // basic block of the inlined function.
1043 //
1044 TerminatorInst *Br = OrigBB->getTerminator();
1045 assert(Br && Br->getOpcode() == Instruction::Br &&
1046 "splitBasicBlock broken!");
1047 Br->setOperand(0, FirstNewBlock);
1050 // Now that the function is correct, make it a little bit nicer. In
1051 // particular, move the basic blocks inserted from the end of the function
1052 // into the space made by splitting the source basic block.
1053 Caller->getBasicBlockList().splice(AfterCallBB, Caller->getBasicBlockList(),
1054 FirstNewBlock, Caller->end());
1056 // Handle all of the return instructions that we just cloned in, and eliminate
1057 // any users of the original call/invoke instruction.
1058 const Type *RTy = CalledFunc->getReturnType();
1060 PHINode *PHI = 0;
1061 if (Returns.size() > 1) {
1062 // The PHI node should go at the front of the new basic block to merge all
1063 // possible incoming values.
1064 if (!TheCall->use_empty()) {
1065 PHI = PHINode::Create(RTy, Returns.size(), TheCall->getName(),
1066 AfterCallBB->begin());
1067 // Anything that used the result of the function call should now use the
1068 // PHI node as their operand.
1069 TheCall->replaceAllUsesWith(PHI);
1070 }
1072 // Loop over all of the return instructions adding entries to the PHI node
1073 // as appropriate.
1074 if (PHI) {
1075 for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
1076 ReturnInst *RI = Returns[i];
1077 assert(RI->getReturnValue()->getType() == PHI->getType() &&
1078 "Ret value not consistent in function!");
1079 PHI->addIncoming(RI->getReturnValue(), RI->getParent());
1080 }
1081 }
1084 // Add a branch to the merge points and remove return instructions.
1085 for (unsigned i = 0, e = Returns.size(); i != e; ++i) {
1086 ReturnInst *RI = Returns[i];
1087 BranchInst::Create(AfterCallBB, RI);
1088 RI->eraseFromParent();
1089 }
1090 } else if (!Returns.empty()) {
1091 // Otherwise, if there is exactly one return value, just replace anything
1092 // using the return value of the call with the computed value.
1093 if (!TheCall->use_empty()) {
1094 if (TheCall == Returns[0]->getReturnValue())
1095 TheCall->replaceAllUsesWith(UndefValue::get(TheCall->getType()));
1096 else
1097 TheCall->replaceAllUsesWith(Returns[0]->getReturnValue());
1098 }
1100 // Splice the code from the return block into the block that it will return
1101 // to, which contains the code that was after the call.
1102 BasicBlock *ReturnBB = Returns[0]->getParent();
1103 AfterCallBB->getInstList().splice(AfterCallBB->begin(),
1104 ReturnBB->getInstList());
1106 // Update PHI nodes that use the ReturnBB to use the AfterCallBB.
1107 ReturnBB->replaceAllUsesWith(AfterCallBB);
1109 // Delete the return instruction now and empty ReturnBB now.
1110 Returns[0]->eraseFromParent();
1111 ReturnBB->eraseFromParent();
1112 } else if (!TheCall->use_empty()) {
1113 // No returns, but something is using the return value of the call. Just
1114 // nuke the result.
1115 TheCall->replaceAllUsesWith(UndefValue::get(TheCall->getType()));
1116 }
1118 // Since we are now done with the Call/Invoke, we can delete it.
1119 TheCall->eraseFromParent();
1121 // We should always be able to fold the entry block of the function into the
1122 // single predecessor of the block...
1123 assert(cast<BranchInst>(Br)->isUnconditional() && "splitBasicBlock broken!");
1124 BasicBlock *CalleeEntry = cast<BranchInst>(Br)->getSuccessor(0);
1126 // Splice the code entry block into calling block, right before the
1127 // unconditional branch.
1128 OrigBB->getInstList().splice(Br, CalleeEntry->getInstList());
1129 CalleeEntry->replaceAllUsesWith(OrigBB); // Update PHI nodes
1131 // Remove the unconditional branch.
1132 OrigBB->getInstList().erase(Br);
1134 // Now we can remove the CalleeEntry block, which is now empty.
1135 Caller->getBasicBlockList().erase(CalleeEntry);
1137 // If we inserted a phi node, check to see if it has a single value (e.g. all
1138 // the entries are the same or undef). If so, remove the PHI so it doesn't
1139 // block other optimizations.
1140 if (PHI)
1141 if (Value *V = SimplifyInstruction(PHI, IFI.TD)) {
1142 PHI->replaceAllUsesWith(V);
1143 PHI->eraseFromParent();
1144 }
1146 return true;
1147 }