]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - test/Analysis/TypeBasedAliasAnalysis/functionattrs.ll
e9fb9418e70433dd73968dcc4f1043695611d424
[opencl/llvm.git] / test / Analysis / TypeBasedAliasAnalysis / functionattrs.ll
1 ; RUN: opt < %s -tbaa -basicaa -functionattrs -S | FileCheck %s
3 ; FunctionAttrs should make use of TBAA.
5 ; Add the readnone attribute, since the only access is a store which TBAA
6 ; says is to constant memory.
7 ;
8 ; It's unusual to see a store to constant memory, but it isn't necessarily
9 ; invalid, as it's possible that this only happens after optimization on a
10 ; code path which isn't ever executed.
12 ; CHECK: define void @test0_yes(i32* nocapture %p) #0 {
13 define void @test0_yes(i32* %p) nounwind {
14   store i32 0, i32* %p, !tbaa !1
15   ret void
16 }
18 ; CHECK: define void @test0_no(i32* nocapture %p) #1 {
19 define void @test0_no(i32* %p) nounwind {
20   store i32 0, i32* %p, !tbaa !2
21   ret void
22 }
24 ; Add the readonly attribute, since there's just a call to a function which 
25 ; TBAA says doesn't modify any memory.
27 ; CHECK: define void @test1_yes(i32* nocapture %p) #2 {
28 define void @test1_yes(i32* %p) nounwind {
29   call void @callee(i32* %p), !tbaa !1
30   ret void
31 }
33 ; CHECK: define void @test1_no(i32* %p) #1 {
34 define void @test1_no(i32* %p) nounwind {
35   call void @callee(i32* %p), !tbaa !2
36   ret void
37 }
39 ; Add the readonly attribute, as above, but this time BasicAA will say
40 ; that the function accesses memory through its arguments, which TBAA
41 ; still says that the function doesn't write to memory.
42 ;
43 ; This is unusual, since the function is memcpy, but as above, this
44 ; isn't necessarily invalid.
46 ; CHECK: define void @test2_yes(i8* nocapture %p, i8* nocapture %q, i64 %n) #0 {
47 define void @test2_yes(i8* %p, i8* %q, i64 %n) nounwind {
48   call void @llvm.memcpy.p0i8.p0i8.i64(i8* %p, i8* %q, i64 %n, i32 1, i1 false), !tbaa !1
49   ret void
50 }
52 ; CHECK: define void @test2_no(i8* nocapture %p, i8* nocapture readonly %q, i64 %n) #1 {
53 define void @test2_no(i8* %p, i8* %q, i64 %n) nounwind {
54   call void @llvm.memcpy.p0i8.p0i8.i64(i8* %p, i8* %q, i64 %n, i32 1, i1 false), !tbaa !2
55   ret void
56 }
58 ; Similar to the others, va_arg only accesses memory through its operand.
60 ; CHECK: define i32 @test3_yes(i8* nocapture %p) #0 {
61 define i32 @test3_yes(i8* %p) nounwind {
62   %t = va_arg i8* %p, i32, !tbaa !1
63   ret i32 %t
64 }
66 ; CHECK: define i32 @test3_no(i8* nocapture %p) #1 {
67 define i32 @test3_no(i8* %p) nounwind {
68   %t = va_arg i8* %p, i32, !tbaa !2
69   ret i32 %t
70 }
72 declare void @callee(i32* %p) nounwind
73 declare void @llvm.memcpy.p0i8.p0i8.i64(i8*, i8*, i64, i32, i1) nounwind
75 ; CHECK: attributes #0 = { nounwind readnone }
76 ; CHECK: attributes #1 = { nounwind }
77 ; CHECK: attributes #2 = { nounwind readonly }
79 ; Root note.
80 !0 = metadata !{ }
82 ; Invariant memory.
83 !1 = metadata !{metadata !3, metadata !3, i64 0, i1 1 }
84 ; Not invariant memory.
85 !2 = metadata !{metadata !3, metadata !3, i64 0, i1 0 }
86 !3 = metadata !{ metadata !"foo", metadata !0 }