1 configure_lit_site_cfg(
2 ${CMAKE_CURRENT_SOURCE_DIR}/lit.site.cfg.in
3 ${CMAKE_CURRENT_BINARY_DIR}/lit.site.cfg
4 )
5 configure_lit_site_cfg(
6 ${CMAKE_CURRENT_SOURCE_DIR}/Unit/lit.site.cfg.in
7 ${CMAKE_CURRENT_BINARY_DIR}/Unit/lit.site.cfg
8 )
10 # Don't include check-llvm into check-all without LLVM_BUILD_TOOLS.
11 if(NOT LLVM_BUILD_TOOLS)
12 set(EXCLUDE_FROM_ALL ON)
13 endif()
15 # Set the depends list as a variable so that it can grow conditionally.
16 # NOTE: Sync the substitutions in test/lit.cfg when adding to this list.
17 set(LLVM_TEST_DEPENDS
18 llvm-config
19 UnitTests
20 BugpointPasses
21 LLVMHello
22 llc
23 lli
24 lli-child-target
25 llvm-ar
26 llvm-as
27 llvm-bcanalyzer
28 llvm-c-test
29 llvm-cov
30 llvm-diff
31 llvm-dis
32 llvm-extract
33 llvm-dwarfdump
34 llvm-link
35 llvm-lto
36 llvm-mc
37 llvm-mcmarkup
38 llvm-nm
39 llvm-objdump
40 llvm-readobj
41 llvm-rtdyld
42 llvm-symbolizer
43 llvm-tblgen
44 macho-dump
45 opt
46 profile_rt-shared
47 FileCheck
48 count
49 not
50 yaml2obj
51 obj2yaml
52 )
54 # If Intel JIT events are supported, depend on a tool that tests the listener.
55 if( LLVM_USE_INTEL_JITEVENTS )
56 set(LLVM_TEST_DEPENDS ${LLVM_TEST_DEPENDS} llvm-jitlistener)
57 endif( LLVM_USE_INTEL_JITEVENTS )
59 add_lit_testsuite(check-llvm "Running the LLVM regression tests"
60 ${CMAKE_CURRENT_BINARY_DIR}
61 PARAMS llvm_site_config=${CMAKE_CURRENT_BINARY_DIR}/lit.site.cfg
62 llvm_unit_site_config=${CMAKE_CURRENT_BINARY_DIR}/Unit/lit.site.cfg
63 DEPENDS ${LLVM_TEST_DEPENDS}
64 )
65 set_target_properties(check-llvm PROPERTIES FOLDER "Tests")
67 # Setup a legacy alias for 'check-llvm'. This will likely change to be an
68 # alias for 'check-all' at some point in the future.
69 add_custom_target(check)
70 add_dependencies(check check-llvm)
71 set_target_properties(check PROPERTIES FOLDER "Tests")