]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - test/CodeGen/ARM/2013-04-16-AAPCS-C4-vs-VFP.ll
Mass update to CodeGen tests to use CHECK-LABEL for labels corresponding to function...
[opencl/llvm.git] / test / CodeGen / ARM / 2013-04-16-AAPCS-C4-vs-VFP.ll
1 ;Check 5.5 Parameter Passing --> Stage C --> C.4 statement, when NSAA is not
2 ;equal to SP.
3 ;
4 ; Our purpose: make NSAA != SP, and only after start to use GPRs. 
5 ;
6 ;Co-Processor register candidates may be either in VFP or in stack, so after
7 ;all VFP are allocated, stack is used. We can use stack without GPR allocation
8 ;in that case, passing 9 f64 params, for example.
9 ;First eight params goes to d0-d7, ninth one goes to the stack.
10 ;Now, as 10th parameter, we pass i32, and it must go to R0.
11 ;
12 ;5.5 Parameter Passing, Stage C:
13 ;
14 ;C.2.cp If the argument is a CPRC then any co-processor registers in that class
15 ;that are unallocated are marked as unavailable. The NSAA is adjusted upwards
16 ;until it is correctly aligned for the argument and the argument is copied to
17 ;the memory at the adjusted NSAA. The NSAA is further incremented by the size
18 ;of the argument. The argument has now been allocated.
19 ;...
20 ;C.4 If the size in words of the argument is not more than r4 minus NCRN, the
21 ;argument is copied into core registers, starting at the NCRN. The NCRN is
22 ;incremented by the number of registers used. Successive registers hold the
23 ;parts of the argument they would hold if its value were loaded into those
24 ;registers from memory using an LDM instruction. The argument has now been
25 ;allocated.
26 ;
27 ;What is actually checked here:
28 ;Here we check that i32 param goes to r0.
29 ;
30 ;Current test-case was produced with command:
31 ;arm-linux-gnueabihf-clang -mcpu=cortex-a9 params-to-GPR.c -S -O1 -emit-llvm
32 ;
33 ;// params-to-GRP.c:
34 ;
35 ;void fooUseI32(unsigned);
36 ;
37 ;void foo(long double p0,
38 ;         long double p1,
39 ;         long double p2,
40 ;         long double p3,
41 ;         long double p4,
42 ;         long double p5,
43 ;         long double p6,
44 ;         long double p7,
45 ;         long double p8,
46 ;         unsigned p9) {
47 ;  fooUseI32(p9);
48 ;}
49 ;
50 ;void doFoo() {
51 ;  foo( 1,2,3,4,5,6,7,8,9, 43 );
52 ;}
54 ;RUN: llc -mtriple=thumbv7-linux-gnueabihf -float-abi=hard < %s | FileCheck %s
55 ;
56 ;CHECK-LABEL:     foo:
57 ;CHECK-NOT:     mov r0
58 ;CHECK-NOT:     ldr r0
59 ;CHECK:         bl fooUseI32
60 ;CHECK-LABEL:     doFoo:
61 ;CHECK:         movs    r0, #43
62 ;CHECK:         bl      foo
64 define void @foo(double %p0, ; --> D0
65                  double %p1, ; --> D1
66                  double %p2, ; --> D2
67                  double %p3, ; --> D3
68                  double %p4, ; --> D4
69                  double %p5, ; --> D5
70                  double %p6, ; --> D6
71                  double %p7, ; --> D7
72                  double %p8, ; --> Stack
73                  i32 %p9) #0 { ; --> R0, not Stack+8
74 entry:
75   tail call void @fooUseI32(i32 %p9)
76   ret void
77 }
79 declare void @fooUseI32(i32)
81 define void @doFoo() {
82 entry:
83   tail call void @foo(double 23.0, ; --> D0
84                       double 23.1, ; --> D1
85                       double 23.2, ; --> D2
86                       double 23.3, ; --> D3
87                       double 23.4, ; --> D4
88                       double 23.5, ; --> D5
89                       double 23.6, ; --> D6
90                       double 23.7, ; --> D7
91                       double 23.8, ; --> Stack
92                       i32 43)      ; --> R0, not Stack+8
93   ret void
94 }