1 ; RUN: llc < %s -mtriple=armv7-apple-darwin | FileCheck %s
3 ; PR7158
4 define i32 @test_pr7158() nounwind {
5 bb.nph55.bb.nph55.split_crit_edge:
6 br label %bb3
8 bb3: ; preds = %bb3, %bb.nph55.bb.nph55.split_crit_edge
9 br i1 undef, label %bb.i19, label %bb3
11 bb.i19: ; preds = %bb.i19, %bb3
12 %0 = insertelement <4 x float> undef, float undef, i32 3 ; <<4 x float>> [#uses=3]
13 %1 = fmul <4 x float> %0, %0 ; <<4 x float>> [#uses=1]
14 %2 = bitcast <4 x float> %1 to <2 x double> ; <<2 x double>> [#uses=0]
15 %3 = fmul <4 x float> %0, undef ; <<4 x float>> [#uses=0]
16 br label %bb.i19
17 }
19 ; Check that the DAG combiner does not arbitrarily modify BUILD_VECTORs
20 ; after legalization.
21 define void @test_illegal_build_vector() nounwind {
22 entry:
23 store <2 x i64> undef, <2 x i64>* undef, align 16
24 %0 = load <16 x i8>* undef, align 16 ; <<16 x i8>> [#uses=1]
25 %1 = or <16 x i8> zeroinitializer, %0 ; <<16 x i8>> [#uses=1]
26 store <16 x i8> %1, <16 x i8>* undef, align 16
27 ret void
28 }
30 ; Radar 8407927: Make sure that VMOVRRD gets optimized away when the result is
31 ; converted back to be used as a vector type.
32 ; CHECK-LABEL: test_vmovrrd_combine:
33 define <4 x i32> @test_vmovrrd_combine() nounwind {
34 entry:
35 br i1 undef, label %bb1, label %bb2
37 bb1:
38 %0 = bitcast <2 x i64> zeroinitializer to <2 x double>
39 %1 = extractelement <2 x double> %0, i32 0
40 %2 = bitcast double %1 to i64
41 %3 = insertelement <1 x i64> undef, i64 %2, i32 0
42 ; CHECK-NOT: vmov s
43 ; CHECK: vext.8
44 %4 = shufflevector <1 x i64> %3, <1 x i64> undef, <2 x i32> <i32 0, i32 1>
45 %tmp2006.3 = bitcast <2 x i64> %4 to <16 x i8>
46 %5 = shufflevector <16 x i8> %tmp2006.3, <16 x i8> undef, <16 x i32> <i32 4, i32 5, i32 6, i32 7, i32 8, i32 9, i32 10, i32 11, i32 12, i32 13, i32 14, i32 15, i32 16, i32 17, i32 18, i32 19>
47 %tmp2004.3 = bitcast <16 x i8> %5 to <4 x i32>
48 br i1 undef, label %bb2, label %bb1
50 bb2:
51 %result = phi <4 x i32> [ undef, %entry ], [ %tmp2004.3, %bb1 ]
52 ret <4 x i32> %result
53 }
55 ; Test trying to do a ShiftCombine on illegal types.
56 ; The vector should be split first.
57 define void @lshrIllegalType(<8 x i32>* %A) nounwind {
58 %tmp1 = load <8 x i32>* %A
59 %tmp2 = lshr <8 x i32> %tmp1, < i32 3, i32 3, i32 3, i32 3, i32 3, i32 3, i32 3, i32 3>
60 store <8 x i32> %tmp2, <8 x i32>* %A
61 ret void
62 }
64 ; Test folding a binary vector operation with constant BUILD_VECTOR
65 ; operands with i16 elements.
66 define void @test_i16_constant_fold() nounwind optsize {
67 entry:
68 %0 = sext <4 x i1> zeroinitializer to <4 x i16>
69 %1 = add <4 x i16> %0, zeroinitializer
70 %2 = shufflevector <4 x i16> %1, <4 x i16> undef, <8 x i32> <i32 0, i32 1, i32 2, i32 3, i32 4, i32 5, i32 6, i32 7>
71 %3 = add <8 x i16> %2, <i16 1, i16 1, i16 1, i16 1, i16 1, i16 1, i16 1, i16 1>
72 %4 = trunc <8 x i16> %3 to <8 x i8>
73 tail call void @llvm.arm.neon.vst1.v8i8(i8* undef, <8 x i8> %4, i32 1)
74 unreachable
75 }
77 declare void @llvm.arm.neon.vst1.v8i8(i8*, <8 x i8>, i32) nounwind
79 ; Test that loads and stores of i64 vector elements are handled as f64 values
80 ; so they are not split up into i32 values. Radar 8755338.
81 define void @i64_buildvector(i64* %ptr, <2 x i64>* %vp) nounwind {
82 ; CHECK: i64_buildvector
83 ; CHECK: vldr
84 %t0 = load i64* %ptr, align 4
85 %t1 = insertelement <2 x i64> undef, i64 %t0, i32 0
86 store <2 x i64> %t1, <2 x i64>* %vp
87 ret void
88 }
90 define void @i64_insertelement(i64* %ptr, <2 x i64>* %vp) nounwind {
91 ; CHECK: i64_insertelement
92 ; CHECK: vldr
93 %t0 = load i64* %ptr, align 4
94 %vec = load <2 x i64>* %vp
95 %t1 = insertelement <2 x i64> %vec, i64 %t0, i32 0
96 store <2 x i64> %t1, <2 x i64>* %vp
97 ret void
98 }
100 define void @i64_extractelement(i64* %ptr, <2 x i64>* %vp) nounwind {
101 ; CHECK: i64_extractelement
102 ; CHECK: vstr
103 %vec = load <2 x i64>* %vp
104 %t1 = extractelement <2 x i64> %vec, i32 0
105 store i64 %t1, i64* %ptr
106 ret void
107 }
109 ; Test trying to do a AND Combine on illegal types.
110 define void @andVec(<3 x i8>* %A) nounwind {
111 %tmp = load <3 x i8>* %A, align 4
112 %and = and <3 x i8> %tmp, <i8 7, i8 7, i8 7>
113 store <3 x i8> %and, <3 x i8>* %A
114 ret void
115 }
118 ; Test trying to do an OR Combine on illegal types.
119 define void @orVec(<3 x i8>* %A) nounwind {
120 %tmp = load <3 x i8>* %A, align 4
121 %or = or <3 x i8> %tmp, <i8 7, i8 7, i8 7>
122 store <3 x i8> %or, <3 x i8>* %A
123 ret void
124 }
126 ; The following test was hitting an assertion in the DAG combiner when
127 ; constant folding the multiply because the "sext undef" was translated to
128 ; a BUILD_VECTOR with i32 0 operands, which did not match the i16 operands
129 ; of the other BUILD_VECTOR.
130 define i16 @foldBuildVectors() {
131 %1 = sext <8 x i8> undef to <8 x i16>
132 %2 = mul <8 x i16> %1, <i16 255, i16 255, i16 255, i16 255, i16 255, i16 255, i16 255, i16 255>
133 %3 = extractelement <8 x i16> %2, i32 0
134 ret i16 %3
135 }
137 ; Test that we are generating vrev and vext for reverse shuffles of v8i16
138 ; shuffles.
139 ; CHECK-LABEL: reverse_v8i16:
140 define void @reverse_v8i16(<8 x i16>* %loadaddr, <8 x i16>* %storeaddr) {
141 %v0 = load <8 x i16>* %loadaddr
142 ; CHECK: vrev64.16
143 ; CHECK: vext.16
144 %v1 = shufflevector <8 x i16> %v0, <8 x i16> undef,
145 <8 x i32> <i32 7, i32 6, i32 5, i32 4, i32 3, i32 2, i32 1, i32 0>
146 store <8 x i16> %v1, <8 x i16>* %storeaddr
147 ret void
148 }
150 ; Test that we are generating vrev and vext for reverse shuffles of v16i8
151 ; shuffles.
152 ; CHECK-LABEL: reverse_v16i8:
153 define void @reverse_v16i8(<16 x i8>* %loadaddr, <16 x i8>* %storeaddr) {
154 %v0 = load <16 x i8>* %loadaddr
155 ; CHECK: vrev64.8
156 ; CHECK: vext.8
157 %v1 = shufflevector <16 x i8> %v0, <16 x i8> undef,
158 <16 x i32> <i32 15, i32 14, i32 13, i32 12, i32 11, i32 10, i32 9, i32 8,
159 i32 7, i32 6, i32 5, i32 4, i32 3, i32 2, i32 1, i32 0>
160 store <16 x i8> %v1, <16 x i8>* %storeaddr
161 ret void
162 }
164 ; <rdar://problem/14170854>.
165 ; vldr cannot handle unaligned loads.
166 ; Fall back to vld1.32, which can, instead of using the general purpose loads
167 ; followed by a costly sequence of instructions to build the vector register.
168 ; CHECK-LABEL: t3:
169 ; CHECK: vld1.32 {[[REG:d[0-9]+]][0]}
170 ; CHECK: vld1.32 {[[REG]][1]}
171 ; CHECK: vmull.u8 q{{[0-9]+}}, [[REG]], [[REG]]
172 define <8 x i16> @t3(i8 zeroext %xf, i8* nocapture %sp0, i8* nocapture %sp1, i32* nocapture %outp) {
173 entry:
174 %pix_sp0.0.cast = bitcast i8* %sp0 to i32*
175 %pix_sp0.0.copyload = load i32* %pix_sp0.0.cast, align 1
176 %pix_sp1.0.cast = bitcast i8* %sp1 to i32*
177 %pix_sp1.0.copyload = load i32* %pix_sp1.0.cast, align 1
178 %vecinit = insertelement <2 x i32> undef, i32 %pix_sp0.0.copyload, i32 0
179 %vecinit1 = insertelement <2 x i32> %vecinit, i32 %pix_sp1.0.copyload, i32 1
180 %0 = bitcast <2 x i32> %vecinit1 to <8 x i8>
181 %vmull.i = tail call <8 x i16> @llvm.arm.neon.vmullu.v8i16(<8 x i8> %0, <8 x i8> %0)
182 ret <8 x i16> %vmull.i
183 }
185 ; Function Attrs: nounwind readnone
186 declare <8 x i16> @llvm.arm.neon.vmullu.v8i16(<8 x i8>, <8 x i8>)
188 ; Check that (insert_vector_elt (load)) => (vector_load).
189 ; Thus, check that scalar_to_vector do not interfer with that.
190 define <8 x i16> @t4(i8* nocapture %sp0) {
191 ; CHECK-LABEL: t4:
192 ; CHECK: vld1.32 {{{d[0-9]+}}[0]}, [r0]
193 entry:
194 %pix_sp0.0.cast = bitcast i8* %sp0 to i32*
195 %pix_sp0.0.copyload = load i32* %pix_sp0.0.cast, align 1
196 %vec = insertelement <2 x i32> undef, i32 %pix_sp0.0.copyload, i32 0
197 %0 = bitcast <2 x i32> %vec to <8 x i8>
198 %vmull.i = tail call <8 x i16> @llvm.arm.neon.vmullu.v8i16(<8 x i8> %0, <8 x i8> %0)
199 ret <8 x i16> %vmull.i
200 }
202 ; Make sure vector load is used for all three loads.
203 ; Lowering to build vector was breaking the single use property of the load of
204 ; %pix_sp0.0.copyload.
205 ; CHECK-LABEL: t5:
206 ; CHECK: vld1.32 {[[REG1:d[0-9]+]][1]}, [r0]
207 ; CHECK: vorr [[REG2:d[0-9]+]], [[REG1]], [[REG1]]
208 ; CHECK: vld1.32 {[[REG1]][0]}, [r1]
209 ; CHECK: vld1.32 {[[REG2]][0]}, [r2]
210 ; CHECK: vmull.u8 q{{[0-9]+}}, [[REG1]], [[REG2]]
211 define <8 x i16> @t5(i8* nocapture %sp0, i8* nocapture %sp1, i8* nocapture %sp2) {
212 entry:
213 %pix_sp0.0.cast = bitcast i8* %sp0 to i32*
214 %pix_sp0.0.copyload = load i32* %pix_sp0.0.cast, align 1
215 %pix_sp1.0.cast = bitcast i8* %sp1 to i32*
216 %pix_sp1.0.copyload = load i32* %pix_sp1.0.cast, align 1
217 %pix_sp2.0.cast = bitcast i8* %sp2 to i32*
218 %pix_sp2.0.copyload = load i32* %pix_sp2.0.cast, align 1
219 %vec = insertelement <2 x i32> undef, i32 %pix_sp0.0.copyload, i32 1
220 %vecinit1 = insertelement <2 x i32> %vec, i32 %pix_sp1.0.copyload, i32 0
221 %vecinit2 = insertelement <2 x i32> %vec, i32 %pix_sp2.0.copyload, i32 0
222 %0 = bitcast <2 x i32> %vecinit1 to <8 x i8>
223 %1 = bitcast <2 x i32> %vecinit2 to <8 x i8>
224 %vmull.i = tail call <8 x i16> @llvm.arm.neon.vmullu.v8i16(<8 x i8> %0, <8 x i8> %1)
225 ret <8 x i16> %vmull.i
226 }
228 ; <rdar://problem/14989896> Make sure we manage to truncate a vector from an
229 ; illegal type to a legal type.
230 define <2 x i8> @test_truncate(<2 x i128> %in) {
231 ; CHECK-LABEL: test_truncate:
232 ; CHECK: mov [[BASE:r[0-9]+]], sp
233 ; CHECK-NEXT: vld1.32 {[[REG1:d[0-9]+]][0]}, {{\[}}[[BASE]]:32]
234 ; CHECK-NEXT: add [[BASE2:r[0-9]+]], [[BASE]], #4
235 ; CHECK-NEXT: vld1.32 {[[REG1]][1]}, {{\[}}[[BASE2]]:32]
236 ; REG2 Should map on the same Q register as REG1, i.e., REG2 = REG1 - 1, but we
237 ; cannot express that.
238 ; CHECK-NEXT: vmov.32 [[REG2:d[0-9]+]][0], r0
239 ; CHECK-NEXT: vmov.32 [[REG2]][1], r1
240 ; The Q register used here should match floor(REG1/2), but we cannot express that.
241 ; CHECK-NEXT: vmovn.i64 [[RES:d[0-9]+]], q{{[0-9]+}}
242 ; CHECK-NEXT: vmov r0, r1, [[RES]]
243 entry:
244 %res = trunc <2 x i128> %in to <2 x i8>
245 ret <2 x i8> %res
246 }