1 ; Test the handling of base + index + displacement addresses for large frames,
2 ; in cases where both 12-bit and 20-bit displacements are allowed.
3 ;
4 ; RUN: llc < %s -mtriple=s390x-linux-gnu | FileCheck -check-prefix=CHECK-NOFP %s
5 ; RUN: llc < %s -mtriple=s390x-linux-gnu -disable-fp-elim | FileCheck -check-prefix=CHECK-FP %s
7 ; This file tests what happens when a displacement is converted from
8 ; being relative to the start of a frame object to being relative to
9 ; the frame itself. In some cases the test is only possible if two
10 ; objects are allocated.
11 ;
12 ; Rather than rely on a particular order for those objects, the tests
13 ; instead allocate two objects of the same size and apply the test to
14 ; both of them. For consistency, all tests follow this model, even if
15 ; one object would actually be enough.
17 ; First check the highest offset that is in range of the 12-bit form.
18 ;
19 ; The last in-range doubleword offset is 4088. Since the frame has two
20 ; emergency spill slots at 160(%r15), the amount that we need to allocate
21 ; in order to put another object at offset 4088 is 4088 - 176 = 3912 bytes.
22 define void @f1(i8 %byte) {
23 ; CHECK-NOFP-LABEL: f1:
24 ; CHECK-NOFP: stc %r2, 4095(%r15)
25 ; CHECK-NOFP: br %r14
26 ;
27 ; CHECK-FP-LABEL: f1:
28 ; CHECK-FP: stc %r2, 4095(%r11)
29 ; CHECK-FP: br %r14
30 %region1 = alloca [3912 x i8], align 8
31 %region2 = alloca [3912 x i8], align 8
32 %ptr1 = getelementptr inbounds [3912 x i8]* %region1, i64 0, i64 7
33 %ptr2 = getelementptr inbounds [3912 x i8]* %region2, i64 0, i64 7
34 store volatile i8 %byte, i8 *%ptr1
35 store volatile i8 %byte, i8 *%ptr2
36 ret void
37 }
39 ; Test the first offset that is out-of-range of the 12-bit form.
40 define void @f2(i8 %byte) {
41 ; CHECK-NOFP-LABEL: f2:
42 ; CHECK-NOFP: stcy %r2, 4096(%r15)
43 ; CHECK-NOFP: br %r14
44 ;
45 ; CHECK-FP-LABEL: f2:
46 ; CHECK-FP: stcy %r2, 4096(%r11)
47 ; CHECK-FP: br %r14
48 %region1 = alloca [3912 x i8], align 8
49 %region2 = alloca [3912 x i8], align 8
50 %ptr1 = getelementptr inbounds [3912 x i8]* %region1, i64 0, i64 8
51 %ptr2 = getelementptr inbounds [3912 x i8]* %region2, i64 0, i64 8
52 store volatile i8 %byte, i8 *%ptr1
53 store volatile i8 %byte, i8 *%ptr2
54 ret void
55 }
57 ; Test the last offset that is in range of the 20-bit form.
58 ;
59 ; The last in-range doubleword offset is 524280, so by the same reasoning
60 ; as above, we need to allocate objects of 524280 - 176 = 524104 bytes.
61 define void @f3(i8 %byte) {
62 ; CHECK-NOFP-LABEL: f3:
63 ; CHECK-NOFP: stcy %r2, 524287(%r15)
64 ; CHECK-NOFP: br %r14
65 ;
66 ; CHECK-FP-LABEL: f3:
67 ; CHECK-FP: stcy %r2, 524287(%r11)
68 ; CHECK-FP: br %r14
69 %region1 = alloca [524104 x i8], align 8
70 %region2 = alloca [524104 x i8], align 8
71 %ptr1 = getelementptr inbounds [524104 x i8]* %region1, i64 0, i64 7
72 %ptr2 = getelementptr inbounds [524104 x i8]* %region2, i64 0, i64 7
73 store volatile i8 %byte, i8 *%ptr1
74 store volatile i8 %byte, i8 *%ptr2
75 ret void
76 }
78 ; Test the first out-of-range offset. We can't use an index register here,
79 ; and the offset is also out of LAY's range, so expect a constant load
80 ; followed by an addition.
81 define void @f4(i8 %byte) {
82 ; CHECK-NOFP-LABEL: f4:
83 ; CHECK-NOFP: llilh %r1, 8
84 ; CHECK-NOFP: stc %r2, 0(%r1,%r15)
85 ; CHECK-NOFP: br %r14
86 ;
87 ; CHECK-FP-LABEL: f4:
88 ; CHECK-FP: llilh %r1, 8
89 ; CHECK-FP: stc %r2, 0(%r1,%r11)
90 ; CHECK-FP: br %r14
91 %region1 = alloca [524104 x i8], align 8
92 %region2 = alloca [524104 x i8], align 8
93 %ptr1 = getelementptr inbounds [524104 x i8]* %region1, i64 0, i64 8
94 %ptr2 = getelementptr inbounds [524104 x i8]* %region2, i64 0, i64 8
95 store volatile i8 %byte, i8 *%ptr1
96 store volatile i8 %byte, i8 *%ptr2
97 ret void
98 }
100 ; Add 4095 to the previous offset, to test the other end of the STC range.
101 ; The instruction will actually be STCY before frame lowering.
102 define void @f5(i8 %byte) {
103 ; CHECK-NOFP-LABEL: f5:
104 ; CHECK-NOFP: llilh %r1, 8
105 ; CHECK-NOFP: stc %r2, 4095(%r1,%r15)
106 ; CHECK-NOFP: br %r14
107 ;
108 ; CHECK-FP-LABEL: f5:
109 ; CHECK-FP: llilh %r1, 8
110 ; CHECK-FP: stc %r2, 4095(%r1,%r11)
111 ; CHECK-FP: br %r14
112 %region1 = alloca [524104 x i8], align 8
113 %region2 = alloca [524104 x i8], align 8
114 %ptr1 = getelementptr inbounds [524104 x i8]* %region1, i64 0, i64 4103
115 %ptr2 = getelementptr inbounds [524104 x i8]* %region2, i64 0, i64 4103
116 store volatile i8 %byte, i8 *%ptr1
117 store volatile i8 %byte, i8 *%ptr2
118 ret void
119 }
121 ; Test the next offset after that, which uses STCY instead of STC.
122 define void @f6(i8 %byte) {
123 ; CHECK-NOFP-LABEL: f6:
124 ; CHECK-NOFP: llilh %r1, 8
125 ; CHECK-NOFP: stcy %r2, 4096(%r1,%r15)
126 ; CHECK-NOFP: br %r14
127 ;
128 ; CHECK-FP-LABEL: f6:
129 ; CHECK-FP: llilh %r1, 8
130 ; CHECK-FP: stcy %r2, 4096(%r1,%r11)
131 ; CHECK-FP: br %r14
132 %region1 = alloca [524104 x i8], align 8
133 %region2 = alloca [524104 x i8], align 8
134 %ptr1 = getelementptr inbounds [524104 x i8]* %region1, i64 0, i64 4104
135 %ptr2 = getelementptr inbounds [524104 x i8]* %region2, i64 0, i64 4104
136 store volatile i8 %byte, i8 *%ptr1
137 store volatile i8 %byte, i8 *%ptr2
138 ret void
139 }
141 ; Now try an offset of 524287 from the start of the object, with the
142 ; object being at offset 1048576 (1 << 20). The backend prefers to create
143 ; anchors 0x10000 bytes apart, so that the high part can be loaded using
144 ; LLILH while still using STC in more cases than 0x40000 anchors would.
145 define void @f7(i8 %byte) {
146 ; CHECK-NOFP-LABEL: f7:
147 ; CHECK-NOFP: llilh %r1, 23
148 ; CHECK-NOFP: stcy %r2, 65535(%r1,%r15)
149 ; CHECK-NOFP: br %r14
150 ;
151 ; CHECK-FP-LABEL: f7:
152 ; CHECK-FP: llilh %r1, 23
153 ; CHECK-FP: stcy %r2, 65535(%r1,%r11)
154 ; CHECK-FP: br %r14
155 %region1 = alloca [1048400 x i8], align 8
156 %region2 = alloca [1048400 x i8], align 8
157 %ptr1 = getelementptr inbounds [1048400 x i8]* %region1, i64 0, i64 524287
158 %ptr2 = getelementptr inbounds [1048400 x i8]* %region2, i64 0, i64 524287
159 store volatile i8 %byte, i8 *%ptr1
160 store volatile i8 %byte, i8 *%ptr2
161 ret void
162 }
164 ; Keep the object-relative offset the same but bump the size of the
165 ; objects by one doubleword.
166 define void @f8(i8 %byte) {
167 ; CHECK-NOFP-LABEL: f8:
168 ; CHECK-NOFP: llilh %r1, 24
169 ; CHECK-NOFP: stc %r2, 7(%r1,%r15)
170 ; CHECK-NOFP: br %r14
171 ;
172 ; CHECK-FP-LABEL: f8:
173 ; CHECK-FP: llilh %r1, 24
174 ; CHECK-FP: stc %r2, 7(%r1,%r11)
175 ; CHECK-FP: br %r14
176 %region1 = alloca [1048408 x i8], align 8
177 %region2 = alloca [1048408 x i8], align 8
178 %ptr1 = getelementptr inbounds [1048408 x i8]* %region1, i64 0, i64 524287
179 %ptr2 = getelementptr inbounds [1048408 x i8]* %region2, i64 0, i64 524287
180 store volatile i8 %byte, i8 *%ptr1
181 store volatile i8 %byte, i8 *%ptr2
182 ret void
183 }
185 ; Check a case where the original displacement is out of range. The backend
186 ; should force separate address logic from the outset. We don't yet do any
187 ; kind of anchor optimization, so there should be no offset on the STC itself.
188 ;
189 ; Before frame lowering this is an LA followed by the AGFI seen below.
190 ; The LA then gets lowered into the LLILH/LA form. The exact sequence
191 ; isn't that important though.
192 define void @f9(i8 %byte) {
193 ; CHECK-NOFP-LABEL: f9:
194 ; CHECK-NOFP: llilh [[R1:%r[1-5]]], 16
195 ; CHECK-NOFP: la [[R2:%r[1-5]]], 8([[R1]],%r15)
196 ; CHECK-NOFP: agfi [[R2]], 524288
197 ; CHECK-NOFP: stc %r2, 0([[R2]])
198 ; CHECK-NOFP: br %r14
199 ;
200 ; CHECK-FP-LABEL: f9:
201 ; CHECK-FP: llilh [[R1:%r[1-5]]], 16
202 ; CHECK-FP: la [[R2:%r[1-5]]], 8([[R1]],%r11)
203 ; CHECK-FP: agfi [[R2]], 524288
204 ; CHECK-FP: stc %r2, 0([[R2]])
205 ; CHECK-FP: br %r14
206 %region1 = alloca [1048408 x i8], align 8
207 %region2 = alloca [1048408 x i8], align 8
208 %ptr1 = getelementptr inbounds [1048408 x i8]* %region1, i64 0, i64 524288
209 %ptr2 = getelementptr inbounds [1048408 x i8]* %region2, i64 0, i64 524288
210 store volatile i8 %byte, i8 *%ptr1
211 store volatile i8 %byte, i8 *%ptr2
212 ret void
213 }
215 ; Repeat f4 in a case that needs the emergency spill slots (because all
216 ; call-clobbered registers are live and no call-saved ones have been
217 ; allocated).
218 define void @f10(i32 *%vptr, i8 %byte) {
219 ; CHECK-NOFP-LABEL: f10:
220 ; CHECK-NOFP: stg [[REGISTER:%r[1-9][0-4]?]], [[OFFSET:160|168]](%r15)
221 ; CHECK-NOFP: llilh [[REGISTER]], 8
222 ; CHECK-NOFP: stc %r3, 0([[REGISTER]],%r15)
223 ; CHECK-NOFP: lg [[REGISTER]], [[OFFSET]](%r15)
224 ; CHECK-NOFP: br %r14
225 ;
226 ; CHECK-FP-LABEL: f10:
227 ; CHECK-FP: stg [[REGISTER:%r[1-9][0-4]?]], [[OFFSET:160|168]](%r11)
228 ; CHECK-FP: llilh [[REGISTER]], 8
229 ; CHECK-FP: stc %r3, 0([[REGISTER]],%r11)
230 ; CHECK-FP: lg [[REGISTER]], [[OFFSET]](%r11)
231 ; CHECK-FP: br %r14
232 %i0 = load volatile i32 *%vptr
233 %i1 = load volatile i32 *%vptr
234 %i4 = load volatile i32 *%vptr
235 %i5 = load volatile i32 *%vptr
236 %region1 = alloca [524104 x i8], align 8
237 %region2 = alloca [524104 x i8], align 8
238 %ptr1 = getelementptr inbounds [524104 x i8]* %region1, i64 0, i64 8
239 %ptr2 = getelementptr inbounds [524104 x i8]* %region2, i64 0, i64 8
240 store volatile i8 %byte, i8 *%ptr1
241 store volatile i8 %byte, i8 *%ptr2
242 store volatile i32 %i0, i32 *%vptr
243 store volatile i32 %i1, i32 *%vptr
244 store volatile i32 %i4, i32 *%vptr
245 store volatile i32 %i5, i32 *%vptr
246 ret void
247 }
249 ; And again with maximum register pressure. The only spill slots that the
250 ; NOFP case needs are the emergency ones, so the offsets are the same as for f4.
251 ; However, the FP case uses %r11 as the frame pointer and must therefore
252 ; spill a second register. This leads to an extra displacement of 8.
253 define void @f11(i32 *%vptr, i8 %byte) {
254 ; CHECK-NOFP-LABEL: f11:
255 ; CHECK-NOFP: stmg %r6, %r15,
256 ; CHECK-NOFP: stg [[REGISTER:%r[1-9][0-4]?]], [[OFFSET:160|168]](%r15)
257 ; CHECK-NOFP: llilh [[REGISTER]], 8
258 ; CHECK-NOFP: stc %r3, 0([[REGISTER]],%r15)
259 ; CHECK-NOFP: lg [[REGISTER]], [[OFFSET]](%r15)
260 ; CHECK-NOFP: lmg %r6, %r15,
261 ; CHECK-NOFP: br %r14
262 ;
263 ; CHECK-FP-LABEL: f11:
264 ; CHECK-FP: stmg %r6, %r15,
265 ; CHECK-FP: stg [[REGISTER:%r[1-9][0-4]?]], [[OFFSET:160|168]](%r11)
266 ; CHECK-FP: llilh [[REGISTER]], 8
267 ; CHECK-FP: stc %r3, 8([[REGISTER]],%r11)
268 ; CHECK-FP: lg [[REGISTER]], [[OFFSET]](%r11)
269 ; CHECK-FP: lmg %r6, %r15,
270 ; CHECK-FP: br %r14
271 %i0 = load volatile i32 *%vptr
272 %i1 = load volatile i32 *%vptr
273 %i4 = load volatile i32 *%vptr
274 %i5 = load volatile i32 *%vptr
275 %i6 = load volatile i32 *%vptr
276 %i7 = load volatile i32 *%vptr
277 %i8 = load volatile i32 *%vptr
278 %i9 = load volatile i32 *%vptr
279 %i10 = load volatile i32 *%vptr
280 %i11 = load volatile i32 *%vptr
281 %i12 = load volatile i32 *%vptr
282 %i13 = load volatile i32 *%vptr
283 %i14 = load volatile i32 *%vptr
284 %region1 = alloca [524104 x i8], align 8
285 %region2 = alloca [524104 x i8], align 8
286 %ptr1 = getelementptr inbounds [524104 x i8]* %region1, i64 0, i64 8
287 %ptr2 = getelementptr inbounds [524104 x i8]* %region2, i64 0, i64 8
288 store volatile i8 %byte, i8 *%ptr1
289 store volatile i8 %byte, i8 *%ptr2
290 store volatile i32 %i0, i32 *%vptr
291 store volatile i32 %i1, i32 *%vptr
292 store volatile i32 %i4, i32 *%vptr
293 store volatile i32 %i5, i32 *%vptr
294 store volatile i32 %i6, i32 *%vptr
295 store volatile i32 %i7, i32 *%vptr
296 store volatile i32 %i8, i32 *%vptr
297 store volatile i32 %i9, i32 *%vptr
298 store volatile i32 %i10, i32 *%vptr
299 store volatile i32 %i11, i32 *%vptr
300 store volatile i32 %i12, i32 *%vptr
301 store volatile i32 %i13, i32 *%vptr
302 store volatile i32 %i14, i32 *%vptr
303 ret void
304 }
306 ; Repeat f4 in a case where the index register is already occupied.
307 define void @f12(i8 %byte, i64 %index) {
308 ; CHECK-NOFP-LABEL: f12:
309 ; CHECK-NOFP: llilh %r1, 8
310 ; CHECK-NOFP: agr %r1, %r15
311 ; CHECK-NOFP: stc %r2, 0(%r3,%r1)
312 ; CHECK-NOFP: br %r14
313 ;
314 ; CHECK-FP-LABEL: f12:
315 ; CHECK-FP: llilh %r1, 8
316 ; CHECK-FP: agr %r1, %r11
317 ; CHECK-FP: stc %r2, 0(%r3,%r1)
318 ; CHECK-FP: br %r14
319 %region1 = alloca [524104 x i8], align 8
320 %region2 = alloca [524104 x i8], align 8
321 %index1 = add i64 %index, 8
322 %ptr1 = getelementptr inbounds [524104 x i8]* %region1, i64 0, i64 %index1
323 %ptr2 = getelementptr inbounds [524104 x i8]* %region2, i64 0, i64 %index1
324 store volatile i8 %byte, i8 *%ptr1
325 store volatile i8 %byte, i8 *%ptr2
326 ret void
327 }