]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - test/CodeGen/X86/fast-isel-gep.ll
[X86][AVX] Added (V)MOVDDUP / (V)MOVSLDUP / (V)MOVSHDUP memory folding + tests.
[opencl/llvm.git] / test / CodeGen / X86 / fast-isel-gep.ll
1 ; RUN: llc < %s -mtriple=x86_64-linux -O0 | FileCheck %s --check-prefix=X64
2 ; RUN: llc < %s -mtriple=x86_64-windows-itanium -O0 | FileCheck %s --check-prefix=X64
3 ; RUN: llc < %s -march=x86 -O0 | FileCheck %s --check-prefix=X32
5 ; GEP indices are interpreted as signed integers, so they
6 ; should be sign-extended to 64 bits on 64-bit targets.
7 ; PR3181
8 define i32 @test1(i32 %t3, i32* %t1) nounwind {
9        %t9 = getelementptr i32* %t1, i32 %t3           ; <i32*> [#uses=1]
10        %t15 = load i32* %t9            ; <i32> [#uses=1]
11        ret i32 %t15
12 ; X32-LABEL: test1:
13 ; X32:          movl    (%eax,%ecx,4), %eax
14 ; X32:          ret
16 ; X64-LABEL: test1:
17 ; X64:          movslq  %e[[A0:di|cx]], %rax
18 ; X64:          movl    (%r[[A1:si|dx]],%rax,4), %eax
19 ; X64:          ret
21 }
22 define i32 @test2(i64 %t3, i32* %t1) nounwind {
23        %t9 = getelementptr i32* %t1, i64 %t3           ; <i32*> [#uses=1]
24        %t15 = load i32* %t9            ; <i32> [#uses=1]
25        ret i32 %t15
26 ; X32-LABEL: test2:
27 ; X32:          movl    (%edx,%ecx,4), %e
28 ; X32:          ret
30 ; X64-LABEL: test2:
31 ; X64:          movl    (%r[[A1]],%r[[A0]],4), %eax
32 ; X64:          ret
33 }
37 ; PR4984
38 define i8 @test3(i8* %start) nounwind {
39 entry:
40   %A = getelementptr i8* %start, i64 -2               ; <i8*> [#uses=1]
41   %B = load i8* %A, align 1                       ; <i8> [#uses=1]
42   ret i8 %B
43   
44   
45 ; X32-LABEL: test3:
46 ; X32:          movl    4(%esp), %eax
47 ; X32:          movb    -2(%eax), %al
48 ; X32:          ret
50 ; X64-LABEL: test3:
51 ; X64:          movb    -2(%r[[A0]]), %al
52 ; X64:          ret
54 }
56 define double @test4(i64 %x, double* %p) nounwind {
57 entry:
58   %x.addr = alloca i64, align 8                   ; <i64*> [#uses=2]
59   %p.addr = alloca double*, align 8               ; <double**> [#uses=2]
60   store i64 %x, i64* %x.addr
61   store double* %p, double** %p.addr
62   %tmp = load i64* %x.addr                        ; <i64> [#uses=1]
63   %add = add nsw i64 %tmp, 16                     ; <i64> [#uses=1]
64   %tmp1 = load double** %p.addr                   ; <double*> [#uses=1]
65   %arrayidx = getelementptr inbounds double* %tmp1, i64 %add ; <double*> [#uses=1]
66   %tmp2 = load double* %arrayidx                  ; <double> [#uses=1]
67   ret double %tmp2
69 ; X32-LABEL: test4:
70 ; X32: 128(%e{{.*}},%e{{.*}},8)
71 ; X64-LABEL: test4:
72 ; X64: 128(%r{{.*}},%r{{.*}},8)
73 }
75 ; PR8961 - Make sure the sext for the GEP addressing comes before the load that
76 ; is folded.
77 define i64 @test5(i8* %A, i32 %I, i64 %B) nounwind {
78   %v8 = getelementptr i8* %A, i32 %I
79   %v9 = bitcast i8* %v8 to i64*
80   %v10 = load i64* %v9
81   %v11 = add i64 %B, %v10
82   ret i64 %v11
83 ; X64-LABEL: test5:
84 ; X64: movslq   %e[[A1]], %rax
85 ; X64-NEXT: (%r[[A0]],%rax),
86 ; X64: ret
87 }
89 ; PR9500, rdar://9156159 - Don't do non-local address mode folding,
90 ; because it may require values which wouldn't otherwise be live out
91 ; of their blocks.
92 define void @test6() {
93 if.end:                                           ; preds = %if.then, %invoke.cont
94   %tmp15 = load i64* undef
95   %dec = add i64 %tmp15, 13
96   store i64 %dec, i64* undef
97   %call17 = invoke i8* @_ZNK18G__FastAllocString4dataEv()
98           to label %invoke.cont16 unwind label %lpad
100 invoke.cont16:                                    ; preds = %if.then14
101   %arrayidx18 = getelementptr inbounds i8* %call17, i64 %dec
102   store i8 0, i8* %arrayidx18
103   unreachable
105 lpad:                                             ; preds = %if.end19, %if.then14, %if.end, %entry
106   %exn = landingpad {i8*, i32} personality i32 (...)* @__gxx_personality_v0
107             cleanup
108   unreachable
110 declare i8* @_ZNK18G__FastAllocString4dataEv() nounwind
113 ; PR10605 / rdar://9930964 - Don't fold loads incorrectly.  The load should
114 ; happen before the store.  
115 define i32 @test7({i32,i32,i32}* %tmp1, i32 %tmp71, i32 %tmp63) nounwind  {
116 ; X64-LABEL: test7:
117 ; X64:    movl  8({{%rdi|%rcx}}), %eax
118 ; X64:     movl $4, 8({{%rdi|%rcx}})
121   %tmp29 = getelementptr inbounds {i32,i32,i32}* %tmp1, i32 0, i32 2
122   %tmp30 = load i32* %tmp29, align 4
124   %p2 = getelementptr inbounds {i32,i32,i32}* %tmp1, i32 0, i32 2
125   store i32 4, i32* %p2
126   
127   %tmp72 = or i32 %tmp71, %tmp30
128   %tmp73 = icmp ne i32 %tmp63, 32
129   br i1 %tmp73, label %T, label %F
131 T:
132   ret i32 %tmp72
134 F:
135   ret i32 4
138 declare i32 @__gxx_personality_v0(...)