fd24bf841688591e1c98ba64882ed5eac71d3ce4
1 ; RUN: llc < %s | FileCheck %s
3 target datalayout = "e-i64:64-f80:128-n8:16:32:64-S128"
4 target triple = "x86_64-pc-linux-gnu"
6 ; This test is checking to make sure that we reuse the same stack slots
7 ; for GC values spilled over two different call sites. Since the order
8 ; of GC arguments differ, niave lowering code would insert loads and
9 ; stores to rearrange items on the stack. We need to make sure (for
10 ; performance) that this doesn't happen.
11 define i32 @back_to_back_calls(i32* %a, i32* %b, i32* %c) #1 {
12 ; CHECK-LABEL: back_to_back_calls
13 ; The exact stores don't matter, but there need to be three stack slots created
14 ; CHECK: movq %rdx, 16(%rsp)
15 ; CHECK: movq %rdi, 8(%rsp)
16 ; CHECK: movq %rsi, (%rsp)
17 %safepoint_token = tail call i32 (void ()*, i32, i32, ...)* @llvm.experimental.gc.statepoint.p0f_isVoidf(void ()* undef, i32 0, i32 0, i32 5, i32 0, i32 -1, i32 0, i32 0, i32 0, i32* %a, i32* %b, i32* %c)
18 %a1 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token, i32 9, i32 9)
19 %b1 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token, i32 9, i32 10)
20 %c1 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token, i32 9, i32 11)
21 ; CHECK: callq
22 ; This is the key check. There should NOT be any memory moves here
23 ; CHECK-NOT: movq
24 %safepoint_token2 = tail call i32 (void ()*, i32, i32, ...)* @llvm.experimental.gc.statepoint.p0f_isVoidf(void ()* undef, i32 0, i32 0, i32 5, i32 0, i32 -1, i32 0, i32 0, i32 0, i32* %c1, i32* %b1, i32* %a1)
25 %a2 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token2, i32 9, i32 11)
26 %b2 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token2, i32 9, i32 10)
27 %c2 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token2, i32 9, i32 9)
28 ; CHECK: callq
29 ret i32 1
30 }
32 ; This test simply checks that minor changes in vm state don't prevent slots
33 ; being reused for gc values.
34 define i32 @reserve_first(i32* %a, i32* %b, i32* %c) #1 {
35 ; CHECK-LABEL: reserve_first
36 ; The exact stores don't matter, but there need to be three stack slots created
37 ; CHECK: movq %rdx, 16(%rsp)
38 ; CHECK: movq %rdi, 8(%rsp)
39 ; CHECK: movq %rsi, (%rsp)
40 %safepoint_token = tail call i32 (void ()*, i32, i32, ...)* @llvm.experimental.gc.statepoint.p0f_isVoidf(void ()* undef, i32 0, i32 0, i32 5, i32 0, i32 -1, i32 0, i32 0, i32 0, i32* %a, i32* %b, i32* %c)
41 %a1 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token, i32 9, i32 9)
42 %b1 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token, i32 9, i32 10)
43 %c1 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token, i32 9, i32 11)
44 ; CHECK: callq
45 ; This is the key check. There should NOT be any memory moves here
46 ; CHECK-NOT: movq
47 %safepoint_token2 = tail call i32 (void ()*, i32, i32, ...)* @llvm.experimental.gc.statepoint.p0f_isVoidf(void ()* undef, i32 0, i32 0, i32 5, i32* %a1, i32 0, i32* %c1, i32 0, i32 0, i32* %c1, i32* %b1, i32* %a1)
48 %a2 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token2, i32 9, i32 11)
49 %b2 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token2, i32 9, i32 10)
50 %c2 = tail call coldcc i32* @llvm.experimental.gc.relocate.p0i32(i32 %safepoint_token2, i32 9, i32 9)
51 ; CHECK: callq
52 ret i32 1
53 }
55 ; Function Attrs: nounwind
56 declare i32* @llvm.experimental.gc.relocate.p0i32(i32, i32, i32) #3
58 declare i32 @llvm.experimental.gc.statepoint.p0f_isVoidf(void ()*, i32, i32, ...)
60 attributes #1 = { uwtable }