1 ; RUN: llc -split-dwarf=Enable -O0 < %s -mtriple=x86_64-unknown-linux-gnu -filetype=obj | llvm-dwarfdump -debug-dump=info - | FileCheck %s
3 ; Test the emission of gmlt-like inlining information into the skeleton unit.
4 ; This allows inline-aware symbolication/backtracing given only the linked
5 ; executable, without needing access to the .dwos.
7 ; A simple example of inlining generated with clang -gsplit-dwarf
9 ; A member function is used to force emission of the declaration of the
10 ; function into the .dwo file, which may be shared with other CUs in the dwo ;
11 ; under fission, but should not be shared with the skeleton's CU. This also
12 ; tests the general case of context emission, which is suppressed in gmlt-like
13 ; data.
15 ; Include a template just to test template parameters are not emitted in
16 ; gmlt-like data.
18 ; And some varargs to make sure DW_TAG_unspecified_parameters is not emitted.
20 ; And a using declaration in a nested lexical_block... because that shouldn't
21 ; be emitted either.
23 ; Minor complication: after generating the LLVM IR, it was manually edited so
24 ; that the 'f1()' call from f3 was reordered to appear between the two inlined
25 ; f1 calls from f2. This causes f2's inlined_subroutine to use DW_AT_ranges,
26 ; thus exercising range list generation/referencing which was buggy.
28 ; struct foo {
29 ; template<typename T>
30 ; static void f2();
31 ; static void f3(...);
32 ; };
33 ;
34 ; void f1();
35 ;
36 ; template<typename T>
37 ; inline __attribute__((always_inline)) void foo::f2() {
38 ; f1();
39 ; f1();
40 ; }
41 ;
42 ; void foo::f3(...) {
43 ; if (true) {
44 ; f1();
45 ; f2<int>();
46 ; using ::foo;
47 ; }
48 ; }
50 ; Check that we emit the usual gmlt-like data for this file, including brief
51 ; descriptions of subprograms with inlined scopes.
53 ; FIXME: Once tools support indexed addresses in the skeleton CU, we should use
54 ; those (DW_FORM_addr would become DW_FORM_GNU_addr_index below) since those
55 ; addresses will already be in the address pool anyway.
57 ; CHECK: DW_TAG_subprogram
58 ; CHECK-NEXT: DW_AT_name {{.*}} "f2<int>"
59 ; CHECK-NOT: DW_
60 ; CHECK: DW_TAG_subprogram
61 ; CHECK-NEXT: DW_AT_low_pc [DW_FORM_addr]
62 ; CHECK-NEXT: DW_AT_high_pc
63 ; CHECK-NEXT: DW_AT_name {{.*}} "f3"
64 ; CHECK-NOT: {{DW_|NULL}}
65 ; CHECK: DW_TAG_inlined_subroutine
66 ; CHECK-NEXT: DW_AT_abstract_origin {{.*}} "f2<int>"
67 ; CHECK-NEXT: DW_AT_ranges
68 ; CHECK-NEXT: DW_AT_call_file
69 ; CHECK-NEXT: DW_AT_call_line {{.*}} (18)
70 ; CHECK-NOT: DW_
72 ; Function Attrs: uwtable
73 define void @_ZN3foo2f3Ez(...) #0 align 2 {
74 entry:
75 call void @_Z2f1v(), !dbg !26
76 call void @_Z2f1v(), !dbg !25
77 call void @_Z2f1v(), !dbg !28
78 ret void, !dbg !29
79 }
81 declare void @_Z2f1v() #1
83 attributes #0 = { uwtable "less-precise-fpmad"="false" "no-frame-pointer-elim"="true" "no-frame-pointer-elim-non-leaf" "no-infs-fp-math"="false" "no-nans-fp-math"="false" "stack-protector-buffer-size"="8" "unsafe-fp-math"="false" "use-soft-float"="false" }
84 attributes #1 = { "less-precise-fpmad"="false" "no-frame-pointer-elim"="true" "no-frame-pointer-elim-non-leaf" "no-infs-fp-math"="false" "no-nans-fp-math"="false" "stack-protector-buffer-size"="8" "unsafe-fp-math"="false" "use-soft-float"="false" }
86 !llvm.dbg.cu = !{!0}
87 !llvm.module.flags = !{!22, !23}
88 !llvm.ident = !{!24}
90 !0 = !{!"0x11\004\00clang version 3.6.0 \000\00\000\00fission-inline.dwo\001", !1, !2, !3, !9, !2, !18} ; [ DW_TAG_compile_unit ] [/tmp/dbginfo/fission-inline.cpp] [DW_LANG_C_plus_plus]
91 !1 = !{!"fission-inline.cpp", !"/tmp/dbginfo"}
92 !2 = !{}
93 !3 = !{!4}
94 !4 = !{!"0x13\00foo\001\008\008\000\000\000", !1, null, null, !5, null, null, !"_ZTS3foo"} ; [ DW_TAG_structure_type ] [foo] [line 1, size 8, align 8, offset 0] [def] [from ]
95 !5 = !{!6}
96 !6 = !{!"0x2e\00f3\00f3\00_ZN3foo2f3Ez\004\000\000\000\000\00256\000\004", !1, !"_ZTS3foo", !7, null, null, null, null, null} ; [ DW_TAG_subprogram ] [line 4] [f3]
97 !7 = !{!"0x15\00\000\000\000\000\000\000", null, null, null, !8, null, null, null} ; [ DW_TAG_subroutine_type ] [line 0, size 0, align 0, offset 0] [from ]
98 !8 = !{null, null}
99 !9 = !{!10, !11}
100 !10 = !{!"0x2e\00f3\00f3\00_ZN3foo2f3Ez\0015\000\001\000\000\00256\000\0015", !1, !"_ZTS3foo", !7, null, void (...)* @_ZN3foo2f3Ez, null, !6, !2} ; [ DW_TAG_subprogram ] [line 15] [def] [f3]
101 !11 = !{!"0x2e\00f2<int>\00f2<int>\00_ZN3foo2f2IiEEvv\0010\000\001\000\000\00256\000\0010", !1, !"_ZTS3foo", !12, null, null, !14, !17, !2} ; [ DW_TAG_subprogram ] [line 10] [def] [f2<int>]
102 !12 = !{!"0x15\00\000\000\000\000\000\000", null, null, null, !13, null, null, null} ; [ DW_TAG_subroutine_type ] [line 0, size 0, align 0, offset 0] [from ]
103 !13 = !{null}
104 !14 = !{!15}
105 !15 = !{!"0x2f\00T\000\000", null, !16, null} ; [ DW_TAG_template_type_parameter ]
106 !16 = !{!"0x24\00int\000\0032\0032\000\000\005", null, null} ; [ DW_TAG_base_type ] [int] [line 0, size 32, align 32, offset 0, enc DW_ATE_signed]
107 !17 = !{!"0x2e\00f2<int>\00f2<int>\00_ZN3foo2f2IiEEvv\0010\000\000\000\000\00256\000\0010", !1, !"_ZTS3foo", !12, null, null, !14, null, null} ; [ DW_TAG_subprogram ] [line 10] [f2<int>]
108 !18 = !{!19}
109 !19 = !{!"0x8\0019\00", !20, !"_ZTS3foo"} ; [ DW_TAG_imported_declaration ]
110 !20 = !{!"0xb\0016\0013\001", !1, !21} ; [ DW_TAG_lexical_block ] [/tmp/dbginfo/fission-inline.cpp]
111 !21 = !{!"0xb\0016\007\000", !1, !10} ; [ DW_TAG_lexical_block ] [/tmp/dbginfo/fission-inline.cpp]
112 !22 = !{i32 2, !"Dwarf Version", i32 4}
113 !23 = !{i32 2, !"Debug Info Version", i32 2}
114 !24 = !{!"clang version 3.6.0 "}
115 !25 = !MDLocation(line: 17, column: 5, scope: !20)
116 !26 = !MDLocation(line: 11, column: 3, scope: !11, inlinedAt: !27)
117 !27 = !MDLocation(line: 18, column: 5, scope: !20)
118 !28 = !MDLocation(line: 12, column: 3, scope: !11, inlinedAt: !27)
119 !29 = !MDLocation(line: 21, column: 1, scope: !10)