1 ; REQUIRES: object-emission
3 ; RUN: %llc_dwarf < %s -filetype=obj | llvm-dwarfdump -debug-dump=info - | FileCheck %s
5 ; Built with clang from the following source:
6 ; void f1(int);
7 ; __attribute__((always_inline)) inline void f2(int i) { f1(i); }
8 ;
9 ; #define MULTICALL \
10 ; f2(x); \
11 ; f2(y);
12 ;
13 ; void f3(int x, int y) { MULTICALL; }
15 ; FIXME: This produces only one inlined_subroutine, with two formal_parameters
16 ; (both named "this"), one for each of the actual inlined subroutines. ;
17 ; Inlined scopes are differentiated by the combination of 'inlined at' (call)
18 ; location and the location within the function. If two calls to the same
19 ; function occur at the same location the scopes end up conflated and there
20 ; appears to be only one inlined function.
21 ; To fix this, we'd need to add some kind of unique metadata per call site, possibly something like:
22 ;
23 ; !42 = !MDLocation(line: 1, scope: !43, inlinedAt: !44)
24 ; !44 = !MDLocation(line: 2, scope: !45)
25 ;
26 ; ->
27 ;
28 ; !42 = !MDLocation(line: 1, scope: !43, inlinedAt: !44)
29 ; !44 = !{!45, !44}
30 ; !45 = !MDLocation(line: 2, scope: !45)
31 ;
32 ; since cycles in metadata are not uniqued, the !44 node would not be shared
33 ; between calls to the same function from the same location, ensuring separate
34 ; inlined subroutines would be generated.
35 ;
36 ; Once this is done, the (insufficient) hack in clang that adds column
37 ; information to call sites to differentiate inlined callers can be removed as it
38 ; will no longer be necessary.
39 ;
40 ; While it might be nice to omit the duplicate parameter in this case (while
41 ; we wait/work on the real fix), it's actually better to leave it in because it
42 ; allows us to hold the invariant that every DbgVariable has a DIE, every time.
43 ; This has proved valuable in finding other bugs, so I want to avoid removing the
44 ; invariant/assertion. Besides, we don't know which one's the right one anyway...
46 ; CHECK: DW_TAG_subprogram
47 ; CHECK: DW_TAG_inlined_subroutine
48 ; CHECK: DW_TAG_formal_parameter
49 ; CHECK-NOT: DW_TAG
50 ; CHECK: DW_TAG_formal_parameter
51 ; CHECK-NOT: DW_TAG
52 ; CHECK: NULL
53 ; CHECK-NOT: DW_TAG
54 ; CHECK: NULL
56 ; Function Attrs: uwtable
57 define void @_Z2f3ii(i32 %x, i32 %y) #0 {
58 entry:
59 %i.addr.i1 = alloca i32, align 4
60 %i.addr.i = alloca i32, align 4
61 %x.addr = alloca i32, align 4
62 %y.addr = alloca i32, align 4
63 store i32 %x, i32* %x.addr, align 4
64 call void @llvm.dbg.declare(metadata i32* %x.addr, metadata !15, metadata !16), !dbg !17
65 store i32 %y, i32* %y.addr, align 4
66 call void @llvm.dbg.declare(metadata i32* %y.addr, metadata !18, metadata !16), !dbg !19
67 %0 = load i32* %x.addr, align 4, !dbg !20
68 store i32 %0, i32* %i.addr.i, align 4, !dbg !20
69 call void @llvm.dbg.declare(metadata i32* %i.addr.i, metadata !21, metadata !16), !dbg !22
70 %1 = load i32* %i.addr.i, align 4, !dbg !23
71 call void @_Z2f1i(i32 %1), !dbg !23
72 %2 = load i32* %y.addr, align 4, !dbg !20
73 store i32 %2, i32* %i.addr.i1, align 4, !dbg !20
74 call void @llvm.dbg.declare(metadata i32* %i.addr.i1, metadata !21, metadata !16), !dbg !22
75 %3 = load i32* %i.addr.i1, align 4, !dbg !23
76 call void @_Z2f1i(i32 %3), !dbg !23
77 ret void, !dbg !24
78 }
80 ; Function Attrs: nounwind readnone
81 declare void @llvm.dbg.declare(metadata, metadata, metadata) #1
83 declare void @_Z2f1i(i32) #2
85 attributes #0 = { uwtable "less-precise-fpmad"="false" "no-frame-pointer-elim"="true" "no-frame-pointer-elim-non-leaf" "no-infs-fp-math"="false" "no-nans-fp-math"="false" "stack-protector-buffer-size"="8" "unsafe-fp-math"="false" "use-soft-float"="false" }
86 attributes #1 = { nounwind readnone }
87 attributes #2 = { "less-precise-fpmad"="false" "no-frame-pointer-elim"="true" "no-frame-pointer-elim-non-leaf" "no-infs-fp-math"="false" "no-nans-fp-math"="false" "stack-protector-buffer-size"="8" "unsafe-fp-math"="false" "use-soft-float"="false" }
89 !llvm.dbg.cu = !{!0}
90 !llvm.module.flags = !{!12, !13}
91 !llvm.ident = !{!14}
93 !0 = !{!"0x11\004\00clang version 3.6.0 \000\00\000\00\001", !1, !2, !2, !3, !2, !2} ; [ DW_TAG_compile_unit ] [/tmp/dbginfo/duplicate_inline.cpp] [DW_LANG_C_plus_plus]
94 !1 = !{!"duplicate_inline.cpp", !"/tmp/dbginfo"}
95 !2 = !{}
96 !3 = !{!4, !9}
97 !4 = !{!"0x2e\00f3\00f3\00_Z2f3ii\008\000\001\000\000\00256\000\008", !1, !5, !6, null, void (i32, i32)* @_Z2f3ii, null, null, !2} ; [ DW_TAG_subprogram ] [line 8] [def] [f3]
98 !5 = !{!"0x29", !1} ; [ DW_TAG_file_type ] [/tmp/dbginfo/duplicate_inline.cpp]
99 !6 = !{!"0x15\00\000\000\000\000\000\000", null, null, null, !7, null, null, null} ; [ DW_TAG_subroutine_type ] [line 0, size 0, align 0, offset 0] [from ]
100 !7 = !{null, !8, !8}
101 !8 = !{!"0x24\00int\000\0032\0032\000\000\005", null, null} ; [ DW_TAG_base_type ] [int] [line 0, size 32, align 32, offset 0, enc DW_ATE_signed]
102 !9 = !{!"0x2e\00f2\00f2\00_Z2f2i\002\000\001\000\000\00256\000\002", !1, !5, !10, null, null, null, null, !2} ; [ DW_TAG_subprogram ] [line 2] [def] [f2]
103 !10 = !{!"0x15\00\000\000\000\000\000\000", null, null, null, !11, null, null, null} ; [ DW_TAG_subroutine_type ] [line 0, size 0, align 0, offset 0] [from ]
104 !11 = !{null, !8}
105 !12 = !{i32 2, !"Dwarf Version", i32 4}
106 !13 = !{i32 2, !"Debug Info Version", i32 2}
107 !14 = !{!"clang version 3.6.0 "}
108 !15 = !{!"0x101\00x\0016777224\000", !4, !5, !8} ; [ DW_TAG_arg_variable ] [x] [line 8]
109 !16 = !{!"0x102"} ; [ DW_TAG_expression ]
110 !17 = !MDLocation(line: 8, column: 13, scope: !4)
111 !18 = !{!"0x101\00y\0033554440\000", !4, !5, !8} ; [ DW_TAG_arg_variable ] [y] [line 8]
112 !19 = !MDLocation(line: 8, column: 20, scope: !4)
113 !20 = !MDLocation(line: 8, column: 25, scope: !4)
114 !21 = !{!"0x101\00i\0016777218\000", !9, !5, !8} ; [ DW_TAG_arg_variable ] [i] [line 2]
115 !22 = !MDLocation(line: 2, column: 51, scope: !9, inlinedAt: !20)
116 !23 = !MDLocation(line: 2, column: 56, scope: !9, inlinedAt: !20)
117 !24 = !MDLocation(line: 8, column: 36, scope: !4)