]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - test/DebugInfo/missing-abstract-variable.ll
Revert "Revert "DI: Fold constant arguments into a single MDString""
[opencl/llvm.git] / test / DebugInfo / missing-abstract-variable.ll
1 ; REQUIRES: object-emission
3 ; RUN: %llc_dwarf -O0 -filetype=obj < %s | llvm-dwarfdump -debug-dump=info - | FileCheck %s
5 ; The formal parameter 'b' for Function 'x' when inlined within 'a' is lost on
6 ; mips and powerpc64 (and on x86_64 at at least -O2). Presumably this is a
7 ; SelectionDAG issue (do mips/powerpc64 use FastISel?).
8 ; XFAIL: mips, powerpc64, s390x
10 ; Build from the following source with clang -O2.
12 ; The important details are that 'x's abstract definition is first built during
13 ; the definition of 'b', where the parameter to 'x' is constant and so 'x's 's'
14 ; variable is optimized away. No abstract definition DIE for 's' is constructed.
15 ; Then, during 'a' emission, the abstract DbgVariable for 's' is created, but
16 ; the abstract DIE isn't (since the abstract definition for 'b' is already
17 ; built). This results in 's' inlined in 'a' being emitted with its name, line,
18 ; file there, rather than referencing an abstract definition.
20 ; extern int t;
21 ;
22 ; void f(int);
23 ;
24 ; inline void x(bool b) {
25 ;   if (b) {
26 ;     int s = t;
27 ;     f(s);
28 ;   }
29 ;   f(0);
30 ; }
31 ;
32 ; void b() {
33 ;   x(false);
34 ; }
35 ;
36 ; void a(bool u) {
37 ;   x(u);
38 ; }
40 ; CHECK: [[ABS_X:.*]]: DW_TAG_subprogram
41 ; CHECK-NOT: DW_TAG
42 ; CHECK:   DW_AT_name {{.*}} "x"
43 ; CHECK-NOT: {{DW_TAG|NULL}}
44 ; CHECK: [[ABS_B:.*]]:   DW_TAG_formal_parameter
45 ; CHECK-NOT: DW_TAG
46 ; CHECK:     DW_AT_name {{.*}} "b"
47 ; CHECK-NOT: {{DW_TAG|NULL}}
48 ; CHECK:       DW_TAG_lexical_block
49 ; CHECK-NOT: {{DW_TAG|NULL}}
50 ; CHECK: [[ABS_S:.*]]:       DW_TAG_variable
51 ; CHECK-NOT: DW_TAG
52 ; CHECK:         DW_AT_name {{.*}} "s"
54 ; CHECK: DW_TAG_subprogram
55 ; CHECK-NOT: DW_TAG
56 ; CHECK:   DW_AT_name {{.*}} "b"
57 ; CHECK-NOT: {{DW_TAG|NULL}}
58 ; CHECK:   DW_TAG_inlined_subroutine
59 ; CHECK-NOT: DW_TAG
60 ; CHECK:     DW_AT_abstract_origin {{.*}} {[[ABS_X]]}
61 ; CHECK-NOT: {{DW_TAG|NULL}}
62 ; CHECK:     DW_TAG_formal_parameter
63 ; CHECK-NOT: DW_TAG
64 ; CHECK:       DW_AT_abstract_origin {{.*}} {[[ABS_B]]}
65 ; Notice 'x's local variable 's' is missing. Not necessarily a bug here,
66 ; since it's been optimized entirely away and it should be described in
67 ; abstract subprogram.
68 ; CHECK-NOT: DW_TAG
69 ; CHECK: NULL
70 ; CHECK-NOT: DW_TAG
71 ; CHECK: NULL
73 ; CHECK: DW_TAG_subprogram
74 ; CHECK-NOT: DW_TAG
75 ; CHECK:   DW_AT_name {{.*}} "a"
76 ; CHECK-NOT: {{DW_TAG|NULL}}
77 ; CHECK:   DW_TAG_formal_parameter
78 ; CHECK-NOT: {{DW_TAG|NULL}}
79 ; CHECK:   DW_TAG_inlined_subroutine
80 ; CHECK-NOT: DW_TAG
81 ; CHECK:     DW_AT_abstract_origin {{.*}} {[[ABS_X]]}
82 ; CHECK-NOT: {{DW_TAG|NULL}}
83 ; FIXME: This formal parameter goes missing at least at -O2 (& on
84 ; mips/powerpc), maybe before that. Perhaps SelectionDAG is to blame (and
85 ; fastisel succeeds).
86 ; CHECK:     DW_TAG_formal_parameter
87 ; CHECK-NOT: DW_TAG
88 ; CHECK:       DW_AT_abstract_origin {{.*}} {[[ABS_B]]}
90 ; CHECK-NOT: {{DW_TAG|NULL}}
91 ; CHECK:     DW_TAG_lexical_block
92 ; CHECK-NOT: {{DW_TAG|NULL}}
93 ; CHECK:       DW_TAG_variable
94 ; CHECK-NOT: DW_TAG
95 ; CHECK:         DW_AT_abstract_origin {{.*}} {[[ABS_S]]}
97 @t = external global i32
99 ; Function Attrs: uwtable
100 define void @_Z1bv() #0 {
101 entry:
102   tail call void @llvm.dbg.value(metadata !24, i64 0, metadata !25, metadata !{metadata !"0x102"}), !dbg !27
103   tail call void @_Z1fi(i32 0), !dbg !28
104   ret void, !dbg !29
107 ; Function Attrs: uwtable
108 define void @_Z1ab(i1 zeroext %u) #0 {
109 entry:
110   tail call void @llvm.dbg.value(metadata !{i1 %u}, i64 0, metadata !13, metadata !{metadata !"0x102"}), !dbg !30
111   tail call void @llvm.dbg.value(metadata !{i1 %u}, i64 0, metadata !31, metadata !{metadata !"0x102"}), !dbg !33
112   br i1 %u, label %if.then.i, label %_Z1xb.exit, !dbg !34
114 if.then.i:                                        ; preds = %entry
115   %0 = load i32* @t, align 4, !dbg !35, !tbaa !36
116   tail call void @llvm.dbg.value(metadata !{i32 %0}, i64 0, metadata !40, metadata !{metadata !"0x102"}), !dbg !35
117   tail call void @_Z1fi(i32 %0), !dbg !41
118   br label %_Z1xb.exit, !dbg !42
120 _Z1xb.exit:                                       ; preds = %entry, %if.then.i
121   tail call void @_Z1fi(i32 0), !dbg !43
122   ret void, !dbg !44
125 declare void @_Z1fi(i32) #1
127 ; Function Attrs: nounwind readnone
128 declare void @llvm.dbg.value(metadata, i64, metadata, metadata) #2
130 attributes #0 = { uwtable "less-precise-fpmad"="false" "no-frame-pointer-elim"="false" "no-infs-fp-math"="false" "no-nans-fp-math"="false" "stack-protector-buffer-size"="8" "unsafe-fp-math"="false" "use-soft-float"="false" }
131 attributes #1 = { "less-precise-fpmad"="false" "no-frame-pointer-elim"="false" "no-infs-fp-math"="false" "no-nans-fp-math"="false" "stack-protector-buffer-size"="8" "unsafe-fp-math"="false" "use-soft-float"="false" }
132 attributes #2 = { nounwind readnone }
134 !llvm.dbg.cu = !{!0}
135 !llvm.module.flags = !{!21, !22}
136 !llvm.ident = !{!23}
138 !0 = metadata !{metadata !"0x11\004\00clang version 3.5.0 \001\00\000\00\001", metadata !1, metadata !2, metadata !2, metadata !3, metadata !2, metadata !2} ; [ DW_TAG_compile_unit ] [/tmp/dbginfo/missing-abstract-variables.cc] [DW_LANG_C_plus_plus]
139 !1 = metadata !{metadata !"missing-abstract-variables.cc", metadata !"/tmp/dbginfo"}
140 !2 = metadata !{}
141 !3 = metadata !{metadata !4, metadata !8, metadata !14}
142 !4 = metadata !{metadata !"0x2e\00b\00b\00_Z1bv\0013\000\001\000\006\00256\001\0013", metadata !1, metadata !5, metadata !6, null, void ()* @_Z1bv, null, null, metadata !2} ; [ DW_TAG_subprogram ] [line 13] [def] [b]
143 !5 = metadata !{metadata !"0x29", metadata !1}          ; [ DW_TAG_file_type ] [/tmp/dbginfo/missing-abstract-variables.cc]
144 !6 = metadata !{metadata !"0x15\00\000\000\000\000\000\000", i32 0, null, null, metadata !7, null, null, null} ; [ DW_TAG_subroutine_type ] [line 0, size 0, align 0, offset 0] [from ]
145 !7 = metadata !{null}
146 !8 = metadata !{metadata !"0x2e\00a\00a\00_Z1ab\0017\000\001\000\006\00256\001\0017", metadata !1, metadata !5, metadata !9, null, void (i1)* @_Z1ab, null, null, metadata !12} ; [ DW_TAG_subprogram ] [line 17] [def] [a]
147 !9 = metadata !{metadata !"0x15\00\000\000\000\000\000\000", i32 0, null, null, metadata !10, null, null, null} ; [ DW_TAG_subroutine_type ] [line 0, size 0, align 0, offset 0] [from ]
148 !10 = metadata !{null, metadata !11}
149 !11 = metadata !{metadata !"0x24\00bool\000\008\008\000\000\002", null, null} ; [ DW_TAG_base_type ] [bool] [line 0, size 8, align 8, offset 0, enc DW_ATE_boolean]
150 !12 = metadata !{metadata !13}
151 !13 = metadata !{metadata !"0x101\00u\0016777233\000", metadata !8, metadata !5, metadata !11} ; [ DW_TAG_arg_variable ] [u] [line 17]
152 !14 = metadata !{metadata !"0x2e\00x\00x\00_Z1xb\005\000\001\000\006\00256\001\005", metadata !1, metadata !5, metadata !9, null, null, null, null, metadata !15} ; [ DW_TAG_subprogram ] [line 5] [def] [x]
153 !15 = metadata !{metadata !16, metadata !17}
154 !16 = metadata !{metadata !"0x101\00b\0016777221\000", metadata !14, metadata !5, metadata !11} ; [ DW_TAG_arg_variable ] [b] [line 5]
155 !17 = metadata !{metadata !"0x100\00s\007\000", metadata !18, metadata !5, metadata !20} ; [ DW_TAG_auto_variable ] [s] [line 7]
156 !18 = metadata !{metadata !"0xb\006\000\000", metadata !1, metadata !19} ; [ DW_TAG_lexical_block ] [/tmp/dbginfo/missing-abstract-variables.cc]
157 !19 = metadata !{metadata !"0xb\006\000\000", metadata !1, metadata !14} ; [ DW_TAG_lexical_block ] [/tmp/dbginfo/missing-abstract-variables.cc]
158 !20 = metadata !{metadata !"0x24\00int\000\0032\0032\000\000\005", null, null} ; [ DW_TAG_base_type ] [int] [line 0, size 32, align 32, offset 0, enc DW_ATE_signed]
159 !21 = metadata !{i32 2, metadata !"Dwarf Version", i32 4}
160 !22 = metadata !{i32 2, metadata !"Debug Info Version", i32 2}
161 !23 = metadata !{metadata !"clang version 3.5.0 "}
162 !24 = metadata !{i1 false}
163 !25 = metadata !{metadata !"0x101\00b\0016777221\000", metadata !14, metadata !5, metadata !11, metadata !26} ; [ DW_TAG_arg_variable ] [b] [line 5]
164 !26 = metadata !{i32 14, i32 0, metadata !4, null}
165 !27 = metadata !{i32 5, i32 0, metadata !14, metadata !26}
166 !28 = metadata !{i32 10, i32 0, metadata !14, metadata !26}
167 !29 = metadata !{i32 15, i32 0, metadata !4, null}
168 !30 = metadata !{i32 17, i32 0, metadata !8, null}
169 !31 = metadata !{metadata !"0x101\00b\0016777221\000", metadata !14, metadata !5, metadata !11, metadata !32} ; [ DW_TAG_arg_variable ] [b] [line 5]
170 !32 = metadata !{i32 18, i32 0, metadata !8, null}
171 !33 = metadata !{i32 5, i32 0, metadata !14, metadata !32}
172 !34 = metadata !{i32 6, i32 0, metadata !19, metadata !32}
173 !35 = metadata !{i32 7, i32 0, metadata !18, metadata !32}
174 !36 = metadata !{metadata !37, metadata !37, i64 0}
175 !37 = metadata !{metadata !"int", metadata !38, i64 0}
176 !38 = metadata !{metadata !"omnipotent char", metadata !39, i64 0}
177 !39 = metadata !{metadata !"Simple C/C++ TBAA"}
178 !40 = metadata !{metadata !"0x100\00s\007\000", metadata !18, metadata !5, metadata !20, metadata !32} ; [ DW_TAG_auto_variable ] [s] [line 7]
179 !41 = metadata !{i32 8, i32 0, metadata !18, metadata !32}
180 !42 = metadata !{i32 9, i32 0, metadata !18, metadata !32}
181 !43 = metadata !{i32 10, i32 0, metadata !14, metadata !32}
182 !44 = metadata !{i32 19, i32 0, metadata !8, null}