1 ##----------------------------------------------------------*- Makefile -*-===##
2 ##
3 ## Common rules for generating, linking, and compiling via LLVM. This is
4 ## used to implement a robust testing framework for LLVM
5 ##
6 ##-------------------------------------------------------------------------===##
8 # If the user specified a TEST= option on the command line, we do not want to do
9 # the default testing type. Instead, we change the default target to be the
10 # test:: target.
11 #
12 ifdef TEST
13 test::
14 endif
16 # We do not want to make .d files for tests!
17 DISABLE_AUTO_DEPENDENCIES=1
19 include ${LEVEL}/Makefile.common
21 # Specify ENABLE_STATS on the command line to enable -stats and -time-passes
22 # output from gccas and gccld.
23 ifdef ENABLE_STATS
24 STATS = -stats -time-passes
25 endif
27 .PHONY: clean default
29 # These files, which might be intermediate results, should not be deleted by
30 # make
31 .PRECIOUS: Output/%.bc Output/%.ll
32 .PRECIOUS: Output/%.tbc Output/%.tll
33 .PRECIOUS: Output/.dir
34 .PRECIOUS: Output/%.llvm.bc
35 .PRECIOUS: Output/%.llvm
37 LCCFLAGS += -O2 -Wall
38 LCXXFLAGS += -O2 -Wall
39 LLCFLAGS =
40 TESTRUNR = @echo Running test: $<; \
41 PATH="$(LLVMTOOLCURRENT):$(PATH)" \
42 $(LLVM_SRC_ROOT)/test/TestRunner.sh
44 LLCLIBS := $(LLCLIBS) -lm
46 clean::
47 $(RM) -f a.out core
48 $(RM) -rf Output/
50 # LLVM Assemble from Output/X.ll to Output/X.bc. Output/X.ll must have come
51 # from GCC output, so use GCCAS.
52 #
53 Output/%.bc: Output/%.ll $(LGCCAS)
54 -$(LGCCAS) $(STATS) $< -o $@
56 # LLVM Assemble from X.ll to Output/X.bc. Because we are coming directly from
57 # LLVM source, use the non-transforming assembler.
58 #
59 Output/%.bc: %.ll $(LLVMAS) Output/.dir
60 -$(LLVMAS) $< -o $@
62 ## Cancel built-in implicit rules that override above rules
63 %: %.s
65 %: %.c
67 %.o: %.c