]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - opencl/llvm.git/blob - tools/llvm-objdump/COFFDump.cpp
Re-submit r191472 with a fix for big endian.
[opencl/llvm.git] / tools / llvm-objdump / COFFDump.cpp
1 //===-- COFFDump.cpp - COFF-specific dumper ---------------------*- C++ -*-===//
2 //
3 //                     The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 ///
10 /// \file
11 /// \brief This file implements the COFF-specific dumper for llvm-objdump.
12 /// It outputs the Win64 EH data structures as plain text.
13 /// The encoding of the unwind codes is decribed in MSDN:
14 /// http://msdn.microsoft.com/en-us/library/ck9asaa9.aspx
15 ///
16 //===----------------------------------------------------------------------===//
18 #include "llvm-objdump.h"
19 #include "llvm/Object/COFF.h"
20 #include "llvm/Object/ObjectFile.h"
21 #include "llvm/Support/Format.h"
22 #include "llvm/Support/SourceMgr.h"
23 #include "llvm/Support/Win64EH.h"
24 #include "llvm/Support/raw_ostream.h"
25 #include "llvm/Support/system_error.h"
26 #include <algorithm>
27 #include <cstring>
29 using namespace llvm;
30 using namespace object;
31 using namespace llvm::Win64EH;
33 // Returns the name of the unwind code.
34 static StringRef getUnwindCodeTypeName(uint8_t Code) {
35   switch(Code) {
36   default: llvm_unreachable("Invalid unwind code");
37   case UOP_PushNonVol: return "UOP_PushNonVol";
38   case UOP_AllocLarge: return "UOP_AllocLarge";
39   case UOP_AllocSmall: return "UOP_AllocSmall";
40   case UOP_SetFPReg: return "UOP_SetFPReg";
41   case UOP_SaveNonVol: return "UOP_SaveNonVol";
42   case UOP_SaveNonVolBig: return "UOP_SaveNonVolBig";
43   case UOP_SaveXMM128: return "UOP_SaveXMM128";
44   case UOP_SaveXMM128Big: return "UOP_SaveXMM128Big";
45   case UOP_PushMachFrame: return "UOP_PushMachFrame";
46   }
47 }
49 // Returns the name of a referenced register.
50 static StringRef getUnwindRegisterName(uint8_t Reg) {
51   switch(Reg) {
52   default: llvm_unreachable("Invalid register");
53   case 0: return "RAX";
54   case 1: return "RCX";
55   case 2: return "RDX";
56   case 3: return "RBX";
57   case 4: return "RSP";
58   case 5: return "RBP";
59   case 6: return "RSI";
60   case 7: return "RDI";
61   case 8: return "R8";
62   case 9: return "R9";
63   case 10: return "R10";
64   case 11: return "R11";
65   case 12: return "R12";
66   case 13: return "R13";
67   case 14: return "R14";
68   case 15: return "R15";
69   }
70 }
72 // Calculates the number of array slots required for the unwind code.
73 static unsigned getNumUsedSlots(const UnwindCode &UnwindCode) {
74   switch (UnwindCode.getUnwindOp()) {
75   default: llvm_unreachable("Invalid unwind code");
76   case UOP_PushNonVol:
77   case UOP_AllocSmall:
78   case UOP_SetFPReg:
79   case UOP_PushMachFrame:
80     return 1;
81   case UOP_SaveNonVol:
82   case UOP_SaveXMM128:
83     return 2;
84   case UOP_SaveNonVolBig:
85   case UOP_SaveXMM128Big:
86     return 3;
87   case UOP_AllocLarge:
88     return (UnwindCode.getOpInfo() == 0) ? 2 : 3;
89   }
90 }
92 // Prints one unwind code. Because an unwind code can occupy up to 3 slots in
93 // the unwind codes array, this function requires that the correct number of
94 // slots is provided.
95 static void printUnwindCode(ArrayRef<UnwindCode> UCs) {
96   assert(UCs.size() >= getNumUsedSlots(UCs[0]));
97   outs() <<  format("    0x%02x: ", unsigned(UCs[0].u.CodeOffset))
98          << getUnwindCodeTypeName(UCs[0].getUnwindOp());
99   switch (UCs[0].getUnwindOp()) {
100   case UOP_PushNonVol:
101     outs() << " " << getUnwindRegisterName(UCs[0].getOpInfo());
102     break;
103   case UOP_AllocLarge:
104     if (UCs[0].getOpInfo() == 0) {
105       outs() << " " << UCs[1].FrameOffset;
106     } else {
107       outs() << " " << UCs[1].FrameOffset
108                        + (static_cast<uint32_t>(UCs[2].FrameOffset) << 16);
109     }
110     break;
111   case UOP_AllocSmall:
112     outs() << " " << ((UCs[0].getOpInfo() + 1) * 8);
113     break;
114   case UOP_SetFPReg:
115     outs() << " ";
116     break;
117   case UOP_SaveNonVol:
118     outs() << " " << getUnwindRegisterName(UCs[0].getOpInfo())
119            << format(" [0x%04x]", 8 * UCs[1].FrameOffset);
120     break;
121   case UOP_SaveNonVolBig:
122     outs() << " " << getUnwindRegisterName(UCs[0].getOpInfo())
123            << format(" [0x%08x]", UCs[1].FrameOffset
124                     + (static_cast<uint32_t>(UCs[2].FrameOffset) << 16));
125     break;
126   case UOP_SaveXMM128:
127     outs() << " XMM" << static_cast<uint32_t>(UCs[0].getOpInfo())
128            << format(" [0x%04x]", 16 * UCs[1].FrameOffset);
129     break;
130   case UOP_SaveXMM128Big:
131     outs() << " XMM" << UCs[0].getOpInfo()
132            << format(" [0x%08x]", UCs[1].FrameOffset
133                            + (static_cast<uint32_t>(UCs[2].FrameOffset) << 16));
134     break;
135   case UOP_PushMachFrame:
136     outs() << " " << (UCs[0].getOpInfo() ? "w/o" : "w")
137            << " error code";
138     break;
139   }
140   outs() << "\n";
143 static void printAllUnwindCodes(ArrayRef<UnwindCode> UCs) {
144   for (const UnwindCode *I = UCs.begin(), *E = UCs.end(); I < E; ) {
145     unsigned UsedSlots = getNumUsedSlots(*I);
146     if (UsedSlots > UCs.size()) {
147       outs() << "Unwind data corrupted: Encountered unwind op "
148              << getUnwindCodeTypeName((*I).getUnwindOp())
149              << " which requires " << UsedSlots
150              << " slots, but only " << UCs.size()
151              << " remaining in buffer";
152       return ;
153     }
154     printUnwindCode(ArrayRef<UnwindCode>(I, E));
155     I += UsedSlots;
156   }
159 // Given a symbol sym this functions returns the address and section of it.
160 static error_code resolveSectionAndAddress(const COFFObjectFile *Obj,
161                                            const SymbolRef &Sym,
162                                            const coff_section *&ResolvedSection,
163                                            uint64_t &ResolvedAddr) {
164   if (error_code ec = Sym.getAddress(ResolvedAddr)) return ec;
165   section_iterator iter(Obj->begin_sections());
166   if (error_code ec = Sym.getSection(iter)) return ec;
167   ResolvedSection = Obj->getCOFFSection(iter);
168   return object_error::success;
171 // Given a vector of relocations for a section and an offset into this section
172 // the function returns the symbol used for the relocation at the offset.
173 static error_code resolveSymbol(const std::vector<RelocationRef> &Rels,
174                                 uint64_t Offset, SymbolRef &Sym) {
175   for (std::vector<RelocationRef>::const_iterator I = Rels.begin(),
176                                                   E = Rels.end();
177                                                   I != E; ++I) {
178     uint64_t Ofs;
179     if (error_code ec = I->getOffset(Ofs)) return ec;
180     if (Ofs == Offset) {
181       Sym = *I->getSymbol();
182       break;
183     }
184   }
185   return object_error::success;
188 // Given a vector of relocations for a section and an offset into this section
189 // the function resolves the symbol used for the relocation at the offset and
190 // returns the section content and the address inside the content pointed to
191 // by the symbol.
192 static error_code getSectionContents(const COFFObjectFile *Obj,
193                                      const std::vector<RelocationRef> &Rels,
194                                      uint64_t Offset,
195                                      ArrayRef<uint8_t> &Contents,
196                                      uint64_t &Addr) {
197   SymbolRef Sym;
198   if (error_code ec = resolveSymbol(Rels, Offset, Sym)) return ec;
199   const coff_section *Section;
200   if (error_code ec = resolveSectionAndAddress(Obj, Sym, Section, Addr))
201     return ec;
202   if (error_code ec = Obj->getSectionContents(Section, Contents)) return ec;
203   return object_error::success;
206 // Given a vector of relocations for a section and an offset into this section
207 // the function returns the name of the symbol used for the relocation at the
208 // offset.
209 static error_code resolveSymbolName(const std::vector<RelocationRef> &Rels,
210                                     uint64_t Offset, StringRef &Name) {
211   SymbolRef Sym;
212   if (error_code ec = resolveSymbol(Rels, Offset, Sym)) return ec;
213   if (error_code ec = Sym.getName(Name)) return ec;
214   return object_error::success;
217 static void printCOFFSymbolAddress(llvm::raw_ostream &Out,
218                                    const std::vector<RelocationRef> &Rels,
219                                    uint64_t Offset, uint32_t Disp) {
220   StringRef Sym;
221   if (error_code ec = resolveSymbolName(Rels, Offset, Sym)) {
222     error(ec);
223     return ;
224   }
225   Out << Sym;
226   if (Disp > 0)
227     Out << format(" + 0x%04x", Disp);
230 // Prints import tables. The import table is a table containing the list of
231 // DLL name and symbol names which will be linked by the loader.
232 static void printImportTables(const COFFObjectFile *Obj) {
233   outs() << "The Import Tables:\n";
234   error_code ec;
235   for (import_directory_iterator i = Obj->getImportDirectoryBegin(),
236                                  e = Obj->getImportDirectoryEnd();
237        i != e; i = i.increment(ec)) {
238     if (ec)
239       return;
241     const import_directory_table_entry *Dir;
242     StringRef Name;
243     if (i->getImportTableEntry(Dir)) return;
244     if (i->getName(Name)) return;
246     outs() << format("  lookup %08x time %08x fwd %08x name %08x addr %08x\n\n",
247                      static_cast<uint32_t>(Dir->ImportLookupTableRVA),
248                      static_cast<uint32_t>(Dir->TimeDateStamp),
249                      static_cast<uint32_t>(Dir->ForwarderChain),
250                      static_cast<uint32_t>(Dir->NameRVA),
251                      static_cast<uint32_t>(Dir->ImportAddressTableRVA));
252     outs() << "    DLL Name: " << Name << "\n";
253     outs() << "    Hint/Ord  Name\n";
254     const import_lookup_table_entry32 *entry;
255     if (i->getImportLookupEntry(entry))
256       return;
257     for (; entry->data; ++entry) {
258       if (entry->isOrdinal()) {
259         outs() << format("      % 6d\n", entry->getOrdinal());
260         continue;
261       }
262       uint16_t Hint;
263       StringRef Name;
264       if (Obj->getHintName(entry->getHintNameRVA(), Hint, Name))
265         return;
266       outs() << format("      % 6d  ", Hint) << Name << "\n";
267     }
268     outs() << "\n";
269   }
272 void llvm::printCOFFUnwindInfo(const COFFObjectFile *Obj) {
273   const coff_file_header *Header;
274   if (error(Obj->getCOFFHeader(Header))) return;
276   if (Header->Machine != COFF::IMAGE_FILE_MACHINE_AMD64) {
277     errs() << "Unsupported image machine type "
278               "(currently only AMD64 is supported).\n";
279     return;
280   }
282   const coff_section *Pdata = 0;
284   error_code ec;
285   for (section_iterator SI = Obj->begin_sections(),
286                         SE = Obj->end_sections();
287                         SI != SE; SI.increment(ec)) {
288     if (error(ec)) return;
290     StringRef Name;
291     if (error(SI->getName(Name))) continue;
293     if (Name != ".pdata") continue;
295     Pdata = Obj->getCOFFSection(SI);
296     std::vector<RelocationRef> Rels;
297     for (relocation_iterator RI = SI->begin_relocations(),
298                              RE = SI->end_relocations();
299                              RI != RE; RI.increment(ec)) {
300       if (error(ec)) break;
301       Rels.push_back(*RI);
302     }
304     // Sort relocations by address.
305     std::sort(Rels.begin(), Rels.end(), RelocAddressLess);
307     ArrayRef<uint8_t> Contents;
308     if (error(Obj->getSectionContents(Pdata, Contents))) continue;
309     if (Contents.empty()) continue;
311     ArrayRef<RuntimeFunction> RFs(
312                   reinterpret_cast<const RuntimeFunction *>(Contents.data()),
313                                   Contents.size() / sizeof(RuntimeFunction));
314     for (const RuntimeFunction *I = RFs.begin(), *E = RFs.end(); I < E; ++I) {
315       const uint64_t SectionOffset = std::distance(RFs.begin(), I)
316                                      * sizeof(RuntimeFunction);
318       outs() << "Function Table:\n";
320       outs() << "  Start Address: ";
321       printCOFFSymbolAddress(outs(), Rels, SectionOffset +
322                              /*offsetof(RuntimeFunction, StartAddress)*/ 0,
323                              I->StartAddress);
324       outs() << "\n";
326       outs() << "  End Address: ";
327       printCOFFSymbolAddress(outs(), Rels, SectionOffset +
328                              /*offsetof(RuntimeFunction, EndAddress)*/ 4,
329                              I->EndAddress);
330       outs() << "\n";
332       outs() << "  Unwind Info Address: ";
333       printCOFFSymbolAddress(outs(), Rels, SectionOffset +
334                              /*offsetof(RuntimeFunction, UnwindInfoOffset)*/ 8,
335                              I->UnwindInfoOffset);
336       outs() << "\n";
338       ArrayRef<uint8_t> XContents;
339       uint64_t UnwindInfoOffset = 0;
340       if (error(getSectionContents(Obj, Rels, SectionOffset +
341                               /*offsetof(RuntimeFunction, UnwindInfoOffset)*/ 8,
342                                    XContents, UnwindInfoOffset))) continue;
343       if (XContents.empty()) continue;
345       UnwindInfoOffset += I->UnwindInfoOffset;
346       if (UnwindInfoOffset > XContents.size()) continue;
348       const Win64EH::UnwindInfo *UI =
349                             reinterpret_cast<const Win64EH::UnwindInfo *>
350                               (XContents.data() + UnwindInfoOffset);
352       // The casts to int are required in order to output the value as number.
353       // Without the casts the value would be interpreted as char data (which
354       // results in garbage output).
355       outs() << "  Version: " << static_cast<int>(UI->getVersion()) << "\n";
356       outs() << "  Flags: " << static_cast<int>(UI->getFlags());
357       if (UI->getFlags()) {
358           if (UI->getFlags() & UNW_ExceptionHandler)
359             outs() << " UNW_ExceptionHandler";
360           if (UI->getFlags() & UNW_TerminateHandler)
361             outs() << " UNW_TerminateHandler";
362           if (UI->getFlags() & UNW_ChainInfo)
363             outs() << " UNW_ChainInfo";
364       }
365       outs() << "\n";
366       outs() << "  Size of prolog: "
367              << static_cast<int>(UI->PrologSize) << "\n";
368       outs() << "  Number of Codes: "
369              << static_cast<int>(UI->NumCodes) << "\n";
370       // Maybe this should move to output of UOP_SetFPReg?
371       if (UI->getFrameRegister()) {
372         outs() << "  Frame register: "
373                 << getUnwindRegisterName(UI->getFrameRegister())
374                 << "\n";
375         outs() << "  Frame offset: "
376                 << 16 * UI->getFrameOffset()
377                 << "\n";
378       } else {
379         outs() << "  No frame pointer used\n";
380       }
381       if (UI->getFlags() & (UNW_ExceptionHandler | UNW_TerminateHandler)) {
382         // FIXME: Output exception handler data
383       } else if (UI->getFlags() & UNW_ChainInfo) {
384         // FIXME: Output chained unwind info
385       }
387       if (UI->NumCodes)
388         outs() << "  Unwind Codes:\n";
390       printAllUnwindCodes(ArrayRef<UnwindCode>(&UI->UnwindCodes[0],
391                           UI->NumCodes));
393       outs() << "\n\n";
394       outs().flush();
395     }
396   }
399 void llvm::printCOFFFileHeader(const object::ObjectFile *Obj) {
400   printImportTables(dyn_cast<const COFFObjectFile>(Obj));