1 //===-- COFFDump.cpp - COFF-specific dumper ---------------------*- C++ -*-===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 ///
10 /// \file
11 /// \brief This file implements the COFF-specific dumper for llvm-objdump.
12 /// It outputs the Win64 EH data structures as plain text.
13 /// The encoding of the unwind codes is described in MSDN:
14 /// http://msdn.microsoft.com/en-us/library/ck9asaa9.aspx
15 ///
16 //===----------------------------------------------------------------------===//
18 #include "llvm-objdump.h"
19 #include "llvm/Object/COFF.h"
20 #include "llvm/Object/ObjectFile.h"
21 #include "llvm/Support/Format.h"
22 #include "llvm/Support/SourceMgr.h"
23 #include "llvm/Support/Win64EH.h"
24 #include "llvm/Support/raw_ostream.h"
25 #include "llvm/Support/system_error.h"
26 #include <algorithm>
27 #include <cstring>
29 using namespace llvm;
30 using namespace object;
31 using namespace llvm::Win64EH;
33 // Returns the name of the unwind code.
34 static StringRef getUnwindCodeTypeName(uint8_t Code) {
35 switch(Code) {
36 default: llvm_unreachable("Invalid unwind code");
37 case UOP_PushNonVol: return "UOP_PushNonVol";
38 case UOP_AllocLarge: return "UOP_AllocLarge";
39 case UOP_AllocSmall: return "UOP_AllocSmall";
40 case UOP_SetFPReg: return "UOP_SetFPReg";
41 case UOP_SaveNonVol: return "UOP_SaveNonVol";
42 case UOP_SaveNonVolBig: return "UOP_SaveNonVolBig";
43 case UOP_SaveXMM128: return "UOP_SaveXMM128";
44 case UOP_SaveXMM128Big: return "UOP_SaveXMM128Big";
45 case UOP_PushMachFrame: return "UOP_PushMachFrame";
46 }
47 }
49 // Returns the name of a referenced register.
50 static StringRef getUnwindRegisterName(uint8_t Reg) {
51 switch(Reg) {
52 default: llvm_unreachable("Invalid register");
53 case 0: return "RAX";
54 case 1: return "RCX";
55 case 2: return "RDX";
56 case 3: return "RBX";
57 case 4: return "RSP";
58 case 5: return "RBP";
59 case 6: return "RSI";
60 case 7: return "RDI";
61 case 8: return "R8";
62 case 9: return "R9";
63 case 10: return "R10";
64 case 11: return "R11";
65 case 12: return "R12";
66 case 13: return "R13";
67 case 14: return "R14";
68 case 15: return "R15";
69 }
70 }
72 // Calculates the number of array slots required for the unwind code.
73 static unsigned getNumUsedSlots(const UnwindCode &UnwindCode) {
74 switch (UnwindCode.getUnwindOp()) {
75 default: llvm_unreachable("Invalid unwind code");
76 case UOP_PushNonVol:
77 case UOP_AllocSmall:
78 case UOP_SetFPReg:
79 case UOP_PushMachFrame:
80 return 1;
81 case UOP_SaveNonVol:
82 case UOP_SaveXMM128:
83 return 2;
84 case UOP_SaveNonVolBig:
85 case UOP_SaveXMM128Big:
86 return 3;
87 case UOP_AllocLarge:
88 return (UnwindCode.getOpInfo() == 0) ? 2 : 3;
89 }
90 }
92 // Prints one unwind code. Because an unwind code can occupy up to 3 slots in
93 // the unwind codes array, this function requires that the correct number of
94 // slots is provided.
95 static void printUnwindCode(ArrayRef<UnwindCode> UCs) {
96 assert(UCs.size() >= getNumUsedSlots(UCs[0]));
97 outs() << format(" 0x%02x: ", unsigned(UCs[0].u.CodeOffset))
98 << getUnwindCodeTypeName(UCs[0].getUnwindOp());
99 switch (UCs[0].getUnwindOp()) {
100 case UOP_PushNonVol:
101 outs() << " " << getUnwindRegisterName(UCs[0].getOpInfo());
102 break;
103 case UOP_AllocLarge:
104 if (UCs[0].getOpInfo() == 0) {
105 outs() << " " << UCs[1].FrameOffset;
106 } else {
107 outs() << " " << UCs[1].FrameOffset
108 + (static_cast<uint32_t>(UCs[2].FrameOffset) << 16);
109 }
110 break;
111 case UOP_AllocSmall:
112 outs() << " " << ((UCs[0].getOpInfo() + 1) * 8);
113 break;
114 case UOP_SetFPReg:
115 outs() << " ";
116 break;
117 case UOP_SaveNonVol:
118 outs() << " " << getUnwindRegisterName(UCs[0].getOpInfo())
119 << format(" [0x%04x]", 8 * UCs[1].FrameOffset);
120 break;
121 case UOP_SaveNonVolBig:
122 outs() << " " << getUnwindRegisterName(UCs[0].getOpInfo())
123 << format(" [0x%08x]", UCs[1].FrameOffset
124 + (static_cast<uint32_t>(UCs[2].FrameOffset) << 16));
125 break;
126 case UOP_SaveXMM128:
127 outs() << " XMM" << static_cast<uint32_t>(UCs[0].getOpInfo())
128 << format(" [0x%04x]", 16 * UCs[1].FrameOffset);
129 break;
130 case UOP_SaveXMM128Big:
131 outs() << " XMM" << UCs[0].getOpInfo()
132 << format(" [0x%08x]", UCs[1].FrameOffset
133 + (static_cast<uint32_t>(UCs[2].FrameOffset) << 16));
134 break;
135 case UOP_PushMachFrame:
136 outs() << " " << (UCs[0].getOpInfo() ? "w/o" : "w")
137 << " error code";
138 break;
139 }
140 outs() << "\n";
141 }
143 static void printAllUnwindCodes(ArrayRef<UnwindCode> UCs) {
144 for (const UnwindCode *I = UCs.begin(), *E = UCs.end(); I < E; ) {
145 unsigned UsedSlots = getNumUsedSlots(*I);
146 if (UsedSlots > UCs.size()) {
147 outs() << "Unwind data corrupted: Encountered unwind op "
148 << getUnwindCodeTypeName((*I).getUnwindOp())
149 << " which requires " << UsedSlots
150 << " slots, but only " << UCs.size()
151 << " remaining in buffer";
152 return ;
153 }
154 printUnwindCode(ArrayRef<UnwindCode>(I, E));
155 I += UsedSlots;
156 }
157 }
159 // Given a symbol sym this functions returns the address and section of it.
160 static error_code resolveSectionAndAddress(const COFFObjectFile *Obj,
161 const SymbolRef &Sym,
162 const coff_section *&ResolvedSection,
163 uint64_t &ResolvedAddr) {
164 if (error_code EC = Sym.getAddress(ResolvedAddr))
165 return EC;
166 section_iterator iter(Obj->section_begin());
167 if (error_code EC = Sym.getSection(iter))
168 return EC;
169 ResolvedSection = Obj->getCOFFSection(iter);
170 return object_error::success;
171 }
173 // Given a vector of relocations for a section and an offset into this section
174 // the function returns the symbol used for the relocation at the offset.
175 static error_code resolveSymbol(const std::vector<RelocationRef> &Rels,
176 uint64_t Offset, SymbolRef &Sym) {
177 for (std::vector<RelocationRef>::const_iterator I = Rels.begin(),
178 E = Rels.end();
179 I != E; ++I) {
180 uint64_t Ofs;
181 if (error_code EC = I->getOffset(Ofs))
182 return EC;
183 if (Ofs == Offset) {
184 Sym = *I->getSymbol();
185 return object_error::success;
186 }
187 }
188 return object_error::parse_failed;
189 }
191 // Given a vector of relocations for a section and an offset into this section
192 // the function resolves the symbol used for the relocation at the offset and
193 // returns the section content and the address inside the content pointed to
194 // by the symbol.
195 static error_code getSectionContents(const COFFObjectFile *Obj,
196 const std::vector<RelocationRef> &Rels,
197 uint64_t Offset,
198 ArrayRef<uint8_t> &Contents,
199 uint64_t &Addr) {
200 SymbolRef Sym;
201 if (error_code EC = resolveSymbol(Rels, Offset, Sym))
202 return EC;
203 const coff_section *Section;
204 if (error_code EC = resolveSectionAndAddress(Obj, Sym, Section, Addr))
205 return EC;
206 if (error_code EC = Obj->getSectionContents(Section, Contents))
207 return EC;
208 return object_error::success;
209 }
211 // Given a vector of relocations for a section and an offset into this section
212 // the function returns the name of the symbol used for the relocation at the
213 // offset.
214 static error_code resolveSymbolName(const std::vector<RelocationRef> &Rels,
215 uint64_t Offset, StringRef &Name) {
216 SymbolRef Sym;
217 if (error_code EC = resolveSymbol(Rels, Offset, Sym))
218 return EC;
219 if (error_code EC = Sym.getName(Name))
220 return EC;
221 return object_error::success;
222 }
224 static void printCOFFSymbolAddress(llvm::raw_ostream &Out,
225 const std::vector<RelocationRef> &Rels,
226 uint64_t Offset, uint32_t Disp) {
227 StringRef Sym;
228 if (!resolveSymbolName(Rels, Offset, Sym)) {
229 Out << Sym;
230 if (Disp > 0)
231 Out << format(" + 0x%04x", Disp);
232 } else {
233 Out << format("0x%04x", Disp);
234 }
235 }
237 static void
238 printSEHTable(const COFFObjectFile *Obj, uint32_t TableVA, int Count) {
239 if (Count == 0)
240 return;
242 const pe32_header *PE32Header;
243 if (error(Obj->getPE32Header(PE32Header)))
244 return;
245 uint32_t ImageBase = PE32Header->ImageBase;
246 uintptr_t IntPtr = 0;
247 if (error(Obj->getVaPtr(TableVA, IntPtr)))
248 return;
249 const support::ulittle32_t *P = (const support::ulittle32_t *)IntPtr;
250 outs() << "SEH Table:";
251 for (int I = 0; I < Count; ++I)
252 outs() << format(" 0x%x", P[I] + ImageBase);
253 outs() << "\n\n";
254 }
256 static void printLoadConfiguration(const COFFObjectFile *Obj) {
257 // Skip if it's not executable.
258 const pe32_header *PE32Header;
259 if (error(Obj->getPE32Header(PE32Header)))
260 return;
261 if (!PE32Header)
262 return;
264 const coff_file_header *Header;
265 if (error(Obj->getCOFFHeader(Header)))
266 return;
267 // Currently only x86 is supported
268 if (Header->Machine != COFF::IMAGE_FILE_MACHINE_I386)
269 return;
271 const data_directory *DataDir;
272 if (error(Obj->getDataDirectory(COFF::LOAD_CONFIG_TABLE, DataDir)))
273 return;
274 uintptr_t IntPtr = 0;
275 if (DataDir->RelativeVirtualAddress == 0)
276 return;
277 if (error(Obj->getRvaPtr(DataDir->RelativeVirtualAddress, IntPtr)))
278 return;
280 auto *LoadConf = reinterpret_cast<const coff_load_configuration32 *>(IntPtr);
281 outs() << "Load configuration:"
282 << "\n Timestamp: " << LoadConf->TimeDateStamp
283 << "\n Major Version: " << LoadConf->MajorVersion
284 << "\n Minor Version: " << LoadConf->MinorVersion
285 << "\n GlobalFlags Clear: " << LoadConf->GlobalFlagsClear
286 << "\n GlobalFlags Set: " << LoadConf->GlobalFlagsSet
287 << "\n Critical Section Default Timeout: " << LoadConf->CriticalSectionDefaultTimeout
288 << "\n Decommit Free Block Threshold: " << LoadConf->DeCommitFreeBlockThreshold
289 << "\n Decommit Total Free Threshold: " << LoadConf->DeCommitTotalFreeThreshold
290 << "\n Lock Prefix Table: " << LoadConf->LockPrefixTable
291 << "\n Maximum Allocation Size: " << LoadConf->MaximumAllocationSize
292 << "\n Virtual Memory Threshold: " << LoadConf->VirtualMemoryThreshold
293 << "\n Process Affinity Mask: " << LoadConf->ProcessAffinityMask
294 << "\n Process Heap Flags: " << LoadConf->ProcessHeapFlags
295 << "\n CSD Version: " << LoadConf->CSDVersion
296 << "\n Security Cookie: " << LoadConf->SecurityCookie
297 << "\n SEH Table: " << LoadConf->SEHandlerTable
298 << "\n SEH Count: " << LoadConf->SEHandlerCount
299 << "\n\n";
300 printSEHTable(Obj, LoadConf->SEHandlerTable, LoadConf->SEHandlerCount);
301 outs() << "\n";
302 }
304 // Prints import tables. The import table is a table containing the list of
305 // DLL name and symbol names which will be linked by the loader.
306 static void printImportTables(const COFFObjectFile *Obj) {
307 import_directory_iterator I = Obj->import_directory_begin();
308 import_directory_iterator E = Obj->import_directory_end();
309 if (I == E)
310 return;
311 outs() << "The Import Tables:\n";
312 for (; I != E; I = ++I) {
313 const import_directory_table_entry *Dir;
314 StringRef Name;
315 if (I->getImportTableEntry(Dir)) return;
316 if (I->getName(Name)) return;
318 outs() << format(" lookup %08x time %08x fwd %08x name %08x addr %08x\n\n",
319 static_cast<uint32_t>(Dir->ImportLookupTableRVA),
320 static_cast<uint32_t>(Dir->TimeDateStamp),
321 static_cast<uint32_t>(Dir->ForwarderChain),
322 static_cast<uint32_t>(Dir->NameRVA),
323 static_cast<uint32_t>(Dir->ImportAddressTableRVA));
324 outs() << " DLL Name: " << Name << "\n";
325 outs() << " Hint/Ord Name\n";
326 const import_lookup_table_entry32 *entry;
327 if (I->getImportLookupEntry(entry))
328 return;
329 for (; entry->data; ++entry) {
330 if (entry->isOrdinal()) {
331 outs() << format(" % 6d\n", entry->getOrdinal());
332 continue;
333 }
334 uint16_t Hint;
335 StringRef Name;
336 if (Obj->getHintName(entry->getHintNameRVA(), Hint, Name))
337 return;
338 outs() << format(" % 6d ", Hint) << Name << "\n";
339 }
340 outs() << "\n";
341 }
342 }
344 // Prints export tables. The export table is a table containing the list of
345 // exported symbol from the DLL.
346 static void printExportTable(const COFFObjectFile *Obj) {
347 outs() << "Export Table:\n";
348 export_directory_iterator I = Obj->export_directory_begin();
349 export_directory_iterator E = Obj->export_directory_end();
350 if (I == E)
351 return;
352 StringRef DllName;
353 uint32_t OrdinalBase;
354 if (I->getDllName(DllName))
355 return;
356 if (I->getOrdinalBase(OrdinalBase))
357 return;
358 outs() << " DLL name: " << DllName << "\n";
359 outs() << " Ordinal base: " << OrdinalBase << "\n";
360 outs() << " Ordinal RVA Name\n";
361 for (; I != E; I = ++I) {
362 uint32_t Ordinal;
363 if (I->getOrdinal(Ordinal))
364 return;
365 uint32_t RVA;
366 if (I->getExportRVA(RVA))
367 return;
368 outs() << format(" % 4d %# 8x", Ordinal, RVA);
370 StringRef Name;
371 if (I->getSymbolName(Name))
372 continue;
373 if (!Name.empty())
374 outs() << " " << Name;
375 outs() << "\n";
376 }
377 }
379 // Given the COFF object file, this function returns the relocations for .pdata
380 // and the pointer to "runtime function" structs.
381 static bool getPDataSection(const COFFObjectFile *Obj,
382 std::vector<RelocationRef> &Rels,
383 const RuntimeFunction *&RFStart, int &NumRFs) {
384 for (section_iterator SI = Obj->section_begin(), SE = Obj->section_end();
385 SI != SE; ++SI) {
386 StringRef Name;
387 if (error(SI->getName(Name)))
388 continue;
389 if (Name != ".pdata")
390 continue;
392 const coff_section *Pdata = Obj->getCOFFSection(SI);
393 for (relocation_iterator RI = SI->relocation_begin(),
394 RE = SI->relocation_end();
395 RI != RE; ++RI)
396 Rels.push_back(*RI);
398 // Sort relocations by address.
399 std::sort(Rels.begin(), Rels.end(), RelocAddressLess);
401 ArrayRef<uint8_t> Contents;
402 if (error(Obj->getSectionContents(Pdata, Contents)))
403 continue;
404 if (Contents.empty())
405 continue;
407 RFStart = reinterpret_cast<const RuntimeFunction *>(Contents.data());
408 NumRFs = Contents.size() / sizeof(RuntimeFunction);
409 return true;
410 }
411 return false;
412 }
414 static void printWin64EHUnwindInfo(const Win64EH::UnwindInfo *UI) {
415 // The casts to int are required in order to output the value as number.
416 // Without the casts the value would be interpreted as char data (which
417 // results in garbage output).
418 outs() << " Version: " << static_cast<int>(UI->getVersion()) << "\n";
419 outs() << " Flags: " << static_cast<int>(UI->getFlags());
420 if (UI->getFlags()) {
421 if (UI->getFlags() & UNW_ExceptionHandler)
422 outs() << " UNW_ExceptionHandler";
423 if (UI->getFlags() & UNW_TerminateHandler)
424 outs() << " UNW_TerminateHandler";
425 if (UI->getFlags() & UNW_ChainInfo)
426 outs() << " UNW_ChainInfo";
427 }
428 outs() << "\n";
429 outs() << " Size of prolog: " << static_cast<int>(UI->PrologSize) << "\n";
430 outs() << " Number of Codes: " << static_cast<int>(UI->NumCodes) << "\n";
431 // Maybe this should move to output of UOP_SetFPReg?
432 if (UI->getFrameRegister()) {
433 outs() << " Frame register: "
434 << getUnwindRegisterName(UI->getFrameRegister()) << "\n";
435 outs() << " Frame offset: " << 16 * UI->getFrameOffset() << "\n";
436 } else {
437 outs() << " No frame pointer used\n";
438 }
439 if (UI->getFlags() & (UNW_ExceptionHandler | UNW_TerminateHandler)) {
440 // FIXME: Output exception handler data
441 } else if (UI->getFlags() & UNW_ChainInfo) {
442 // FIXME: Output chained unwind info
443 }
445 if (UI->NumCodes)
446 outs() << " Unwind Codes:\n";
448 printAllUnwindCodes(ArrayRef<UnwindCode>(&UI->UnwindCodes[0], UI->NumCodes));
450 outs() << "\n";
451 outs().flush();
452 }
454 /// Prints out the given RuntimeFunction struct for x64, assuming that Obj is
455 /// pointing to an executable file.
456 static void printRuntimeFunction(const COFFObjectFile *Obj,
457 const RuntimeFunction &RF) {
458 if (!RF.StartAddress)
459 return;
460 outs() << "Function Table:\n"
461 << format(" Start Address: 0x%04x\n", RF.StartAddress)
462 << format(" End Address: 0x%04x\n", RF.EndAddress)
463 << format(" Unwind Info Address: 0x%04x\n", RF.UnwindInfoOffset);
464 uintptr_t addr;
465 if (Obj->getRvaPtr(RF.UnwindInfoOffset, addr))
466 return;
467 printWin64EHUnwindInfo(reinterpret_cast<const Win64EH::UnwindInfo *>(addr));
468 }
470 /// Prints out the given RuntimeFunction struct for x64, assuming that Obj is
471 /// pointing to an object file. Unlike executable, fields in RuntimeFunction
472 /// struct are filled with zeros, but instead there are relocations pointing to
473 /// them so that the linker will fill targets' RVAs to the fields at link
474 /// time. This function interprets the relocations to find the data to be used
475 /// in the resulting executable.
476 static void printRuntimeFunctionRels(const COFFObjectFile *Obj,
477 const RuntimeFunction &RF,
478 uint64_t SectionOffset,
479 const std::vector<RelocationRef> &Rels) {
480 outs() << "Function Table:\n";
481 outs() << " Start Address: ";
482 printCOFFSymbolAddress(outs(), Rels,
483 SectionOffset +
484 /*offsetof(RuntimeFunction, StartAddress)*/ 0,
485 RF.StartAddress);
486 outs() << "\n";
488 outs() << " End Address: ";
489 printCOFFSymbolAddress(outs(), Rels,
490 SectionOffset +
491 /*offsetof(RuntimeFunction, EndAddress)*/ 4,
492 RF.EndAddress);
493 outs() << "\n";
495 outs() << " Unwind Info Address: ";
496 printCOFFSymbolAddress(outs(), Rels,
497 SectionOffset +
498 /*offsetof(RuntimeFunction, UnwindInfoOffset)*/ 8,
499 RF.UnwindInfoOffset);
500 outs() << "\n";
502 ArrayRef<uint8_t> XContents;
503 uint64_t UnwindInfoOffset = 0;
504 if (error(getSectionContents(
505 Obj, Rels, SectionOffset +
506 /*offsetof(RuntimeFunction, UnwindInfoOffset)*/ 8,
507 XContents, UnwindInfoOffset)))
508 return;
509 if (XContents.empty())
510 return;
512 UnwindInfoOffset += RF.UnwindInfoOffset;
513 if (UnwindInfoOffset > XContents.size())
514 return;
516 auto *UI = reinterpret_cast<const Win64EH::UnwindInfo *>(XContents.data() +
517 UnwindInfoOffset);
518 printWin64EHUnwindInfo(UI);
519 }
521 void llvm::printCOFFUnwindInfo(const COFFObjectFile *Obj) {
522 const coff_file_header *Header;
523 if (error(Obj->getCOFFHeader(Header)))
524 return;
526 if (Header->Machine != COFF::IMAGE_FILE_MACHINE_AMD64) {
527 errs() << "Unsupported image machine type "
528 "(currently only AMD64 is supported).\n";
529 return;
530 }
532 std::vector<RelocationRef> Rels;
533 const RuntimeFunction *RFStart;
534 int NumRFs;
535 if (!getPDataSection(Obj, Rels, RFStart, NumRFs))
536 return;
537 ArrayRef<RuntimeFunction> RFs(RFStart, NumRFs);
539 bool IsExecutable = Rels.empty();
540 if (IsExecutable) {
541 for (const RuntimeFunction &RF : RFs)
542 printRuntimeFunction(Obj, RF);
543 return;
544 }
546 for (const RuntimeFunction &RF : RFs) {
547 uint64_t SectionOffset =
548 std::distance(RFs.begin(), &RF) * sizeof(RuntimeFunction);
549 printRuntimeFunctionRels(Obj, RF, SectionOffset, Rels);
550 }
551 }
553 void llvm::printCOFFFileHeader(const object::ObjectFile *Obj) {
554 const COFFObjectFile *file = dyn_cast<const COFFObjectFile>(Obj);
555 printLoadConfiguration(file);
556 printImportTables(file);
557 printExportTable(file);
558 }