1 //===- FileCheck.cpp - Check that File's Contents match what is expected --===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // FileCheck does a line-by line check of a file that validates whether it
11 // contains the expected content. This is useful for regression tests etc.
12 //
13 // This program exits with an error status of 2 on error, exit status of 0 if
14 // the file matched the expected contents, and exit status of 1 if it did not
15 // contain the expected contents.
16 //
17 //===----------------------------------------------------------------------===//
19 #include "llvm/ADT/OwningPtr.h"
20 #include "llvm/ADT/SmallString.h"
21 #include "llvm/ADT/StringExtras.h"
22 #include "llvm/ADT/StringMap.h"
23 #include "llvm/ADT/StringSet.h"
24 #include "llvm/Support/CommandLine.h"
25 #include "llvm/Support/MemoryBuffer.h"
26 #include "llvm/Support/PrettyStackTrace.h"
27 #include "llvm/Support/Regex.h"
28 #include "llvm/Support/Signals.h"
29 #include "llvm/Support/SourceMgr.h"
30 #include "llvm/Support/raw_ostream.h"
31 #include "llvm/Support/system_error.h"
32 #include <algorithm>
33 #include <cctype>
34 #include <map>
35 #include <string>
36 #include <vector>
37 using namespace llvm;
39 static cl::opt<std::string>
40 CheckFilename(cl::Positional, cl::desc("<check-file>"), cl::Required);
42 static cl::opt<std::string>
43 InputFilename("input-file", cl::desc("File to check (defaults to stdin)"),
44 cl::init("-"), cl::value_desc("filename"));
46 static cl::list<std::string>
47 CheckPrefixes("check-prefix",
48 cl::desc("Prefix to use from check file (defaults to 'CHECK')"));
50 static cl::opt<bool>
51 NoCanonicalizeWhiteSpace("strict-whitespace",
52 cl::desc("Do not treat all horizontal whitespace as equivalent"));
54 typedef cl::list<std::string>::const_iterator prefix_iterator;
56 //===----------------------------------------------------------------------===//
57 // Pattern Handling Code.
58 //===----------------------------------------------------------------------===//
60 namespace Check {
61 enum CheckType {
62 CheckNone = 0,
63 CheckPlain,
64 CheckNext,
65 CheckNot,
66 CheckDAG,
67 CheckLabel,
69 /// MatchEOF - When set, this pattern only matches the end of file. This is
70 /// used for trailing CHECK-NOTs.
71 CheckEOF
72 };
73 }
75 class Pattern {
76 SMLoc PatternLoc;
78 Check::CheckType CheckTy;
80 /// FixedStr - If non-empty, this pattern is a fixed string match with the
81 /// specified fixed string.
82 StringRef FixedStr;
84 /// RegEx - If non-empty, this is a regex pattern.
85 std::string RegExStr;
87 /// \brief Contains the number of line this pattern is in.
88 unsigned LineNumber;
90 /// VariableUses - Entries in this vector map to uses of a variable in the
91 /// pattern, e.g. "foo[[bar]]baz". In this case, the RegExStr will contain
92 /// "foobaz" and we'll get an entry in this vector that tells us to insert the
93 /// value of bar at offset 3.
94 std::vector<std::pair<StringRef, unsigned> > VariableUses;
96 /// VariableDefs - Maps definitions of variables to their parenthesized
97 /// capture numbers.
98 /// E.g. for the pattern "foo[[bar:.*]]baz", VariableDefs will map "bar" to 1.
99 std::map<StringRef, unsigned> VariableDefs;
101 public:
103 Pattern(Check::CheckType Ty)
104 : CheckTy(Ty) { }
106 /// getLoc - Return the location in source code.
107 SMLoc getLoc() const { return PatternLoc; }
109 /// ParsePattern - Parse the given string into the Pattern. Prefix provides
110 /// which prefix is being matched, SM provides the SourceMgr used for error
111 /// reports, and LineNumber is the line number in the input file from which
112 /// the pattern string was read. Returns true in case of an error, false
113 /// otherwise.
114 bool ParsePattern(StringRef PatternStr,
115 StringRef Prefix,
116 SourceMgr &SM,
117 unsigned LineNumber);
119 /// Match - Match the pattern string against the input buffer Buffer. This
120 /// returns the position that is matched or npos if there is no match. If
121 /// there is a match, the size of the matched string is returned in MatchLen.
122 ///
123 /// The VariableTable StringMap provides the current values of filecheck
124 /// variables and is updated if this match defines new values.
125 size_t Match(StringRef Buffer, size_t &MatchLen,
126 StringMap<StringRef> &VariableTable) const;
128 /// PrintFailureInfo - Print additional information about a failure to match
129 /// involving this pattern.
130 void PrintFailureInfo(const SourceMgr &SM, StringRef Buffer,
131 const StringMap<StringRef> &VariableTable) const;
133 bool hasVariable() const { return !(VariableUses.empty() &&
134 VariableDefs.empty()); }
136 Check::CheckType getCheckTy() const { return CheckTy; }
138 private:
139 bool AddRegExToRegEx(StringRef RS, unsigned &CurParen, SourceMgr &SM);
140 void AddBackrefToRegEx(unsigned BackrefNum);
142 /// ComputeMatchDistance - Compute an arbitrary estimate for the quality of
143 /// matching this pattern at the start of \arg Buffer; a distance of zero
144 /// should correspond to a perfect match.
145 unsigned ComputeMatchDistance(StringRef Buffer,
146 const StringMap<StringRef> &VariableTable) const;
148 /// \brief Evaluates expression and stores the result to \p Value.
149 /// \return true on success. false when the expression has invalid syntax.
150 bool EvaluateExpression(StringRef Expr, std::string &Value) const;
152 /// \brief Finds the closing sequence of a regex variable usage or
153 /// definition. Str has to point in the beginning of the definition
154 /// (right after the opening sequence).
155 /// \return offset of the closing sequence within Str, or npos if it was not
156 /// found.
157 size_t FindRegexVarEnd(StringRef Str);
158 };
161 bool Pattern::ParsePattern(StringRef PatternStr,
162 StringRef Prefix,
163 SourceMgr &SM,
164 unsigned LineNumber) {
165 this->LineNumber = LineNumber;
166 PatternLoc = SMLoc::getFromPointer(PatternStr.data());
168 // Ignore trailing whitespace.
169 while (!PatternStr.empty() &&
170 (PatternStr.back() == ' ' || PatternStr.back() == '\t'))
171 PatternStr = PatternStr.substr(0, PatternStr.size()-1);
173 // Check that there is something on the line.
174 if (PatternStr.empty()) {
175 SM.PrintMessage(PatternLoc, SourceMgr::DK_Error,
176 "found empty check string with prefix '" +
177 Prefix + ":'");
178 return true;
179 }
181 // Check to see if this is a fixed string, or if it has regex pieces.
182 if (PatternStr.size() < 2 ||
183 (PatternStr.find("{{") == StringRef::npos &&
184 PatternStr.find("[[") == StringRef::npos)) {
185 FixedStr = PatternStr;
186 return false;
187 }
189 // Paren value #0 is for the fully matched string. Any new parenthesized
190 // values add from there.
191 unsigned CurParen = 1;
193 // Otherwise, there is at least one regex piece. Build up the regex pattern
194 // by escaping scary characters in fixed strings, building up one big regex.
195 while (!PatternStr.empty()) {
196 // RegEx matches.
197 if (PatternStr.startswith("{{")) {
198 // This is the start of a regex match. Scan for the }}.
199 size_t End = PatternStr.find("}}");
200 if (End == StringRef::npos) {
201 SM.PrintMessage(SMLoc::getFromPointer(PatternStr.data()),
202 SourceMgr::DK_Error,
203 "found start of regex string with no end '}}'");
204 return true;
205 }
207 // Enclose {{}} patterns in parens just like [[]] even though we're not
208 // capturing the result for any purpose. This is required in case the
209 // expression contains an alternation like: CHECK: abc{{x|z}}def. We
210 // want this to turn into: "abc(x|z)def" not "abcx|zdef".
211 RegExStr += '(';
212 ++CurParen;
214 if (AddRegExToRegEx(PatternStr.substr(2, End-2), CurParen, SM))
215 return true;
216 RegExStr += ')';
218 PatternStr = PatternStr.substr(End+2);
219 continue;
220 }
222 // Named RegEx matches. These are of two forms: [[foo:.*]] which matches .*
223 // (or some other regex) and assigns it to the FileCheck variable 'foo'. The
224 // second form is [[foo]] which is a reference to foo. The variable name
225 // itself must be of the form "[a-zA-Z_][0-9a-zA-Z_]*", otherwise we reject
226 // it. This is to catch some common errors.
227 if (PatternStr.startswith("[[")) {
228 // Find the closing bracket pair ending the match. End is going to be an
229 // offset relative to the beginning of the match string.
230 size_t End = FindRegexVarEnd(PatternStr.substr(2));
232 if (End == StringRef::npos) {
233 SM.PrintMessage(SMLoc::getFromPointer(PatternStr.data()),
234 SourceMgr::DK_Error,
235 "invalid named regex reference, no ]] found");
236 return true;
237 }
239 StringRef MatchStr = PatternStr.substr(2, End);
240 PatternStr = PatternStr.substr(End+4);
242 // Get the regex name (e.g. "foo").
243 size_t NameEnd = MatchStr.find(':');
244 StringRef Name = MatchStr.substr(0, NameEnd);
246 if (Name.empty()) {
247 SM.PrintMessage(SMLoc::getFromPointer(Name.data()), SourceMgr::DK_Error,
248 "invalid name in named regex: empty name");
249 return true;
250 }
252 // Verify that the name/expression is well formed. FileCheck currently
253 // supports @LINE, @LINE+number, @LINE-number expressions. The check here
254 // is relaxed, more strict check is performed in \c EvaluateExpression.
255 bool IsExpression = false;
256 for (unsigned i = 0, e = Name.size(); i != e; ++i) {
257 if (i == 0 && Name[i] == '@') {
258 if (NameEnd != StringRef::npos) {
259 SM.PrintMessage(SMLoc::getFromPointer(Name.data()),
260 SourceMgr::DK_Error,
261 "invalid name in named regex definition");
262 return true;
263 }
264 IsExpression = true;
265 continue;
266 }
267 if (Name[i] != '_' && !isalnum(Name[i]) &&
268 (!IsExpression || (Name[i] != '+' && Name[i] != '-'))) {
269 SM.PrintMessage(SMLoc::getFromPointer(Name.data()+i),
270 SourceMgr::DK_Error, "invalid name in named regex");
271 return true;
272 }
273 }
275 // Name can't start with a digit.
276 if (isdigit(static_cast<unsigned char>(Name[0]))) {
277 SM.PrintMessage(SMLoc::getFromPointer(Name.data()), SourceMgr::DK_Error,
278 "invalid name in named regex");
279 return true;
280 }
282 // Handle [[foo]].
283 if (NameEnd == StringRef::npos) {
284 // Handle variables that were defined earlier on the same line by
285 // emitting a backreference.
286 if (VariableDefs.find(Name) != VariableDefs.end()) {
287 unsigned VarParenNum = VariableDefs[Name];
288 if (VarParenNum < 1 || VarParenNum > 9) {
289 SM.PrintMessage(SMLoc::getFromPointer(Name.data()),
290 SourceMgr::DK_Error,
291 "Can't back-reference more than 9 variables");
292 return true;
293 }
294 AddBackrefToRegEx(VarParenNum);
295 } else {
296 VariableUses.push_back(std::make_pair(Name, RegExStr.size()));
297 }
298 continue;
299 }
301 // Handle [[foo:.*]].
302 VariableDefs[Name] = CurParen;
303 RegExStr += '(';
304 ++CurParen;
306 if (AddRegExToRegEx(MatchStr.substr(NameEnd+1), CurParen, SM))
307 return true;
309 RegExStr += ')';
310 }
312 // Handle fixed string matches.
313 // Find the end, which is the start of the next regex.
314 size_t FixedMatchEnd = PatternStr.find("{{");
315 FixedMatchEnd = std::min(FixedMatchEnd, PatternStr.find("[["));
316 RegExStr += Regex::escape(PatternStr.substr(0, FixedMatchEnd));
317 PatternStr = PatternStr.substr(FixedMatchEnd);
318 }
320 return false;
321 }
323 bool Pattern::AddRegExToRegEx(StringRef RS, unsigned &CurParen,
324 SourceMgr &SM) {
325 Regex R(RS);
326 std::string Error;
327 if (!R.isValid(Error)) {
328 SM.PrintMessage(SMLoc::getFromPointer(RS.data()), SourceMgr::DK_Error,
329 "invalid regex: " + Error);
330 return true;
331 }
333 RegExStr += RS.str();
334 CurParen += R.getNumMatches();
335 return false;
336 }
338 void Pattern::AddBackrefToRegEx(unsigned BackrefNum) {
339 assert(BackrefNum >= 1 && BackrefNum <= 9 && "Invalid backref number");
340 std::string Backref = std::string("\\") +
341 std::string(1, '0' + BackrefNum);
342 RegExStr += Backref;
343 }
345 bool Pattern::EvaluateExpression(StringRef Expr, std::string &Value) const {
346 // The only supported expression is @LINE([\+-]\d+)?
347 if (!Expr.startswith("@LINE"))
348 return false;
349 Expr = Expr.substr(StringRef("@LINE").size());
350 int Offset = 0;
351 if (!Expr.empty()) {
352 if (Expr[0] == '+')
353 Expr = Expr.substr(1);
354 else if (Expr[0] != '-')
355 return false;
356 if (Expr.getAsInteger(10, Offset))
357 return false;
358 }
359 Value = llvm::itostr(LineNumber + Offset);
360 return true;
361 }
363 /// Match - Match the pattern string against the input buffer Buffer. This
364 /// returns the position that is matched or npos if there is no match. If
365 /// there is a match, the size of the matched string is returned in MatchLen.
366 size_t Pattern::Match(StringRef Buffer, size_t &MatchLen,
367 StringMap<StringRef> &VariableTable) const {
368 // If this is the EOF pattern, match it immediately.
369 if (CheckTy == Check::CheckEOF) {
370 MatchLen = 0;
371 return Buffer.size();
372 }
374 // If this is a fixed string pattern, just match it now.
375 if (!FixedStr.empty()) {
376 MatchLen = FixedStr.size();
377 return Buffer.find(FixedStr);
378 }
380 // Regex match.
382 // If there are variable uses, we need to create a temporary string with the
383 // actual value.
384 StringRef RegExToMatch = RegExStr;
385 std::string TmpStr;
386 if (!VariableUses.empty()) {
387 TmpStr = RegExStr;
389 unsigned InsertOffset = 0;
390 for (unsigned i = 0, e = VariableUses.size(); i != e; ++i) {
391 std::string Value;
393 if (VariableUses[i].first[0] == '@') {
394 if (!EvaluateExpression(VariableUses[i].first, Value))
395 return StringRef::npos;
396 } else {
397 StringMap<StringRef>::iterator it =
398 VariableTable.find(VariableUses[i].first);
399 // If the variable is undefined, return an error.
400 if (it == VariableTable.end())
401 return StringRef::npos;
403 // Look up the value and escape it so that we can put it into the regex.
404 Value += Regex::escape(it->second);
405 }
407 // Plop it into the regex at the adjusted offset.
408 TmpStr.insert(TmpStr.begin()+VariableUses[i].second+InsertOffset,
409 Value.begin(), Value.end());
410 InsertOffset += Value.size();
411 }
413 // Match the newly constructed regex.
414 RegExToMatch = TmpStr;
415 }
418 SmallVector<StringRef, 4> MatchInfo;
419 if (!Regex(RegExToMatch, Regex::Newline).match(Buffer, &MatchInfo))
420 return StringRef::npos;
422 // Successful regex match.
423 assert(!MatchInfo.empty() && "Didn't get any match");
424 StringRef FullMatch = MatchInfo[0];
426 // If this defines any variables, remember their values.
427 for (std::map<StringRef, unsigned>::const_iterator I = VariableDefs.begin(),
428 E = VariableDefs.end();
429 I != E; ++I) {
430 assert(I->second < MatchInfo.size() && "Internal paren error");
431 VariableTable[I->first] = MatchInfo[I->second];
432 }
434 MatchLen = FullMatch.size();
435 return FullMatch.data()-Buffer.data();
436 }
438 unsigned Pattern::ComputeMatchDistance(StringRef Buffer,
439 const StringMap<StringRef> &VariableTable) const {
440 // Just compute the number of matching characters. For regular expressions, we
441 // just compare against the regex itself and hope for the best.
442 //
443 // FIXME: One easy improvement here is have the regex lib generate a single
444 // example regular expression which matches, and use that as the example
445 // string.
446 StringRef ExampleString(FixedStr);
447 if (ExampleString.empty())
448 ExampleString = RegExStr;
450 // Only compare up to the first line in the buffer, or the string size.
451 StringRef BufferPrefix = Buffer.substr(0, ExampleString.size());
452 BufferPrefix = BufferPrefix.split('\n').first;
453 return BufferPrefix.edit_distance(ExampleString);
454 }
456 void Pattern::PrintFailureInfo(const SourceMgr &SM, StringRef Buffer,
457 const StringMap<StringRef> &VariableTable) const{
458 // If this was a regular expression using variables, print the current
459 // variable values.
460 if (!VariableUses.empty()) {
461 for (unsigned i = 0, e = VariableUses.size(); i != e; ++i) {
462 SmallString<256> Msg;
463 raw_svector_ostream OS(Msg);
464 StringRef Var = VariableUses[i].first;
465 if (Var[0] == '@') {
466 std::string Value;
467 if (EvaluateExpression(Var, Value)) {
468 OS << "with expression \"";
469 OS.write_escaped(Var) << "\" equal to \"";
470 OS.write_escaped(Value) << "\"";
471 } else {
472 OS << "uses incorrect expression \"";
473 OS.write_escaped(Var) << "\"";
474 }
475 } else {
476 StringMap<StringRef>::const_iterator it = VariableTable.find(Var);
478 // Check for undefined variable references.
479 if (it == VariableTable.end()) {
480 OS << "uses undefined variable \"";
481 OS.write_escaped(Var) << "\"";
482 } else {
483 OS << "with variable \"";
484 OS.write_escaped(Var) << "\" equal to \"";
485 OS.write_escaped(it->second) << "\"";
486 }
487 }
489 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), SourceMgr::DK_Note,
490 OS.str());
491 }
492 }
494 // Attempt to find the closest/best fuzzy match. Usually an error happens
495 // because some string in the output didn't exactly match. In these cases, we
496 // would like to show the user a best guess at what "should have" matched, to
497 // save them having to actually check the input manually.
498 size_t NumLinesForward = 0;
499 size_t Best = StringRef::npos;
500 double BestQuality = 0;
502 // Use an arbitrary 4k limit on how far we will search.
503 for (size_t i = 0, e = std::min(size_t(4096), Buffer.size()); i != e; ++i) {
504 if (Buffer[i] == '\n')
505 ++NumLinesForward;
507 // Patterns have leading whitespace stripped, so skip whitespace when
508 // looking for something which looks like a pattern.
509 if (Buffer[i] == ' ' || Buffer[i] == '\t')
510 continue;
512 // Compute the "quality" of this match as an arbitrary combination of the
513 // match distance and the number of lines skipped to get to this match.
514 unsigned Distance = ComputeMatchDistance(Buffer.substr(i), VariableTable);
515 double Quality = Distance + (NumLinesForward / 100.);
517 if (Quality < BestQuality || Best == StringRef::npos) {
518 Best = i;
519 BestQuality = Quality;
520 }
521 }
523 // Print the "possible intended match here" line if we found something
524 // reasonable and not equal to what we showed in the "scanning from here"
525 // line.
526 if (Best && Best != StringRef::npos && BestQuality < 50) {
527 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data() + Best),
528 SourceMgr::DK_Note, "possible intended match here");
530 // FIXME: If we wanted to be really friendly we would show why the match
531 // failed, as it can be hard to spot simple one character differences.
532 }
533 }
535 size_t Pattern::FindRegexVarEnd(StringRef Str) {
536 // Offset keeps track of the current offset within the input Str
537 size_t Offset = 0;
538 // [...] Nesting depth
539 size_t BracketDepth = 0;
541 while (!Str.empty()) {
542 if (Str.startswith("]]") && BracketDepth == 0)
543 return Offset;
544 if (Str[0] == '\\') {
545 // Backslash escapes the next char within regexes, so skip them both.
546 Str = Str.substr(2);
547 Offset += 2;
548 } else {
549 switch (Str[0]) {
550 default:
551 break;
552 case '[':
553 BracketDepth++;
554 break;
555 case ']':
556 assert(BracketDepth > 0 && "Invalid regex");
557 BracketDepth--;
558 break;
559 }
560 Str = Str.substr(1);
561 Offset++;
562 }
563 }
565 return StringRef::npos;
566 }
569 //===----------------------------------------------------------------------===//
570 // Check Strings.
571 //===----------------------------------------------------------------------===//
573 /// CheckString - This is a check that we found in the input file.
574 struct CheckString {
575 /// Pat - The pattern to match.
576 Pattern Pat;
578 /// Prefix - Which prefix name this check matched.
579 StringRef Prefix;
581 /// Loc - The location in the match file that the check string was specified.
582 SMLoc Loc;
584 /// CheckTy - Specify what kind of check this is. e.g. CHECK-NEXT: directive,
585 /// as opposed to a CHECK: directive.
586 Check::CheckType CheckTy;
588 /// DagNotStrings - These are all of the strings that are disallowed from
589 /// occurring between this match string and the previous one (or start of
590 /// file).
591 std::vector<Pattern> DagNotStrings;
594 CheckString(const Pattern &P,
595 StringRef S,
596 SMLoc L,
597 Check::CheckType Ty)
598 : Pat(P), Prefix(S), Loc(L), CheckTy(Ty) {}
600 /// Check - Match check string and its "not strings" and/or "dag strings".
601 size_t Check(const SourceMgr &SM, StringRef Buffer, bool IsLabelScanMode,
602 size_t &MatchLen, StringMap<StringRef> &VariableTable) const;
604 /// CheckNext - Verify there is a single line in the given buffer.
605 bool CheckNext(const SourceMgr &SM, StringRef Buffer) const;
607 /// CheckNot - Verify there's no "not strings" in the given buffer.
608 bool CheckNot(const SourceMgr &SM, StringRef Buffer,
609 const std::vector<const Pattern *> &NotStrings,
610 StringMap<StringRef> &VariableTable) const;
612 /// CheckDag - Match "dag strings" and their mixed "not strings".
613 size_t CheckDag(const SourceMgr &SM, StringRef Buffer,
614 std::vector<const Pattern *> &NotStrings,
615 StringMap<StringRef> &VariableTable) const;
616 };
618 /// Canonicalize whitespaces in the input file. Line endings are replaced
619 /// with UNIX-style '\n'.
620 ///
621 /// \param PreserveHorizontal Don't squash consecutive horizontal whitespace
622 /// characters to a single space.
623 static MemoryBuffer *CanonicalizeInputFile(MemoryBuffer *MB,
624 bool PreserveHorizontal) {
625 SmallString<128> NewFile;
626 NewFile.reserve(MB->getBufferSize());
628 for (const char *Ptr = MB->getBufferStart(), *End = MB->getBufferEnd();
629 Ptr != End; ++Ptr) {
630 // Eliminate trailing dosish \r.
631 if (Ptr <= End - 2 && Ptr[0] == '\r' && Ptr[1] == '\n') {
632 continue;
633 }
635 // If current char is not a horizontal whitespace or if horizontal
636 // whitespace canonicalization is disabled, dump it to output as is.
637 if (PreserveHorizontal || (*Ptr != ' ' && *Ptr != '\t')) {
638 NewFile.push_back(*Ptr);
639 continue;
640 }
642 // Otherwise, add one space and advance over neighboring space.
643 NewFile.push_back(' ');
644 while (Ptr+1 != End &&
645 (Ptr[1] == ' ' || Ptr[1] == '\t'))
646 ++Ptr;
647 }
649 // Free the old buffer and return a new one.
650 MemoryBuffer *MB2 =
651 MemoryBuffer::getMemBufferCopy(NewFile.str(), MB->getBufferIdentifier());
653 delete MB;
654 return MB2;
655 }
657 static bool IsPartOfWord(char c) {
658 return (isalnum(c) || c == '-' || c == '_');
659 }
661 // Get the size of the prefix extension.
662 static size_t CheckTypeSize(Check::CheckType Ty) {
663 switch (Ty) {
664 case Check::CheckNone:
665 return 0;
667 case Check::CheckPlain:
668 return sizeof(":") - 1;
670 case Check::CheckNext:
671 return sizeof("-NEXT:") - 1;
673 case Check::CheckNot:
674 return sizeof("-NOT:") - 1;
676 case Check::CheckDAG:
677 return sizeof("-DAG:") - 1;
679 case Check::CheckLabel:
680 return sizeof("-LABEL:") - 1;
682 case Check::CheckEOF:
683 llvm_unreachable("Should not be using EOF size");
684 }
686 llvm_unreachable("Bad check type");
687 }
689 static Check::CheckType FindCheckType(StringRef Buffer, StringRef Prefix) {
690 char NextChar = Buffer[Prefix.size()];
692 // Verify that the : is present after the prefix.
693 if (NextChar == ':')
694 return Check::CheckPlain;
696 if (NextChar != '-')
697 return Check::CheckNone;
699 StringRef Rest = Buffer.drop_front(Prefix.size() + 1);
700 if (Rest.startswith("NEXT:"))
701 return Check::CheckNext;
703 if (Rest.startswith("NOT:"))
704 return Check::CheckNot;
706 if (Rest.startswith("DAG:"))
707 return Check::CheckDAG;
709 if (Rest.startswith("LABEL:"))
710 return Check::CheckLabel;
712 return Check::CheckNone;
713 }
715 // From the given position, find the next character after the word.
716 static size_t SkipWord(StringRef Str, size_t Loc) {
717 while (Loc < Str.size() && IsPartOfWord(Str[Loc]))
718 ++Loc;
719 return Loc;
720 }
722 // Try to find the first match in buffer for any prefix. If a valid match is
723 // found, return that prefix and set its type and location. If there are almost
724 // matches (e.g. the actual prefix string is found, but is not an actual check
725 // string), but no valid match, return an empty string and set the position to
726 // resume searching from. If no partial matches are found, return an empty
727 // string and the location will be StringRef::npos. If one prefix is a substring
728 // of another, the maximal match should be found. e.g. if "A" and "AA" are
729 // prefixes then AA-CHECK: should match the second one.
730 static StringRef FindFirstCandidateMatch(StringRef &Buffer,
731 Check::CheckType &CheckTy,
732 size_t &CheckLoc) {
733 StringRef FirstPrefix;
734 size_t FirstLoc = StringRef::npos;
735 size_t SearchLoc = StringRef::npos;
736 Check::CheckType FirstTy = Check::CheckNone;
738 CheckTy = Check::CheckNone;
739 CheckLoc = StringRef::npos;
741 for (prefix_iterator I = CheckPrefixes.begin(), E = CheckPrefixes.end();
742 I != E; ++I) {
743 StringRef Prefix(*I);
744 size_t PrefixLoc = Buffer.find(Prefix);
746 if (PrefixLoc == StringRef::npos)
747 continue;
749 // Track where we are searching for invalid prefixes that look almost right.
750 // We need to only advance to the first partial match on the next attempt
751 // since a partial match could be a substring of a later, valid prefix.
752 // Need to skip to the end of the word, otherwise we could end up
753 // matching a prefix in a substring later.
754 if (PrefixLoc < SearchLoc)
755 SearchLoc = SkipWord(Buffer, PrefixLoc);
757 // We only want to find the first match to avoid skipping some.
758 if (PrefixLoc > FirstLoc)
759 continue;
760 // If one matching check-prefix is a prefix of another, choose the
761 // longer one.
762 if (PrefixLoc == FirstLoc && Prefix.size() < FirstPrefix.size())
763 continue;
765 StringRef Rest = Buffer.drop_front(PrefixLoc);
766 // Make sure we have actually found the prefix, and not a word containing
767 // it. This should also prevent matching the wrong prefix when one is a
768 // substring of another.
769 if (PrefixLoc != 0 && IsPartOfWord(Buffer[PrefixLoc - 1]))
770 FirstTy = Check::CheckNone;
771 else
772 FirstTy = FindCheckType(Rest, Prefix);
774 FirstLoc = PrefixLoc;
775 FirstPrefix = Prefix;
776 }
778 // If the first prefix is invalid, we should continue the search after it.
779 if (FirstTy == Check::CheckNone) {
780 CheckLoc = SearchLoc;
781 return "";
782 }
784 CheckTy = FirstTy;
785 CheckLoc = FirstLoc;
786 return FirstPrefix;
787 }
789 static StringRef FindFirstMatchingPrefix(StringRef &Buffer,
790 unsigned &LineNumber,
791 Check::CheckType &CheckTy,
792 size_t &CheckLoc) {
793 while (!Buffer.empty()) {
794 StringRef Prefix = FindFirstCandidateMatch(Buffer, CheckTy, CheckLoc);
795 // If we found a real match, we are done.
796 if (!Prefix.empty()) {
797 LineNumber += Buffer.substr(0, CheckLoc).count('\n');
798 return Prefix;
799 }
801 // We didn't find any almost matches either, we are also done.
802 if (CheckLoc == StringRef::npos)
803 return StringRef();
805 LineNumber += Buffer.substr(0, CheckLoc + 1).count('\n');
807 // Advance to the last possible match we found and try again.
808 Buffer = Buffer.drop_front(CheckLoc + 1);
809 }
811 return StringRef();
812 }
814 /// ReadCheckFile - Read the check file, which specifies the sequence of
815 /// expected strings. The strings are added to the CheckStrings vector.
816 /// Returns true in case of an error, false otherwise.
817 static bool ReadCheckFile(SourceMgr &SM,
818 std::vector<CheckString> &CheckStrings) {
819 OwningPtr<MemoryBuffer> File;
820 if (error_code ec =
821 MemoryBuffer::getFileOrSTDIN(CheckFilename, File)) {
822 errs() << "Could not open check file '" << CheckFilename << "': "
823 << ec.message() << '\n';
824 return true;
825 }
827 // If we want to canonicalize whitespace, strip excess whitespace from the
828 // buffer containing the CHECK lines. Remove DOS style line endings.
829 MemoryBuffer *F =
830 CanonicalizeInputFile(File.take(), NoCanonicalizeWhiteSpace);
832 SM.AddNewSourceBuffer(F, SMLoc());
834 // Find all instances of CheckPrefix followed by : in the file.
835 StringRef Buffer = F->getBuffer();
836 std::vector<Pattern> DagNotMatches;
838 // LineNumber keeps track of the line on which CheckPrefix instances are
839 // found.
840 unsigned LineNumber = 1;
842 while (1) {
843 Check::CheckType CheckTy;
844 size_t PrefixLoc;
846 // See if a prefix occurs in the memory buffer.
847 StringRef UsedPrefix = FindFirstMatchingPrefix(Buffer,
848 LineNumber,
849 CheckTy,
850 PrefixLoc);
851 if (UsedPrefix.empty())
852 break;
854 Buffer = Buffer.drop_front(PrefixLoc);
856 // Location to use for error messages.
857 const char *UsedPrefixStart = Buffer.data() + (PrefixLoc == 0 ? 0 : 1);
859 // PrefixLoc is to the start of the prefix. Skip to the end.
860 Buffer = Buffer.drop_front(UsedPrefix.size() + CheckTypeSize(CheckTy));
862 // Okay, we found the prefix, yay. Remember the rest of the line, but ignore
863 // leading and trailing whitespace.
864 Buffer = Buffer.substr(Buffer.find_first_not_of(" \t"));
866 // Scan ahead to the end of line.
867 size_t EOL = Buffer.find_first_of("\n\r");
869 // Remember the location of the start of the pattern, for diagnostics.
870 SMLoc PatternLoc = SMLoc::getFromPointer(Buffer.data());
872 // Parse the pattern.
873 Pattern P(CheckTy);
874 if (P.ParsePattern(Buffer.substr(0, EOL), UsedPrefix, SM, LineNumber))
875 return true;
877 // Verify that CHECK-LABEL lines do not define or use variables
878 if ((CheckTy == Check::CheckLabel) && P.hasVariable()) {
879 SM.PrintMessage(SMLoc::getFromPointer(UsedPrefixStart),
880 SourceMgr::DK_Error,
881 "found '" + UsedPrefix + "-LABEL:'"
882 " with variable definition or use");
883 return true;
884 }
886 Buffer = Buffer.substr(EOL);
888 // Verify that CHECK-NEXT lines have at least one CHECK line before them.
889 if ((CheckTy == Check::CheckNext) && CheckStrings.empty()) {
890 SM.PrintMessage(SMLoc::getFromPointer(UsedPrefixStart),
891 SourceMgr::DK_Error,
892 "found '" + UsedPrefix + "-NEXT:' without previous '"
893 + UsedPrefix + ": line");
894 return true;
895 }
897 // Handle CHECK-DAG/-NOT.
898 if (CheckTy == Check::CheckDAG || CheckTy == Check::CheckNot) {
899 DagNotMatches.push_back(P);
900 continue;
901 }
903 // Okay, add the string we captured to the output vector and move on.
904 CheckStrings.push_back(CheckString(P,
905 UsedPrefix,
906 PatternLoc,
907 CheckTy));
908 std::swap(DagNotMatches, CheckStrings.back().DagNotStrings);
909 }
911 // Add an EOF pattern for any trailing CHECK-DAG/-NOTs, and use the first
912 // prefix as a filler for the error message.
913 if (!DagNotMatches.empty()) {
914 CheckStrings.push_back(CheckString(Pattern(Check::CheckEOF),
915 CheckPrefixes[0],
916 SMLoc::getFromPointer(Buffer.data()),
917 Check::CheckEOF));
918 std::swap(DagNotMatches, CheckStrings.back().DagNotStrings);
919 }
921 if (CheckStrings.empty()) {
922 errs() << "error: no check strings found with prefix"
923 << (CheckPrefixes.size() > 1 ? "es " : " ");
924 for (size_t I = 0, N = CheckPrefixes.size(); I != N; ++I) {
925 StringRef Prefix(CheckPrefixes[I]);
926 errs() << '\'' << Prefix << ":'";
927 if (I != N - 1)
928 errs() << ", ";
929 }
931 errs() << '\n';
932 return true;
933 }
935 return false;
936 }
938 static void PrintCheckFailed(const SourceMgr &SM, const SMLoc &Loc,
939 const Pattern &Pat, StringRef Buffer,
940 StringMap<StringRef> &VariableTable) {
941 // Otherwise, we have an error, emit an error message.
942 SM.PrintMessage(Loc, SourceMgr::DK_Error,
943 "expected string not found in input");
945 // Print the "scanning from here" line. If the current position is at the
946 // end of a line, advance to the start of the next line.
947 Buffer = Buffer.substr(Buffer.find_first_not_of(" \t\n\r"));
949 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), SourceMgr::DK_Note,
950 "scanning from here");
952 // Allow the pattern to print additional information if desired.
953 Pat.PrintFailureInfo(SM, Buffer, VariableTable);
954 }
956 static void PrintCheckFailed(const SourceMgr &SM, const CheckString &CheckStr,
957 StringRef Buffer,
958 StringMap<StringRef> &VariableTable) {
959 PrintCheckFailed(SM, CheckStr.Loc, CheckStr.Pat, Buffer, VariableTable);
960 }
962 /// CountNumNewlinesBetween - Count the number of newlines in the specified
963 /// range.
964 static unsigned CountNumNewlinesBetween(StringRef Range) {
965 unsigned NumNewLines = 0;
966 while (1) {
967 // Scan for newline.
968 Range = Range.substr(Range.find_first_of("\n\r"));
969 if (Range.empty()) return NumNewLines;
971 ++NumNewLines;
973 // Handle \n\r and \r\n as a single newline.
974 if (Range.size() > 1 &&
975 (Range[1] == '\n' || Range[1] == '\r') &&
976 (Range[0] != Range[1]))
977 Range = Range.substr(1);
978 Range = Range.substr(1);
979 }
980 }
982 size_t CheckString::Check(const SourceMgr &SM, StringRef Buffer,
983 bool IsLabelScanMode, size_t &MatchLen,
984 StringMap<StringRef> &VariableTable) const {
985 size_t LastPos = 0;
986 std::vector<const Pattern *> NotStrings;
988 // IsLabelScanMode is true when we are scanning forward to find CHECK-LABEL
989 // bounds; we have not processed variable definitions within the bounded block
990 // yet so cannot handle any final CHECK-DAG yet; this is handled when going
991 // over the block again (including the last CHECK-LABEL) in normal mode.
992 if (!IsLabelScanMode) {
993 // Match "dag strings" (with mixed "not strings" if any).
994 LastPos = CheckDag(SM, Buffer, NotStrings, VariableTable);
995 if (LastPos == StringRef::npos)
996 return StringRef::npos;
997 }
999 // Match itself from the last position after matching CHECK-DAG.
1000 StringRef MatchBuffer = Buffer.substr(LastPos);
1001 size_t MatchPos = Pat.Match(MatchBuffer, MatchLen, VariableTable);
1002 if (MatchPos == StringRef::npos) {
1003 PrintCheckFailed(SM, *this, MatchBuffer, VariableTable);
1004 return StringRef::npos;
1005 }
1006 MatchPos += LastPos;
1008 // Similar to the above, in "label-scan mode" we can't yet handle CHECK-NEXT
1009 // or CHECK-NOT
1010 if (!IsLabelScanMode) {
1011 StringRef SkippedRegion = Buffer.substr(LastPos, MatchPos);
1013 // If this check is a "CHECK-NEXT", verify that the previous match was on
1014 // the previous line (i.e. that there is one newline between them).
1015 if (CheckNext(SM, SkippedRegion))
1016 return StringRef::npos;
1018 // If this match had "not strings", verify that they don't exist in the
1019 // skipped region.
1020 if (CheckNot(SM, SkippedRegion, NotStrings, VariableTable))
1021 return StringRef::npos;
1022 }
1024 return MatchPos;
1025 }
1027 bool CheckString::CheckNext(const SourceMgr &SM, StringRef Buffer) const {
1028 if (CheckTy != Check::CheckNext)
1029 return false;
1031 // Count the number of newlines between the previous match and this one.
1032 assert(Buffer.data() !=
1033 SM.getMemoryBuffer(
1034 SM.FindBufferContainingLoc(
1035 SMLoc::getFromPointer(Buffer.data())))->getBufferStart() &&
1036 "CHECK-NEXT can't be the first check in a file");
1038 unsigned NumNewLines = CountNumNewlinesBetween(Buffer);
1040 if (NumNewLines == 0) {
1041 SM.PrintMessage(Loc, SourceMgr::DK_Error, Prefix +
1042 "-NEXT: is on the same line as previous match");
1043 SM.PrintMessage(SMLoc::getFromPointer(Buffer.end()),
1044 SourceMgr::DK_Note, "'next' match was here");
1045 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), SourceMgr::DK_Note,
1046 "previous match ended here");
1047 return true;
1048 }
1050 if (NumNewLines != 1) {
1051 SM.PrintMessage(Loc, SourceMgr::DK_Error, Prefix +
1052 "-NEXT: is not on the line after the previous match");
1053 SM.PrintMessage(SMLoc::getFromPointer(Buffer.end()),
1054 SourceMgr::DK_Note, "'next' match was here");
1055 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), SourceMgr::DK_Note,
1056 "previous match ended here");
1057 return true;
1058 }
1060 return false;
1061 }
1063 bool CheckString::CheckNot(const SourceMgr &SM, StringRef Buffer,
1064 const std::vector<const Pattern *> &NotStrings,
1065 StringMap<StringRef> &VariableTable) const {
1066 for (unsigned ChunkNo = 0, e = NotStrings.size();
1067 ChunkNo != e; ++ChunkNo) {
1068 const Pattern *Pat = NotStrings[ChunkNo];
1069 assert((Pat->getCheckTy() == Check::CheckNot) && "Expect CHECK-NOT!");
1071 size_t MatchLen = 0;
1072 size_t Pos = Pat->Match(Buffer, MatchLen, VariableTable);
1074 if (Pos == StringRef::npos) continue;
1076 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()+Pos),
1077 SourceMgr::DK_Error,
1078 Prefix + "-NOT: string occurred!");
1079 SM.PrintMessage(Pat->getLoc(), SourceMgr::DK_Note,
1080 Prefix + "-NOT: pattern specified here");
1081 return true;
1082 }
1084 return false;
1085 }
1087 size_t CheckString::CheckDag(const SourceMgr &SM, StringRef Buffer,
1088 std::vector<const Pattern *> &NotStrings,
1089 StringMap<StringRef> &VariableTable) const {
1090 if (DagNotStrings.empty())
1091 return 0;
1093 size_t LastPos = 0;
1094 size_t StartPos = LastPos;
1096 for (unsigned ChunkNo = 0, e = DagNotStrings.size();
1097 ChunkNo != e; ++ChunkNo) {
1098 const Pattern &Pat = DagNotStrings[ChunkNo];
1100 assert((Pat.getCheckTy() == Check::CheckDAG ||
1101 Pat.getCheckTy() == Check::CheckNot) &&
1102 "Invalid CHECK-DAG or CHECK-NOT!");
1104 if (Pat.getCheckTy() == Check::CheckNot) {
1105 NotStrings.push_back(&Pat);
1106 continue;
1107 }
1109 assert((Pat.getCheckTy() == Check::CheckDAG) && "Expect CHECK-DAG!");
1111 size_t MatchLen = 0, MatchPos;
1113 // CHECK-DAG always matches from the start.
1114 StringRef MatchBuffer = Buffer.substr(StartPos);
1115 MatchPos = Pat.Match(MatchBuffer, MatchLen, VariableTable);
1116 // With a group of CHECK-DAGs, a single mismatching means the match on
1117 // that group of CHECK-DAGs fails immediately.
1118 if (MatchPos == StringRef::npos) {
1119 PrintCheckFailed(SM, Pat.getLoc(), Pat, MatchBuffer, VariableTable);
1120 return StringRef::npos;
1121 }
1122 // Re-calc it as the offset relative to the start of the original string.
1123 MatchPos += StartPos;
1125 if (!NotStrings.empty()) {
1126 if (MatchPos < LastPos) {
1127 // Reordered?
1128 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data() + MatchPos),
1129 SourceMgr::DK_Error,
1130 Prefix + "-DAG: found a match of CHECK-DAG"
1131 " reordering across a CHECK-NOT");
1132 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data() + LastPos),
1133 SourceMgr::DK_Note,
1134 Prefix + "-DAG: the farthest match of CHECK-DAG"
1135 " is found here");
1136 SM.PrintMessage(NotStrings[0]->getLoc(), SourceMgr::DK_Note,
1137 Prefix + "-NOT: the crossed pattern specified"
1138 " here");
1139 SM.PrintMessage(Pat.getLoc(), SourceMgr::DK_Note,
1140 Prefix + "-DAG: the reordered pattern specified"
1141 " here");
1142 return StringRef::npos;
1143 }
1144 // All subsequent CHECK-DAGs should be matched from the farthest
1145 // position of all precedent CHECK-DAGs (including this one.)
1146 StartPos = LastPos;
1147 // If there's CHECK-NOTs between two CHECK-DAGs or from CHECK to
1148 // CHECK-DAG, verify that there's no 'not' strings occurred in that
1149 // region.
1150 StringRef SkippedRegion = Buffer.substr(LastPos, MatchPos);
1151 if (CheckNot(SM, SkippedRegion, NotStrings, VariableTable))
1152 return StringRef::npos;
1153 // Clear "not strings".
1154 NotStrings.clear();
1155 }
1157 // Update the last position with CHECK-DAG matches.
1158 LastPos = std::max(MatchPos + MatchLen, LastPos);
1159 }
1161 return LastPos;
1162 }
1164 // A check prefix must contain only alphanumeric, hyphens and underscores.
1165 static bool ValidateCheckPrefix(StringRef CheckPrefix) {
1166 Regex Validator("^[a-zA-Z0-9_-]*$");
1167 return Validator.match(CheckPrefix);
1168 }
1170 static bool ValidateCheckPrefixes() {
1171 StringSet<> PrefixSet;
1173 for (prefix_iterator I = CheckPrefixes.begin(), E = CheckPrefixes.end();
1174 I != E; ++I) {
1175 StringRef Prefix(*I);
1177 if (!PrefixSet.insert(Prefix))
1178 return false;
1180 if (!ValidateCheckPrefix(Prefix))
1181 return false;
1182 }
1184 return true;
1185 }
1187 // I don't think there's a way to specify an initial value for cl::list,
1188 // so if nothing was specified, add the default
1189 static void AddCheckPrefixIfNeeded() {
1190 if (CheckPrefixes.empty())
1191 CheckPrefixes.push_back("CHECK");
1192 }
1194 int main(int argc, char **argv) {
1195 sys::PrintStackTraceOnErrorSignal();
1196 PrettyStackTraceProgram X(argc, argv);
1197 cl::ParseCommandLineOptions(argc, argv);
1199 if (!ValidateCheckPrefixes()) {
1200 errs() << "Supplied check-prefix is invalid! Prefixes must be unique and "
1201 "start with a letter and contain only alphanumeric characters, "
1202 "hyphens and underscores\n";
1203 return 2;
1204 }
1206 AddCheckPrefixIfNeeded();
1208 SourceMgr SM;
1210 // Read the expected strings from the check file.
1211 std::vector<CheckString> CheckStrings;
1212 if (ReadCheckFile(SM, CheckStrings))
1213 return 2;
1215 // Open the file to check and add it to SourceMgr.
1216 OwningPtr<MemoryBuffer> File;
1217 if (error_code ec =
1218 MemoryBuffer::getFileOrSTDIN(InputFilename, File)) {
1219 errs() << "Could not open input file '" << InputFilename << "': "
1220 << ec.message() << '\n';
1221 return 2;
1222 }
1224 if (File->getBufferSize() == 0) {
1225 errs() << "FileCheck error: '" << InputFilename << "' is empty.\n";
1226 return 2;
1227 }
1229 // Remove duplicate spaces in the input file if requested.
1230 // Remove DOS style line endings.
1231 MemoryBuffer *F =
1232 CanonicalizeInputFile(File.take(), NoCanonicalizeWhiteSpace);
1234 SM.AddNewSourceBuffer(F, SMLoc());
1236 /// VariableTable - This holds all the current filecheck variables.
1237 StringMap<StringRef> VariableTable;
1239 // Check that we have all of the expected strings, in order, in the input
1240 // file.
1241 StringRef Buffer = F->getBuffer();
1243 bool hasError = false;
1245 unsigned i = 0, j = 0, e = CheckStrings.size();
1247 while (true) {
1248 StringRef CheckRegion;
1249 if (j == e) {
1250 CheckRegion = Buffer;
1251 } else {
1252 const CheckString &CheckLabelStr = CheckStrings[j];
1253 if (CheckLabelStr.CheckTy != Check::CheckLabel) {
1254 ++j;
1255 continue;
1256 }
1258 // Scan to next CHECK-LABEL match, ignoring CHECK-NOT and CHECK-DAG
1259 size_t MatchLabelLen = 0;
1260 size_t MatchLabelPos = CheckLabelStr.Check(SM, Buffer, true,
1261 MatchLabelLen, VariableTable);
1262 if (MatchLabelPos == StringRef::npos) {
1263 hasError = true;
1264 break;
1265 }
1267 CheckRegion = Buffer.substr(0, MatchLabelPos + MatchLabelLen);
1268 Buffer = Buffer.substr(MatchLabelPos + MatchLabelLen);
1269 ++j;
1270 }
1272 for ( ; i != j; ++i) {
1273 const CheckString &CheckStr = CheckStrings[i];
1275 // Check each string within the scanned region, including a second check
1276 // of any final CHECK-LABEL (to verify CHECK-NOT and CHECK-DAG)
1277 size_t MatchLen = 0;
1278 size_t MatchPos = CheckStr.Check(SM, CheckRegion, false, MatchLen,
1279 VariableTable);
1281 if (MatchPos == StringRef::npos) {
1282 hasError = true;
1283 i = j;
1284 break;
1285 }
1287 CheckRegion = CheckRegion.substr(MatchPos + MatchLen);
1288 }
1290 if (j == e)
1291 break;
1292 }
1294 return hasError ? 1 : 0;
1295 }