1 //===- FileCheck.cpp - Check that File's Contents match what is expected --===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // FileCheck does a line-by line check of a file that validates whether it
11 // contains the expected content. This is useful for regression tests etc.
12 //
13 // This program exits with an error status of 2 on error, exit status of 0 if
14 // the file matched the expected contents, and exit status of 1 if it did not
15 // contain the expected contents.
16 //
17 //===----------------------------------------------------------------------===//
19 #include "llvm/Support/CommandLine.h"
20 #include "llvm/Support/MemoryBuffer.h"
21 #include "llvm/Support/PrettyStackTrace.h"
22 #include "llvm/Support/SourceMgr.h"
23 #include "llvm/Support/raw_ostream.h"
24 #include "llvm/System/Signals.h"
25 using namespace llvm;
27 static cl::opt<std::string>
28 CheckFilename(cl::Positional, cl::desc("<check-file>"), cl::Required);
30 static cl::opt<std::string>
31 InputFilename("input-file", cl::desc("File to check (defaults to stdin)"),
32 cl::init("-"), cl::value_desc("filename"));
34 static cl::opt<std::string>
35 CheckPrefix("check-prefix", cl::init("CHECK"),
36 cl::desc("Prefix to use from check file (defaults to 'CHECK')"));
38 static cl::opt<bool>
39 NoCanonicalizeWhiteSpace("strict-whitespace",
40 cl::desc("Do not treat all horizontal whitespace as equivalent"));
42 /// CheckString - This is a check that we found in the input file.
43 struct CheckString {
44 /// Str - The string to match.
45 std::string Str;
47 /// Loc - The location in the match file that the check string was specified.
48 SMLoc Loc;
50 CheckString(const std::string &S, SMLoc L) : Str(S), Loc(L) {}
51 };
54 /// FindFixedStringInBuffer - This works like strstr, except for two things:
55 /// 1) it handles 'nul' characters in memory buffers. 2) it returns the end of
56 /// the memory buffer on match failure instead of null.
57 static const char *FindFixedStringInBuffer(StringRef Str, const char *CurPtr,
58 const MemoryBuffer &MB) {
59 assert(!Str.empty() && "Can't find an empty string");
60 const char *BufEnd = MB.getBufferEnd();
62 while (1) {
63 // Scan for the first character in the match string.
64 CurPtr = (char*)memchr(CurPtr, Str[0], BufEnd-CurPtr);
66 // If we didn't find the first character of the string, then we failed to
67 // match.
68 if (CurPtr == 0) return BufEnd;
70 // If the match string is one character, then we win.
71 if (Str.size() == 1) return CurPtr;
73 // Otherwise, verify that the rest of the string matches.
74 if (Str.size() <= unsigned(BufEnd-CurPtr) &&
75 memcmp(CurPtr+1, Str.data()+1, Str.size()-1) == 0)
76 return CurPtr;
78 // If not, advance past this character and try again.
79 ++CurPtr;
80 }
81 }
83 /// ReadCheckFile - Read the check file, which specifies the sequence of
84 /// expected strings. The strings are added to the CheckStrings vector.
85 static bool ReadCheckFile(SourceMgr &SM,
86 std::vector<CheckString> &CheckStrings) {
87 // Open the check file, and tell SourceMgr about it.
88 std::string ErrorStr;
89 MemoryBuffer *F =
90 MemoryBuffer::getFileOrSTDIN(CheckFilename.c_str(), &ErrorStr);
91 if (F == 0) {
92 errs() << "Could not open check file '" << CheckFilename << "': "
93 << ErrorStr << '\n';
94 return true;
95 }
96 SM.AddNewSourceBuffer(F, SMLoc());
98 // Find all instances of CheckPrefix followed by : in the file. The
99 // MemoryBuffer is guaranteed to be nul terminated, but may have nul's
100 // embedded into it. We don't support check strings with embedded nuls.
101 std::string Prefix = CheckPrefix + ":";
102 const char *CurPtr = F->getBufferStart(), *BufferEnd = F->getBufferEnd();
104 while (1) {
105 // See if Prefix occurs in the memory buffer.
106 const char *Ptr = FindFixedStringInBuffer(Prefix, CurPtr, *F);
108 // If we didn't find a match, we're done.
109 if (Ptr == BufferEnd)
110 break;
112 // Okay, we found the prefix, yay. Remember the rest of the line, but
113 // ignore leading and trailing whitespace.
114 Ptr += Prefix.size();
115 while (*Ptr == ' ' || *Ptr == '\t')
116 ++Ptr;
118 // Scan ahead to the end of line.
119 CurPtr = Ptr;
120 while (CurPtr != BufferEnd && *CurPtr != '\n' && *CurPtr != '\r')
121 ++CurPtr;
123 // Ignore trailing whitespace.
124 while (CurPtr[-1] == ' ' || CurPtr[-1] == '\t')
125 --CurPtr;
127 // Check that there is something on the line.
128 if (Ptr >= CurPtr) {
129 SM.PrintMessage(SMLoc::getFromPointer(CurPtr),
130 "found empty check string with prefix '"+Prefix+"'",
131 "error");
132 return true;
133 }
135 // Okay, add the string we captured to the output vector and move on.
136 CheckStrings.push_back(CheckString(std::string(Ptr, CurPtr),
137 SMLoc::getFromPointer(Ptr)));
138 }
140 if (CheckStrings.empty()) {
141 errs() << "error: no check strings found with prefix '" << Prefix << "'\n";
142 return true;
143 }
145 return false;
146 }
148 // CanonicalizeCheckStrings - Replace all sequences of horizontal whitespace in
149 // the check strings with a single space.
150 static void CanonicalizeCheckStrings(std::vector<CheckString> &CheckStrings) {
151 for (unsigned i = 0, e = CheckStrings.size(); i != e; ++i) {
152 std::string &Str = CheckStrings[i].Str;
154 for (unsigned C = 0; C != Str.size(); ++C) {
155 // If C is not a horizontal whitespace, skip it.
156 if (Str[C] != ' ' && Str[C] != '\t')
157 continue;
159 // Replace the character with space, then remove any other space
160 // characters after it.
161 Str[C] = ' ';
163 while (C+1 != Str.size() &&
164 (Str[C+1] == ' ' || Str[C+1] == '\t'))
165 Str.erase(Str.begin()+C+1);
166 }
167 }
168 }
170 /// CanonicalizeInputFile - Remove duplicate horizontal space from the specified
171 /// memory buffer, free it, and return a new one.
172 static MemoryBuffer *CanonicalizeInputFile(MemoryBuffer *MB) {
173 SmallVector<char, 16> NewFile;
174 NewFile.reserve(MB->getBufferSize());
176 for (const char *Ptr = MB->getBufferStart(), *End = MB->getBufferEnd();
177 Ptr != End; ++Ptr) {
178 // If C is not a horizontal whitespace, skip it.
179 if (*Ptr != ' ' && *Ptr != '\t') {
180 NewFile.push_back(*Ptr);
181 continue;
182 }
184 // Otherwise, add one space and advance over neighboring space.
185 NewFile.push_back(' ');
186 while (Ptr+1 != End &&
187 (Ptr[1] == ' ' || Ptr[1] == '\t'))
188 ++Ptr;
189 }
191 // Free the old buffer and return a new one.
192 MemoryBuffer *MB2 =
193 MemoryBuffer::getMemBufferCopy(NewFile.data(),
194 NewFile.data() + NewFile.size(),
195 MB->getBufferIdentifier());
197 delete MB;
198 return MB2;
199 }
202 int main(int argc, char **argv) {
203 sys::PrintStackTraceOnErrorSignal();
204 PrettyStackTraceProgram X(argc, argv);
205 cl::ParseCommandLineOptions(argc, argv);
207 SourceMgr SM;
209 // Read the expected strings from the check file.
210 std::vector<CheckString> CheckStrings;
211 if (ReadCheckFile(SM, CheckStrings))
212 return 2;
214 // Remove duplicate spaces in the check strings if requested.
215 if (!NoCanonicalizeWhiteSpace)
216 CanonicalizeCheckStrings(CheckStrings);
218 // Open the file to check and add it to SourceMgr.
219 std::string ErrorStr;
220 MemoryBuffer *F =
221 MemoryBuffer::getFileOrSTDIN(InputFilename.c_str(), &ErrorStr);
222 if (F == 0) {
223 errs() << "Could not open input file '" << InputFilename << "': "
224 << ErrorStr << '\n';
225 return true;
226 }
228 // Remove duplicate spaces in the input file if requested.
229 if (!NoCanonicalizeWhiteSpace)
230 F = CanonicalizeInputFile(F);
232 SM.AddNewSourceBuffer(F, SMLoc());
234 // Check that we have all of the expected strings, in order, in the input
235 // file.
236 const char *CurPtr = F->getBufferStart(), *BufferEnd = F->getBufferEnd();
238 for (unsigned StrNo = 0, e = CheckStrings.size(); StrNo != e; ++StrNo) {
239 const CheckString &CheckStr = CheckStrings[StrNo];
241 // Find StrNo in the file.
242 const char *Ptr = FindFixedStringInBuffer(CheckStr.Str, CurPtr, *F);
244 // If we found a match, we're done, move on.
245 if (Ptr != BufferEnd) {
246 CurPtr = Ptr + CheckStr.Str.size();
247 continue;
248 }
250 // Otherwise, we have an error, emit an error message.
251 SM.PrintMessage(CheckStr.Loc, "expected string not found in input",
252 "error");
254 // Print the "scanning from here" line. If the current position is at the
255 // end of a line, advance to the start of the next line.
256 const char *Scan = CurPtr;
257 while (Scan != BufferEnd &&
258 (*Scan == ' ' || *Scan == '\t'))
259 ++Scan;
260 if (*Scan == '\n' || *Scan == '\r')
261 CurPtr = Scan+1;
264 SM.PrintMessage(SMLoc::getFromPointer(CurPtr), "scanning from here",
265 "note");
266 return 1;
267 }
269 return 0;
270 }