1 //===- FileCheck.cpp - Check that File's Contents match what is expected --===//
2 //
3 // The LLVM Compiler Infrastructure
4 //
5 // This file is distributed under the University of Illinois Open Source
6 // License. See LICENSE.TXT for details.
7 //
8 //===----------------------------------------------------------------------===//
9 //
10 // FileCheck does a line-by line check of a file that validates whether it
11 // contains the expected content. This is useful for regression tests etc.
12 //
13 // This program exits with an error status of 2 on error, exit status of 0 if
14 // the file matched the expected contents, and exit status of 1 if it did not
15 // contain the expected contents.
16 //
17 //===----------------------------------------------------------------------===//
19 #include "llvm/ADT/OwningPtr.h"
20 #include "llvm/ADT/SmallString.h"
21 #include "llvm/ADT/StringExtras.h"
22 #include "llvm/ADT/StringMap.h"
23 #include "llvm/Support/CommandLine.h"
24 #include "llvm/Support/MemoryBuffer.h"
25 #include "llvm/Support/PrettyStackTrace.h"
26 #include "llvm/Support/Regex.h"
27 #include "llvm/Support/Signals.h"
28 #include "llvm/Support/SourceMgr.h"
29 #include "llvm/Support/raw_ostream.h"
30 #include "llvm/Support/system_error.h"
31 #include <algorithm>
32 #include <map>
33 #include <string>
34 #include <vector>
35 using namespace llvm;
37 static cl::opt<std::string>
38 CheckFilename(cl::Positional, cl::desc("<check-file>"), cl::Required);
40 static cl::opt<std::string>
41 InputFilename("input-file", cl::desc("File to check (defaults to stdin)"),
42 cl::init("-"), cl::value_desc("filename"));
44 static cl::opt<std::string>
45 CheckPrefix("check-prefix", cl::init("CHECK"),
46 cl::desc("Prefix to use from check file (defaults to 'CHECK')"));
48 static cl::opt<bool>
49 NoCanonicalizeWhiteSpace("strict-whitespace",
50 cl::desc("Do not treat all horizontal whitespace as equivalent"));
52 //===----------------------------------------------------------------------===//
53 // Pattern Handling Code.
54 //===----------------------------------------------------------------------===//
56 class Pattern {
57 SMLoc PatternLoc;
59 /// MatchEOF - When set, this pattern only matches the end of file. This is
60 /// used for trailing CHECK-NOTs.
61 bool MatchEOF;
63 /// MatchNot
64 bool MatchNot;
66 /// MatchDag
67 bool MatchDag;
69 /// FixedStr - If non-empty, this pattern is a fixed string match with the
70 /// specified fixed string.
71 StringRef FixedStr;
73 /// RegEx - If non-empty, this is a regex pattern.
74 std::string RegExStr;
76 /// \brief Contains the number of line this pattern is in.
77 unsigned LineNumber;
79 /// VariableUses - Entries in this vector map to uses of a variable in the
80 /// pattern, e.g. "foo[[bar]]baz". In this case, the RegExStr will contain
81 /// "foobaz" and we'll get an entry in this vector that tells us to insert the
82 /// value of bar at offset 3.
83 std::vector<std::pair<StringRef, unsigned> > VariableUses;
85 /// VariableDefs - Maps definitions of variables to their parenthesized
86 /// capture numbers.
87 /// E.g. for the pattern "foo[[bar:.*]]baz", VariableDefs will map "bar" to 1.
88 std::map<StringRef, unsigned> VariableDefs;
90 public:
92 Pattern(bool matchEOF = false)
93 : MatchEOF(matchEOF), MatchNot(false), MatchDag(false) { }
95 /// getLoc - Return the location in source code.
96 SMLoc getLoc() const { return PatternLoc; }
98 /// ParsePattern - Parse the given string into the Pattern. SM provides the
99 /// SourceMgr used for error reports, and LineNumber is the line number in
100 /// the input file from which the pattern string was read.
101 /// Returns true in case of an error, false otherwise.
102 bool ParsePattern(StringRef PatternStr, SourceMgr &SM, unsigned LineNumber);
104 /// Match - Match the pattern string against the input buffer Buffer. This
105 /// returns the position that is matched or npos if there is no match. If
106 /// there is a match, the size of the matched string is returned in MatchLen.
107 ///
108 /// The VariableTable StringMap provides the current values of filecheck
109 /// variables and is updated if this match defines new values.
110 size_t Match(StringRef Buffer, size_t &MatchLen,
111 StringMap<StringRef> &VariableTable) const;
113 /// PrintFailureInfo - Print additional information about a failure to match
114 /// involving this pattern.
115 void PrintFailureInfo(const SourceMgr &SM, StringRef Buffer,
116 const StringMap<StringRef> &VariableTable) const;
118 bool hasVariable() const { return !(VariableUses.empty() &&
119 VariableDefs.empty()); }
121 void setMatchNot(bool Not) { MatchNot = Not; }
122 bool getMatchNot() const { return MatchNot; }
124 void setMatchDag(bool Dag) { MatchDag = Dag; }
125 bool getMatchDag() const { return MatchDag; }
127 private:
128 static void AddFixedStringToRegEx(StringRef FixedStr, std::string &TheStr);
129 bool AddRegExToRegEx(StringRef RS, unsigned &CurParen, SourceMgr &SM);
130 void AddBackrefToRegEx(unsigned BackrefNum);
132 /// ComputeMatchDistance - Compute an arbitrary estimate for the quality of
133 /// matching this pattern at the start of \arg Buffer; a distance of zero
134 /// should correspond to a perfect match.
135 unsigned ComputeMatchDistance(StringRef Buffer,
136 const StringMap<StringRef> &VariableTable) const;
138 /// \brief Evaluates expression and stores the result to \p Value.
139 /// \return true on success. false when the expression has invalid syntax.
140 bool EvaluateExpression(StringRef Expr, std::string &Value) const;
142 /// \brief Finds the closing sequence of a regex variable usage or
143 /// definition. Str has to point in the beginning of the definition
144 /// (right after the opening sequence).
145 /// \return offset of the closing sequence within Str, or npos if it was not
146 /// found.
147 size_t FindRegexVarEnd(StringRef Str);
148 };
151 bool Pattern::ParsePattern(StringRef PatternStr, SourceMgr &SM,
152 unsigned LineNumber) {
153 this->LineNumber = LineNumber;
154 PatternLoc = SMLoc::getFromPointer(PatternStr.data());
156 // Ignore trailing whitespace.
157 while (!PatternStr.empty() &&
158 (PatternStr.back() == ' ' || PatternStr.back() == '\t'))
159 PatternStr = PatternStr.substr(0, PatternStr.size()-1);
161 // Check that there is something on the line.
162 if (PatternStr.empty()) {
163 SM.PrintMessage(PatternLoc, SourceMgr::DK_Error,
164 "found empty check string with prefix '" +
165 CheckPrefix+":'");
166 return true;
167 }
169 // Check to see if this is a fixed string, or if it has regex pieces.
170 if (PatternStr.size() < 2 ||
171 (PatternStr.find("{{") == StringRef::npos &&
172 PatternStr.find("[[") == StringRef::npos)) {
173 FixedStr = PatternStr;
174 return false;
175 }
177 // Paren value #0 is for the fully matched string. Any new parenthesized
178 // values add from there.
179 unsigned CurParen = 1;
181 // Otherwise, there is at least one regex piece. Build up the regex pattern
182 // by escaping scary characters in fixed strings, building up one big regex.
183 while (!PatternStr.empty()) {
184 // RegEx matches.
185 if (PatternStr.startswith("{{")) {
186 // This is the start of a regex match. Scan for the }}.
187 size_t End = PatternStr.find("}}");
188 if (End == StringRef::npos) {
189 SM.PrintMessage(SMLoc::getFromPointer(PatternStr.data()),
190 SourceMgr::DK_Error,
191 "found start of regex string with no end '}}'");
192 return true;
193 }
195 // Enclose {{}} patterns in parens just like [[]] even though we're not
196 // capturing the result for any purpose. This is required in case the
197 // expression contains an alternation like: CHECK: abc{{x|z}}def. We
198 // want this to turn into: "abc(x|z)def" not "abcx|zdef".
199 RegExStr += '(';
200 ++CurParen;
202 if (AddRegExToRegEx(PatternStr.substr(2, End-2), CurParen, SM))
203 return true;
204 RegExStr += ')';
206 PatternStr = PatternStr.substr(End+2);
207 continue;
208 }
210 // Named RegEx matches. These are of two forms: [[foo:.*]] which matches .*
211 // (or some other regex) and assigns it to the FileCheck variable 'foo'. The
212 // second form is [[foo]] which is a reference to foo. The variable name
213 // itself must be of the form "[a-zA-Z_][0-9a-zA-Z_]*", otherwise we reject
214 // it. This is to catch some common errors.
215 if (PatternStr.startswith("[[")) {
216 // Find the closing bracket pair ending the match. End is going to be an
217 // offset relative to the beginning of the match string.
218 size_t End = FindRegexVarEnd(PatternStr.substr(2));
220 if (End == StringRef::npos) {
221 SM.PrintMessage(SMLoc::getFromPointer(PatternStr.data()),
222 SourceMgr::DK_Error,
223 "invalid named regex reference, no ]] found");
224 return true;
225 }
227 StringRef MatchStr = PatternStr.substr(2, End);
228 PatternStr = PatternStr.substr(End+4);
230 // Get the regex name (e.g. "foo").
231 size_t NameEnd = MatchStr.find(':');
232 StringRef Name = MatchStr.substr(0, NameEnd);
234 if (Name.empty()) {
235 SM.PrintMessage(SMLoc::getFromPointer(Name.data()), SourceMgr::DK_Error,
236 "invalid name in named regex: empty name");
237 return true;
238 }
240 // Verify that the name/expression is well formed. FileCheck currently
241 // supports @LINE, @LINE+number, @LINE-number expressions. The check here
242 // is relaxed, more strict check is performed in \c EvaluateExpression.
243 bool IsExpression = false;
244 for (unsigned i = 0, e = Name.size(); i != e; ++i) {
245 if (i == 0 && Name[i] == '@') {
246 if (NameEnd != StringRef::npos) {
247 SM.PrintMessage(SMLoc::getFromPointer(Name.data()),
248 SourceMgr::DK_Error,
249 "invalid name in named regex definition");
250 return true;
251 }
252 IsExpression = true;
253 continue;
254 }
255 if (Name[i] != '_' && !isalnum(Name[i]) &&
256 (!IsExpression || (Name[i] != '+' && Name[i] != '-'))) {
257 SM.PrintMessage(SMLoc::getFromPointer(Name.data()+i),
258 SourceMgr::DK_Error, "invalid name in named regex");
259 return true;
260 }
261 }
263 // Name can't start with a digit.
264 if (isdigit(static_cast<unsigned char>(Name[0]))) {
265 SM.PrintMessage(SMLoc::getFromPointer(Name.data()), SourceMgr::DK_Error,
266 "invalid name in named regex");
267 return true;
268 }
270 // Handle [[foo]].
271 if (NameEnd == StringRef::npos) {
272 // Handle variables that were defined earlier on the same line by
273 // emitting a backreference.
274 if (VariableDefs.find(Name) != VariableDefs.end()) {
275 unsigned VarParenNum = VariableDefs[Name];
276 if (VarParenNum < 1 || VarParenNum > 9) {
277 SM.PrintMessage(SMLoc::getFromPointer(Name.data()),
278 SourceMgr::DK_Error,
279 "Can't back-reference more than 9 variables");
280 return true;
281 }
282 AddBackrefToRegEx(VarParenNum);
283 } else {
284 VariableUses.push_back(std::make_pair(Name, RegExStr.size()));
285 }
286 continue;
287 }
289 // Handle [[foo:.*]].
290 VariableDefs[Name] = CurParen;
291 RegExStr += '(';
292 ++CurParen;
294 if (AddRegExToRegEx(MatchStr.substr(NameEnd+1), CurParen, SM))
295 return true;
297 RegExStr += ')';
298 }
300 // Handle fixed string matches.
301 // Find the end, which is the start of the next regex.
302 size_t FixedMatchEnd = PatternStr.find("{{");
303 FixedMatchEnd = std::min(FixedMatchEnd, PatternStr.find("[["));
304 AddFixedStringToRegEx(PatternStr.substr(0, FixedMatchEnd), RegExStr);
305 PatternStr = PatternStr.substr(FixedMatchEnd);
306 }
308 return false;
309 }
311 void Pattern::AddFixedStringToRegEx(StringRef FixedStr, std::string &TheStr) {
312 // Add the characters from FixedStr to the regex, escaping as needed. This
313 // avoids "leaning toothpicks" in common patterns.
314 for (unsigned i = 0, e = FixedStr.size(); i != e; ++i) {
315 switch (FixedStr[i]) {
316 // These are the special characters matched in "p_ere_exp".
317 case '(':
318 case ')':
319 case '^':
320 case '$':
321 case '|':
322 case '*':
323 case '+':
324 case '?':
325 case '.':
326 case '[':
327 case '\\':
328 case '{':
329 TheStr += '\\';
330 // FALL THROUGH.
331 default:
332 TheStr += FixedStr[i];
333 break;
334 }
335 }
336 }
338 bool Pattern::AddRegExToRegEx(StringRef RS, unsigned &CurParen,
339 SourceMgr &SM) {
340 Regex R(RS);
341 std::string Error;
342 if (!R.isValid(Error)) {
343 SM.PrintMessage(SMLoc::getFromPointer(RS.data()), SourceMgr::DK_Error,
344 "invalid regex: " + Error);
345 return true;
346 }
348 RegExStr += RS.str();
349 CurParen += R.getNumMatches();
350 return false;
351 }
353 void Pattern::AddBackrefToRegEx(unsigned BackrefNum) {
354 assert(BackrefNum >= 1 && BackrefNum <= 9 && "Invalid backref number");
355 std::string Backref = std::string("\\") +
356 std::string(1, '0' + BackrefNum);
357 RegExStr += Backref;
358 }
360 bool Pattern::EvaluateExpression(StringRef Expr, std::string &Value) const {
361 // The only supported expression is @LINE([\+-]\d+)?
362 if (!Expr.startswith("@LINE"))
363 return false;
364 Expr = Expr.substr(StringRef("@LINE").size());
365 int Offset = 0;
366 if (!Expr.empty()) {
367 if (Expr[0] == '+')
368 Expr = Expr.substr(1);
369 else if (Expr[0] != '-')
370 return false;
371 if (Expr.getAsInteger(10, Offset))
372 return false;
373 }
374 Value = llvm::itostr(LineNumber + Offset);
375 return true;
376 }
378 /// Match - Match the pattern string against the input buffer Buffer. This
379 /// returns the position that is matched or npos if there is no match. If
380 /// there is a match, the size of the matched string is returned in MatchLen.
381 size_t Pattern::Match(StringRef Buffer, size_t &MatchLen,
382 StringMap<StringRef> &VariableTable) const {
383 // If this is the EOF pattern, match it immediately.
384 if (MatchEOF) {
385 MatchLen = 0;
386 return Buffer.size();
387 }
389 // If this is a fixed string pattern, just match it now.
390 if (!FixedStr.empty()) {
391 MatchLen = FixedStr.size();
392 return Buffer.find(FixedStr);
393 }
395 // Regex match.
397 // If there are variable uses, we need to create a temporary string with the
398 // actual value.
399 StringRef RegExToMatch = RegExStr;
400 std::string TmpStr;
401 if (!VariableUses.empty()) {
402 TmpStr = RegExStr;
404 unsigned InsertOffset = 0;
405 for (unsigned i = 0, e = VariableUses.size(); i != e; ++i) {
406 std::string Value;
408 if (VariableUses[i].first[0] == '@') {
409 if (!EvaluateExpression(VariableUses[i].first, Value))
410 return StringRef::npos;
411 } else {
412 StringMap<StringRef>::iterator it =
413 VariableTable.find(VariableUses[i].first);
414 // If the variable is undefined, return an error.
415 if (it == VariableTable.end())
416 return StringRef::npos;
418 // Look up the value and escape it so that we can plop it into the regex.
419 AddFixedStringToRegEx(it->second, Value);
420 }
422 // Plop it into the regex at the adjusted offset.
423 TmpStr.insert(TmpStr.begin()+VariableUses[i].second+InsertOffset,
424 Value.begin(), Value.end());
425 InsertOffset += Value.size();
426 }
428 // Match the newly constructed regex.
429 RegExToMatch = TmpStr;
430 }
433 SmallVector<StringRef, 4> MatchInfo;
434 if (!Regex(RegExToMatch, Regex::Newline).match(Buffer, &MatchInfo))
435 return StringRef::npos;
437 // Successful regex match.
438 assert(!MatchInfo.empty() && "Didn't get any match");
439 StringRef FullMatch = MatchInfo[0];
441 // If this defines any variables, remember their values.
442 for (std::map<StringRef, unsigned>::const_iterator I = VariableDefs.begin(),
443 E = VariableDefs.end();
444 I != E; ++I) {
445 assert(I->second < MatchInfo.size() && "Internal paren error");
446 VariableTable[I->first] = MatchInfo[I->second];
447 }
449 MatchLen = FullMatch.size();
450 return FullMatch.data()-Buffer.data();
451 }
453 unsigned Pattern::ComputeMatchDistance(StringRef Buffer,
454 const StringMap<StringRef> &VariableTable) const {
455 // Just compute the number of matching characters. For regular expressions, we
456 // just compare against the regex itself and hope for the best.
457 //
458 // FIXME: One easy improvement here is have the regex lib generate a single
459 // example regular expression which matches, and use that as the example
460 // string.
461 StringRef ExampleString(FixedStr);
462 if (ExampleString.empty())
463 ExampleString = RegExStr;
465 // Only compare up to the first line in the buffer, or the string size.
466 StringRef BufferPrefix = Buffer.substr(0, ExampleString.size());
467 BufferPrefix = BufferPrefix.split('\n').first;
468 return BufferPrefix.edit_distance(ExampleString);
469 }
471 void Pattern::PrintFailureInfo(const SourceMgr &SM, StringRef Buffer,
472 const StringMap<StringRef> &VariableTable) const{
473 // If this was a regular expression using variables, print the current
474 // variable values.
475 if (!VariableUses.empty()) {
476 for (unsigned i = 0, e = VariableUses.size(); i != e; ++i) {
477 SmallString<256> Msg;
478 raw_svector_ostream OS(Msg);
479 StringRef Var = VariableUses[i].first;
480 if (Var[0] == '@') {
481 std::string Value;
482 if (EvaluateExpression(Var, Value)) {
483 OS << "with expression \"";
484 OS.write_escaped(Var) << "\" equal to \"";
485 OS.write_escaped(Value) << "\"";
486 } else {
487 OS << "uses incorrect expression \"";
488 OS.write_escaped(Var) << "\"";
489 }
490 } else {
491 StringMap<StringRef>::const_iterator it = VariableTable.find(Var);
493 // Check for undefined variable references.
494 if (it == VariableTable.end()) {
495 OS << "uses undefined variable \"";
496 OS.write_escaped(Var) << "\"";
497 } else {
498 OS << "with variable \"";
499 OS.write_escaped(Var) << "\" equal to \"";
500 OS.write_escaped(it->second) << "\"";
501 }
502 }
504 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), SourceMgr::DK_Note,
505 OS.str());
506 }
507 }
509 // Attempt to find the closest/best fuzzy match. Usually an error happens
510 // because some string in the output didn't exactly match. In these cases, we
511 // would like to show the user a best guess at what "should have" matched, to
512 // save them having to actually check the input manually.
513 size_t NumLinesForward = 0;
514 size_t Best = StringRef::npos;
515 double BestQuality = 0;
517 // Use an arbitrary 4k limit on how far we will search.
518 for (size_t i = 0, e = std::min(size_t(4096), Buffer.size()); i != e; ++i) {
519 if (Buffer[i] == '\n')
520 ++NumLinesForward;
522 // Patterns have leading whitespace stripped, so skip whitespace when
523 // looking for something which looks like a pattern.
524 if (Buffer[i] == ' ' || Buffer[i] == '\t')
525 continue;
527 // Compute the "quality" of this match as an arbitrary combination of the
528 // match distance and the number of lines skipped to get to this match.
529 unsigned Distance = ComputeMatchDistance(Buffer.substr(i), VariableTable);
530 double Quality = Distance + (NumLinesForward / 100.);
532 if (Quality < BestQuality || Best == StringRef::npos) {
533 Best = i;
534 BestQuality = Quality;
535 }
536 }
538 // Print the "possible intended match here" line if we found something
539 // reasonable and not equal to what we showed in the "scanning from here"
540 // line.
541 if (Best && Best != StringRef::npos && BestQuality < 50) {
542 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data() + Best),
543 SourceMgr::DK_Note, "possible intended match here");
545 // FIXME: If we wanted to be really friendly we would show why the match
546 // failed, as it can be hard to spot simple one character differences.
547 }
548 }
550 size_t Pattern::FindRegexVarEnd(StringRef Str) {
551 // Offset keeps track of the current offset within the input Str
552 size_t Offset = 0;
553 // [...] Nesting depth
554 size_t BracketDepth = 0;
556 while (!Str.empty()) {
557 if (Str.startswith("]]") && BracketDepth == 0)
558 return Offset;
559 if (Str[0] == '\\') {
560 // Backslash escapes the next char within regexes, so skip them both.
561 Str = Str.substr(2);
562 Offset += 2;
563 } else {
564 switch (Str[0]) {
565 default:
566 break;
567 case '[':
568 BracketDepth++;
569 break;
570 case ']':
571 assert(BracketDepth > 0 && "Invalid regex");
572 BracketDepth--;
573 break;
574 }
575 Str = Str.substr(1);
576 Offset++;
577 }
578 }
580 return StringRef::npos;
581 }
584 //===----------------------------------------------------------------------===//
585 // Check Strings.
586 //===----------------------------------------------------------------------===//
588 /// CheckString - This is a check that we found in the input file.
589 struct CheckString {
590 /// Pat - The pattern to match.
591 Pattern Pat;
593 /// Loc - The location in the match file that the check string was specified.
594 SMLoc Loc;
596 /// IsCheckNext - This is true if this is a CHECK-NEXT: directive (as opposed
597 /// to a CHECK: directive.
598 bool IsCheckNext;
600 /// IsCheckLabel - This is true if this is a CHECK-LABEL: directive (as
601 /// opposed to a CHECK: directive.
602 bool IsCheckLabel;
604 /// DagNotStrings - These are all of the strings that are disallowed from
605 /// occurring between this match string and the previous one (or start of
606 /// file).
607 std::vector<Pattern> DagNotStrings;
609 CheckString(const Pattern &P, SMLoc L, bool isCheckNext, bool isCheckLabel)
610 : Pat(P), Loc(L), IsCheckNext(isCheckNext), IsCheckLabel(isCheckLabel) {}
612 /// Check - Match check string and its "not strings" and/or "dag strings".
613 size_t Check(const SourceMgr &SM, StringRef Buffer, bool IsLabel,
614 size_t &MatchLen, StringMap<StringRef> &VariableTable) const;
616 /// CheckNext - Verify there is a single line in the given buffer.
617 bool CheckNext(const SourceMgr &SM, StringRef Buffer) const;
619 /// CheckNot - Verify there's no "not strings" in the given buffer.
620 bool CheckNot(const SourceMgr &SM, StringRef Buffer,
621 const std::vector<const Pattern *> &NotStrings,
622 StringMap<StringRef> &VariableTable) const;
624 /// CheckDag - Match "dag strings" and their mixed "not strings".
625 size_t CheckDag(const SourceMgr &SM, StringRef Buffer,
626 std::vector<const Pattern *> &NotStrings,
627 StringMap<StringRef> &VariableTable) const;
628 };
630 /// Canonicalize whitespaces in the input file. Line endings are replaced
631 /// with UNIX-style '\n'.
632 ///
633 /// \param PreserveHorizontal Don't squash consecutive horizontal whitespace
634 /// characters to a single space.
635 static MemoryBuffer *CanonicalizeInputFile(MemoryBuffer *MB,
636 bool PreserveHorizontal) {
637 SmallString<128> NewFile;
638 NewFile.reserve(MB->getBufferSize());
640 for (const char *Ptr = MB->getBufferStart(), *End = MB->getBufferEnd();
641 Ptr != End; ++Ptr) {
642 // Eliminate trailing dosish \r.
643 if (Ptr <= End - 2 && Ptr[0] == '\r' && Ptr[1] == '\n') {
644 continue;
645 }
647 // If current char is not a horizontal whitespace or if horizontal
648 // whitespace canonicalization is disabled, dump it to output as is.
649 if (PreserveHorizontal || (*Ptr != ' ' && *Ptr != '\t')) {
650 NewFile.push_back(*Ptr);
651 continue;
652 }
654 // Otherwise, add one space and advance over neighboring space.
655 NewFile.push_back(' ');
656 while (Ptr+1 != End &&
657 (Ptr[1] == ' ' || Ptr[1] == '\t'))
658 ++Ptr;
659 }
661 // Free the old buffer and return a new one.
662 MemoryBuffer *MB2 =
663 MemoryBuffer::getMemBufferCopy(NewFile.str(), MB->getBufferIdentifier());
665 delete MB;
666 return MB2;
667 }
670 /// ReadCheckFile - Read the check file, which specifies the sequence of
671 /// expected strings. The strings are added to the CheckStrings vector.
672 /// Returns true in case of an error, false otherwise.
673 static bool ReadCheckFile(SourceMgr &SM,
674 std::vector<CheckString> &CheckStrings) {
675 OwningPtr<MemoryBuffer> File;
676 if (error_code ec =
677 MemoryBuffer::getFileOrSTDIN(CheckFilename, File)) {
678 errs() << "Could not open check file '" << CheckFilename << "': "
679 << ec.message() << '\n';
680 return true;
681 }
683 // If we want to canonicalize whitespace, strip excess whitespace from the
684 // buffer containing the CHECK lines. Remove DOS style line endings.
685 MemoryBuffer *F =
686 CanonicalizeInputFile(File.take(), NoCanonicalizeWhiteSpace);
688 SM.AddNewSourceBuffer(F, SMLoc());
690 // Find all instances of CheckPrefix followed by : in the file.
691 StringRef Buffer = F->getBuffer();
692 std::vector<Pattern> DagNotMatches;
694 // LineNumber keeps track of the line on which CheckPrefix instances are
695 // found.
696 unsigned LineNumber = 1;
698 while (1) {
699 // See if Prefix occurs in the memory buffer.
700 size_t PrefixLoc = Buffer.find(CheckPrefix);
701 // If we didn't find a match, we're done.
702 if (PrefixLoc == StringRef::npos)
703 break;
705 LineNumber += Buffer.substr(0, PrefixLoc).count('\n');
707 Buffer = Buffer.substr(PrefixLoc);
709 const char *CheckPrefixStart = Buffer.data();
711 // When we find a check prefix, keep track of whether we find CHECK: or
712 // CHECK-NEXT:
713 bool IsCheckNext = false, IsCheckNot = false, IsCheckDag = false,
714 IsCheckLabel = false;
716 // Verify that the : is present after the prefix.
717 if (Buffer[CheckPrefix.size()] == ':') {
718 Buffer = Buffer.substr(CheckPrefix.size()+1);
719 } else if (Buffer.size() > CheckPrefix.size()+6 &&
720 memcmp(Buffer.data()+CheckPrefix.size(), "-NEXT:", 6) == 0) {
721 Buffer = Buffer.substr(CheckPrefix.size()+6);
722 IsCheckNext = true;
723 } else if (Buffer.size() > CheckPrefix.size()+5 &&
724 memcmp(Buffer.data()+CheckPrefix.size(), "-NOT:", 5) == 0) {
725 Buffer = Buffer.substr(CheckPrefix.size()+5);
726 IsCheckNot = true;
727 } else if (Buffer.size() > CheckPrefix.size()+5 &&
728 memcmp(Buffer.data()+CheckPrefix.size(), "-DAG:", 5) == 0) {
729 Buffer = Buffer.substr(CheckPrefix.size()+5);
730 IsCheckDag = true;
731 } else if (Buffer.size() > CheckPrefix.size()+7 &&
732 memcmp(Buffer.data()+CheckPrefix.size(), "-LABEL:", 7) == 0) {
733 Buffer = Buffer.substr(CheckPrefix.size()+7);
734 IsCheckLabel = true;
735 } else {
736 Buffer = Buffer.substr(1);
737 continue;
738 }
740 // Okay, we found the prefix, yay. Remember the rest of the line, but
741 // ignore leading and trailing whitespace.
742 Buffer = Buffer.substr(Buffer.find_first_not_of(" \t"));
744 // Scan ahead to the end of line.
745 size_t EOL = Buffer.find_first_of("\n\r");
747 // Remember the location of the start of the pattern, for diagnostics.
748 SMLoc PatternLoc = SMLoc::getFromPointer(Buffer.data());
750 // Parse the pattern.
751 Pattern P;
752 if (P.ParsePattern(Buffer.substr(0, EOL), SM, LineNumber))
753 return true;
755 // Verify that CHECK-LABEL lines do not define or use variables
756 if (IsCheckLabel && P.hasVariable()) {
757 SM.PrintMessage(SMLoc::getFromPointer(CheckPrefixStart),
758 SourceMgr::DK_Error,
759 "found '"+CheckPrefix+"-LABEL:' with variable definition"
760 " or use'");
761 return true;
762 }
764 P.setMatchNot(IsCheckNot);
765 P.setMatchDag(IsCheckDag);
767 Buffer = Buffer.substr(EOL);
769 // Verify that CHECK-NEXT lines have at least one CHECK line before them.
770 if (IsCheckNext && CheckStrings.empty()) {
771 SM.PrintMessage(SMLoc::getFromPointer(CheckPrefixStart),
772 SourceMgr::DK_Error,
773 "found '"+CheckPrefix+"-NEXT:' without previous '"+
774 CheckPrefix+ ": line");
775 return true;
776 }
778 // Handle CHECK-DAG/-NOT.
779 if (IsCheckDag || IsCheckNot) {
780 DagNotMatches.push_back(P);
781 continue;
782 }
784 // Okay, add the string we captured to the output vector and move on.
785 CheckStrings.push_back(CheckString(P,
786 PatternLoc,
787 IsCheckNext,
788 IsCheckLabel));
789 std::swap(DagNotMatches, CheckStrings.back().DagNotStrings);
790 }
792 // Add an EOF pattern for any trailing CHECK-DAG/-NOTs.
793 if (!DagNotMatches.empty()) {
794 CheckStrings.push_back(CheckString(Pattern(true),
795 SMLoc::getFromPointer(Buffer.data()),
796 false,
797 false));
798 std::swap(DagNotMatches, CheckStrings.back().DagNotStrings);
799 }
801 if (CheckStrings.empty()) {
802 errs() << "error: no check strings found with prefix '" << CheckPrefix
803 << ":'\n";
804 return true;
805 }
807 return false;
808 }
810 static void PrintCheckFailed(const SourceMgr &SM, const SMLoc &Loc,
811 const Pattern &Pat, StringRef Buffer,
812 StringMap<StringRef> &VariableTable) {
813 // Otherwise, we have an error, emit an error message.
814 SM.PrintMessage(Loc, SourceMgr::DK_Error,
815 "expected string not found in input");
817 // Print the "scanning from here" line. If the current position is at the
818 // end of a line, advance to the start of the next line.
819 Buffer = Buffer.substr(Buffer.find_first_not_of(" \t\n\r"));
821 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), SourceMgr::DK_Note,
822 "scanning from here");
824 // Allow the pattern to print additional information if desired.
825 Pat.PrintFailureInfo(SM, Buffer, VariableTable);
826 }
828 static void PrintCheckFailed(const SourceMgr &SM, const CheckString &CheckStr,
829 StringRef Buffer,
830 StringMap<StringRef> &VariableTable) {
831 PrintCheckFailed(SM, CheckStr.Loc, CheckStr.Pat, Buffer, VariableTable);
832 }
834 /// CountNumNewlinesBetween - Count the number of newlines in the specified
835 /// range.
836 static unsigned CountNumNewlinesBetween(StringRef Range) {
837 unsigned NumNewLines = 0;
838 while (1) {
839 // Scan for newline.
840 Range = Range.substr(Range.find_first_of("\n\r"));
841 if (Range.empty()) return NumNewLines;
843 ++NumNewLines;
845 // Handle \n\r and \r\n as a single newline.
846 if (Range.size() > 1 &&
847 (Range[1] == '\n' || Range[1] == '\r') &&
848 (Range[0] != Range[1]))
849 Range = Range.substr(1);
850 Range = Range.substr(1);
851 }
852 }
854 size_t CheckString::Check(const SourceMgr &SM, StringRef Buffer,
855 bool IsLabel, size_t &MatchLen,
856 StringMap<StringRef> &VariableTable) const {
857 size_t LastPos = 0;
858 std::vector<const Pattern *> NotStrings;
860 if (!IsLabel) {
861 // Match "dag strings" (with mixed "not strings" if any).
862 LastPos = CheckDag(SM, Buffer, NotStrings, VariableTable);
863 if (LastPos == StringRef::npos)
864 return StringRef::npos;
865 }
867 // Match itself from the last position after matching CHECK-DAG.
868 StringRef MatchBuffer = Buffer.substr(LastPos);
869 size_t MatchPos = Pat.Match(MatchBuffer, MatchLen, VariableTable);
870 if (MatchPos == StringRef::npos) {
871 PrintCheckFailed(SM, *this, MatchBuffer, VariableTable);
872 return StringRef::npos;
873 }
874 MatchPos += LastPos;
876 if (!IsLabel) {
877 StringRef SkippedRegion = Buffer.substr(LastPos, MatchPos);
879 // If this check is a "CHECK-NEXT", verify that the previous match was on
880 // the previous line (i.e. that there is one newline between them).
881 if (CheckNext(SM, SkippedRegion))
882 return StringRef::npos;
884 // If this match had "not strings", verify that they don't exist in the
885 // skipped region.
886 if (CheckNot(SM, SkippedRegion, NotStrings, VariableTable))
887 return StringRef::npos;
888 }
890 return MatchPos;
891 }
893 bool CheckString::CheckNext(const SourceMgr &SM, StringRef Buffer) const {
894 if (!IsCheckNext)
895 return false;
897 // Count the number of newlines between the previous match and this one.
898 assert(Buffer.data() !=
899 SM.getMemoryBuffer(
900 SM.FindBufferContainingLoc(
901 SMLoc::getFromPointer(Buffer.data())))->getBufferStart() &&
902 "CHECK-NEXT can't be the first check in a file");
904 unsigned NumNewLines = CountNumNewlinesBetween(Buffer);
906 if (NumNewLines == 0) {
907 SM.PrintMessage(Loc, SourceMgr::DK_Error, CheckPrefix+
908 "-NEXT: is on the same line as previous match");
909 SM.PrintMessage(SMLoc::getFromPointer(Buffer.end()),
910 SourceMgr::DK_Note, "'next' match was here");
911 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), SourceMgr::DK_Note,
912 "previous match ended here");
913 return true;
914 }
916 if (NumNewLines != 1) {
917 SM.PrintMessage(Loc, SourceMgr::DK_Error, CheckPrefix+
918 "-NEXT: is not on the line after the previous match");
919 SM.PrintMessage(SMLoc::getFromPointer(Buffer.end()),
920 SourceMgr::DK_Note, "'next' match was here");
921 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()), SourceMgr::DK_Note,
922 "previous match ended here");
923 return true;
924 }
926 return false;
927 }
929 bool CheckString::CheckNot(const SourceMgr &SM, StringRef Buffer,
930 const std::vector<const Pattern *> &NotStrings,
931 StringMap<StringRef> &VariableTable) const {
932 for (unsigned ChunkNo = 0, e = NotStrings.size();
933 ChunkNo != e; ++ChunkNo) {
934 const Pattern *Pat = NotStrings[ChunkNo];
935 assert(Pat->getMatchNot() && "Expect CHECK-NOT!");
937 size_t MatchLen = 0;
938 size_t Pos = Pat->Match(Buffer, MatchLen, VariableTable);
940 if (Pos == StringRef::npos) continue;
942 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data()+Pos),
943 SourceMgr::DK_Error,
944 CheckPrefix+"-NOT: string occurred!");
945 SM.PrintMessage(Pat->getLoc(), SourceMgr::DK_Note,
946 CheckPrefix+"-NOT: pattern specified here");
947 return true;
948 }
950 return false;
951 }
953 size_t CheckString::CheckDag(const SourceMgr &SM, StringRef Buffer,
954 std::vector<const Pattern *> &NotStrings,
955 StringMap<StringRef> &VariableTable) const {
956 if (DagNotStrings.empty())
957 return 0;
959 size_t LastPos = 0;
960 size_t StartPos = LastPos;
962 for (unsigned ChunkNo = 0, e = DagNotStrings.size();
963 ChunkNo != e; ++ChunkNo) {
964 const Pattern &Pat = DagNotStrings[ChunkNo];
966 assert((Pat.getMatchDag() ^ Pat.getMatchNot()) &&
967 "Invalid CHECK-DAG or CHECK-NOT!");
969 if (Pat.getMatchNot()) {
970 NotStrings.push_back(&Pat);
971 continue;
972 }
974 assert(Pat.getMatchDag() && "Expect CHECK-DAG!");
976 size_t MatchLen = 0, MatchPos;
978 // CHECK-DAG always matches from the start.
979 StringRef MatchBuffer = Buffer.substr(StartPos);
980 MatchPos = Pat.Match(MatchBuffer, MatchLen, VariableTable);
981 // With a group of CHECK-DAGs, a single mismatching means the match on
982 // that group of CHECK-DAGs fails immediately.
983 if (MatchPos == StringRef::npos) {
984 PrintCheckFailed(SM, Pat.getLoc(), Pat, MatchBuffer, VariableTable);
985 return StringRef::npos;
986 }
987 // Re-calc it as the offset relative to the start of the original string.
988 MatchPos += StartPos;
990 if (!NotStrings.empty()) {
991 if (MatchPos < LastPos) {
992 // Reordered?
993 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data() + MatchPos),
994 SourceMgr::DK_Error,
995 CheckPrefix+"-DAG: found a match of CHECK-DAG"
996 " reordering across a CHECK-NOT");
997 SM.PrintMessage(SMLoc::getFromPointer(Buffer.data() + LastPos),
998 SourceMgr::DK_Note,
999 CheckPrefix+"-DAG: the farthest match of CHECK-DAG"
1000 " is found here");
1001 SM.PrintMessage(NotStrings[0]->getLoc(), SourceMgr::DK_Note,
1002 CheckPrefix+"-NOT: the crossed pattern specified"
1003 " here");
1004 SM.PrintMessage(Pat.getLoc(), SourceMgr::DK_Note,
1005 CheckPrefix+"-DAG: the reordered pattern specified"
1006 " here");
1007 return StringRef::npos;
1008 }
1009 // All subsequent CHECK-DAGs should be matched from the farthest
1010 // position of all precedent CHECK-DAGs (including this one.)
1011 StartPos = LastPos;
1012 // If there's CHECK-NOTs between two CHECK-DAGs or from CHECK to
1013 // CHECK-DAG, verify that there's no 'not' strings occurred in that
1014 // region.
1015 StringRef SkippedRegion = Buffer.substr(LastPos, MatchPos);
1016 if (CheckNot(SM, SkippedRegion, NotStrings, VariableTable))
1017 return StringRef::npos;
1018 // Clear "not strings".
1019 NotStrings.clear();
1020 }
1022 // Update the last position with CHECK-DAG matches.
1023 LastPos = std::max(MatchPos + MatchLen, LastPos);
1024 }
1026 return LastPos;
1027 }
1029 int main(int argc, char **argv) {
1030 sys::PrintStackTraceOnErrorSignal();
1031 PrettyStackTraceProgram X(argc, argv);
1032 cl::ParseCommandLineOptions(argc, argv);
1034 SourceMgr SM;
1036 // Read the expected strings from the check file.
1037 std::vector<CheckString> CheckStrings;
1038 if (ReadCheckFile(SM, CheckStrings))
1039 return 2;
1041 // Open the file to check and add it to SourceMgr.
1042 OwningPtr<MemoryBuffer> File;
1043 if (error_code ec =
1044 MemoryBuffer::getFileOrSTDIN(InputFilename, File)) {
1045 errs() << "Could not open input file '" << InputFilename << "': "
1046 << ec.message() << '\n';
1047 return 2;
1048 }
1050 if (File->getBufferSize() == 0) {
1051 errs() << "FileCheck error: '" << InputFilename << "' is empty.\n";
1052 return 2;
1053 }
1055 // Remove duplicate spaces in the input file if requested.
1056 // Remove DOS style line endings.
1057 MemoryBuffer *F =
1058 CanonicalizeInputFile(File.take(), NoCanonicalizeWhiteSpace);
1060 SM.AddNewSourceBuffer(F, SMLoc());
1062 /// VariableTable - This holds all the current filecheck variables.
1063 StringMap<StringRef> VariableTable;
1065 // Check that we have all of the expected strings, in order, in the input
1066 // file.
1067 StringRef Buffer = F->getBuffer();
1069 bool hasError = false;
1071 unsigned i = 0, j = 0, e = CheckStrings.size();
1073 while (true) {
1074 StringRef CheckRegion;
1075 if (j == e) {
1076 CheckRegion = Buffer;
1077 } else {
1078 const CheckString &CheckLabelStr = CheckStrings[j];
1079 if (!CheckLabelStr.IsCheckLabel) {
1080 ++j;
1081 continue;
1082 }
1084 // Scan to next CHECK-LABEL match, ignoring CHECK-NOT and CHECK-DAG
1085 size_t MatchLabelLen = 0;
1086 size_t MatchLabelPos = CheckLabelStr.Check(SM, Buffer, true,
1087 MatchLabelLen, VariableTable);
1088 if (MatchLabelPos == StringRef::npos) {
1089 hasError = true;
1090 break;
1091 }
1093 CheckRegion = Buffer.substr(0, MatchLabelPos + MatchLabelLen);
1094 Buffer = Buffer.substr(MatchLabelPos + MatchLabelLen);
1095 ++j;
1096 }
1098 for ( ; i != j; ++i) {
1099 const CheckString &CheckStr = CheckStrings[i];
1101 // Check each string within the scanned region, including a second check
1102 // of any final CHECK-LABEL (to verify CHECK-NOT and CHECK-DAG)
1103 size_t MatchLen = 0;
1104 size_t MatchPos = CheckStr.Check(SM, CheckRegion, false, MatchLen,
1105 VariableTable);
1107 if (MatchPos == StringRef::npos) {
1108 hasError = true;
1109 i = j;
1110 break;
1111 }
1113 CheckRegion = CheckRegion.substr(MatchPos + MatchLen);
1114 }
1116 if (j == e)
1117 break;
1118 }
1120 return hasError ? 1 : 0;
1121 }