#===-- Makefile.common - Common make rules for LLVM -------*- makefile -*--==== # # This file is included by all of the LLVM makefiles. This file defines common # rules to do things like compile a .cpp file or generate dependancy info. # These are platform dependant, so this is the file used to specify these # system dependant operations. # # The following functionality can be set by setting incoming variables. # The variable $(LEVEL) *must* be set: # # 1. LEVEL - The level of the current subdirectory from the top of the # MagicStats view. This level should be expressed as a path, for # example, ../.. for two levels deep. # # 2. DIRS - A list of subdirectories to be built. Fake targets are set up # so that each of the targets "all", "install", and "clean" each build # the subdirectories before the local target. DIRS are guaranteed to be # built in order. # # 3. PARALLEL_DIRS - A list of subdirectories to be built, but that may be # built in any order. All DIRS are built in order before PARALLEL_DIRS are # built, which are then built in any order. # # 4. Source - If specified, this sets the source code filenames. If this # is not set, it defaults to be all of the .cpp, .c, .y, and .l files # in the current directory. Also, if you want to build files in addition # to the local files, you can use the ExtraSource variable # #===-----------------------------------------------------------------------==== # Configuration file to set paths specific to local installation of LLVM # include $(LEVEL)/Makefile.config # These are options that can either be enabled here, or can be enabled on the # make command line (ie, make ENABLE_PROFILING=1) # # When ENABLE_PROFILING is enabled, the llvm source base is built with profile # information to allow gprof to be used to get execution frequencies. # #ENABLE_PROFILING = 1 # When ENABLE_PURIFY is enabled, the LLVM tools are linked with purify (which # must be locally installed) to allow for some automated memory error debugging. # #ENABLE_PURIFY = 1 # When ENABLE_OPTIMIZED is enabled, Release builds of all of the LLVM code are # turned on, and Debug builds are turned off. # #ENABLE_OPTIMIZED = 1 # Figure out how to do platform specific stuff on this platform. This is really # gross and should be autoconfiscated (automake actually), but should hopefully # work on Linux and solaris (SunOS). # UNAME := $(shell uname) include $(LEVEL)/Makefile.$(UNAME) ifdef SHARED_LIBRARY # if SHARED_LIBRARY is specified, the default is to build the dynamic lib dynamic :: endif # Default Rule: Make sure it's also a :: rule all :: # Default for install is to at least build everything... install :: # Figure out which directory to build stuff into. We want to build into the # /shared directory by default because it is guaranteed to be local to the # current machine. # ifeq ($(LLVM_OBJ_DIR),.) BUILD_ROOT = $(LLVM_OBJ_DIR) BUILD_ROOT_TOP = $(LEVEL) else BUILD_ROOT := $(LLVM_OBJ_DIR)$(patsubst $(HOME)%,%,$(shell pwd)) # Calculate the BUILD_ROOT_TOP variable, which is the top of the llvm/ tree. # Note that although this is just equal to $(BUILD_ROOT)/$(LEVEL), we cannot use # this expression because some of the directories on the source tree may not # exist in the build tree (for example the test/ heirarchy). Thus we evaluate # the directory to eliminate the ../'s # TOP_DIRECTORY := $(shell cd $(LEVEL); pwd) BUILD_ROOT_TOP := $(LLVM_OBJ_DIR)$(patsubst $(HOME)%,%,$(TOP_DIRECTORY)) endif #-------------------------------------------------------------------- # Variables derived from configuration options... #-------------------------------------------------------------------- #BinInstDir=/usr/local/bin #LibInstDir=/usrl/local/lib/xxx #DocInstDir=/usr/doc/xxx BURG_OPTS = -I PURIFY := $(PURIFY) -cache-dir="$(BUILD_ROOT_TOP)/../purifycache" -chain-length="30" -messages=all # Shorthand for commonly accessed directories LIBDEBUG := $(BUILD_ROOT_TOP)/lib/Debug LIBRELEASE := $(BUILD_ROOT_TOP)/lib/Release LIBPROFILE := $(BUILD_ROOT_TOP)/lib/Profile TOOLDEBUG := $(BUILD_ROOT_TOP)/tools/Debug TOOLRELEASE := $(BUILD_ROOT_TOP)/tools/Release TOOLPROFILE := $(BUILD_ROOT_TOP)/tools/Profile # Verbosity levels ifdef VERBOSE VERB := else VERB := @ endif #--------------------------------------------------------- # Compilation options... #--------------------------------------------------------- # Special tools used while building the LLVM tree. Burg is built as part of the # utils directory. # BURG := $(TOOLDEBUG)/burg RunBurg := $(BURG) $(BURG_OPTS) # Enable this for profiling support with 'gprof' # This automatically enables optimized builds. ifdef ENABLE_PROFILING PROFILE = -pg ENABLE_OPTIMIZED = 1 else PROFILE = endif # By default, strip symbol information from executable ifdef KEEP_SYMBOLS STRIP = STRIP_WARN_MSG = else STRIP = $(PLATFORMSTRIPOPTS) STRIP_WARN_MSG = "(without symbols) " endif # Allow gnu extensions... CPPFLAGS += -D_GNU_SOURCE # -Wno-unused-parameter CompileCommonOpts := -Wall -W -Wwrite-strings -Wno-unused -I$(LEVEL)/include # Compile a cpp file, don't link... Compile := $(CXX) -c $(CPPFLAGS) $(CXXFLAGS) $(CompileCommonOpts) CompileG := $(Compile) -g -D_DEBUG CompileO := $(Compile) -O3 -DNDEBUG -finline-functions -felide-constructors -fshort-enums ## DISABLE -freg-struct-return because of gcc3.2 bug CompileP := $(CompileO) $(PROFILE) # Compile a c file, don't link... CompileC := $(CC) -c $(CPPFLAGS) $(CCFLAGS) $(CompileCommonOpts) CompileCG := $(CompileC) -g -D_DEBUG CompileCO := $(CompileC) -O3 -DNDEBUG -finline-functions -fshort-enums ## DISABLE -freg-struct-return because of gcc3.2 bug CompileCP := $(CompileCO) $(PROFILE) # Link final executable ifdef ENABLE_PURIFY # To enable purify, build with 'gmake ENABLE_PURIFY=1' Link := $(PURIFY) $(CXX) -static else Link := $(CXX) endif LinkG := $(Link) -g -L$(LIBDEBUG) $(STRIP) LinkO := $(Link) -O3 -L$(LIBRELEASE) LinkP := $(Link) -O3 -L$(LIBPROFILE) $(PROFILE) # Create one .o file from a bunch of .o files... Relink = ld -r # MakeSO - Create a .so file from a .o files... MakeSO := $(CXX) $(MakeSharedObjectOption) MakeSOO := $(MakeSO) -O3 MakeSOP := $(MakeSOO) $(PROFILE) # Create dependancy file from CPP file, send to stdout. Depend := $(CXX) -MM -I$(LEVEL)/include $(CPPFLAGS) DependC := $(CC) -MM -I$(LEVEL)/include $(CPPFLAGS) # Archive a bunch of .o files into a .a file... AR = ar cq BISON = bison #---------------------------------------------------------- # Source includes all of the cpp files, and objects are derived from the # source files... # The local Makefile can list other Source files via ExtraSource = ... # ifndef Source Source := $(ExtraSource) $(wildcard *.cpp *.c *.y *.l) endif Objs := $(sort $(patsubst Debug/%.o, %.o, $(addsuffix .o,$(basename $(Source))))) ObjectsO := $(addprefix $(BUILD_ROOT)/Release/,$(Objs)) ObjectsP := $(addprefix $(BUILD_ROOT)/Profile/,$(Objs)) ObjectsG := $(addprefix $(BUILD_ROOT)/Debug/,$(Objs)) #--------------------------------------------------------- # Handle the DIRS and PARALLEL_DIRS options #--------------------------------------------------------- ifdef DIRS all install clean test :: $(VERB) for dir in ${DIRS}; do \ (cd $$dir; $(MAKE) $@) || exit 1; \ done endif # Handle PARALLEL_DIRS ifdef PARALLEL_DIRS all :: $(addsuffix /.makeall , $(PARALLEL_DIRS)) install :: $(addsuffix /.makeinstall, $(PARALLEL_DIRS)) clean :: $(addsuffix /.makeclean , $(PARALLEL_DIRS)) test :: $(addsuffix /.maketest , $(PARALLEL_DIRS)) %/.makeall %/.makeinstall %/.makeclean %/.maketest: $(VERB) cd $(@D); $(MAKE) $(subst $(@D)/.make,,$@) endif #--------------------------------------------------------- # Handle the LIBRARYNAME option - used when building libs... #--------------------------------------------------------- # # When libraries are built, they are allowed to optionally define the # DONT_BUILD_RELINKED make variable, which, when defined, prevents a .o file # from being built for the library. This .o files may then be linked to by a # tool if the tool does not need (or want) the semantics a .a file provides # (linking in only object files that are "needed"). If a library is never to # be used in this way, it is better to define DONT_BUILD_RELINKED, and define # BUILD_ARCHIVE instead. # # Some libraries must be built as .a files (libscalar for example) because if # it's built as a .o file, then all of the constituent .o files in it will be # linked into tools (for example gccas) even if they only use one of the parts # of it. For this reason, sometimes it's useful to use libraries as .a files. ifdef LIBRARYNAME # Make sure there isn't any extranous whitespace on the LIBRARYNAME option LIBRARYNAME := $(strip $(LIBRARYNAME)) LIBNAME_O := $(LIBRELEASE)/lib$(LIBRARYNAME).so LIBNAME_P := $(LIBPROFILE)/lib$(LIBRARYNAME).so LIBNAME_G := $(LIBDEBUG)/lib$(LIBRARYNAME).so LIBNAME_AO := $(LIBRELEASE)/lib$(LIBRARYNAME).a LIBNAME_AP := $(LIBPROFILE)/lib$(LIBRARYNAME).a LIBNAME_AG := $(LIBDEBUG)/lib$(LIBRARYNAME).a LIBNAME_OBJO := $(LIBRELEASE)/$(LIBRARYNAME).o LIBNAME_OBJP := $(LIBPROFILE)/$(LIBRARYNAME).o LIBNAME_OBJG := $(LIBDEBUG)/$(LIBRARYNAME).o ifndef ENABLE_OPTIMIZED BUILD_LIBNAME_G := $(LIBNAME_G) ifndef DONT_BUILD_RELINKED BUILD_LIBNAME_OBJG := $(LIBNAME_OBJG) endif ifdef BUILD_ARCHIVE BUILD_LIBNAME_AG := $(LIBNAME_AG) endif endif # If optimized builds are enabled... ifdef ENABLE_OPTIMIZED ifdef ENABLE_PROFILING BUILD_LIBNAME_O := $(LIBNAME_P) ifndef DONT_BUILD_RELINKED BUILD_LIBNAME_OBJO := $(LIBNAME_OBJP) endif ifdef BUILD_ARCHIVE BUILD_LIBNAME_AO := $(LIBNAME_AP) endif else BUILD_LIBNAME_O := $(LIBNAME_O) ifndef DONT_BUILD_RELINKED BUILD_LIBNAME_OBJO := $(LIBNAME_OBJO) endif ifdef BUILD_ARCHIVE BUILD_LIBNAME_AO := $(LIBNAME_AO) endif endif endif all:: $(BUILD_LIBNAME_AG) $(BUILD_LIBNAME_OBJG) # Debug all:: $(BUILD_LIBNAME_AO) $(BUILD_LIBNAME_OBJO) # Release all:: $(BUILD_LIBNAME_AP) $(BUILD_LIBNAME_OBJP) # Profile dynamic:: $(BUILD_LIBNAME_G) $(BUILD_LIBNAME_O) $(BUILD_LIBNAME_P) # .so files $(LIBNAME_O): $(ObjectsO) $(LibSubDirs) $(LIBRELEASE)/.dir @echo ======= Linking $(LIBRARYNAME) release library ======= $(VERB) $(MakeSOO) -o $@ $(ObjectsO) $(LibSubDirs) $(LibLinkOpts) $(LIBNAME_P): $(ObjectsP) $(LibSubDirs) $(LIBPROFILE)/.dir @echo ======= Linking $(LIBRARYNAME) profile library ======= $(VERB) $(MakeSOP) -o $@ $(ObjectsP) $(LibSubDirs) $(LibLinkOpts) $(LIBNAME_G): $(ObjectsG) $(LibSubDirs) $(LIBDEBUG)/.dir @echo ======= Linking $(LIBRARYNAME) debug library ======= $(VERB) $(MakeSO) -g -o $@ $(ObjectsG) $(LibSubDirs) $(LibLinkOpts) $(LIBNAME_AO): $(ObjectsO) $(LibSubDirs) $(LIBRELEASE)/.dir @echo ======= Linking $(LIBRARYNAME) release library ======= @rm -f $@ $(VERB) $(AR) $@ $(ObjectsO) $(LibSubDirs) $(LIBNAME_AP): $(ObjectsP) $(LibSubDirs) $(LIBPROFILE)/.dir @echo ======= Linking $(LIBRARYNAME) profile library ======= @rm -f $@ $(VERB) $(AR) $@ $(ObjectsP) $(LibSubDirs) $(LIBNAME_AG): $(ObjectsG) $(LibSubDirs) $(LIBDEBUG)/.dir @echo ======= Linking $(LIBRARYNAME) debug library ======= @rm -f $@ $(VERB) $(AR) $@ $(ObjectsG) $(LibSubDirs) $(LIBNAME_OBJO): $(ObjectsO) $(LibSubDirs) $(LIBRELEASE)/.dir @echo "Linking $@" $(VERB) $(Relink) -o $@ $(ObjectsO) $(LibSubDirs) $(LIBNAME_OBJP): $(ObjectsP) $(LibSubDirs) $(LIBPROFILE)/.dir @echo "Linking $@" $(VERB) $(Relink) -o $@ $(ObjectsP) $(LibSubDirs) $(LIBNAME_OBJG): $(ObjectsG) $(LibSubDirs) $(LIBDEBUG)/.dir @echo "Linking $@" $(VERB) $(Relink) -o $@ $(ObjectsG) $(LibSubDirs) endif #------------------------------------------------------------------------ # Create a TAGS database for emacs #------------------------------------------------------------------------ ifeq ($(LEVEL), .) tags: etags -l c++ `find include lib tools -name '*.cpp' -o -name '*.h'` all:: tags endif #------------------------------------------------------------------------ # Handle the TOOLNAME option - used when building tool executables... #------------------------------------------------------------------------ # # The TOOLNAME option should be used with a USEDLIBS variable that tells the # libraries (and the order of the libs) that should be linked to the # tool. USEDLIBS should contain a list of library names (some with .a extension) # that are automatically linked in as .o files unless the .a suffix is added. # ifdef TOOLNAME # TOOLEXENAME* - These compute the output filenames to generate... TOOLEXENAME_G := $(BUILD_ROOT_TOP)/tools/Debug/$(TOOLNAME) TOOLEXENAME_O := $(BUILD_ROOT_TOP)/tools/Release/$(TOOLNAME) TOOLEXENAME_P := $(BUILD_ROOT_TOP)/tools/Profile/$(TOOLNAME) ifndef ENABLE_OPTIMIZED TOOLEXENAMES := $(TOOLEXENAME_G) else ifdef ENABLE_PROFILING TOOLEXENAMES := $(TOOLEXENAME_P) else TOOLEXENAMES := $(TOOLEXENAME_O) endif endif # USED_LIBS_OPTIONS - Compute the options line that add -llib1 -llib2, etc. USED_LIBS_OPTIONS := $(patsubst %.a.o, -l%, $(addsuffix .o, $(USEDLIBS))) USED_LIBS_OPTIONS_G := $(patsubst %.o, $(LIBDEBUG)/%.o, $(USED_LIBS_OPTIONS)) USED_LIBS_OPTIONS_O := $(patsubst %.o, $(LIBRELEASE)/%.o,$(USED_LIBS_OPTIONS)) USED_LIBS_OPTIONS_P := $(patsubst %.o, $(LIBPROFILE)/%.o,$(USED_LIBS_OPTIONS)) # USED_LIB_PATHS - Compute the path of the libraries used so that tools are # rebuilt if libraries change. This has to make sure to handle .a/.so and .o # files seperately. # STATICUSEDLIBS := $(patsubst %.a.o, lib%.a, $(addsuffix .o, $(USEDLIBS))) USED_LIB_PATHS_G := $(addprefix $(LIBDEBUG)/, $(STATICUSEDLIBS)) USED_LIB_PATHS_O := $(addprefix $(LIBRELEASE)/, $(STATICUSEDLIBS)) USED_LIB_PATHS_P := $(addprefix $(LIBPROFILE)/, $(STATICUSEDLIBS)) LINK_OPTS := $(TOOLLINKOPTS) $(PLATFORMLINKOPTS) # Tell make that we need to rebuild subdirectories before we can link the tool. # This affects things like LLI which has library subdirectories. $(USED_LIB_PATHS_G) $(USED_LIB_PATHS_O) $(USED_LIB_PATHS_P): \ $(addsuffix /.makeall, $(PARALLEL_DIRS)) all:: $(TOOLEXENAMES) clean:: $(VERB) rm -f $(TOOLEXENAMES) $(TOOLEXENAME_G): $(ObjectsG) $(USED_LIB_PATHS_G) $(TOOLDEBUG)/.dir @echo ======= Linking $(TOOLNAME) debug executable $(STRIP_WARN_MSG) ======= $(VERB) $(LinkG) -o $@ $(ObjectsG) $(USED_LIBS_OPTIONS_G) $(LINK_OPTS) $(TOOLEXENAME_O): $(ObjectsO) $(USED_LIB_PATHS_O) $(TOOLRELEASE)/.dir @echo ======= Linking $(TOOLNAME) release executable ======= $(VERB) $(LinkO) -o $@ $(ObjectsO) $(USED_LIBS_OPTIONS_O) $(LINK_OPTS) $(TOOLEXENAME_P): $(ObjectsP) $(USED_LIB_PATHS_P) $(TOOLPROFILE)/.dir @echo ======= Linking $(TOOLNAME) profile executable ======= $(VERB) $(LinkP) -o $@ $(ObjectsP) $(USED_LIBS_OPTIONS_P) $(LINK_OPTS) endif #--------------------------------------------------------- .PRECIOUS: $(BUILD_ROOT)/Depend/.dir .PRECIOUS: $(BUILD_ROOT)/Debug/.dir $(BUILD_ROOT)/Release/.dir # Create dependencies for the *.cpp files... $(BUILD_ROOT)/Depend/%.d: %.cpp $(BUILD_ROOT)/Depend/.dir $(VERB) $(Depend) $< | sed 's|$*\.o *|$(BUILD_ROOT)/Release/& $(BUILD_ROOT)/Profile/& $(BUILD_ROOT)/Debug/& $(BUILD_ROOT)/Depend/$(@F)|g' > $@ # Create dependencies for the *.c files... $(BUILD_ROOT)/Depend/%.d: %.c $(BUILD_ROOT)/Depend/.dir $(VERB) $(DependC) $< | sed 's|$*\.o *|Release/& Profile/& Debug/& Depend/$(@F)|g' > $@ # Create .o files in the ObjectFiles directory from the .cpp and .c files... $(BUILD_ROOT)/Release/%.o: %.cpp $(BUILD_ROOT)/Release/.dir @echo "Compiling $<" $(VERB) $(CompileO) $< -o $@ $(BUILD_ROOT)/Release/%.o: %.c $(BUILD_ROOT)/Release/.dir $(VERB) $(CompileCO) $< -o $@ $(BUILD_ROOT)/Profile/%.o: %.cpp $(BUILD_ROOT)/Profile/.dir @echo "Compiling $<" $(VERB) $(CompileP) $< -o $@ $(BUILD_ROOT)/Profile/%.o: %.c $(BUILD_ROOT)/Profile/.dir @echo "Compiling $<" $(VERB) $(CompileCP) $< -o $@ $(BUILD_ROOT)/Debug/%.o: %.cpp $(BUILD_ROOT)/Debug/.dir @echo "Compiling $<" $(VERB) $(CompileG) $< -o $@ $(BUILD_ROOT)/Debug/%.o: %.c $(BUILD_ROOT)/Debug/.dir $(VERB) $(CompileCG) $< -o $@ # # Rules for building lex/yacc files # LEX_FILES = $(filter %.l, $(Source)) LEX_OUTPUT = $(LEX_FILES:%.l=%.cpp) YACC_FILES = $(filter %.y, $(Source)) YACC_OUTPUT = $(addprefix $(YACC_FILES:%.y=%), .h .cpp .output) .PRECIOUS: $(LEX_OUTPUT) $(YACC_OUTPUT) # Create a .cpp source file from a flex input file... this uses sed to cut down # on the warnings emited by GCC... # # The last line is a gross hack to work around flex aparently not being able to # resize the buffer on a large token input. Currently, for uninitialized string # buffers in LLVM we can generate very long tokens, so this is a hack around it. # FIXME. (f.e. char Buffer[10000]; ) # %.cpp: %.l flex -t $< | sed '/^find_rule/d' | \ sed 's/void yyunput/inline void yyunput/' | \ sed 's/void \*yy_flex_realloc/inline void *yy_flex_realloc/' | \ sed 's/#define YY_BUF_SIZE 16384/#define YY_BUF_SIZE (16384*64)/' > $@ # Rule for building the bison parsers... %.cpp %.h : %.y $(VERB) $(BISON) -v -d -p $(<:%Parser.y=%) $*.y $(VERB) mv -f $*.tab.c $*.cpp $(VERB) mv -f $*.tab.h $*.h # To create the directories... %/.dir: $(VERB) mkdir -p $* @date > $@ # To create postscript files from dot files... %.ps: %.dot dot -Tps < $< > $@ # 'make clean' nukes the tree clean:: $(VERB) rm -rf $(BUILD_ROOT)/Debug $(BUILD_ROOT)/Release $(BUILD_ROOT)/Profile $(BUILD_ROOT)/Depend $(VERB) rm -f core core.[0-9][0-9]* *.o *.d *.so *~ *.flc $(VERB) rm -f $(LEX_OUTPUT) $(YACC_OUTPUT) # If dependancies were generated for the file that included this file, # include the dependancies now... # SourceDepend := $(addsuffix .d,$(addprefix $(BUILD_ROOT)/Depend/,$(basename $(filter-out Debug/%, $(Source))))) ifneq ($(SourceDepend),) -include $(SourceDepend) endif