#===-- Makefile.config - Local configuration for LLVM ------*- Makefile -*--===# # # The LLVM Compiler Infrastructure # # This file is distributed under the University of Illinois Open Source # License. See LICENSE.TXT for details. # #===------------------------------------------------------------------------===# # # This file is included by Makefile.common. It defines paths and other # values specific to a particular installation of LLVM. # #===------------------------------------------------------------------------===# # Define LLVM specific info and directories based on the autoconf variables LLVMPackageName := @PACKAGE_NAME@ LLVMVersion := @PACKAGE_VERSION@ LLVM_CONFIGTIME := @LLVM_CONFIGTIME@ ########################################################################### # Directory Configuration # This section of the Makefile determines what is where. To be # specific, there are several locations that need to be defined: # # o LLVM_SRC_ROOT : The root directory of the LLVM source code. # o LLVM_OBJ_ROOT : The root directory containing the built LLVM code. # # o PROJ_SRC_DIR : The directory containing the code to build. # o PROJ_SRC_ROOT : The root directory of the code to build. # # o PROJ_OBJ_DIR : The directory in which compiled code will be placed. # o PROJ_OBJ_ROOT : The root directory in which compiled code is placed. # ########################################################################### PWD := @BINPWD@ # Set the project name to LLVM if its not defined ifndef PROJECT_NAME PROJECT_NAME := $(LLVMPackageName) endif PROJ_OBJ_DIR := $(shell $(PWD)) PROJ_OBJ_ROOT := $(shell cd $(PROJ_OBJ_DIR)/$(LEVEL); $(PWD)) ifeq ($(PROJECT_NAME),llvm) LLVM_SRC_ROOT := $(shell cd @abs_top_srcdir@; $(PWD)) LLVM_OBJ_ROOT := $(shell cd @abs_top_builddir@; $(PWD)) PROJ_SRC_ROOT := $(shell cd $(LLVM_SRC_ROOT); $(PWD)) PROJ_SRC_DIR := $(shell cd $(LLVM_SRC_ROOT)/$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR)); $(PWD)) prefix := @prefix@ PROJ_prefix := $(prefix) PROJ_VERSION := $(LLVMVersion) else ifndef PROJ_SRC_ROOT $(error Projects must define PROJ_SRC_ROOT) endif ifndef PROJ_OBJ_ROOT $(error Projects must define PROJ_OBJ_ROOT) endif ifndef PROJ_INSTALL_ROOT $(error Projects must define PROJ_INSTALL_ROOT) endif ifndef LLVM_SRC_ROOT $(error Projects must define LLVM_SRC_ROOT) endif ifndef LLVM_OBJ_ROOT $(error Projects must define LLVM_OBJ_ROOT) endif PROJ_SRC_DIR := $(shell cd $(PROJ_SRC_ROOT)/$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR)); $(PWD)) prefix := $(PROJ_INSTALL_ROOT) PROJ_prefix := $(prefix) ifndef PROJ_VERSION PROJ_VERSION := 1.0 endif endif LLVMMAKE := $(LLVM_SRC_ROOT)/make PROJ_bindir := $(DESTDIR)$(PROJ_prefix)/bin PROJ_libdir := $(DESTDIR)$(PROJ_prefix)/lib PROJ_datadir := $(DESTDIR)$(PROJ_prefix)/share PROJ_docsdir := $(DESTDIR)$(PROJ_prefix)/docs/llvm PROJ_etcdir := $(DESTDIR)$(PROJ_prefix)/etc/llvm PROJ_includedir := $(DESTDIR)$(PROJ_prefix)/include PROJ_infodir := $(DESTDIR)$(PROJ_prefix)/info PROJ_mandir := $(DESTDIR)$(PROJ_prefix)/share/man # Determine if we're on a unix type operating system LLVM_ON_UNIX:=@LLVM_ON_UNIX@ LLVM_ON_WIN32:=@LLVM_ON_WIN32@ # Target operating system for which LLVM will be compiled. OS=@OS@ # Target hardware architecture ARCH=@ARCH@ # Indicates, whether we're cross-compiling LLVM or not LLVM_CROSS_COMPILING=@LLVM_CROSS_COMPILING@ # Executable file extension for build platform (mainly for # tablegen call if we're cross-compiling). BUILD_EXEEXT=@BUILD_EXEEXT@ # Compilers for the build platflorm (mainly for tablegen # call if we're cross-compiling). BUILD_CC=@BUILD_CC@ BUILD_CXX=@BUILD_CXX@ # Target triple (cpu-vendor-os) for which we should generate code TARGET_TRIPLE=@target@ # Extra options to compile LLVM with EXTRA_OPTIONS=@EXTRA_OPTIONS@ # Endian-ness of the target ENDIAN=@ENDIAN@ # Path to the C++ compiler to use. This is an optional setting, which defaults # to whatever your gmake defaults to. CXX = @CXX@ # Path to the CC binary, which use used by testcases for native builds. CC := @CC@ # Linker flags. LDFLAGS+=@LDFLAGS@ # Path to the library archiver program. AR_PATH = @AR@ # Path to the nm program NM_PATH = @NM@ # The pathnames of the programs we require to build BISON := @BISON@ CMP := @CMP@ CP := @CP@ DATE := @DATE@ FIND := @FIND@ FLEX := @LEX@ GREP := @GREP@ INSTALL := @INSTALL@ MKDIR := $(LLVM_SRC_ROOT)/autoconf/mkinstalldirs MV := @MV@ RANLIB := @RANLIB@ RM := @RM@ SED := @SED@ TAR := @TAR@ YACC := @YACC@ # Paths to miscellaneous programs we hope are present but might not be PERL := @PERL@ BZIP2 := @BZIP2@ DOT := @DOT@ DOXYGEN := @DOXYGEN@ GROFF := @GROFF@ GZIP := @GZIP@ OCAMLC := @OCAMLC@ OCAMLOPT := @OCAMLOPT@ OCAMLDEP := @OCAMLDEP@ OCAMLDOC := @OCAMLDOC@ POD2HTML := @POD2HTML@ POD2MAN := @POD2MAN@ RUNTEST := @RUNTEST@ TCLSH := @TCLSH@ ZIP := @ZIP@ HAVE_PERL := @HAVE_PERL@ HAVE_PTHREAD := @HAVE_PTHREAD@ LIBS := @LIBS@ # Targets that we should build TARGETS_TO_BUILD=@TARGETS_TO_BUILD@ # Path to location for LLVM C/C++ front-end. You can modify this if you # want to override the value set by configure. LLVMGCCDIR := @LLVMGCCDIR@ # Determine the target for which LLVM should generate code. ifeq (@LLVMGCC_MAJVERS@,3) LLVMGCCARCH := @target@/3.4-llvm else LLVMGCCARCH := @target@/@LLVMGCC_VERSION@ endif # Determine the path where the library executables are LLVMGCCLIBEXEC := @LLVMGCCLIBEXEC@ # Full pathnames of LLVM C/C++ front-end 'cc1' and 'cc1plus' binaries: LLVMGCC := @LLVMGCC@ LLVMGXX := @LLVMGXX@ LLVMCC1 := @LLVMCC1@ LLVMCC1PLUS := @LLVMCC1PLUS@ LLVMGCC_VERSION := @LLVMGCC_VERSION@ LLVMGCC_MAJVERS := @LLVMGCC_MAJVERS@ LLVMGCC_LANGS := @LLVMGCC_LANGS@ # Path to directory where object files should be stored during a build. # Set OBJ_ROOT to "." if you do not want to use a separate place for # object files. OBJ_ROOT := . # These are options that can either be enabled here, or can be enabled on the # make command line (ie, make ENABLE_PROFILING=1): # When ENABLE_OPTIMIZED is enabled, LLVM code is optimized and output is put # into the "Release" directories. Otherwise, LLVM code is not optimized and # output is put in the "Debug" directories. #ENABLE_OPTIMIZED = 1 @ENABLE_OPTIMIZED@ # When DISABLE_ASSERTIONS is enabled, builds of all of the LLVM code will # exclude assertion checks, otherwise they are included. #DISABLE_ASSERTIONS = 1 @DISABLE_ASSERTIONS@ # When ENABLE_EXPENSIVE_CHECKS is enabled, builds of all of the LLVM # code will include expensive checks, otherwise they are excluded. #ENABLE_EXPENSIVE_CHECKS = 0 @ENABLE_EXPENSIVE_CHECKS@ # When DEBUG_RUNTIME is enabled, the runtime libraries will retain debug # symbols. #DEBUG_RUNTIME = 1 @DEBUG_RUNTIME@ # When ENABLE_PROFILING is enabled, the llvm source base is built with profile # information to allow gprof to be used to get execution frequencies. #ENABLE_PROFILING = 1 # When ENABLE_DOXYGEN is enabled, the doxygen documentation will be built ENABLE_DOXYGEN = @ENABLE_DOXYGEN@ # Do we want to enable threads? ENABLE_THREADS := @ENABLE_THREADS@ # Do we want to build with position independent code? ENABLE_PIC := @ENABLE_PIC@ # Use -fvisibility-inlines-hidden? ENABLE_VISIBILITY_INLINES_HIDDEN := @ENABLE_VISIBILITY_INLINES_HIDDEN@ # This option tells the Makefiles to produce verbose output. # It essentially prints the commands that make is executing #VERBOSE = 1 # Enable JIT for this platform TARGET_HAS_JIT = @TARGET_HAS_JIT@ # Shared library extension for host platform. SHLIBEXT = @SHLIBEXT@ # Executable file extension for host platform. EXEEXT = @EXEEXT@ # Things we just assume are "there" ECHO := echo # Get the options for causing archives to link all their content instead of # just missing symbols, and the inverse of that. This is used for certain LLVM # tools that permit loadable modules. It ensures that the LLVM symbols will be # available to those loadable modules. LINKALL := @LINKALL@ NOLINKALL := @NOLINKALL@ # Get the value of HUGE_VAL_SANITY which will be either "yes" or "no" depending # on the check. HUGE_VAL_SANITY = @HUGE_VAL_SANITY@ # Bindings that we should build BINDINGS_TO_BUILD := @BINDINGS_TO_BUILD@ ALL_BINDINGS := @ALL_BINDINGS@ OCAML_LIBDIR := @OCAML_LIBDIR@ # When compiling under Mingw/Cygwin, executables such as tblgen # expect Windows paths, whereas the build system uses Unix paths. # The function SYSPATH transforms Unix paths into Windows paths. ifneq (,$(findstring -mno-cygwin, $(CXX))) SYSPATH = $(shell echo $(1) | cygpath -m -f -) else SYSPATH = $(1) endif