#===- ./Makefile -------------------------------------------*- Makefile -*--===# # # The LLVM Compiler Infrastructure # # This file is distributed under the University of Illinois Open Source # License. See LICENSE.TXT for details. # #===------------------------------------------------------------------------===# LEVEL := . # Top-Level LLVM Build Stages: # 1. Build lib/Support and lib/TableGen, which are used by utils (tblgen). # 2. Build utils, which is used by VMCore. # 3. Build VMCore, which builds the Intrinsics.inc file used by libs. # 4. Build libs, which are needed by llvm-config. # 5. Build llvm-config, which determines inter-lib dependencies for tools. # 6. Build tools, runtime, docs. # # When cross-compiling, there are some things (tablegen) that need to # be build for the build system first. # If "RC_ProjectName" exists in the environment, and its value is # "llvmCore", then this is an "Apple-style" build; search for # "Apple-style" in the comments for more info. Anything else is a # normal build. ifneq ($(findstring llvmCore, $(RC_ProjectName)),llvmCore) # Normal build (not "Apple-style"). ifeq ($(BUILD_DIRS_ONLY),1) DIRS := lib/Support lib/TableGen utils tools/llvm-config OPTIONAL_DIRS := tools/clang/utils/TableGen else DIRS := lib/Support lib/TableGen utils lib/VMCore lib tools/llvm-shlib \ tools/llvm-config tools runtime docs unittests OPTIONAL_DIRS := projects bindings endif ifeq ($(BUILD_EXAMPLES),1) OPTIONAL_DIRS += examples endif EXTRA_DIST := test unittests llvm.spec include win32 Xcode include $(LEVEL)/Makefile.config ifneq ($(ENABLE_SHARED),1) DIRS := $(filter-out tools/llvm-shlib, $(DIRS)) endif ifneq ($(ENABLE_DOCS),1) DIRS := $(filter-out docs, $(DIRS)) endif ifeq ($(MAKECMDGOALS),libs-only) DIRS := $(filter-out tools runtime docs, $(DIRS)) OPTIONAL_DIRS := endif ifeq ($(MAKECMDGOALS),install-libs) DIRS := $(filter-out tools runtime docs, $(DIRS)) OPTIONAL_DIRS := $(filter bindings, $(OPTIONAL_DIRS)) endif ifeq ($(MAKECMDGOALS),tools-only) DIRS := $(filter-out runtime docs, $(DIRS)) OPTIONAL_DIRS := endif ifeq ($(MAKECMDGOALS),install-clang) DIRS := tools/clang/tools/driver tools/clang/lib/Headers \ tools/clang/tools/libclang tools/clang/tools/c-index-test \ tools/clang/include/clang-c \ tools/clang/runtime tools/clang/docs \ tools/lto runtime OPTIONAL_DIRS := NO_INSTALL = 1 endif ifeq ($(MAKECMDGOALS),install-clang-c) DIRS := tools/clang/tools/driver tools/clang/lib/Headers \ tools/clang/tools/libclang tools/clang/tools/c-index-test \ tools/clang/include/clang-c OPTIONAL_DIRS := NO_INSTALL = 1 endif ifeq ($(MAKECMDGOALS),clang-only) DIRS := $(filter-out tools docs unittests, $(DIRS)) \ tools/clang tools/lto OPTIONAL_DIRS := endif ifeq ($(MAKECMDGOALS),unittests) DIRS := $(filter-out tools runtime docs, $(DIRS)) utils unittests OPTIONAL_DIRS := endif # Use NO_INSTALL define of the Makefile of each directory for deciding # if the directory is installed or not ifeq ($(MAKECMDGOALS),install) OPTIONAL_DIRS := $(filter bindings, $(OPTIONAL_DIRS)) endif # Don't build unittests when ONLY_TOOLS is set. ifneq ($(ONLY_TOOLS),) DIRS := $(filter-out unittests, $(DIRS)) endif # If we're cross-compiling, build the build-hosted tools first ifeq ($(LLVM_CROSS_COMPILING),1) all:: cross-compile-build-tools clean:: $(Verb) rm -rf BuildTools cross-compile-build-tools: $(Verb) if [ ! -f BuildTools/Makefile ]; then \ $(MKDIR) BuildTools; \ cd BuildTools ; \ unset CFLAGS ; \ unset CXXFLAGS ; \ $(PROJ_SRC_DIR)/configure --build=$(BUILD_TRIPLE) \ --host=$(BUILD_TRIPLE) --target=$(BUILD_TRIPLE) \ --disable-polly ; \ cd .. ; \ fi; \ (unset SDKROOT; \ $(MAKE) -C BuildTools \ BUILD_DIRS_ONLY=1 \ UNIVERSAL= \ TARGET_NATIVE_ARCH="$(TARGET_NATIVE_ARCH)" \ TARGETS_TO_BUILD="$(TARGETS_TO_BUILD)" \ ENABLE_OPTIMIZED=$(ENABLE_OPTIMIZED) \ ENABLE_PROFILING=$(ENABLE_PROFILING) \ ENABLE_COVERAGE=$(ENABLE_COVERAGE) \ DISABLE_ASSERTIONS=$(DISABLE_ASSERTIONS) \ ENABLE_EXPENSIVE_CHECKS=$(ENABLE_EXPENSIVE_CHECKS) \ ENABLE_LIBCPP=$(ENABLE_LIBCPP) \ CFLAGS= \ CXXFLAGS= \ ) || exit 1; endif # Include the main makefile machinery. include $(LLVM_SRC_ROOT)/Makefile.rules # Specify options to pass to configure script when we're # running the dist-check target DIST_CHECK_CONFIG_OPTIONS = --with-llvmgccdir=$(LLVMGCCDIR) .PHONY: debug-opt-prof debug-opt-prof: $(Echo) Building Debug Version $(Verb) $(MAKE) $(Echo) $(Echo) Building Optimized Version $(Echo) $(Verb) $(MAKE) ENABLE_OPTIMIZED=1 $(Echo) $(Echo) Building Profiling Version $(Echo) $(Verb) $(MAKE) ENABLE_PROFILING=1 dist-hook:: $(Echo) Eliminating files constructed by configure $(Verb) $(RM) -f \ $(TopDistDir)/include/llvm/Config/config.h \ $(TopDistDir)/include/llvm/Support/DataTypes.h clang-only: all tools-only: all libs-only: all install-clang: install install-clang-c: install install-libs: install # If SHOW_DIAGNOSTICS is enabled, clear the diagnostics file first. ifeq ($(SHOW_DIAGNOSTICS),1) clean-diagnostics: $(Verb) rm -f $(LLVM_OBJ_ROOT)/$(BuildMode)/diags .PHONY: clean-diagnostics all-local:: clean-diagnostics endif #------------------------------------------------------------------------ # Make sure the generated headers are up-to-date. This must be kept in # sync with the AC_CONFIG_HEADER invocations in autoconf/configure.ac #------------------------------------------------------------------------ FilesToConfig := \ include/llvm/Config/config.h \ include/llvm/Config/Targets.def \ include/llvm/Config/AsmPrinters.def \ include/llvm/Config/AsmParsers.def \ include/llvm/Config/Disassemblers.def \ include/llvm/Support/DataTypes.h FilesToConfigPATH := $(addprefix $(LLVM_OBJ_ROOT)/,$(FilesToConfig)) all-local:: $(FilesToConfigPATH) $(FilesToConfigPATH) : $(LLVM_OBJ_ROOT)/% : $(LLVM_SRC_ROOT)/%.in $(Echo) Regenerating $* $(Verb) cd $(LLVM_OBJ_ROOT) && $(ConfigStatusScript) $* .PRECIOUS: $(FilesToConfigPATH) # NOTE: This needs to remain as the last target definition in this file so # that it gets executed last. ifneq ($(BUILD_DIRS_ONLY),1) all:: $(Echo) '*****' Completed $(BuildMode) Build ifneq ($(ENABLE_OPTIMIZED),1) $(Echo) '*****' Note: Debug build can be 10 times slower than an $(Echo) '*****' optimized build. Use 'make ENABLE_OPTIMIZED=1' to $(Echo) '*****' make an optimized build. Alternatively you can $(Echo) '*****' configure with --enable-optimized. ifeq ($(SHOW_DIAGNOSTICS),1) $(Verb) if test -s $(LLVM_OBJ_ROOT)/$(BuildMode)/diags; then \ $(LLVM_SRC_ROOT)/utils/clang-parse-diagnostics-file -a \ $(LLVM_OBJ_ROOT)/$(BuildMode)/diags; \ fi endif endif endif check-llvm2cpp: $(Verb)$(MAKE) check TESTSUITE=Feature RUNLLVM2CPP=1 srpm: $(LLVM_OBJ_ROOT)/llvm.spec rpmbuild -bs $(LLVM_OBJ_ROOT)/llvm.spec rpm: $(LLVM_OBJ_ROOT)/llvm.spec rpmbuild -bb --target $(TARGET_TRIPLE) $(LLVM_OBJ_ROOT)/llvm.spec show-footprint: $(Verb) du -sk $(LibDir) $(Verb) du -sk $(ToolDir) $(Verb) du -sk $(ExmplDir) $(Verb) du -sk $(ObjDir) build-for-llvm-top: $(Verb) if test ! -f ./config.status ; then \ ./configure --prefix="$(LLVM_TOP)/install" \ --with-llvm-gcc="$(LLVM_TOP)/llvm-gcc" ; \ fi $(Verb) $(MAKE) tools-only SVN = svn SVN-UPDATE-OPTIONS = AWK = awk SUB-SVN-DIRS = $(AWK) '/\?\ \ \ \ \ \ / {print $$2}' \ | LC_ALL=C xargs $(SVN) info 2>/dev/null \ | $(AWK) '/^Path:\ / {print $$2}' update: $(SVN) $(SVN-UPDATE-OPTIONS) update $(LLVM_SRC_ROOT) @ $(SVN) status $(LLVM_SRC_ROOT) | $(SUB-SVN-DIRS) | xargs $(SVN) $(SVN-UPDATE-OPTIONS) update happiness: update all check-all .PHONY: srpm rpm update happiness # declare all targets at this level to be serial: .NOTPARALLEL: else # Building "Apple-style." # In an Apple-style build, once configuration is done, lines marked # "Apple-style" are removed with sed! Please don't remove these! # Look for the string "Apple-style" in utils/buildit/build_llvm. include $(shell find . -name GNUmakefile) # Building "Apple-style." endif # Building "Apple-style."