# This CMake module is responsible for interpreting the user defined LLVM_ # options and executing the appropriate CMake commands to realize the users' # selections. include(AddLLVMDefinitions) include(CheckCCompilerFlag) if( CMAKE_COMPILER_IS_GNUCXX ) set(LLVM_COMPILER_IS_GCC_COMPATIBLE ON) elseif( "${CMAKE_CXX_COMPILER_ID}" MATCHES "Clang" ) set(LLVM_COMPILER_IS_GCC_COMPATIBLE ON) endif() # Run-time build mode; It is used for unittests. if(MSVC_IDE) # Expect "$(Configuration)", "$(OutDir)", etc. # It is expanded by msbuild or similar. set(RUNTIME_BUILD_MODE "${CMAKE_CFG_INTDIR}") elseif(NOT CMAKE_BUILD_TYPE STREQUAL "") # Expect "Release" "Debug", etc. # Or unittests could not run. set(RUNTIME_BUILD_MODE ${CMAKE_BUILD_TYPE}) else() # It might be "." set(RUNTIME_BUILD_MODE "${CMAKE_CFG_INTDIR}") endif() if( LLVM_ENABLE_ASSERTIONS ) # MSVC doesn't like _DEBUG on release builds. See PR 4379. if( NOT MSVC ) add_definitions( -D_DEBUG ) endif() # On Release builds cmake automatically defines NDEBUG, so we # explicitly undefine it: if( uppercase_CMAKE_BUILD_TYPE STREQUAL "RELEASE" ) add_definitions( -UNDEBUG ) endif() else() if( NOT uppercase_CMAKE_BUILD_TYPE STREQUAL "RELEASE" ) if( NOT MSVC_IDE AND NOT XCODE ) add_definitions( -DNDEBUG ) endif() endif() endif() if(WIN32) if(CYGWIN) set(LLVM_ON_WIN32 0) set(LLVM_ON_UNIX 1) else(CYGWIN) set(LLVM_ON_WIN32 1) set(LLVM_ON_UNIX 0) endif(CYGWIN) set(LTDL_SHLIB_EXT ".dll") set(EXEEXT ".exe") # Maximum path length is 160 for non-unicode paths set(MAXPATHLEN 160) else(WIN32) if(UNIX) set(LLVM_ON_WIN32 0) set(LLVM_ON_UNIX 1) if(APPLE) set(LTDL_SHLIB_EXT ".dylib") else(APPLE) set(LTDL_SHLIB_EXT ".so") endif(APPLE) set(EXEEXT "") # FIXME: Maximum path length is currently set to 'safe' fixed value set(MAXPATHLEN 2024) else(UNIX) MESSAGE(SEND_ERROR "Unable to determine platform") endif(UNIX) endif(WIN32) if( LLVM_ENABLE_PIC ) if( XCODE ) # Xcode has -mdynamic-no-pic on by default, which overrides -fPIC. I don't # know how to disable this, so just force ENABLE_PIC off for now. message(WARNING "-fPIC not supported with Xcode.") elseif( WIN32 OR CYGWIN) # On Windows all code is PIC. MinGW warns if -fPIC is used. else() include(CheckCXXCompilerFlag) check_cxx_compiler_flag("-fPIC" SUPPORTS_FPIC_FLAG) if( SUPPORTS_FPIC_FLAG ) message(STATUS "Building with -fPIC") set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -fPIC") set(CMAKE_C_FLAGS "${CMAKE_C_FLAGS} -fPIC") else( SUPPORTS_FPIC_FLAG ) message(WARNING "-fPIC not supported.") endif() if( WIN32 OR CYGWIN) # MinGW warns if -fvisibility-inlines-hidden is used. else() check_cxx_compiler_flag("-fvisibility-inlines-hidden" SUPPORTS_FVISIBILITY_INLINES_HIDDEN_FLAG) if( SUPPORTS_FVISIBILITY_INLINES_HIDDEN_FLAG ) set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -fvisibility-inlines-hidden") endif() endif() endif() endif() if( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 ) # TODO: support other platforms and toolchains. if( LLVM_BUILD_32_BITS ) message(STATUS "Building 32 bits executables and libraries.") add_llvm_definitions( -m32 ) set(CMAKE_EXE_LINKER_FLAGS "${CMAKE_EXE_LINKER_FLAGS} -m32") set(CMAKE_SHARED_LINKER_FLAGS "${CMAKE_SHARED_LINKER_FLAGS} -m32") set(CMAKE_MODULE_LINKER_FLAGS "${CMAKE_MODULE_LINKER_FLAGS} -m32") endif( LLVM_BUILD_32_BITS ) endif( CMAKE_SIZEOF_VOID_P EQUAL 8 AND NOT WIN32 ) # On Win32 using MS tools, provide an option to set the number of parallel jobs # to use. if( MSVC_IDE ) set(LLVM_COMPILER_JOBS "0" CACHE STRING "Number of parallel compiler jobs. 0 means use all processors. Default is 0.") if( NOT LLVM_COMPILER_JOBS STREQUAL "1" ) if( LLVM_COMPILER_JOBS STREQUAL "0" ) add_llvm_definitions( /MP ) else() if (MSVC10) message(FATAL_ERROR "Due to a bug in CMake only 0 and 1 is supported for " "LLVM_COMPILER_JOBS when generating for Visual Studio 2010") else() message(STATUS "Number of parallel compiler jobs set to " ${LLVM_COMPILER_JOBS}) add_llvm_definitions( /MP${LLVM_COMPILER_JOBS} ) endif() endif() else() message(STATUS "Parallel compilation disabled") endif() endif() if( MSVC ) include(ChooseMSVCCRT) if( MSVC11 ) add_llvm_definitions(-D_VARIADIC_MAX=10) endif() # Add definitions that make MSVC much less annoying. add_llvm_definitions( # For some reason MS wants to deprecate a bunch of standard functions... -D_CRT_SECURE_NO_DEPRECATE -D_CRT_SECURE_NO_WARNINGS -D_CRT_NONSTDC_NO_DEPRECATE -D_CRT_NONSTDC_NO_WARNINGS -D_SCL_SECURE_NO_DEPRECATE -D_SCL_SECURE_NO_WARNINGS # Disabled warnings. -wd4065 # Suppress 'switch statement contains 'default' but no 'case' labels' -wd4146 # Suppress 'unary minus operator applied to unsigned type, result still unsigned' -wd4180 # Suppress 'qualifier applied to function type has no meaning; ignored' -wd4181 # Suppress 'qualifier applied to reference type; ignored' -wd4224 # Suppress 'nonstandard extension used : formal parameter 'identifier' was previously defined as a type' -wd4244 # Suppress ''argument' : conversion from 'type1' to 'type2', possible loss of data' -wd4267 # Suppress ''var' : conversion from 'size_t' to 'type', possible loss of data' -wd4275 # Suppress 'An exported class was derived from a class that was not exported.' -wd4291 # Suppress ''declaration' : no matching operator delete found; memory will not be freed if initialization throws an exception' -wd4345 # Suppress 'behavior change: an object of POD type constructed with an initializer of the form () will be default-initialized' -wd4351 # Suppress 'new behavior: elements of array 'array' will be default initialized' -wd4355 # Suppress ''this' : used in base member initializer list' -wd4503 # Suppress ''identifier' : decorated name length exceeded, name was truncated' -wd4551 # Suppress 'function call missing argument list' -wd4624 # Suppress ''derived class' : destructor could not be generated because a base class destructor is inaccessible' -wd4715 # Suppress ''function' : not all control paths return a value' -wd4800 # Suppress ''type' : forcing value to bool 'true' or 'false' (performance warning)' # Promoted warnings. -w14062 # Promote 'enumerator in switch of enum is not handled' to level 1 warning. # Promoted warnings to errors. -we4238 # Promote 'nonstandard extension used : class rvalue used as lvalue' to error. -we4239 # Promote 'nonstandard extension used : 'token' : conversion from 'type' to 'type'' to error. ) # Enable warnings if (LLVM_ENABLE_WARNINGS) add_llvm_definitions( /W4 ) if (LLVM_ENABLE_PEDANTIC) # No MSVC equivalent available endif (LLVM_ENABLE_PEDANTIC) endif (LLVM_ENABLE_WARNINGS) if (LLVM_ENABLE_WERROR) add_llvm_definitions( /WX ) endif (LLVM_ENABLE_WERROR) elseif( LLVM_COMPILER_IS_GCC_COMPATIBLE ) if (LLVM_ENABLE_WARNINGS) add_llvm_definitions( -Wall -W -Wno-unused-parameter -Wwrite-strings ) if (LLVM_ENABLE_PEDANTIC) add_llvm_definitions( -pedantic -Wno-long-long ) endif (LLVM_ENABLE_PEDANTIC) check_cxx_compiler_flag("-Werror -Wcovered-switch-default" CXX_SUPPORTS_COVERED_SWITCH_DEFAULT_FLAG) if( CXX_SUPPORTS_COVERED_SWITCH_DEFAULT_FLAG ) set( CMAKE_CXX_FlAGS "${CMAKE_CXX_FLAGS} -Wcovered-switch-default" ) endif() check_c_compiler_flag("-Werror -Wcovered-switch-default" C_SUPPORTS_COVERED_SWITCH_DEFAULT_FLAG) if( C_SUPPORTS_COVERED_SWITCH_DEFAULT_FLAG ) set( CMAKE_C_FlAGS "${CMAKE_C_FLAGS} -Wcovered-switch-default" ) endif() endif (LLVM_ENABLE_WARNINGS) if (LLVM_ENABLE_WERROR) add_llvm_definitions( -Werror ) endif (LLVM_ENABLE_WERROR) endif( MSVC ) add_llvm_definitions( -D__STDC_CONSTANT_MACROS ) add_llvm_definitions( -D__STDC_FORMAT_MACROS ) add_llvm_definitions( -D__STDC_LIMIT_MACROS )