//===-- LiveIntervalAnalysis.h - Live Interval Analysis ---------*- C++ -*-===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the LiveInterval analysis pass. Given some numbering of // each the machine instructions (in this implemention depth-first order) an // interval [i, j) is said to be a live interval for register v if there is no // instruction with number j' > j such that v is live at j' and there is no // instruction with number i' < i such that v is live at i'. In this // implementation intervals can have holes, i.e. an interval might look like // [1,20), [50,65), [1000,1001). // //===----------------------------------------------------------------------===// #ifndef LLVM_CODEGEN_LIVEINTERVAL_ANALYSIS_H #define LLVM_CODEGEN_LIVEINTERVAL_ANALYSIS_H #include "llvm/CodeGen/MachineBasicBlock.h" #include "llvm/CodeGen/MachineFunctionPass.h" #include "llvm/CodeGen/LiveInterval.h" #include "llvm/CodeGen/SlotIndexes.h" #include "llvm/ADT/BitVector.h" #include "llvm/ADT/DenseMap.h" #include "llvm/ADT/SmallPtrSet.h" #include "llvm/ADT/SmallVector.h" #include "llvm/Support/Allocator.h" #include #include namespace llvm { class AliasAnalysis; class LiveVariables; class MachineLoopInfo; class TargetRegisterInfo; class MachineRegisterInfo; class TargetInstrInfo; class TargetRegisterClass; class VirtRegMap; class LiveIntervals : public MachineFunctionPass { MachineFunction* mf_; MachineRegisterInfo* mri_; const TargetMachine* tm_; const TargetRegisterInfo* tri_; const TargetInstrInfo* tii_; AliasAnalysis *aa_; LiveVariables* lv_; SlotIndexes* indexes_; /// Special pool allocator for VNInfo's (LiveInterval val#). /// VNInfo::Allocator VNInfoAllocator; typedef DenseMap Reg2IntervalMap; Reg2IntervalMap r2iMap_; /// allocatableRegs_ - A bit vector of allocatable registers. BitVector allocatableRegs_; /// CloneMIs - A list of clones as result of re-materialization. std::vector CloneMIs; public: static char ID; // Pass identification, replacement for typeid LiveIntervals() : MachineFunctionPass(&ID) {} // Calculate the spill weight to assign to a single instruction. static float getSpillWeight(bool isDef, bool isUse, unsigned loopDepth); // After summing the spill weights of all defs and uses, the final weight // should be normalized, dividing the weight of the interval by its size. // This encourages spilling of intervals that are large and have few uses, // and discourages spilling of small intervals with many uses. void normalizeSpillWeight(LiveInterval &li) { li.weight /= getApproximateInstructionCount(li) + 25; } typedef Reg2IntervalMap::iterator iterator; typedef Reg2IntervalMap::const_iterator const_iterator; const_iterator begin() const { return r2iMap_.begin(); } const_iterator end() const { return r2iMap_.end(); } iterator begin() { return r2iMap_.begin(); } iterator end() { return r2iMap_.end(); } unsigned getNumIntervals() const { return (unsigned)r2iMap_.size(); } LiveInterval &getInterval(unsigned reg) { Reg2IntervalMap::iterator I = r2iMap_.find(reg); assert(I != r2iMap_.end() && "Interval does not exist for register"); return *I->second; } const LiveInterval &getInterval(unsigned reg) const { Reg2IntervalMap::const_iterator I = r2iMap_.find(reg); assert(I != r2iMap_.end() && "Interval does not exist for register"); return *I->second; } bool hasInterval(unsigned reg) const { return r2iMap_.count(reg); } /// getScaledIntervalSize - get the size of an interval in "units," /// where every function is composed of one thousand units. This /// measure scales properly with empty index slots in the function. double getScaledIntervalSize(LiveInterval& I) { return (1000.0 * I.getSize()) / indexes_->getIndexesLength(); } /// getFuncInstructionCount - Return the number of instructions in the /// current function. unsigned getFuncInstructionCount() { return indexes_->getFunctionSize(); } /// getApproximateInstructionCount - computes an estimate of the number /// of instructions in a given LiveInterval. unsigned getApproximateInstructionCount(LiveInterval& I) { double IntervalPercentage = getScaledIntervalSize(I) / 1000.0; return (unsigned)(IntervalPercentage * indexes_->getFunctionSize()); } /// conflictsWithPhysReg - Returns true if the specified register is used or /// defined during the duration of the specified interval. Copies to and /// from li.reg are allowed. This method is only able to analyze simple /// ranges that stay within a single basic block. Anything else is /// considered a conflict. bool conflictsWithPhysReg(const LiveInterval &li, VirtRegMap &vrm, unsigned reg); /// conflictsWithSubPhysRegRef - Similar to conflictsWithPhysRegRef except /// it checks for sub-register reference and it can check use as well. bool conflictsWithSubPhysRegRef(LiveInterval &li, unsigned Reg, bool CheckUse, SmallPtrSet &JoinedCopies); // Interval creation LiveInterval &getOrCreateInterval(unsigned reg) { Reg2IntervalMap::iterator I = r2iMap_.find(reg); if (I == r2iMap_.end()) I = r2iMap_.insert(std::make_pair(reg, createInterval(reg))).first; return *I->second; } /// dupInterval - Duplicate a live interval. The caller is responsible for /// managing the allocated memory. LiveInterval *dupInterval(LiveInterval *li); /// addLiveRangeToEndOfBlock - Given a register and an instruction, /// adds a live range from that instruction to the end of its MBB. LiveRange addLiveRangeToEndOfBlock(unsigned reg, MachineInstr* startInst); // Interval removal void removeInterval(unsigned Reg) { DenseMap::iterator I = r2iMap_.find(Reg); delete I->second; r2iMap_.erase(I); } SlotIndex getZeroIndex() const { return indexes_->getZeroIndex(); } SlotIndex getInvalidIndex() const { return indexes_->getInvalidIndex(); } /// isNotInMIMap - returns true if the specified machine instr has been /// removed or was never entered in the map. bool isNotInMIMap(const MachineInstr* Instr) const { return !indexes_->hasIndex(Instr); } /// Returns the base index of the given instruction. SlotIndex getInstructionIndex(const MachineInstr *instr) const { return indexes_->getInstructionIndex(instr); } /// Returns the instruction associated with the given index. MachineInstr* getInstructionFromIndex(SlotIndex index) const { return indexes_->getInstructionFromIndex(index); } /// Return the first index in the given basic block. SlotIndex getMBBStartIdx(const MachineBasicBlock *mbb) const { return indexes_->getMBBStartIdx(mbb); } /// Return the last index in the given basic block. SlotIndex getMBBEndIdx(const MachineBasicBlock *mbb) const { return indexes_->getMBBEndIdx(mbb); } MachineBasicBlock* getMBBFromIndex(SlotIndex index) const { return indexes_->getMBBFromIndex(index); } SlotIndex getMBBTerminatorGap(const MachineBasicBlock *mbb) { return indexes_->getTerminatorGap(mbb); } SlotIndex InsertMachineInstrInMaps(MachineInstr *MI) { return indexes_->insertMachineInstrInMaps(MI); } void RemoveMachineInstrFromMaps(MachineInstr *MI) { indexes_->removeMachineInstrFromMaps(MI); } void ReplaceMachineInstrInMaps(MachineInstr *MI, MachineInstr *NewMI) { indexes_->replaceMachineInstrInMaps(MI, NewMI); } bool findLiveInMBBs(SlotIndex Start, SlotIndex End, SmallVectorImpl &MBBs) const { return indexes_->findLiveInMBBs(Start, End, MBBs); } void renumber() { indexes_->renumberIndexes(); } VNInfo::Allocator& getVNInfoAllocator() { return VNInfoAllocator; } /// getVNInfoSourceReg - Helper function that parses the specified VNInfo /// copy field and returns the source register that defines it. unsigned getVNInfoSourceReg(const VNInfo *VNI) const; virtual void getAnalysisUsage(AnalysisUsage &AU) const; virtual void releaseMemory(); /// runOnMachineFunction - pass entry point virtual bool runOnMachineFunction(MachineFunction&); /// print - Implement the dump method. virtual void print(raw_ostream &O, const Module* = 0) const; /// addIntervalsForSpills - Create new intervals for spilled defs / uses of /// the given interval. FIXME: It also returns the weight of the spill slot /// (if any is created) by reference. This is temporary. std::vector addIntervalsForSpills(const LiveInterval& i, SmallVectorImpl &SpillIs, const MachineLoopInfo *loopInfo, VirtRegMap& vrm); /// addIntervalsForSpillsFast - Quickly create new intervals for spilled /// defs / uses without remat or splitting. std::vector addIntervalsForSpillsFast(const LiveInterval &li, const MachineLoopInfo *loopInfo, VirtRegMap &vrm); /// spillPhysRegAroundRegDefsUses - Spill the specified physical register /// around all defs and uses of the specified interval. Return true if it /// was able to cut its interval. bool spillPhysRegAroundRegDefsUses(const LiveInterval &li, unsigned PhysReg, VirtRegMap &vrm); /// isReMaterializable - Returns true if every definition of MI of every /// val# of the specified interval is re-materializable. Also returns true /// by reference if all of the defs are load instructions. bool isReMaterializable(const LiveInterval &li, SmallVectorImpl &SpillIs, bool &isLoad); /// isReMaterializable - Returns true if the definition MI of the specified /// val# of the specified interval is re-materializable. bool isReMaterializable(const LiveInterval &li, const VNInfo *ValNo, MachineInstr *MI); /// getRepresentativeReg - Find the largest super register of the specified /// physical register. unsigned getRepresentativeReg(unsigned Reg) const; /// getNumConflictsWithPhysReg - Return the number of uses and defs of the /// specified interval that conflicts with the specified physical register. unsigned getNumConflictsWithPhysReg(const LiveInterval &li, unsigned PhysReg) const; /// processImplicitDefs - Process IMPLICIT_DEF instructions. Add isUndef /// marker to implicit_def defs and their uses. void processImplicitDefs(); /// intervalIsInOneMBB - Returns true if the specified interval is entirely /// within a single basic block. bool intervalIsInOneMBB(const LiveInterval &li) const; private: /// computeIntervals - Compute live intervals. void computeIntervals(); /// handleRegisterDef - update intervals for a register def /// (calls handlePhysicalRegisterDef and /// handleVirtualRegisterDef) void handleRegisterDef(MachineBasicBlock *MBB, MachineBasicBlock::iterator MI, SlotIndex MIIdx, MachineOperand& MO, unsigned MOIdx); /// isPartialRedef - Return true if the specified def at the specific index /// is partially re-defining the specified live interval. A common case of /// this is a definition of the sub-register. bool isPartialRedef(SlotIndex MIIdx, MachineOperand &MO, LiveInterval &interval); /// handleVirtualRegisterDef - update intervals for a virtual /// register def void handleVirtualRegisterDef(MachineBasicBlock *MBB, MachineBasicBlock::iterator MI, SlotIndex MIIdx, MachineOperand& MO, unsigned MOIdx, LiveInterval& interval); /// handlePhysicalRegisterDef - update intervals for a physical register /// def. void handlePhysicalRegisterDef(MachineBasicBlock* mbb, MachineBasicBlock::iterator mi, SlotIndex MIIdx, MachineOperand& MO, LiveInterval &interval, MachineInstr *CopyMI); /// handleLiveInRegister - Create interval for a livein register. void handleLiveInRegister(MachineBasicBlock* mbb, SlotIndex MIIdx, LiveInterval &interval, bool isAlias = false); /// getReMatImplicitUse - If the remat definition MI has one (for now, we /// only allow one) virtual register operand, then its uses are implicitly /// using the register. Returns the virtual register. unsigned getReMatImplicitUse(const LiveInterval &li, MachineInstr *MI) const; /// isValNoAvailableAt - Return true if the val# of the specified interval /// which reaches the given instruction also reaches the specified use /// index. bool isValNoAvailableAt(const LiveInterval &li, MachineInstr *MI, SlotIndex UseIdx) const; /// isReMaterializable - Returns true if the definition MI of the specified /// val# of the specified interval is re-materializable. Also returns true /// by reference if the def is a load. bool isReMaterializable(const LiveInterval &li, const VNInfo *ValNo, MachineInstr *MI, SmallVectorImpl &SpillIs, bool &isLoad); /// tryFoldMemoryOperand - Attempts to fold either a spill / restore from /// slot / to reg or any rematerialized load into ith operand of specified /// MI. If it is successul, MI is updated with the newly created MI and /// returns true. bool tryFoldMemoryOperand(MachineInstr* &MI, VirtRegMap &vrm, MachineInstr *DefMI, SlotIndex InstrIdx, SmallVector &Ops, bool isSS, int FrameIndex, unsigned Reg); /// canFoldMemoryOperand - Return true if the specified load / store /// folding is possible. bool canFoldMemoryOperand(MachineInstr *MI, SmallVector &Ops, bool ReMatLoadSS) const; /// anyKillInMBBAfterIdx - Returns true if there is a kill of the specified /// VNInfo that's after the specified index but is within the basic block. bool anyKillInMBBAfterIdx(const LiveInterval &li, const VNInfo *VNI, MachineBasicBlock *MBB, SlotIndex Idx) const; /// hasAllocatableSuperReg - Return true if the specified physical register /// has any super register that's allocatable. bool hasAllocatableSuperReg(unsigned Reg) const; /// SRInfo - Spill / restore info. struct SRInfo { SlotIndex index; unsigned vreg; bool canFold; SRInfo(SlotIndex i, unsigned vr, bool f) : index(i), vreg(vr), canFold(f) {} }; bool alsoFoldARestore(int Id, SlotIndex index, unsigned vr, BitVector &RestoreMBBs, DenseMap >&RestoreIdxes); void eraseRestoreInfo(int Id, SlotIndex index, unsigned vr, BitVector &RestoreMBBs, DenseMap >&RestoreIdxes); /// handleSpilledImpDefs - Remove IMPLICIT_DEF instructions which are being /// spilled and create empty intervals for their uses. void handleSpilledImpDefs(const LiveInterval &li, VirtRegMap &vrm, const TargetRegisterClass* rc, std::vector &NewLIs); /// rewriteImplicitOps - Rewrite implicit use operands of MI (i.e. uses of /// interval on to-be re-materialized operands of MI) with new register. void rewriteImplicitOps(const LiveInterval &li, MachineInstr *MI, unsigned NewVReg, VirtRegMap &vrm); /// rewriteInstructionForSpills, rewriteInstructionsForSpills - Helper /// functions for addIntervalsForSpills to rewrite uses / defs for the given /// live range. bool rewriteInstructionForSpills(const LiveInterval &li, const VNInfo *VNI, bool TrySplit, SlotIndex index, SlotIndex end, MachineInstr *MI, MachineInstr *OrigDefMI, MachineInstr *DefMI, unsigned Slot, int LdSlot, bool isLoad, bool isLoadSS, bool DefIsReMat, bool CanDelete, VirtRegMap &vrm, const TargetRegisterClass* rc, SmallVector &ReMatIds, const MachineLoopInfo *loopInfo, unsigned &NewVReg, unsigned ImpUse, bool &HasDef, bool &HasUse, DenseMap &MBBVRegsMap, std::vector &NewLIs); void rewriteInstructionsForSpills(const LiveInterval &li, bool TrySplit, LiveInterval::Ranges::const_iterator &I, MachineInstr *OrigDefMI, MachineInstr *DefMI, unsigned Slot, int LdSlot, bool isLoad, bool isLoadSS, bool DefIsReMat, bool CanDelete, VirtRegMap &vrm, const TargetRegisterClass* rc, SmallVector &ReMatIds, const MachineLoopInfo *loopInfo, BitVector &SpillMBBs, DenseMap > &SpillIdxes, BitVector &RestoreMBBs, DenseMap > &RestoreIdxes, DenseMap &MBBVRegsMap, std::vector &NewLIs); // Normalize the spill weight of all the intervals in NewLIs. void normalizeSpillWeights(std::vector &NewLIs); static LiveInterval* createInterval(unsigned Reg); void printInstrs(raw_ostream &O) const; void dumpInstrs() const; }; } // End llvm namespace #endif