//===-- llvm/CodeGen/MachineInstr.h - MachineInstr class --------*- C++ -*-===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file contains the declaration of the MachineInstr class, which is the // basic representation for all target dependent machine instructions used by // the back end. // //===----------------------------------------------------------------------===// #ifndef LLVM_CODEGEN_MACHINEINSTR_H #define LLVM_CODEGEN_MACHINEINSTR_H #include "llvm/CodeGen/MachineOperand.h" #include "llvm/Target/TargetInstrDesc.h" #include "llvm/Target/TargetOpcodes.h" #include "llvm/ADT/ilist.h" #include "llvm/ADT/ilist_node.h" #include "llvm/ADT/STLExtras.h" #include "llvm/ADT/DenseMapInfo.h" #include "llvm/Support/DebugLoc.h" #include namespace llvm { template class SmallVectorImpl; class AliasAnalysis; class TargetInstrDesc; class TargetInstrInfo; class TargetRegisterInfo; class MachineFunction; class MachineMemOperand; //===----------------------------------------------------------------------===// /// MachineInstr - Representation of each machine instruction. /// class MachineInstr : public ilist_node { public: typedef MachineMemOperand **mmo_iterator; /// Flags to specify different kinds of comments to output in /// assembly code. These flags carry semantic information not /// otherwise easily derivable from the IR text. /// enum CommentFlag { ReloadReuse = 0x1 }; private: const TargetInstrDesc *TID; // Instruction descriptor. unsigned short NumImplicitOps; // Number of implicit operands (which // are determined at construction time). unsigned short AsmPrinterFlags; // Various bits of information used by // the AsmPrinter to emit helpful // comments. This is *not* semantic // information. Do not use this for // anything other than to convey comment // information to AsmPrinter. std::vector Operands; // the operands mmo_iterator MemRefs; // information on memory references mmo_iterator MemRefsEnd; MachineBasicBlock *Parent; // Pointer to the owning basic block. DebugLoc debugLoc; // Source line information. // OperandComplete - Return true if it's illegal to add a new operand bool OperandsComplete() const; MachineInstr(const MachineInstr&); // DO NOT IMPLEMENT void operator=(const MachineInstr&); // DO NOT IMPLEMENT // Intrusive list support friend struct ilist_traits; friend struct ilist_traits; void setParent(MachineBasicBlock *P) { Parent = P; } /// MachineInstr ctor - This constructor creates a copy of the given /// MachineInstr in the given MachineFunction. MachineInstr(MachineFunction &, const MachineInstr &); /// MachineInstr ctor - This constructor creates a dummy MachineInstr with /// TID NULL and no operands. MachineInstr(); // The next two constructors have DebugLoc and non-DebugLoc versions; // over time, the non-DebugLoc versions should be phased out and eventually // removed. /// MachineInstr ctor - This constructor creates a MachineInstr and adds the /// implicit operands. It reserves space for the number of operands specified /// by the TargetInstrDesc. The version with a DebugLoc should be preferred. explicit MachineInstr(const TargetInstrDesc &TID, bool NoImp = false); /// MachineInstr ctor - Work exactly the same as the ctor above, except that /// the MachineInstr is created and added to the end of the specified basic /// block. The version with a DebugLoc should be preferred. MachineInstr(MachineBasicBlock *MBB, const TargetInstrDesc &TID); /// MachineInstr ctor - This constructor create a MachineInstr and add the /// implicit operands. It reserves space for number of operands specified by /// TargetInstrDesc. An explicit DebugLoc is supplied. explicit MachineInstr(const TargetInstrDesc &TID, const DebugLoc dl, bool NoImp = false); /// MachineInstr ctor - Work exactly the same as the ctor above, except that /// the MachineInstr is created and added to the end of the specified basic /// block. MachineInstr(MachineBasicBlock *MBB, const DebugLoc dl, const TargetInstrDesc &TID); ~MachineInstr(); // MachineInstrs are pool-allocated and owned by MachineFunction. friend class MachineFunction; public: const MachineBasicBlock* getParent() const { return Parent; } MachineBasicBlock* getParent() { return Parent; } /// getAsmPrinterFlags - Return the asm printer flags bitvector. /// unsigned short getAsmPrinterFlags() const { return AsmPrinterFlags; } /// getAsmPrinterFlag - Return whether an AsmPrinter flag is set. /// bool getAsmPrinterFlag(CommentFlag Flag) const { return AsmPrinterFlags & Flag; } /// setAsmPrinterFlag - Set a flag for the AsmPrinter. /// void setAsmPrinterFlag(CommentFlag Flag) { AsmPrinterFlags |= (unsigned short)Flag; } /// getDebugLoc - Returns the debug location id of this MachineInstr. /// DebugLoc getDebugLoc() const { return debugLoc; } /// getDesc - Returns the target instruction descriptor of this /// MachineInstr. const TargetInstrDesc &getDesc() const { return *TID; } /// getOpcode - Returns the opcode of this MachineInstr. /// int getOpcode() const { return TID->Opcode; } /// Access to explicit operands of the instruction. /// unsigned getNumOperands() const { return (unsigned)Operands.size(); } const MachineOperand& getOperand(unsigned i) const { assert(i < getNumOperands() && "getOperand() out of range!"); return Operands[i]; } MachineOperand& getOperand(unsigned i) { assert(i < getNumOperands() && "getOperand() out of range!"); return Operands[i]; } /// getNumExplicitOperands - Returns the number of non-implicit operands. /// unsigned getNumExplicitOperands() const; /// Access to memory operands of the instruction mmo_iterator memoperands_begin() const { return MemRefs; } mmo_iterator memoperands_end() const { return MemRefsEnd; } bool memoperands_empty() const { return MemRefsEnd == MemRefs; } /// hasOneMemOperand - Return true if this instruction has exactly one /// MachineMemOperand. bool hasOneMemOperand() const { return MemRefsEnd - MemRefs == 1; } enum MICheckType { CheckDefs, // Check all operands for equality IgnoreDefs, // Ignore all definitions IgnoreVRegDefs // Ignore virtual register definitions }; /// isIdenticalTo - Return true if this instruction is identical to (same /// opcode and same operands as) the specified instruction. bool isIdenticalTo(const MachineInstr *Other, MICheckType Check = CheckDefs) const; /// removeFromParent - This method unlinks 'this' from the containing basic /// block, and returns it, but does not delete it. MachineInstr *removeFromParent(); /// eraseFromParent - This method unlinks 'this' from the containing basic /// block and deletes it. void eraseFromParent(); /// isLabel - Returns true if the MachineInstr represents a label. /// bool isLabel() const { return getOpcode() == TargetOpcode::DBG_LABEL || getOpcode() == TargetOpcode::EH_LABEL || getOpcode() == TargetOpcode::GC_LABEL; } bool isDebugLabel() const { return getOpcode() == TargetOpcode::DBG_LABEL; } bool isEHLabel() const { return getOpcode() == TargetOpcode::EH_LABEL; } bool isGCLabel() const { return getOpcode() == TargetOpcode::GC_LABEL; } bool isDebugValue() const { return getOpcode() == TargetOpcode::DBG_VALUE; } bool isPHI() const { return getOpcode() == TargetOpcode::PHI; } bool isKill() const { return getOpcode() == TargetOpcode::KILL; } bool isImplicitDef() const { return getOpcode()==TargetOpcode::IMPLICIT_DEF; } bool isInlineAsm() const { return getOpcode() == TargetOpcode::INLINEASM; } bool isExtractSubreg() const { return getOpcode() == TargetOpcode::EXTRACT_SUBREG; } bool isInsertSubreg() const { return getOpcode() == TargetOpcode::INSERT_SUBREG; } bool isSubregToReg() const { return getOpcode() == TargetOpcode::SUBREG_TO_REG; } bool isRegSequence() const { return getOpcode() == TargetOpcode::REG_SEQUENCE; } /// readsRegister - Return true if the MachineInstr reads the specified /// register. If TargetRegisterInfo is passed, then it also checks if there /// is a read of a super-register. /// This does not count partial redefines of virtual registers as reads: /// %reg1024:6 = OP. bool readsRegister(unsigned Reg, const TargetRegisterInfo *TRI = NULL) const { return findRegisterUseOperandIdx(Reg, false, TRI) != -1; } /// readsVirtualRegister - Return true if the MachineInstr reads the specified /// virtual register. Take into account that a partial define is a /// read-modify-write operation. bool readsVirtualRegister(unsigned Reg) const { return readsWritesVirtualRegister(Reg).first; } /// readsWritesVirtualRegister - Return a pair of bools (reads, writes) /// indicating if this instruction reads or writes Reg. This also considers /// partial defines. /// If Ops is not null, all operand indices for Reg are added. std::pair readsWritesVirtualRegister(unsigned Reg, SmallVectorImpl *Ops = 0) const; /// killsRegister - Return true if the MachineInstr kills the specified /// register. If TargetRegisterInfo is passed, then it also checks if there is /// a kill of a super-register. bool killsRegister(unsigned Reg, const TargetRegisterInfo *TRI = NULL) const { return findRegisterUseOperandIdx(Reg, true, TRI) != -1; } /// definesRegister - Return true if the MachineInstr fully defines the /// specified register. If TargetRegisterInfo is passed, then it also checks /// if there is a def of a super-register. /// NOTE: It's ignoring subreg indices on virtual registers. bool definesRegister(unsigned Reg, const TargetRegisterInfo *TRI=NULL) const { return findRegisterDefOperandIdx(Reg, false, false, TRI) != -1; } /// modifiesRegister - Return true if the MachineInstr modifies (fully define /// or partially define) the specified register. /// NOTE: It's ignoring subreg indices on virtual registers. bool modifiesRegister(unsigned Reg, const TargetRegisterInfo *TRI) const { return findRegisterDefOperandIdx(Reg, false, true, TRI) != -1; } /// registerDefIsDead - Returns true if the register is dead in this machine /// instruction. If TargetRegisterInfo is passed, then it also checks /// if there is a dead def of a super-register. bool registerDefIsDead(unsigned Reg, const TargetRegisterInfo *TRI = NULL) const { return findRegisterDefOperandIdx(Reg, true, false, TRI) != -1; } /// findRegisterUseOperandIdx() - Returns the operand index that is a use of /// the specific register or -1 if it is not found. It further tightens /// the search criteria to a use that kills the register if isKill is true. int findRegisterUseOperandIdx(unsigned Reg, bool isKill = false, const TargetRegisterInfo *TRI = NULL) const; /// findRegisterUseOperand - Wrapper for findRegisterUseOperandIdx, it returns /// a pointer to the MachineOperand rather than an index. MachineOperand *findRegisterUseOperand(unsigned Reg, bool isKill = false, const TargetRegisterInfo *TRI = NULL) { int Idx = findRegisterUseOperandIdx(Reg, isKill, TRI); return (Idx == -1) ? NULL : &getOperand(Idx); } /// findRegisterDefOperandIdx() - Returns the operand index that is a def of /// the specified register or -1 if it is not found. If isDead is true, defs /// that are not dead are skipped. If Overlap is true, then it also looks for /// defs that merely overlap the specified register. If TargetRegisterInfo is /// non-null, then it also checks if there is a def of a super-register. int findRegisterDefOperandIdx(unsigned Reg, bool isDead = false, bool Overlap = false, const TargetRegisterInfo *TRI = NULL) const; /// findRegisterDefOperand - Wrapper for findRegisterDefOperandIdx, it returns /// a pointer to the MachineOperand rather than an index. MachineOperand *findRegisterDefOperand(unsigned Reg, bool isDead = false, const TargetRegisterInfo *TRI = NULL) { int Idx = findRegisterDefOperandIdx(Reg, isDead, false, TRI); return (Idx == -1) ? NULL : &getOperand(Idx); } /// findFirstPredOperandIdx() - Find the index of the first operand in the /// operand list that is used to represent the predicate. It returns -1 if /// none is found. int findFirstPredOperandIdx() const; /// isRegTiedToUseOperand - Given the index of a register def operand, /// check if the register def is tied to a source operand, due to either /// two-address elimination or inline assembly constraints. Returns the /// first tied use operand index by reference is UseOpIdx is not null. bool isRegTiedToUseOperand(unsigned DefOpIdx, unsigned *UseOpIdx = 0) const; /// isRegTiedToDefOperand - Return true if the use operand of the specified /// index is tied to an def operand. It also returns the def operand index by /// reference if DefOpIdx is not null. bool isRegTiedToDefOperand(unsigned UseOpIdx, unsigned *DefOpIdx = 0) const; /// clearKillInfo - Clears kill flags on all operands. /// void clearKillInfo(); /// copyKillDeadInfo - Copies kill / dead operand properties from MI. /// void copyKillDeadInfo(const MachineInstr *MI); /// copyPredicates - Copies predicate operand(s) from MI. void copyPredicates(const MachineInstr *MI); /// addRegisterKilled - We have determined MI kills a register. Look for the /// operand that uses it and mark it as IsKill. If AddIfNotFound is true, /// add a implicit operand if it's not found. Returns true if the operand /// exists / is added. bool addRegisterKilled(unsigned IncomingReg, const TargetRegisterInfo *RegInfo, bool AddIfNotFound = false); /// addRegisterDead - We have determined MI defined a register without a use. /// Look for the operand that defines it and mark it as IsDead. If /// AddIfNotFound is true, add a implicit operand if it's not found. Returns /// true if the operand exists / is added. bool addRegisterDead(unsigned IncomingReg, const TargetRegisterInfo *RegInfo, bool AddIfNotFound = false); /// addRegisterDefined - We have determined MI defines a register. Make sure /// there is an operand defining Reg. void addRegisterDefined(unsigned IncomingReg, const TargetRegisterInfo *RegInfo = 0); /// isSafeToMove - Return true if it is safe to move this instruction. If /// SawStore is set to true, it means that there is a store (or call) between /// the instruction's location and its intended destination. bool isSafeToMove(const TargetInstrInfo *TII, AliasAnalysis *AA, bool &SawStore) const; /// isSafeToReMat - Return true if it's safe to rematerialize the specified /// instruction which defined the specified register instead of copying it. bool isSafeToReMat(const TargetInstrInfo *TII, AliasAnalysis *AA, unsigned DstReg) const; /// hasVolatileMemoryRef - Return true if this instruction may have a /// volatile memory reference, or if the information describing the /// memory reference is not available. Return false if it is known to /// have no volatile memory references. bool hasVolatileMemoryRef() const; /// isInvariantLoad - Return true if this instruction is loading from a /// location whose value is invariant across the function. For example, /// loading a value from the constant pool or from the argument area of /// a function if it does not change. This should only return true of *all* /// loads the instruction does are invariant (if it does multiple loads). bool isInvariantLoad(AliasAnalysis *AA) const; /// isConstantValuePHI - If the specified instruction is a PHI that always /// merges together the same virtual register, return the register, otherwise /// return 0. unsigned isConstantValuePHI() const; /// allDefsAreDead - Return true if all the defs of this instruction are dead. /// bool allDefsAreDead() const; // // Debugging support // void print(raw_ostream &OS, const TargetMachine *TM = 0) const; void dump() const; //===--------------------------------------------------------------------===// // Accessors used to build up machine instructions. /// addOperand - Add the specified operand to the instruction. If it is an /// implicit operand, it is added to the end of the operand list. If it is /// an explicit operand it is added at the end of the explicit operand list /// (before the first implicit operand). void addOperand(const MachineOperand &Op); /// setDesc - Replace the instruction descriptor (thus opcode) of /// the current instruction with a new one. /// void setDesc(const TargetInstrDesc &tid) { TID = &tid; } /// setDebugLoc - Replace current source information with new such. /// Avoid using this, the constructor argument is preferable. /// void setDebugLoc(const DebugLoc dl) { debugLoc = dl; } /// RemoveOperand - Erase an operand from an instruction, leaving it with one /// fewer operand than it started with. /// void RemoveOperand(unsigned i); /// addMemOperand - Add a MachineMemOperand to the machine instruction. /// This function should be used only occasionally. The setMemRefs function /// is the primary method for setting up a MachineInstr's MemRefs list. void addMemOperand(MachineFunction &MF, MachineMemOperand *MO); /// setMemRefs - Assign this MachineInstr's memory reference descriptor /// list. This does not transfer ownership. void setMemRefs(mmo_iterator NewMemRefs, mmo_iterator NewMemRefsEnd) { MemRefs = NewMemRefs; MemRefsEnd = NewMemRefsEnd; } private: /// getRegInfo - If this instruction is embedded into a MachineFunction, /// return the MachineRegisterInfo object for the current function, otherwise /// return null. MachineRegisterInfo *getRegInfo(); /// addImplicitDefUseOperands - Add all implicit def and use operands to /// this instruction. void addImplicitDefUseOperands(); /// RemoveRegOperandsFromUseLists - Unlink all of the register operands in /// this instruction from their respective use lists. This requires that the /// operands already be on their use lists. void RemoveRegOperandsFromUseLists(); /// AddRegOperandsToUseLists - Add all of the register operands in /// this instruction from their respective use lists. This requires that the /// operands not be on their use lists yet. void AddRegOperandsToUseLists(MachineRegisterInfo &RegInfo); }; /// MachineInstrExpressionTrait - Special DenseMapInfo traits to compare /// MachineInstr* by *value* of the instruction rather than by pointer value. /// The hashing and equality testing functions ignore definitions so this is /// useful for CSE, etc. struct MachineInstrExpressionTrait : DenseMapInfo { static inline MachineInstr *getEmptyKey() { return 0; } static inline MachineInstr *getTombstoneKey() { return reinterpret_cast(-1); } static unsigned getHashValue(const MachineInstr* const &MI); static bool isEqual(const MachineInstr* const &LHS, const MachineInstr* const &RHS) { if (RHS == getEmptyKey() || RHS == getTombstoneKey() || LHS == getEmptyKey() || LHS == getTombstoneKey()) return LHS == RHS; return LHS->isIdenticalTo(RHS, MachineInstr::IgnoreVRegDefs); } }; //===----------------------------------------------------------------------===// // Debugging Support inline raw_ostream& operator<<(raw_ostream &OS, const MachineInstr &MI) { MI.print(OS); return OS; } } // End llvm namespace #endif