//===--- llvm/Analysis/DebugInfo.h - Debug Information Helpers --*- C++ -*-===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file defines a bunch of datatypes that are useful for creating and // walking debug info in LLVM IR form. They essentially provide wrappers around // the information in the global variables that's needed when constructing the // DWARF information. // //===----------------------------------------------------------------------===// #ifndef LLVM_DEBUGINFO_H #define LLVM_DEBUGINFO_H #include "llvm/ADT/SmallPtrSet.h" #include "llvm/ADT/SmallVector.h" #include "llvm/ADT/StringRef.h" #include "llvm/Support/Dwarf.h" namespace llvm { class BasicBlock; class Constant; class Function; class GlobalVariable; class Module; class Type; class Value; class DbgDeclareInst; class Instruction; class MDNode; class NamedMDNode; class LLVMContext; class raw_ostream; class DIFile; class DISubprogram; class DILexicalBlock; class DILexicalBlockFile; class DIVariable; class DIType; class DIObjCProperty; /// DIDescriptor - A thin wraper around MDNode to access encoded debug info. /// This should not be stored in a container, because the underlying MDNode /// may change in certain situations. class DIDescriptor { public: enum { FlagPrivate = 1 << 0, FlagProtected = 1 << 1, FlagFwdDecl = 1 << 2, FlagAppleBlock = 1 << 3, FlagBlockByrefStruct = 1 << 4, FlagVirtual = 1 << 5, FlagArtificial = 1 << 6, FlagExplicit = 1 << 7, FlagPrototyped = 1 << 8, FlagObjcClassComplete = 1 << 9, FlagObjectPointer = 1 << 10, FlagVector = 1 << 11, FlagStaticMember = 1 << 12 }; protected: const MDNode *DbgNode; StringRef getStringField(unsigned Elt) const; unsigned getUnsignedField(unsigned Elt) const { return (unsigned)getUInt64Field(Elt); } uint64_t getUInt64Field(unsigned Elt) const; int64_t getInt64Field(unsigned Elt) const; DIDescriptor getDescriptorField(unsigned Elt) const; template DescTy getFieldAs(unsigned Elt) const { return DescTy(getDescriptorField(Elt)); } GlobalVariable *getGlobalVariableField(unsigned Elt) const; Constant *getConstantField(unsigned Elt) const; Function *getFunctionField(unsigned Elt) const; void replaceFunctionField(unsigned Elt, Function *F); public: explicit DIDescriptor() : DbgNode(0) {} explicit DIDescriptor(const MDNode *N) : DbgNode(N) {} explicit DIDescriptor(const DIFile F); explicit DIDescriptor(const DISubprogram F); explicit DIDescriptor(const DILexicalBlockFile F); explicit DIDescriptor(const DILexicalBlock F); explicit DIDescriptor(const DIVariable F); explicit DIDescriptor(const DIType F); bool Verify() const; operator MDNode *() const { return const_cast(DbgNode); } MDNode *operator ->() const { return const_cast(DbgNode); } unsigned getTag() const { return getUnsignedField(0) & ~LLVMDebugVersionMask; } bool isDerivedType() const; bool isCompositeType() const; bool isBasicType() const; bool isVariable() const; bool isSubprogram() const; bool isGlobalVariable() const; bool isScope() const; bool isFile() const; bool isCompileUnit() const; bool isNameSpace() const; bool isLexicalBlockFile() const; bool isLexicalBlock() const; bool isSubrange() const; bool isEnumerator() const; bool isType() const; bool isGlobal() const; bool isUnspecifiedParameter() const; bool isTemplateTypeParameter() const; bool isTemplateValueParameter() const; bool isObjCProperty() const; /// print - print descriptor. void print(raw_ostream &OS) const; /// dump - print descriptor to dbgs() with a newline. void dump() const; }; /// DISubrange - This is used to represent ranges, for array bounds. class DISubrange : public DIDescriptor { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DISubrange(const MDNode *N = 0) : DIDescriptor(N) {} int64_t getLo() const { return getInt64Field(1); } int64_t getCount() const { return getInt64Field(2); } bool Verify() const; }; /// DIArray - This descriptor holds an array of descriptors. class DIArray : public DIDescriptor { public: explicit DIArray(const MDNode *N = 0) : DIDescriptor(N) {} unsigned getNumElements() const; DIDescriptor getElement(unsigned Idx) const { return getDescriptorField(Idx); } }; /// DIScope - A base class for various scopes. class DIScope : public DIDescriptor { protected: friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DIScope(const MDNode *N = 0) : DIDescriptor (N) {} StringRef getFilename() const; StringRef getDirectory() const; }; /// DIFile - This is a wrapper for a file. class DIFile : public DIScope { friend class DIDescriptor; public: explicit DIFile(const MDNode *N = 0) : DIScope(N) { if (DbgNode && !isFile()) DbgNode = 0; } MDNode *getFileNode() const; bool Verify() const; }; /// DICompileUnit - A wrapper for a compile unit. class DICompileUnit : public DIScope { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DICompileUnit(const MDNode *N = 0) : DIScope(N) {} unsigned getLanguage() const { return getUnsignedField(2); } StringRef getProducer() const { return getStringField(3); } bool isOptimized() const { return getUnsignedField(4) != 0; } StringRef getFlags() const { return getStringField(5); } unsigned getRunTimeVersion() const { return getUnsignedField(6); } DIArray getEnumTypes() const; DIArray getRetainedTypes() const; DIArray getSubprograms() const; DIArray getGlobalVariables() const; StringRef getSplitDebugFilename() const { return getStringField(11); } /// Verify - Verify that a compile unit is well formed. bool Verify() const; }; /// DIEnumerator - A wrapper for an enumerator (e.g. X and Y in 'enum {X,Y}'). /// FIXME: it seems strange that this doesn't have either a reference to the /// type/precision or a file/line pair for location info. class DIEnumerator : public DIDescriptor { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DIEnumerator(const MDNode *N = 0) : DIDescriptor(N) {} StringRef getName() const { return getStringField(1); } uint64_t getEnumValue() const { return getUInt64Field(2); } bool Verify() const; }; /// DIType - This is a wrapper for a type. /// FIXME: Types should be factored much better so that CV qualifiers and /// others do not require a huge and empty descriptor full of zeros. class DIType : public DIScope { protected: friend class DIDescriptor; void printInternal(raw_ostream &OS) const; // This ctor is used when the Tag has already been validated by a derived // ctor. DIType(const MDNode *N, bool, bool) : DIScope(N) {} public: /// Verify - Verify that a type descriptor is well formed. bool Verify() const; explicit DIType(const MDNode *N); explicit DIType() {} DIScope getContext() const { return getFieldAs(2); } StringRef getName() const { return getStringField(3); } unsigned getLineNumber() const { return getUnsignedField(4); } uint64_t getSizeInBits() const { return getUInt64Field(5); } uint64_t getAlignInBits() const { return getUInt64Field(6); } // FIXME: Offset is only used for DW_TAG_member nodes. Making every type // carry this is just plain insane. uint64_t getOffsetInBits() const { return getUInt64Field(7); } unsigned getFlags() const { return getUnsignedField(8); } bool isPrivate() const { return (getFlags() & FlagPrivate) != 0; } bool isProtected() const { return (getFlags() & FlagProtected) != 0; } bool isForwardDecl() const { return (getFlags() & FlagFwdDecl) != 0; } // isAppleBlock - Return true if this is the Apple Blocks extension. bool isAppleBlockExtension() const { return (getFlags() & FlagAppleBlock) != 0; } bool isBlockByrefStruct() const { return (getFlags() & FlagBlockByrefStruct) != 0; } bool isVirtual() const { return (getFlags() & FlagVirtual) != 0; } bool isArtificial() const { return (getFlags() & FlagArtificial) != 0; } bool isObjectPointer() const { return (getFlags() & FlagObjectPointer) != 0; } bool isObjcClassComplete() const { return (getFlags() & FlagObjcClassComplete) != 0; } bool isVector() const { return (getFlags() & FlagVector) != 0; } bool isStaticMember() const { return (getFlags() & FlagStaticMember) != 0; } bool isValid() const { return DbgNode && (isBasicType() || isDerivedType() || isCompositeType()); } /// isUnsignedDIType - Return true if type encoding is unsigned. bool isUnsignedDIType(); /// replaceAllUsesWith - Replace all uses of debug info referenced by /// this descriptor. void replaceAllUsesWith(DIDescriptor &D); void replaceAllUsesWith(MDNode *D); }; /// DIBasicType - A basic type, like 'int' or 'float'. class DIBasicType : public DIType { public: explicit DIBasicType(const MDNode *N = 0) : DIType(N) {} unsigned getEncoding() const { return getUnsignedField(9); } /// Verify - Verify that a basic type descriptor is well formed. bool Verify() const; }; /// DIDerivedType - A simple derived type, like a const qualified type, /// a typedef, a pointer or reference, et cetera. Or, a data member of /// a class/struct/union. class DIDerivedType : public DIType { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; protected: explicit DIDerivedType(const MDNode *N, bool, bool) : DIType(N, true, true) {} public: explicit DIDerivedType(const MDNode *N = 0) : DIType(N, true, true) {} DIType getTypeDerivedFrom() const { return getFieldAs(9); } /// getOriginalTypeSize - If this type is derived from a base type then /// return base type size. uint64_t getOriginalTypeSize() const; /// getObjCProperty - Return property node, if this ivar is /// associated with one. MDNode *getObjCProperty() const; DIType getClassType() const { assert(getTag() == dwarf::DW_TAG_ptr_to_member_type); return getFieldAs(10); } Constant *getConstant() const { assert((getTag() == dwarf::DW_TAG_member) && isStaticMember()); return getConstantField(10); } /// Verify - Verify that a derived type descriptor is well formed. bool Verify() const; }; /// DICompositeType - This descriptor holds a type that can refer to multiple /// other types, like a function or struct. /// FIXME: Why is this a DIDerivedType?? class DICompositeType : public DIDerivedType { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DICompositeType(const MDNode *N = 0) : DIDerivedType(N, true, true) { if (N && !isCompositeType()) DbgNode = 0; } DIArray getTypeArray() const { return getFieldAs(10); } unsigned getRunTimeLang() const { return getUnsignedField(11); } DICompositeType getContainingType() const { return getFieldAs(12); } DIArray getTemplateParams() const { return getFieldAs(13); } /// Verify - Verify that a composite type descriptor is well formed. bool Verify() const; }; /// DITemplateTypeParameter - This is a wrapper for template type parameter. class DITemplateTypeParameter : public DIDescriptor { public: explicit DITemplateTypeParameter(const MDNode *N = 0) : DIDescriptor(N) {} DIScope getContext() const { return getFieldAs(1); } StringRef getName() const { return getStringField(2); } DIType getType() const { return getFieldAs(3); } StringRef getFilename() const { return getFieldAs(4).getFilename(); } StringRef getDirectory() const { return getFieldAs(4).getDirectory(); } unsigned getLineNumber() const { return getUnsignedField(5); } unsigned getColumnNumber() const { return getUnsignedField(6); } bool Verify() const; }; /// DITemplateValueParameter - This is a wrapper for template value parameter. class DITemplateValueParameter : public DIDescriptor { public: explicit DITemplateValueParameter(const MDNode *N = 0) : DIDescriptor(N) {} DIScope getContext() const { return getFieldAs(1); } StringRef getName() const { return getStringField(2); } DIType getType() const { return getFieldAs(3); } uint64_t getValue() const { return getUInt64Field(4); } StringRef getFilename() const { return getFieldAs(5).getFilename(); } StringRef getDirectory() const { return getFieldAs(5).getDirectory(); } unsigned getLineNumber() const { return getUnsignedField(6); } unsigned getColumnNumber() const { return getUnsignedField(7); } bool Verify() const; }; /// DISubprogram - This is a wrapper for a subprogram (e.g. a function). class DISubprogram : public DIScope { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DISubprogram(const MDNode *N = 0) : DIScope(N) {} DIScope getContext() const { return getFieldAs(2); } StringRef getName() const { return getStringField(3); } StringRef getDisplayName() const { return getStringField(4); } StringRef getLinkageName() const { return getStringField(5); } unsigned getLineNumber() const { return getUnsignedField(6); } DICompositeType getType() const { return getFieldAs(7); } /// getReturnTypeName - Subprogram return types are encoded either as /// DIType or as DICompositeType. StringRef getReturnTypeName() const { DICompositeType DCT(getFieldAs(7)); if (DCT.Verify()) { DIArray A = DCT.getTypeArray(); DIType T(A.getElement(0)); return T.getName(); } DIType T(getFieldAs(7)); return T.getName(); } /// isLocalToUnit - Return true if this subprogram is local to the current /// compile unit, like 'static' in C. unsigned isLocalToUnit() const { return getUnsignedField(8); } unsigned isDefinition() const { return getUnsignedField(9); } unsigned getVirtuality() const { return getUnsignedField(10); } unsigned getVirtualIndex() const { return getUnsignedField(11); } DICompositeType getContainingType() const { return getFieldAs(12); } unsigned getFlags() const { return getUnsignedField(13); } unsigned isArtificial() const { return (getUnsignedField(13) & FlagArtificial) != 0; } /// isPrivate - Return true if this subprogram has "private" /// access specifier. bool isPrivate() const { return (getUnsignedField(13) & FlagPrivate) != 0; } /// isProtected - Return true if this subprogram has "protected" /// access specifier. bool isProtected() const { return (getUnsignedField(13) & FlagProtected) != 0; } /// isExplicit - Return true if this subprogram is marked as explicit. bool isExplicit() const { return (getUnsignedField(13) & FlagExplicit) != 0; } /// isPrototyped - Return true if this subprogram is prototyped. bool isPrototyped() const { return (getUnsignedField(13) & FlagPrototyped) != 0; } unsigned isOptimized() const; /// getScopeLineNumber - Get the beginning of the scope of the /// function, not necessarily where the name of the program /// starts. unsigned getScopeLineNumber() const { return getUnsignedField(19); } /// Verify - Verify that a subprogram descriptor is well formed. bool Verify() const; /// describes - Return true if this subprogram provides debugging /// information for the function F. bool describes(const Function *F); Function *getFunction() const { return getFunctionField(15); } void replaceFunction(Function *F) { replaceFunctionField(15, F); } DIArray getTemplateParams() const { return getFieldAs(16); } DISubprogram getFunctionDeclaration() const { return getFieldAs(17); } MDNode *getVariablesNodes() const; DIArray getVariables() const; }; /// DIGlobalVariable - This is a wrapper for a global variable. class DIGlobalVariable : public DIDescriptor { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DIGlobalVariable(const MDNode *N = 0) : DIDescriptor(N) {} DIScope getContext() const { return getFieldAs(2); } StringRef getName() const { return getStringField(3); } StringRef getDisplayName() const { return getStringField(4); } StringRef getLinkageName() const { return getStringField(5); } StringRef getFilename() const { return getFieldAs(6).getFilename(); } StringRef getDirectory() const { return getFieldAs(6).getDirectory(); } unsigned getLineNumber() const { return getUnsignedField(7); } DIType getType() const { return getFieldAs(8); } unsigned isLocalToUnit() const { return getUnsignedField(9); } unsigned isDefinition() const { return getUnsignedField(10); } GlobalVariable *getGlobal() const { return getGlobalVariableField(11); } Constant *getConstant() const { return getConstantField(11); } DIDerivedType getStaticDataMemberDeclaration() const { return getFieldAs(12); } /// Verify - Verify that a global variable descriptor is well formed. bool Verify() const; }; /// DIVariable - This is a wrapper for a variable (e.g. parameter, local, /// global etc). class DIVariable : public DIDescriptor { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DIVariable(const MDNode *N = 0) : DIDescriptor(N) {} DIScope getContext() const { return getFieldAs(1); } StringRef getName() const { return getStringField(2); } DIFile getFile() const { return getFieldAs(3); } unsigned getLineNumber() const { return (getUnsignedField(4) << 8) >> 8; } unsigned getArgNumber() const { unsigned L = getUnsignedField(4); return L >> 24; } DIType getType() const { return getFieldAs(5); } /// isArtificial - Return true if this variable is marked as "artificial". bool isArtificial() const { return (getUnsignedField(6) & FlagArtificial) != 0; } bool isObjectPointer() const { return (getUnsignedField(6) & FlagObjectPointer) != 0; } /// getInlinedAt - If this variable is inlined then return inline location. MDNode *getInlinedAt() const; /// Verify - Verify that a variable descriptor is well formed. bool Verify() const; /// HasComplexAddr - Return true if the variable has a complex address. bool hasComplexAddress() const { return getNumAddrElements() > 0; } unsigned getNumAddrElements() const; uint64_t getAddrElement(unsigned Idx) const { return getUInt64Field(Idx+8); } /// isBlockByrefVariable - Return true if the variable was declared as /// a "__block" variable (Apple Blocks). bool isBlockByrefVariable() const { return getType().isBlockByrefStruct(); } /// isInlinedFnArgument - Return true if this variable provides debugging /// information for an inlined function arguments. bool isInlinedFnArgument(const Function *CurFn); void printExtendedName(raw_ostream &OS) const; }; /// DILexicalBlock - This is a wrapper for a lexical block. class DILexicalBlock : public DIScope { public: explicit DILexicalBlock(const MDNode *N = 0) : DIScope(N) {} DIScope getContext() const { return getFieldAs(2); } unsigned getLineNumber() const { return getUnsignedField(3); } unsigned getColumnNumber() const { return getUnsignedField(4); } bool Verify() const; }; /// DILexicalBlockFile - This is a wrapper for a lexical block with /// a filename change. class DILexicalBlockFile : public DIScope { public: explicit DILexicalBlockFile(const MDNode *N = 0) : DIScope(N) {} DIScope getContext() const { if (getScope().isSubprogram()) return getScope(); return getScope().getContext(); } unsigned getLineNumber() const { return getScope().getLineNumber(); } unsigned getColumnNumber() const { return getScope().getColumnNumber(); } StringRef getDirectory() const { return getFieldAs(2).getDirectory(); } StringRef getFilename() const { return getFieldAs(2).getFilename(); } DILexicalBlock getScope() const { return getFieldAs(1); } bool Verify() const; }; /// DINameSpace - A wrapper for a C++ style name space. class DINameSpace : public DIScope { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DINameSpace(const MDNode *N = 0) : DIScope(N) {} DIScope getContext() const { return getFieldAs(2); } StringRef getName() const { return getStringField(3); } unsigned getLineNumber() const { return getUnsignedField(4); } bool Verify() const; }; /// DILocation - This object holds location information. This object /// is not associated with any DWARF tag. class DILocation : public DIDescriptor { public: explicit DILocation(const MDNode *N) : DIDescriptor(N) { } unsigned getLineNumber() const { return getUnsignedField(0); } unsigned getColumnNumber() const { return getUnsignedField(1); } DIScope getScope() const { return getFieldAs(2); } DILocation getOrigLocation() const { return getFieldAs(3); } StringRef getFilename() const { return getScope().getFilename(); } StringRef getDirectory() const { return getScope().getDirectory(); } bool Verify() const; }; class DIObjCProperty : public DIDescriptor { friend class DIDescriptor; void printInternal(raw_ostream &OS) const; public: explicit DIObjCProperty(const MDNode *N) : DIDescriptor(N) { } StringRef getObjCPropertyName() const { return getStringField(1); } DIFile getFile() const { return getFieldAs(2); } unsigned getLineNumber() const { return getUnsignedField(3); } StringRef getObjCPropertyGetterName() const { return getStringField(4); } StringRef getObjCPropertySetterName() const { return getStringField(5); } bool isReadOnlyObjCProperty() { return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_readonly) != 0; } bool isReadWriteObjCProperty() { return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_readwrite) != 0; } bool isAssignObjCProperty() { return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_assign) != 0; } bool isRetainObjCProperty() { return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_retain) != 0; } bool isCopyObjCProperty() { return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_copy) != 0; } bool isNonAtomicObjCProperty() { return (getUnsignedField(6) & dwarf::DW_APPLE_PROPERTY_nonatomic) != 0; } DIType getType() const { return getFieldAs(7); } /// Verify - Verify that a derived type descriptor is well formed. bool Verify() const; }; /// getDISubprogram - Find subprogram that is enclosing this scope. DISubprogram getDISubprogram(const MDNode *Scope); /// getDICompositeType - Find underlying composite type. DICompositeType getDICompositeType(DIType T); /// isSubprogramContext - Return true if Context is either a subprogram /// or another context nested inside a subprogram. bool isSubprogramContext(const MDNode *Context); /// getOrInsertFnSpecificMDNode - Return a NameMDNode that is suitable /// to hold function specific information. NamedMDNode *getOrInsertFnSpecificMDNode(Module &M, DISubprogram SP); /// getFnSpecificMDNode - Return a NameMDNode, if available, that is /// suitable to hold function specific information. NamedMDNode *getFnSpecificMDNode(const Module &M, DISubprogram SP); /// createInlinedVariable - Create a new inlined variable based on current /// variable. /// @param DV Current Variable. /// @param InlinedScope Location at current variable is inlined. DIVariable createInlinedVariable(MDNode *DV, MDNode *InlinedScope, LLVMContext &VMContext); /// cleanseInlinedVariable - Remove inlined scope from the variable. DIVariable cleanseInlinedVariable(MDNode *DV, LLVMContext &VMContext); class DebugInfoFinder { public: /// processModule - Process entire module and collect debug info /// anchors. void processModule(const Module &M); private: /// processType - Process DIType. void processType(DIType DT); /// processLexicalBlock - Process DILexicalBlock. void processLexicalBlock(DILexicalBlock LB); /// processSubprogram - Process DISubprogram. void processSubprogram(DISubprogram SP); /// processDeclare - Process DbgDeclareInst. void processDeclare(const DbgDeclareInst *DDI); /// processLocation - Process DILocation. void processLocation(DILocation Loc); /// addCompileUnit - Add compile unit into CUs. bool addCompileUnit(DICompileUnit CU); /// addGlobalVariable - Add global variable into GVs. bool addGlobalVariable(DIGlobalVariable DIG); // addSubprogram - Add subprogram into SPs. bool addSubprogram(DISubprogram SP); /// addType - Add type into Tys. bool addType(DIType DT); public: typedef SmallVector::const_iterator iterator; iterator compile_unit_begin() const { return CUs.begin(); } iterator compile_unit_end() const { return CUs.end(); } iterator subprogram_begin() const { return SPs.begin(); } iterator subprogram_end() const { return SPs.end(); } iterator global_variable_begin() const { return GVs.begin(); } iterator global_variable_end() const { return GVs.end(); } iterator type_begin() const { return TYs.begin(); } iterator type_end() const { return TYs.end(); } unsigned compile_unit_count() const { return CUs.size(); } unsigned global_variable_count() const { return GVs.size(); } unsigned subprogram_count() const { return SPs.size(); } unsigned type_count() const { return TYs.size(); } private: SmallVector CUs; // Compile Units SmallVector SPs; // Subprograms SmallVector GVs; // Global Variables; SmallVector TYs; // Types SmallPtrSet NodesSeen; }; } // end namespace llvm #endif