//===-- llvm/Metadata.h - Metadata definitions ------------------*- C++ -*-===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // /// @file /// This file contains the declarations for metadata subclasses. /// They represent the different flavors of metadata that live in LLVM. // //===----------------------------------------------------------------------===// #ifndef LLVM_IR_METADATA_H #define LLVM_IR_METADATA_H #include "llvm/ADT/ArrayRef.h" #include "llvm/ADT/DenseMap.h" #include "llvm/ADT/FoldingSet.h" #include "llvm/ADT/ilist_node.h" #include "llvm/ADT/iterator_range.h" #include "llvm/IR/Value.h" namespace llvm { class LLVMContext; class Module; template class SymbolTableListTraits; enum LLVMConstants : uint32_t { DEBUG_METADATA_VERSION = 2 // Current debug info version number. }; //===----------------------------------------------------------------------===// /// \brief A single uniqued string. /// /// These are used to efficiently contain a byte sequence for metadata. /// MDString is always unnamed. class MDString : public Value { virtual void anchor(); MDString(const MDString &) LLVM_DELETED_FUNCTION; explicit MDString(LLVMContext &C); public: static MDString *get(LLVMContext &Context, StringRef Str); static MDString *get(LLVMContext &Context, const char *Str) { return get(Context, Str ? StringRef(Str) : StringRef()); } StringRef getString() const { return getName(); } unsigned getLength() const { return (unsigned)getName().size(); } typedef StringRef::iterator iterator; /// \brief Pointer to the first byte of the string. iterator begin() const { return getName().begin(); } /// \brief Pointer to one byte past the end of the string. iterator end() const { return getName().end(); } /// \brief Methods for support type inquiry through isa, cast, and dyn_cast. static bool classof(const Value *V) { return V->getValueID() == MDStringVal; } }; /// \brief A collection of metadata nodes that might be associated with a /// memory access used by the alias-analysis infrastructure. struct AAMDNodes { explicit AAMDNodes(MDNode *T = nullptr, MDNode *S = nullptr, MDNode *N = nullptr) : TBAA(T), Scope(S), NoAlias(N) {} bool operator==(const AAMDNodes &A) const { return TBAA == A.TBAA && Scope == A.Scope && NoAlias == A.NoAlias; } bool operator!=(const AAMDNodes &A) const { return !(*this == A); } LLVM_EXPLICIT operator bool() const { return TBAA || Scope || NoAlias; } /// \brief The tag for type-based alias analysis. MDNode *TBAA; /// \brief The tag for alias scope specification (used with noalias). MDNode *Scope; /// \brief The tag specifying the noalias scope. MDNode *NoAlias; }; // Specialize DenseMapInfo for AAMDNodes. template<> struct DenseMapInfo { static inline AAMDNodes getEmptyKey() { return AAMDNodes(DenseMapInfo::getEmptyKey(), 0, 0); } static inline AAMDNodes getTombstoneKey() { return AAMDNodes(DenseMapInfo::getTombstoneKey(), 0, 0); } static unsigned getHashValue(const AAMDNodes &Val) { return DenseMapInfo::getHashValue(Val.TBAA) ^ DenseMapInfo::getHashValue(Val.Scope) ^ DenseMapInfo::getHashValue(Val.NoAlias); } static bool isEqual(const AAMDNodes &LHS, const AAMDNodes &RHS) { return LHS == RHS; } }; class MDNodeOperand; //===----------------------------------------------------------------------===// /// \brief A tuple of other values. class MDNode : public Value, public FoldingSetNode { MDNode(const MDNode &) LLVM_DELETED_FUNCTION; void operator=(const MDNode &) LLVM_DELETED_FUNCTION; friend class MDNodeOperand; friend class LLVMContextImpl; friend struct FoldingSetTrait; /// \brief If the MDNode is uniqued cache the hash to speed up lookup. unsigned Hash; /// \brief Subclass data enums. enum { /// FunctionLocalBit - This bit is set if this MDNode is function local. /// This is true when it (potentially transitively) contains a reference to /// something in a function, like an argument, basicblock, or instruction. FunctionLocalBit = 1 << 0, /// NotUniquedBit - This is set on MDNodes that are not uniqued because they /// have a null operand. NotUniquedBit = 1 << 1, /// DestroyFlag - This bit is set by destroy() so the destructor can assert /// that the node isn't being destroyed with a plain 'delete'. DestroyFlag = 1 << 2 }; /// \brief FunctionLocal enums. enum FunctionLocalness { FL_Unknown = -1, FL_No = 0, FL_Yes = 1 }; /// \brief Replace each instance of the given operand with a new value. void replaceOperand(MDNodeOperand *Op, Value *NewVal); ~MDNode(); MDNode(LLVMContext &C, ArrayRef Vals, bool isFunctionLocal); static MDNode *getMDNode(LLVMContext &C, ArrayRef Vals, FunctionLocalness FL, bool Insert = true); public: static MDNode *get(LLVMContext &Context, ArrayRef Vals); /// \brief Construct MDNode with an explicit function-localness. /// /// Don't analyze Vals; trust isFunctionLocal. static MDNode *getWhenValsUnresolved(LLVMContext &Context, ArrayRef Vals, bool isFunctionLocal); static MDNode *getIfExists(LLVMContext &Context, ArrayRef Vals); /// \brief Return a temporary MDNode /// /// For use in constructing cyclic MDNode structures. A temporary MDNode is /// not uniqued, may be RAUW'd, and must be manually deleted with /// deleteTemporary. static MDNode *getTemporary(LLVMContext &Context, ArrayRef Vals); /// \brief Deallocate a node created by getTemporary. /// /// The node must not have any users. static void deleteTemporary(MDNode *N); /// \brief Replace a specific operand. void replaceOperandWith(unsigned i, Value *NewVal); /// \brief Return specified operand. Value *getOperand(unsigned i) const LLVM_READONLY; /// \brief Return number of MDNode operands. unsigned getNumOperands() const { return NumOperands; } /// \brief Return whether MDNode is local to a function. bool isFunctionLocal() const { return (getSubclassDataFromValue() & FunctionLocalBit) != 0; } /// \brief Return the first function-local operand's function. /// /// If this metadata is function-local and recursively has a function-local /// operand, return the first such operand's parent function. Otherwise, /// return null. getFunction() should not be used for performance- critical /// code because it recursively visits all the MDNode's operands. const Function *getFunction() const; /// \brief Calculate a unique identifier for this MDNode. void Profile(FoldingSetNodeID &ID) const; /// \brief Methods for support type inquiry through isa, cast, and dyn_cast: static bool classof(const Value *V) { return V->getValueID() == MDNodeVal; } /// \brief Check whether MDNode is a vtable access. bool isTBAAVtableAccess() const; /// \brief Methods for metadata merging. static MDNode *concatenate(MDNode *A, MDNode *B); static MDNode *intersect(MDNode *A, MDNode *B); static MDNode *getMostGenericTBAA(MDNode *A, MDNode *B); static AAMDNodes getMostGenericAA(const AAMDNodes &A, const AAMDNodes &B); static MDNode *getMostGenericFPMath(MDNode *A, MDNode *B); static MDNode *getMostGenericRange(MDNode *A, MDNode *B); private: /// \brief Delete this node. Only when there are no uses. void destroy(); bool isNotUniqued() const { return (getSubclassDataFromValue() & NotUniquedBit) != 0; } void setIsNotUniqued(); // Shadow Value::setValueSubclassData with a private forwarding method so that // any future subclasses cannot accidentally use it. void setValueSubclassData(unsigned short D) { Value::setValueSubclassData(D); } }; //===----------------------------------------------------------------------===// /// \brief A tuple of MDNodes. /// /// Despite its name, a NamedMDNode isn't itself an MDNode. NamedMDNodes belong /// to modules, have names, and contain lists of MDNodes. class NamedMDNode : public ilist_node { friend class SymbolTableListTraits; friend struct ilist_traits; friend class LLVMContextImpl; friend class Module; NamedMDNode(const NamedMDNode &) LLVM_DELETED_FUNCTION; std::string Name; Module *Parent; void *Operands; // SmallVector, 4> void setParent(Module *M) { Parent = M; } explicit NamedMDNode(const Twine &N); template class op_iterator_impl : public std::iterator { const NamedMDNode *Node; unsigned Idx; op_iterator_impl(const NamedMDNode *N, unsigned i) : Node(N), Idx(i) { } friend class NamedMDNode; public: op_iterator_impl() : Node(nullptr), Idx(0) { } bool operator==(const op_iterator_impl &o) const { return Idx == o.Idx; } bool operator!=(const op_iterator_impl &o) const { return Idx != o.Idx; } op_iterator_impl &operator++() { ++Idx; return *this; } op_iterator_impl operator++(int) { op_iterator_impl tmp(*this); operator++(); return tmp; } op_iterator_impl &operator--() { --Idx; return *this; } op_iterator_impl operator--(int) { op_iterator_impl tmp(*this); operator--(); return tmp; } T1 operator*() const { return Node->getOperand(Idx); } }; public: /// \brief Drop all references and remove the node from parent module. void eraseFromParent(); /// \brief Remove all uses and clear node vector. void dropAllReferences(); ~NamedMDNode(); /// \brief Get the module that holds this named metadata collection. inline Module *getParent() { return Parent; } inline const Module *getParent() const { return Parent; } MDNode *getOperand(unsigned i) const; unsigned getNumOperands() const; void addOperand(Value *M); StringRef getName() const; void print(raw_ostream &ROS) const; void dump() const; // --------------------------------------------------------------------------- // Operand Iterator interface... // typedef op_iterator_impl op_iterator; op_iterator op_begin() { return op_iterator(this, 0); } op_iterator op_end() { return op_iterator(this, getNumOperands()); } typedef op_iterator_impl const_op_iterator; const_op_iterator op_begin() const { return const_op_iterator(this, 0); } const_op_iterator op_end() const { return const_op_iterator(this, getNumOperands()); } inline iterator_range operands() { return iterator_range(op_begin(), op_end()); } inline iterator_range operands() const { return iterator_range(op_begin(), op_end()); } }; } // end llvm namespace #endif