//=- llvm/CodeGen/AggressiveAntiDepBreaker.h - Anti-Dep Support -*- C++ -*-=// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the AggressiveAntiDepBreaker class, which // implements register anti-dependence breaking during post-RA // scheduling. It attempts to break all anti-dependencies within a // block. // //===----------------------------------------------------------------------===// #ifndef LLVM_CODEGEN_AGGRESSIVEANTIDEPBREAKER_H #define LLVM_CODEGEN_AGGRESSIVEANTIDEPBREAKER_H #include "AntiDepBreaker.h" #include "llvm/ADT/BitVector.h" #include "llvm/ADT/SmallSet.h" #include "llvm/CodeGen/MachineBasicBlock.h" #include "llvm/CodeGen/MachineFrameInfo.h" #include "llvm/CodeGen/MachineFunction.h" #include "llvm/CodeGen/MachineRegisterInfo.h" #include "llvm/CodeGen/ScheduleDAG.h" #include "llvm/Target/TargetRegisterInfo.h" #include "llvm/Target/TargetSubtargetInfo.h" #include namespace llvm { class RegisterClassInfo; /// Class AggressiveAntiDepState /// Contains all the state necessary for anti-dep breaking. class AggressiveAntiDepState { public: /// RegisterReference - Information about a register reference /// within a liverange typedef struct { /// Operand - The registers operand MachineOperand *Operand; /// RC - The register class const TargetRegisterClass *RC; } RegisterReference; private: /// NumTargetRegs - Number of non-virtual target registers /// (i.e. TRI->getNumRegs()). const unsigned NumTargetRegs; /// GroupNodes - Implements a disjoint-union data structure to /// form register groups. A node is represented by an index into /// the vector. A node can "point to" itself to indicate that it /// is the parent of a group, or point to another node to indicate /// that it is a member of the same group as that node. std::vector GroupNodes; /// GroupNodeIndices - For each register, the index of the GroupNode /// currently representing the group that the register belongs to. /// Register 0 is always represented by the 0 group, a group /// composed of registers that are not eligible for anti-aliasing. std::vector GroupNodeIndices; /// RegRefs - Map registers to all their references within a live range. std::multimap RegRefs; /// KillIndices - The index of the most recent kill (proceding bottom-up), /// or ~0u if the register is not live. std::vector KillIndices; /// DefIndices - The index of the most recent complete def (proceding bottom /// up), or ~0u if the register is live. std::vector DefIndices; public: AggressiveAntiDepState(const unsigned TargetRegs, MachineBasicBlock *BB); /// GetKillIndices - Return the kill indices. std::vector &GetKillIndices() { return KillIndices; } /// GetDefIndices - Return the define indices. std::vector &GetDefIndices() { return DefIndices; } /// GetRegRefs - Return the RegRefs map. std::multimap& GetRegRefs() { return RegRefs; } // GetGroup - Get the group for a register. The returned value is // the index of the GroupNode representing the group. unsigned GetGroup(unsigned Reg); // GetGroupRegs - Return a vector of the registers belonging to a // group. If RegRefs is non-NULL then only included referenced registers. void GetGroupRegs( unsigned Group, std::vector &Regs, std::multimap *RegRefs); // UnionGroups - Union Reg1's and Reg2's groups to form a new // group. Return the index of the GroupNode representing the // group. unsigned UnionGroups(unsigned Reg1, unsigned Reg2); // LeaveGroup - Remove a register from its current group and place // it alone in its own group. Return the index of the GroupNode // representing the registers new group. unsigned LeaveGroup(unsigned Reg); /// IsLive - Return true if Reg is live bool IsLive(unsigned Reg); }; /// Class AggressiveAntiDepBreaker class AggressiveAntiDepBreaker : public AntiDepBreaker { MachineFunction& MF; MachineRegisterInfo &MRI; const TargetInstrInfo *TII; const TargetRegisterInfo *TRI; const RegisterClassInfo &RegClassInfo; /// CriticalPathSet - The set of registers that should only be /// renamed if they are on the critical path. BitVector CriticalPathSet; /// State - The state used to identify and rename anti-dependence /// registers. AggressiveAntiDepState *State; public: AggressiveAntiDepBreaker(MachineFunction& MFi, const RegisterClassInfo &RCI, TargetSubtargetInfo::RegClassVector& CriticalPathRCs); ~AggressiveAntiDepBreaker(); /// Start - Initialize anti-dep breaking for a new basic block. void StartBlock(MachineBasicBlock *BB) override; /// BreakAntiDependencies - Identifiy anti-dependencies along the critical /// path /// of the ScheduleDAG and break them by renaming registers. /// unsigned BreakAntiDependencies(const std::vector& SUnits, MachineBasicBlock::iterator Begin, MachineBasicBlock::iterator End, unsigned InsertPosIndex, DbgValueVector &DbgValues) override; /// Observe - Update liveness information to account for the current /// instruction, which will not be scheduled. /// void Observe(MachineInstr *MI, unsigned Count, unsigned InsertPosIndex) override; /// Finish - Finish anti-dep breaking for a basic block. void FinishBlock() override; private: /// Keep track of a position in the allocation order for each regclass. typedef std::map RenameOrderType; /// IsImplicitDefUse - Return true if MO represents a register /// that is both implicitly used and defined in MI bool IsImplicitDefUse(MachineInstr *MI, MachineOperand& MO); /// GetPassthruRegs - If MI implicitly def/uses a register, then /// return that register and all subregisters. void GetPassthruRegs(MachineInstr *MI, std::set& PassthruRegs); void HandleLastUse(unsigned Reg, unsigned KillIdx, const char *tag, const char *header = nullptr, const char *footer = nullptr); void PrescanInstruction(MachineInstr *MI, unsigned Count, std::set& PassthruRegs); void ScanInstruction(MachineInstr *MI, unsigned Count); BitVector GetRenameRegisters(unsigned Reg); bool FindSuitableFreeRegisters(unsigned AntiDepGroupIndex, RenameOrderType& RenameOrder, std::map &RenameMap); }; } #endif