//===-- AsmPrinterDwarf.cpp - AsmPrinter Dwarf Support --------------------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the Dwarf emissions parts of AsmPrinter. // //===----------------------------------------------------------------------===// #include "ByteStreamer.h" #include "DwarfExpression.h" #include "llvm/CodeGen/AsmPrinter.h" #include "llvm/ADT/Twine.h" #include "llvm/IR/DataLayout.h" #include "llvm/MC/MCAsmInfo.h" #include "llvm/MC/MCSection.h" #include "llvm/MC/MCStreamer.h" #include "llvm/MC/MCSymbol.h" #include "llvm/MC/MachineLocation.h" #include "llvm/Support/Dwarf.h" #include "llvm/Support/ErrorHandling.h" #include "llvm/Target/TargetFrameLowering.h" #include "llvm/Target/TargetLoweringObjectFile.h" #include "llvm/Target/TargetMachine.h" #include "llvm/Target/TargetRegisterInfo.h" #include "llvm/Target/TargetSubtargetInfo.h" using namespace llvm; #define DEBUG_TYPE "asm-printer" /// DwarfExpression implementation for .debug_loc entries. class DebugLocDwarfExpression : public DwarfExpression { ByteStreamer &BS; public: DebugLocDwarfExpression(TargetMachine &TM, ByteStreamer &BS) : DwarfExpression(TM), BS(BS) {} void EmitOp(uint8_t Op, const char* Comment) override; void EmitSigned(int Value) override; void EmitUnsigned(unsigned Value) override; unsigned getFrameRegister() override { llvm_unreachable("not available"); }; }; void DebugLocDwarfExpression::EmitOp(uint8_t Op, const char* Comment) { BS.EmitInt8(Op, Comment ? Twine(Comment)+Twine(" ")+Twine(dwarf::OperationEncodingString(Op)) : dwarf::OperationEncodingString(Op)); } void DebugLocDwarfExpression::EmitSigned(int Value) { BS.EmitSLEB128(Value, Twine(Value)); } void DebugLocDwarfExpression::EmitUnsigned(unsigned Value) { BS.EmitULEB128(Value, Twine(Value)); } //===----------------------------------------------------------------------===// // Dwarf Emission Helper Routines //===----------------------------------------------------------------------===// /// EmitSLEB128 - emit the specified signed leb128 value. void AsmPrinter::EmitSLEB128(int64_t Value, const char *Desc) const { if (isVerbose() && Desc) OutStreamer.AddComment(Desc); OutStreamer.EmitSLEB128IntValue(Value); } /// EmitULEB128 - emit the specified signed leb128 value. void AsmPrinter::EmitULEB128(uint64_t Value, const char *Desc, unsigned PadTo) const { if (isVerbose() && Desc) OutStreamer.AddComment(Desc); OutStreamer.EmitULEB128IntValue(Value, PadTo); } /// EmitCFAByte - Emit a .byte 42 directive for a DW_CFA_xxx value. void AsmPrinter::EmitCFAByte(unsigned Val) const { if (isVerbose()) { if (Val >= dwarf::DW_CFA_offset && Val < dwarf::DW_CFA_offset + 64) OutStreamer.AddComment("DW_CFA_offset + Reg (" + Twine(Val - dwarf::DW_CFA_offset) + ")"); else OutStreamer.AddComment(dwarf::CallFrameString(Val)); } OutStreamer.EmitIntValue(Val, 1); } static const char *DecodeDWARFEncoding(unsigned Encoding) { switch (Encoding) { case dwarf::DW_EH_PE_absptr: return "absptr"; case dwarf::DW_EH_PE_omit: return "omit"; case dwarf::DW_EH_PE_pcrel: return "pcrel"; case dwarf::DW_EH_PE_udata4: return "udata4"; case dwarf::DW_EH_PE_udata8: return "udata8"; case dwarf::DW_EH_PE_sdata4: return "sdata4"; case dwarf::DW_EH_PE_sdata8: return "sdata8"; case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata4: return "pcrel udata4"; case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata4: return "pcrel sdata4"; case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata8: return "pcrel udata8"; case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata8: return "pcrel sdata8"; case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata4 : return "indirect pcrel udata4"; case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata4 : return "indirect pcrel sdata4"; case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata8 : return "indirect pcrel udata8"; case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata8 : return "indirect pcrel sdata8"; } return ""; } /// EmitEncodingByte - Emit a .byte 42 directive that corresponds to an /// encoding. If verbose assembly output is enabled, we output comments /// describing the encoding. Desc is an optional string saying what the /// encoding is specifying (e.g. "LSDA"). void AsmPrinter::EmitEncodingByte(unsigned Val, const char *Desc) const { if (isVerbose()) { if (Desc) OutStreamer.AddComment(Twine(Desc) + " Encoding = " + Twine(DecodeDWARFEncoding(Val))); else OutStreamer.AddComment(Twine("Encoding = ") + DecodeDWARFEncoding(Val)); } OutStreamer.EmitIntValue(Val, 1); } /// GetSizeOfEncodedValue - Return the size of the encoding in bytes. unsigned AsmPrinter::GetSizeOfEncodedValue(unsigned Encoding) const { if (Encoding == dwarf::DW_EH_PE_omit) return 0; switch (Encoding & 0x07) { default: llvm_unreachable("Invalid encoded value."); case dwarf::DW_EH_PE_absptr: return TM.getSubtargetImpl()->getDataLayout()->getPointerSize(); case dwarf::DW_EH_PE_udata2: return 2; case dwarf::DW_EH_PE_udata4: return 4; case dwarf::DW_EH_PE_udata8: return 8; } } void AsmPrinter::EmitTTypeReference(const GlobalValue *GV, unsigned Encoding) const { if (GV) { const TargetLoweringObjectFile &TLOF = getObjFileLowering(); const MCExpr *Exp = TLOF.getTTypeGlobalReference(GV, Encoding, *Mang, TM, MMI, OutStreamer); OutStreamer.EmitValue(Exp, GetSizeOfEncodedValue(Encoding)); } else OutStreamer.EmitIntValue(0, GetSizeOfEncodedValue(Encoding)); } /// EmitSectionOffset - Emit the 4-byte offset of Label from the start of its /// section. This can be done with a special directive if the target supports /// it (e.g. cygwin) or by emitting it as an offset from a label at the start /// of the section. /// /// SectionLabel is a temporary label emitted at the start of the section that /// Label lives in. void AsmPrinter::EmitSectionOffset(const MCSymbol *Label, const MCSymbol *SectionLabel) const { // On COFF targets, we have to emit the special .secrel32 directive. if (MAI->needsDwarfSectionOffsetDirective()) { OutStreamer.EmitCOFFSecRel32(Label); return; } // Get the section that we're referring to, based on SectionLabel. const MCSection &Section = SectionLabel->getSection(); // If Label has already been emitted, verify that it is in the same section as // section label for sanity. assert((!Label->isInSection() || &Label->getSection() == &Section) && "Section offset using wrong section base for label"); // If the section in question will end up with an address of 0 anyway, we can // just emit an absolute reference to save a relocation. if (Section.isBaseAddressKnownZero()) { OutStreamer.EmitSymbolValue(Label, 4); return; } // Otherwise, emit it as a label difference from the start of the section. EmitLabelDifference(Label, SectionLabel, 4); } // Some targets do not provide a DWARF register number for every // register. This function attempts to emit a DWARF register by // emitting a piece of a super-register or by piecing together // multiple subregisters that alias the register. void AsmPrinter::EmitDwarfRegOpPiece(ByteStreamer &Streamer, const MachineLocation &MLoc, unsigned PieceSizeInBits, unsigned PieceOffsetInBits) const { assert(MLoc.isReg() && "MLoc must be a register"); DebugLocDwarfExpression Expr(TM, Streamer); Expr.AddMachineRegPiece(MLoc.getReg(), PieceSizeInBits, PieceOffsetInBits); } void AsmPrinter::EmitDwarfOpPiece(ByteStreamer &Streamer, unsigned PieceSizeInBits, unsigned PieceOffsetInBits) const { DebugLocDwarfExpression Expr(TM, Streamer); Expr.AddOpPiece(PieceSizeInBits, PieceOffsetInBits); } /// EmitDwarfRegOp - Emit dwarf register operation. void AsmPrinter::EmitDwarfRegOp(ByteStreamer &Streamer, const MachineLocation &MLoc, bool Indirect) const { DebugLocDwarfExpression Expr(TM, Streamer); const TargetRegisterInfo *TRI = TM.getSubtargetImpl()->getRegisterInfo(); int Reg = TRI->getDwarfRegNum(MLoc.getReg(), false); if (Reg < 0) { // We assume that pointers are always in an addressable register. if (Indirect || MLoc.isIndirect()) // FIXME: We have no reasonable way of handling errors in here. The // caller might be in the middle of a dwarf expression. We should // probably assert that Reg >= 0 once debug info generation is more // mature. return Expr.EmitOp(dwarf::DW_OP_nop, "nop (could not find a dwarf register number)"); // Attempt to find a valid super- or sub-register. return Expr.AddMachineRegPiece(MLoc.getReg()); } if (MLoc.isIndirect()) Expr.AddRegIndirect(Reg, MLoc.getOffset(), Indirect); else if (Indirect) Expr.AddRegIndirect(Reg, 0, false); else Expr.AddReg(Reg); } //===----------------------------------------------------------------------===// // Dwarf Lowering Routines //===----------------------------------------------------------------------===// void AsmPrinter::emitCFIInstruction(const MCCFIInstruction &Inst) const { switch (Inst.getOperation()) { default: llvm_unreachable("Unexpected instruction"); case MCCFIInstruction::OpDefCfaOffset: OutStreamer.EmitCFIDefCfaOffset(Inst.getOffset()); break; case MCCFIInstruction::OpDefCfa: OutStreamer.EmitCFIDefCfa(Inst.getRegister(), Inst.getOffset()); break; case MCCFIInstruction::OpDefCfaRegister: OutStreamer.EmitCFIDefCfaRegister(Inst.getRegister()); break; case MCCFIInstruction::OpOffset: OutStreamer.EmitCFIOffset(Inst.getRegister(), Inst.getOffset()); break; case MCCFIInstruction::OpRegister: OutStreamer.EmitCFIRegister(Inst.getRegister(), Inst.getRegister2()); break; case MCCFIInstruction::OpWindowSave: OutStreamer.EmitCFIWindowSave(); break; case MCCFIInstruction::OpSameValue: OutStreamer.EmitCFISameValue(Inst.getRegister()); break; } }