//===-- AsmPrinterDwarf.cpp - AsmPrinter Dwarf Support --------------------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the Dwarf emissions parts of AsmPrinter. // //===----------------------------------------------------------------------===// #define DEBUG_TYPE "asm-printer" #include "llvm/CodeGen/AsmPrinter.h" #include "llvm/MC/MachineLocation.h" #include "llvm/MC/MCAsmInfo.h" #include "llvm/MC/MCSection.h" #include "llvm/MC/MCStreamer.h" #include "llvm/MC/MCSymbol.h" #include "llvm/DataLayout.h" #include "llvm/Target/TargetFrameLowering.h" #include "llvm/Target/TargetLoweringObjectFile.h" #include "llvm/Target/TargetMachine.h" #include "llvm/Target/TargetRegisterInfo.h" #include "llvm/ADT/Twine.h" #include "llvm/Support/Dwarf.h" #include "llvm/Support/ErrorHandling.h" using namespace llvm; //===----------------------------------------------------------------------===// // Dwarf Emission Helper Routines //===----------------------------------------------------------------------===// /// EmitSLEB128 - emit the specified signed leb128 value. void AsmPrinter::EmitSLEB128(int Value, const char *Desc) const { if (isVerbose() && Desc) OutStreamer.AddComment(Desc); OutStreamer.EmitSLEB128IntValue(Value); } /// EmitULEB128 - emit the specified signed leb128 value. void AsmPrinter::EmitULEB128(unsigned Value, const char *Desc, unsigned PadTo) const { if (isVerbose() && Desc) OutStreamer.AddComment(Desc); OutStreamer.EmitULEB128IntValue(Value, 0/*addrspace*/, PadTo); } /// EmitCFAByte - Emit a .byte 42 directive for a DW_CFA_xxx value. void AsmPrinter::EmitCFAByte(unsigned Val) const { if (isVerbose()) { if (Val >= dwarf::DW_CFA_offset && Val < dwarf::DW_CFA_offset+64) OutStreamer.AddComment("DW_CFA_offset + Reg (" + Twine(Val-dwarf::DW_CFA_offset) + ")"); else OutStreamer.AddComment(dwarf::CallFrameString(Val)); } OutStreamer.EmitIntValue(Val, 1, 0/*addrspace*/); } static const char *DecodeDWARFEncoding(unsigned Encoding) { switch (Encoding) { case dwarf::DW_EH_PE_absptr: return "absptr"; case dwarf::DW_EH_PE_omit: return "omit"; case dwarf::DW_EH_PE_pcrel: return "pcrel"; case dwarf::DW_EH_PE_udata4: return "udata4"; case dwarf::DW_EH_PE_udata8: return "udata8"; case dwarf::DW_EH_PE_sdata4: return "sdata4"; case dwarf::DW_EH_PE_sdata8: return "sdata8"; case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata4: return "pcrel udata4"; case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata4: return "pcrel sdata4"; case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_udata8: return "pcrel udata8"; case dwarf::DW_EH_PE_pcrel | dwarf::DW_EH_PE_sdata8: return "pcrel sdata8"; case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel |dwarf::DW_EH_PE_udata4: return "indirect pcrel udata4"; case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel |dwarf::DW_EH_PE_sdata4: return "indirect pcrel sdata4"; case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel |dwarf::DW_EH_PE_udata8: return "indirect pcrel udata8"; case dwarf::DW_EH_PE_indirect | dwarf::DW_EH_PE_pcrel |dwarf::DW_EH_PE_sdata8: return "indirect pcrel sdata8"; } return ""; } /// EmitEncodingByte - Emit a .byte 42 directive that corresponds to an /// encoding. If verbose assembly output is enabled, we output comments /// describing the encoding. Desc is an optional string saying what the /// encoding is specifying (e.g. "LSDA"). void AsmPrinter::EmitEncodingByte(unsigned Val, const char *Desc) const { if (isVerbose()) { if (Desc != 0) OutStreamer.AddComment(Twine(Desc)+" Encoding = " + Twine(DecodeDWARFEncoding(Val))); else OutStreamer.AddComment(Twine("Encoding = ") + DecodeDWARFEncoding(Val)); } OutStreamer.EmitIntValue(Val, 1, 0/*addrspace*/); } /// GetSizeOfEncodedValue - Return the size of the encoding in bytes. unsigned AsmPrinter::GetSizeOfEncodedValue(unsigned Encoding) const { if (Encoding == dwarf::DW_EH_PE_omit) return 0; switch (Encoding & 0x07) { default: llvm_unreachable("Invalid encoded value."); case dwarf::DW_EH_PE_absptr: return TM.getDataLayout()->getPointerSize(); case dwarf::DW_EH_PE_udata2: return 2; case dwarf::DW_EH_PE_udata4: return 4; case dwarf::DW_EH_PE_udata8: return 8; } } void AsmPrinter::EmitReference(const MCSymbol *Sym, unsigned Encoding) const { const TargetLoweringObjectFile &TLOF = getObjFileLowering(); const MCExpr *Exp = TLOF.getExprForDwarfReference(Sym, Encoding, OutStreamer); OutStreamer.EmitAbsValue(Exp, GetSizeOfEncodedValue(Encoding)); } void AsmPrinter::EmitReference(const GlobalValue *GV, unsigned Encoding)const{ const TargetLoweringObjectFile &TLOF = getObjFileLowering(); const MCExpr *Exp = TLOF.getExprForDwarfGlobalReference(GV, Mang, MMI, Encoding, OutStreamer); OutStreamer.EmitValue(Exp, GetSizeOfEncodedValue(Encoding), /*addrspace*/0); } /// EmitSectionOffset - Emit the 4-byte offset of Label from the start of its /// section. This can be done with a special directive if the target supports /// it (e.g. cygwin) or by emitting it as an offset from a label at the start /// of the section. /// /// SectionLabel is a temporary label emitted at the start of the section that /// Label lives in. void AsmPrinter::EmitSectionOffset(const MCSymbol *Label, const MCSymbol *SectionLabel) const { // On COFF targets, we have to emit the special .secrel32 directive. if (MAI->getDwarfSectionOffsetDirective()) { OutStreamer.EmitCOFFSecRel32(Label); return; } // Get the section that we're referring to, based on SectionLabel. const MCSection &Section = SectionLabel->getSection(); // If Label has already been emitted, verify that it is in the same section as // section label for sanity. assert((!Label->isInSection() || &Label->getSection() == &Section) && "Section offset using wrong section base for label"); // If the section in question will end up with an address of 0 anyway, we can // just emit an absolute reference to save a relocation. if (Section.isBaseAddressKnownZero()) { OutStreamer.EmitSymbolValue(Label, 4, 0/*AddrSpace*/); return; } // Otherwise, emit it as a label difference from the start of the section. EmitLabelDifference(Label, SectionLabel, 4); } //===----------------------------------------------------------------------===// // Dwarf Lowering Routines //===----------------------------------------------------------------------===// /// EmitCFIFrameMove - Emit a frame instruction. void AsmPrinter::EmitCFIFrameMove(const MachineMove &Move) const { const TargetRegisterInfo *RI = TM.getRegisterInfo(); const MachineLocation &Dst = Move.getDestination(); const MachineLocation &Src = Move.getSource(); // If advancing cfa. if (Dst.isReg() && Dst.getReg() == MachineLocation::VirtualFP) { if (Src.getReg() == MachineLocation::VirtualFP) { OutStreamer.EmitCFIDefCfaOffset(-Src.getOffset()); } else { // Reg + Offset OutStreamer.EmitCFIDefCfa(RI->getDwarfRegNum(Src.getReg(), true), Src.getOffset()); } } else if (Src.isReg() && Src.getReg() == MachineLocation::VirtualFP) { assert(Dst.isReg() && "Machine move not supported yet."); OutStreamer.EmitCFIDefCfaRegister(RI->getDwarfRegNum(Dst.getReg(), true)); } else { assert(!Dst.isReg() && "Machine move not supported yet."); OutStreamer.EmitCFIOffset(RI->getDwarfRegNum(Src.getReg(), true), Dst.getOffset()); } }