//===-- llvm/CodeGen/DebugLocEntry.h - Entry in debug_loc list -*- C++ -*--===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// #ifndef CODEGEN_ASMPRINTER_DEBUGLOCENTRY_H__ #define CODEGEN_ASMPRINTER_DEBUGLOCENTRY_H__ #include "llvm/IR/Constants.h" #include "llvm/IR/DebugInfo.h" #include "llvm/MC/MachineLocation.h" #include "llvm/MC/MCSymbol.h" namespace llvm { class MDNode; /// \brief This struct describes location entries emitted in the .debug_loc /// section. class DebugLocEntry { // Begin and end symbols for the address range that this location is valid. const MCSymbol *Begin; const MCSymbol *End; public: /// A single location or constant. struct Value { Value(const MDNode *Var, int64_t i) : Variable(Var), EntryKind(E_Integer) { Constant.Int = i; } Value(const MDNode *Var, const ConstantFP *CFP) : Variable(Var), EntryKind(E_ConstantFP) { Constant.CFP = CFP; } Value(const MDNode *Var, const ConstantInt *CIP) : Variable(Var), EntryKind(E_ConstantInt) { Constant.CIP = CIP; } Value(const MDNode *Var, MachineLocation Loc) : Variable(Var), EntryKind(E_Location), Loc(Loc) { } // The variable to which this location entry corresponds. const MDNode *Variable; // Type of entry that this represents. enum EntryType { E_Location, E_Integer, E_ConstantFP, E_ConstantInt }; enum EntryType EntryKind; // Either a constant, union { int64_t Int; const ConstantFP *CFP; const ConstantInt *CIP; } Constant; // Or a location in the machine frame. MachineLocation Loc; bool operator==(const Value &other) const { if (EntryKind != other.EntryKind) return false; switch (EntryKind) { case E_Location: return Loc == other.Loc; case E_Integer: return Constant.Int == other.Constant.Int; case E_ConstantFP: return Constant.CFP == other.Constant.CFP; case E_ConstantInt: return Constant.CIP == other.Constant.CIP; } llvm_unreachable("unhandled EntryKind"); } bool isLocation() const { return EntryKind == E_Location; } bool isInt() const { return EntryKind == E_Integer; } bool isConstantFP() const { return EntryKind == E_ConstantFP; } bool isConstantInt() const { return EntryKind == E_ConstantInt; } int64_t getInt() const { return Constant.Int; } const ConstantFP *getConstantFP() const { return Constant.CFP; } const ConstantInt *getConstantInt() const { return Constant.CIP; } MachineLocation getLoc() const { return Loc; } const MDNode *getVariable() const { return Variable; } }; private: /// A list of locations/constants belonging to this entry. SmallVector Values; public: DebugLocEntry() : Begin(nullptr), End(nullptr) {} DebugLocEntry(const MCSymbol *B, const MCSymbol *E, Value Val) : Begin(B), End(E) { Values.push_back(std::move(Val)); } /// \brief Attempt to merge this DebugLocEntry with Next and return /// true if the merge was successful. Entries can be merged if they /// share the same Loc/Constant and if Next immediately follows this /// Entry. bool Merge(const DebugLocEntry &Next) { // If this and Next are describing different pieces of the same // variable, merge them by appending next's values to the current // list of values. if (Begin == Next.Begin && Values.size() > 0 && Next.Values.size() > 0) { DIVariable Var(Values[0].Variable); DIVariable NextVar(Next.Values[0].Variable); if (Var.getName() == NextVar.getName() && Var.isVariablePiece() && NextVar.isVariablePiece()) { Values.append(Next.Values.begin(), Next.Values.end()); End = Next.End; return true; } } // If this and Next are describing the same variable, merge them. if ((End == Next.Begin && Values == Next.Values)) { End = Next.End; return true; } return false; } const MCSymbol *getBeginSym() const { return Begin; } const MCSymbol *getEndSym() const { return End; } const ArrayRef getValues() const { return Values; } void addValue(Value Val) { assert(DIVariable(Val.Variable).isVariablePiece() && "multi-value DebugLocEntries must be pieces"); Values.push_back(Val); } }; } #endif