//===-- DwarfException.h - Dwarf Exception Framework -----------*- C++ -*--===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file contains support for writing dwarf exception info into asm files. // //===----------------------------------------------------------------------===// #ifndef LLVM_CODEGEN_ASMPRINTER_DWARFEXCEPTION_H #define LLVM_CODEGEN_ASMPRINTER_DWARFEXCEPTION_H #include "AsmPrinterHandler.h" #include "llvm/ADT/DenseMap.h" #include "llvm/CodeGen/AsmPrinter.h" #include namespace llvm { template class SmallVectorImpl; struct LandingPadInfo; class MachineModuleInfo; class MachineInstr; class MachineFunction; class MCAsmInfo; class MCExpr; class MCSymbol; class Function; class ARMTargetStreamer; class AsmPrinter; //===----------------------------------------------------------------------===// /// DwarfException - Emits Dwarf exception handling directives. /// class DwarfException : public AsmPrinterHandler { protected: /// Asm - Target of Dwarf emission. AsmPrinter *Asm; /// MMI - Collected machine module information. MachineModuleInfo *MMI; /// SharedTypeIds - How many leading type ids two landing pads have in common. static unsigned SharedTypeIds(const LandingPadInfo *L, const LandingPadInfo *R); /// PadRange - Structure holding a try-range and the associated landing pad. struct PadRange { // The index of the landing pad. unsigned PadIndex; // The index of the begin and end labels in the landing pad's label lists. unsigned RangeIndex; }; typedef DenseMap RangeMapType; /// ActionEntry - Structure describing an entry in the actions table. struct ActionEntry { int ValueForTypeID; // The value to write - may not be equal to the type id. int NextAction; unsigned Previous; }; /// CallSiteEntry - Structure describing an entry in the call-site table. struct CallSiteEntry { // The 'try-range' is BeginLabel .. EndLabel. MCSymbol *BeginLabel; // zero indicates the start of the function. MCSymbol *EndLabel; // zero indicates the end of the function. // The landing pad starts at PadLabel. MCSymbol *PadLabel; // zero indicates that there is no landing pad. unsigned Action; }; /// ComputeActionsTable - Compute the actions table and gather the first /// action index for each landing pad site. unsigned ComputeActionsTable(const SmallVectorImpl&LPs, SmallVectorImpl &Actions, SmallVectorImpl &FirstActions); /// CallToNoUnwindFunction - Return `true' if this is a call to a function /// marked `nounwind'. Return `false' otherwise. bool CallToNoUnwindFunction(const MachineInstr *MI); /// ComputeCallSiteTable - Compute the call-site table. The entry for an /// invoke has a try-range containing the call, a non-zero landing pad and an /// appropriate action. The entry for an ordinary call has a try-range /// containing the call and zero for the landing pad and the action. Calls /// marked 'nounwind' have no entry and must not be contained in the try-range /// of any entry - they form gaps in the table. Entries must be ordered by /// try-range address. void ComputeCallSiteTable(SmallVectorImpl &CallSites, const RangeMapType &PadMap, const SmallVectorImpl &LPs, const SmallVectorImpl &FirstActions); /// EmitExceptionTable - Emit landing pads and actions. /// /// The general organization of the table is complex, but the basic concepts /// are easy. First there is a header which describes the location and /// organization of the three components that follow. /// 1. The landing pad site information describes the range of code covered /// by the try. In our case it's an accumulation of the ranges covered /// by the invokes in the try. There is also a reference to the landing /// pad that handles the exception once processed. Finally an index into /// the actions table. /// 2. The action table, in our case, is composed of pairs of type ids /// and next action offset. Starting with the action index from the /// landing pad site, each type Id is checked for a match to the current /// exception. If it matches then the exception and type id are passed /// on to the landing pad. Otherwise the next action is looked up. This /// chain is terminated with a next action of zero. If no type id is /// found the frame is unwound and handling continues. /// 3. Type id table contains references to all the C++ typeinfo for all /// catches in the function. This tables is reversed indexed base 1. void EmitExceptionTable(); virtual void EmitTypeInfos(unsigned TTypeEncoding); public: //===--------------------------------------------------------------------===// // Main entry points. // DwarfException(AsmPrinter *A); virtual ~DwarfException(); /// endModule - Emit all exception information that should come after the /// content. virtual void endModule(); /// beginFunction - Gather pre-function exception information. Assumes being /// emitted immediately after the function entry point. virtual void beginFunction(const MachineFunction *MF); /// endFunction - Gather and emit post-function exception information. virtual void endFunction(const MachineFunction *); // We don't need these. virtual void setSymbolSize(const MCSymbol *Sym, uint64_t Size) {} virtual void beginInstruction(const MachineInstr *MI) {} virtual void endInstruction() {} }; class DwarfCFIException : public DwarfException { /// shouldEmitPersonality - Per-function flag to indicate if .cfi_personality /// should be emitted. bool shouldEmitPersonality; /// shouldEmitLSDA - Per-function flag to indicate if .cfi_lsda /// should be emitted. bool shouldEmitLSDA; /// shouldEmitMoves - Per-function flag to indicate if frame moves info /// should be emitted. bool shouldEmitMoves; AsmPrinter::CFIMoveType moveTypeModule; public: //===--------------------------------------------------------------------===// // Main entry points. // DwarfCFIException(AsmPrinter *A); virtual ~DwarfCFIException(); /// endModule - Emit all exception information that should come after the /// content. virtual void endModule(); /// beginFunction - Gather pre-function exception information. Assumes being /// emitted immediately after the function entry point. virtual void beginFunction(const MachineFunction *MF); /// endFunction - Gather and emit post-function exception information. virtual void endFunction(const MachineFunction *); }; class ARMException : public DwarfException { void EmitTypeInfos(unsigned TTypeEncoding); ARMTargetStreamer &getTargetStreamer(); /// shouldEmitCFI - Per-function flag to indicate if frame CFI info /// should be emitted. bool shouldEmitCFI; public: //===--------------------------------------------------------------------===// // Main entry points. // ARMException(AsmPrinter *A); virtual ~ARMException(); /// endModule - Emit all exception information that should come after the /// content. virtual void endModule(); /// beginFunction - Gather pre-function exception information. Assumes being /// emitted immediately after the function entry point. virtual void beginFunction(const MachineFunction *MF); /// endFunction - Gather and emit post-function exception information. virtual void endFunction(const MachineFunction *); }; class Win64Exception : public DwarfException { /// shouldEmitPersonality - Per-function flag to indicate if personality /// info should be emitted. bool shouldEmitPersonality; /// shouldEmitLSDA - Per-function flag to indicate if the LSDA /// should be emitted. bool shouldEmitLSDA; /// shouldEmitMoves - Per-function flag to indicate if frame moves info /// should be emitted. bool shouldEmitMoves; public: //===--------------------------------------------------------------------===// // Main entry points. // Win64Exception(AsmPrinter *A); virtual ~Win64Exception(); /// endModule - Emit all exception information that should come after the /// content. virtual void endModule(); /// beginFunction - Gather pre-function exception information. Assumes being /// emitted immediately after the function entry point. virtual void beginFunction(const MachineFunction *MF); /// endFunction - Gather and emit post-function exception information. virtual void endFunction(const MachineFunction *); }; } // End of namespace llvm #endif