//===-- llvm/CodeGen/DwarfExpression.cpp - Dwarf Debug Framework ----------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file contains support for writing dwarf debug info into asm files. // //===----------------------------------------------------------------------===// #include "DwarfExpression.h" #include "DwarfDebug.h" #include "llvm/ADT/SmallBitVector.h" #include "llvm/CodeGen/AsmPrinter.h" #include "llvm/Support/Dwarf.h" #include "llvm/Target/TargetMachine.h" #include "llvm/Target/TargetRegisterInfo.h" #include "llvm/Target/TargetSubtargetInfo.h" using namespace llvm; const TargetRegisterInfo *DwarfExpression::getTRI() const { return AP.TM.getSubtargetImpl()->getRegisterInfo(); } unsigned DwarfExpression::getDwarfVersion() const { return AP.getDwarfDebug()->getDwarfVersion(); } void DwarfExpression::AddReg(int DwarfReg, const char *Comment) { assert(DwarfReg >= 0 && "invalid negative dwarf register number"); if (DwarfReg < 32) { EmitOp(dwarf::DW_OP_reg0 + DwarfReg, Comment); } else { EmitOp(dwarf::DW_OP_regx, Comment); EmitUnsigned(DwarfReg); } } void DwarfExpression::AddRegIndirect(int DwarfReg, int Offset, bool Deref) { assert(DwarfReg >= 0 && "invalid negative dwarf register number"); if (DwarfReg < 32) { EmitOp(dwarf::DW_OP_breg0 + DwarfReg); } else { EmitOp(dwarf::DW_OP_bregx); EmitUnsigned(DwarfReg); } EmitSigned(Offset); if (Deref) EmitOp(dwarf::DW_OP_deref); } void DwarfExpression::AddOpPiece(unsigned SizeInBits, unsigned OffsetInBits) { assert(SizeInBits > 0 && "piece has size zero"); const unsigned SizeOfByte = 8; if (OffsetInBits > 0 || SizeInBits % SizeOfByte) { EmitOp(dwarf::DW_OP_bit_piece); EmitUnsigned(SizeInBits); EmitUnsigned(OffsetInBits); } else { EmitOp(dwarf::DW_OP_piece); unsigned ByteSize = SizeInBits / SizeOfByte; EmitUnsigned(ByteSize); } } void DwarfExpression::AddShr(unsigned ShiftBy) { EmitOp(dwarf::DW_OP_constu); EmitUnsigned(ShiftBy); EmitOp(dwarf::DW_OP_shr); } bool DwarfExpression::AddMachineRegIndirect(unsigned MachineReg, int Offset) { int DwarfReg = getTRI()->getDwarfRegNum(MachineReg, false); if (DwarfReg < 0) return false; if (isFrameRegister(MachineReg)) { // If variable offset is based in frame register then use fbreg. EmitOp(dwarf::DW_OP_fbreg); EmitSigned(Offset); } else { AddRegIndirect(DwarfReg, Offset); } return true; } bool DwarfExpression::AddMachineRegPiece(unsigned MachineReg, unsigned PieceSizeInBits, unsigned PieceOffsetInBits) { const TargetRegisterInfo *TRI = getTRI(); int Reg = TRI->getDwarfRegNum(MachineReg, false); // If this is a valid register number, emit it. if (Reg >= 0) { AddReg(Reg); if (PieceSizeInBits) AddOpPiece(PieceSizeInBits, PieceOffsetInBits); return true; } // Walk up the super-register chain until we find a valid number. // For example, EAX on x86_64 is a 32-bit piece of RAX with offset 0. for (MCSuperRegIterator SR(MachineReg, TRI); SR.isValid(); ++SR) { Reg = TRI->getDwarfRegNum(*SR, false); if (Reg >= 0) { unsigned Idx = TRI->getSubRegIndex(*SR, MachineReg); unsigned Size = TRI->getSubRegIdxSize(Idx); unsigned RegOffset = TRI->getSubRegIdxOffset(Idx); AddReg(Reg, "super-register"); if (PieceOffsetInBits == RegOffset) { AddOpPiece(Size, RegOffset); } else { // If this is part of a variable in a sub-register at a // non-zero offset, we need to manually shift the value into // place, since the DW_OP_piece describes the part of the // variable, not the position of the subregister. if (RegOffset) AddShr(RegOffset); AddOpPiece(Size, PieceOffsetInBits); } return true; } } // Otherwise, attempt to find a covering set of sub-register numbers. // For example, Q0 on ARM is a composition of D0+D1. // // Keep track of the current position so we can emit the more // efficient DW_OP_piece. unsigned CurPos = PieceOffsetInBits; // The size of the register in bits, assuming 8 bits per byte. unsigned RegSize = TRI->getMinimalPhysRegClass(MachineReg)->getSize() * 8; // Keep track of the bits in the register we already emitted, so we // can avoid emitting redundant aliasing subregs. SmallBitVector Coverage(RegSize, false); for (MCSubRegIterator SR(MachineReg, TRI); SR.isValid(); ++SR) { unsigned Idx = TRI->getSubRegIndex(MachineReg, *SR); unsigned Size = TRI->getSubRegIdxSize(Idx); unsigned Offset = TRI->getSubRegIdxOffset(Idx); Reg = TRI->getDwarfRegNum(*SR, false); // Intersection between the bits we already emitted and the bits // covered by this subregister. SmallBitVector Intersection(RegSize, false); Intersection.set(Offset, Offset + Size); Intersection ^= Coverage; // If this sub-register has a DWARF number and we haven't covered // its range, emit a DWARF piece for it. if (Reg >= 0 && Intersection.any()) { AddReg(Reg, "sub-register"); AddOpPiece(Size, Offset == CurPos ? 0 : Offset); CurPos = Offset + Size; // Mark it as emitted. Coverage.set(Offset, Offset + Size); } } return CurPos > PieceOffsetInBits; } void DwarfExpression::AddSignedConstant(int Value) { EmitOp(dwarf::DW_OP_consts); EmitSigned(Value); // The proper way to describe a constant value is // DW_OP_constu , DW_OP_stack_value. // Unfortunately, DW_OP_stack_value was not available until DWARF-4, // so we will continue to generate DW_OP_constu for DWARF-2 // and DWARF-3. Technically, this is incorrect since DW_OP_const // actually describes a value at a constant addess, not a constant value. // However, in the past there was no better way to describe a constant // value, so the producers and consumers started to rely on heuristics // to disambiguate the value vs. location status of the expression. // See PR21176 for more details. if (getDwarfVersion() >= 4) EmitOp(dwarf::DW_OP_stack_value); } void DwarfExpression::AddUnsignedConstant(unsigned Value) { EmitOp(dwarf::DW_OP_constu); EmitUnsigned(Value); // cf. comment in DwarfExpression::AddSignedConstant(). if (getDwarfVersion() >= 4) EmitOp(dwarf::DW_OP_stack_value); } static unsigned getOffsetOrZero(unsigned OffsetInBits, unsigned PieceOffsetInBits) { if (OffsetInBits == PieceOffsetInBits) return 0; assert(OffsetInBits >= PieceOffsetInBits && "overlapping pieces"); return OffsetInBits; } bool DwarfExpression::AddMachineRegExpression(DIExpression Expr, unsigned MachineReg, unsigned PieceOffsetInBits) { auto I = Expr.begin(); // Pattern-match combinations for which more efficient representations exist // first. if (I == Expr.end()) return AddMachineRegPiece(MachineReg); bool ValidReg = false; switch (*I) { case dwarf::DW_OP_piece: { unsigned SizeOfByte = 8; unsigned OffsetInBits = I.getArg(1) * SizeOfByte; unsigned SizeInBits = I.getArg(2) * SizeOfByte; // Piece always comes at the end of the expression. return AddMachineRegPiece(MachineReg, SizeInBits, getOffsetOrZero(OffsetInBits, PieceOffsetInBits)); } case dwarf::DW_OP_plus: // [DW_OP_reg,Offset,DW_OP_plus,DW_OP_deref] --> [DW_OP_breg,Offset]. if (*std::next(I) == dwarf::DW_OP_deref) { unsigned Offset = I.getArg(1); ValidReg = AddMachineRegIndirect(MachineReg, Offset); std::advance(I, 2); break; } else ValidReg = AddMachineRegPiece(MachineReg); case dwarf::DW_OP_deref: // [DW_OP_reg,DW_OP_deref] --> [DW_OP_breg]. ValidReg = AddMachineRegIndirect(MachineReg); ++I; break; default: llvm_unreachable("unsupported operand"); } if (!ValidReg) return false; // Emit remaining elements of the expression. AddExpression(I, PieceOffsetInBits); return true; } void DwarfExpression::AddExpression(DIExpressionIterator I, unsigned PieceOffsetInBits) { for (; I != DIExpressionIterator(); ++I) { switch (*I) { case dwarf::DW_OP_piece: { unsigned SizeOfByte = 8; unsigned OffsetInBits = I.getArg(1) * SizeOfByte; unsigned SizeInBits = I.getArg(2) * SizeOfByte; AddOpPiece(SizeInBits, getOffsetOrZero(OffsetInBits, PieceOffsetInBits)); break; } case dwarf::DW_OP_plus: EmitOp(dwarf::DW_OP_plus_uconst); EmitUnsigned(I.getArg(1)); break; case dwarf::DW_OP_deref: EmitOp(dwarf::DW_OP_deref); break; default: llvm_unreachable("unhandled opcode found in DIExpression"); } } }