//===-- llvm/CodeGen/DwarfExpression.h - Dwarf Compile Unit ---*- C++ -*--===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file contains support for writing dwarf compile unit. // //===----------------------------------------------------------------------===// #ifndef LLVM_LIB_CODEGEN_ASMPRINTER_DWARFEXPRESSION_H #define LLVM_LIB_CODEGEN_ASMPRINTER_DWARFEXPRESSION_H #include "llvm/IR/DebugInfo.h" #include "llvm/Support/DataTypes.h" namespace llvm { class AsmPrinter; class ByteStreamer; class TargetRegisterInfo; class DwarfUnit; class DIELoc; /// Base class containing the logic for constructing DWARF expressions /// independently of whether they are emitted into a DIE or into a .debug_loc /// entry. class DwarfExpression { protected: const AsmPrinter ≈ // Various convenience accessors that extract things out of AsmPrinter. const TargetRegisterInfo *getTRI() const; unsigned getDwarfVersion() const; public: DwarfExpression(const AsmPrinter &AP) : AP(AP) {} virtual ~DwarfExpression() {} /// Output a dwarf operand and an optional assembler comment. virtual void EmitOp(uint8_t Op, const char *Comment = nullptr) = 0; /// Emit a raw signed value. virtual void EmitSigned(int Value) = 0; /// Emit a raw unsigned value. virtual void EmitUnsigned(unsigned Value) = 0; /// Return whether the given machine register is the frame register in the /// current function. virtual bool isFrameRegister(unsigned MachineReg) = 0; /// Emit a dwarf register operation. void AddReg(int DwarfReg, const char *Comment = nullptr); /// Emit an (double-)indirect dwarf register operation. void AddRegIndirect(int DwarfReg, int Offset, bool Deref = false); /// Emit a dwarf register operation for describing /// - a small value occupying only part of a register or /// - a register representing only part of a value. void AddOpPiece(unsigned SizeInBits, unsigned OffsetInBits = 0); /// Emit a shift-right dwarf expression. void AddShr(unsigned ShiftBy); /// Emit an indirect dwarf register operation for the given machine register. /// \return false if no DWARF register exists for MachineReg. bool AddMachineRegIndirect(unsigned MachineReg, int Offset = 0); /// \brief Emit a partial DWARF register operation. /// \param MachineReg the register /// \param PieceSizeInBits size and /// \param PieceOffsetInBits offset of the piece in bits, if this is one /// piece of an aggregate value. /// /// If size and offset is zero an operation for the entire /// register is emitted: Some targets do not provide a DWARF /// register number for every register. If this is the case, this /// function will attempt to emit a DWARF register by emitting a /// piece of a super-register or by piecing together multiple /// subregisters that alias the register. /// /// \return false if no DWARF register exists for MachineReg. bool AddMachineRegPiece(unsigned MachineReg, unsigned PieceSizeInBits = 0, unsigned PieceOffsetInBits = 0); /// Emit a signed constant. void AddSignedConstant(int Value); /// Emit an unsigned constant. void AddUnsignedConstant(unsigned Value); /// Emit an entire DIExpression on top of a machine register location. /// \param PieceOffsetInBits If this is one piece out of a fragmented /// location, this is the offset of the piece inside the entire variable. /// \return false if no DWARF register exists for MachineReg. bool AddMachineRegExpression(DIExpression Expr, unsigned MachineReg, unsigned PieceOffsetInBits = 0); /// Emit a the operations remaining the DIExpressionIterator I. /// \param PieceOffsetInBits If this is one piece out of a fragmented /// location, this is the offset of the piece inside the entire variable. void AddExpression(DIExpressionIterator I, unsigned PieceOffsetInBits = 0); }; /// DwarfExpression implementation for .debug_loc entries. class DebugLocDwarfExpression : public DwarfExpression { ByteStreamer &BS; public: DebugLocDwarfExpression(const AsmPrinter &AP, ByteStreamer &BS) : DwarfExpression(AP), BS(BS) {} void EmitOp(uint8_t Op, const char *Comment = nullptr) override; void EmitSigned(int Value) override; void EmitUnsigned(unsigned Value) override; bool isFrameRegister(unsigned MachineReg) override; }; /// DwarfExpression implementation for singular DW_AT_location. class DIEDwarfExpression : public DwarfExpression { DwarfUnit &DU; DIELoc ¨ public: DIEDwarfExpression(const AsmPrinter &AP, DwarfUnit &DU, DIELoc &DIE) : DwarfExpression(AP), DU(DU), DIE(DIE) {} void EmitOp(uint8_t Op, const char *Comment = nullptr) override; void EmitSigned(int Value) override; void EmitUnsigned(unsigned Value) override; bool isFrameRegister(unsigned MachineReg) override; }; } #endif