//===-- llvm/CodeGen/DwarfFile.cpp - Dwarf Debug Framework ----------------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// #include "DwarfFile.h" #include "DwarfDebug.h" #include "DwarfUnit.h" #include "llvm/ADT/STLExtras.h" #include "llvm/IR/DataLayout.h" #include "llvm/MC/MCStreamer.h" #include "llvm/Support/LEB128.h" #include "llvm/Target/TargetLoweringObjectFile.h" namespace llvm { DwarfFile::DwarfFile(AsmPrinter *AP, DwarfDebug &DD, StringRef Pref, BumpPtrAllocator &DA) : Asm(AP), DD(DD), StrPool(DA, *Asm, Pref) {} DwarfFile::~DwarfFile() {} // Define a unique number for the abbreviation. // void DwarfFile::assignAbbrevNumber(DIEAbbrev &Abbrev) { // Check the set for priors. DIEAbbrev *InSet = AbbreviationsSet.GetOrInsertNode(&Abbrev); // If it's newly added. if (InSet == &Abbrev) { // Add to abbreviation list. Abbreviations.push_back(&Abbrev); // Assign the vector position + 1 as its number. Abbrev.setNumber(Abbreviations.size()); } else { // Assign existing abbreviation number. Abbrev.setNumber(InSet->getNumber()); } } void DwarfFile::addUnit(std::unique_ptr U) { CUs.push_back(std::move(U)); } // Emit the various dwarf units to the unit section USection with // the abbreviations going into ASection. void DwarfFile::emitUnits(const MCSymbol *ASectionSym) { for (const auto &TheU : CUs) { DIE &Die = TheU->getUnitDie(); const MCSection *USection = TheU->getSection(); Asm->OutStreamer.SwitchSection(USection); TheU->emitHeader(ASectionSym); DD.emitDIE(Die); } } // Compute the size and offset for each DIE. void DwarfFile::computeSizeAndOffsets() { // Offset from the first CU in the debug info section is 0 initially. unsigned SecOffset = 0; // Iterate over each compile unit and set the size and offsets for each // DIE within each compile unit. All offsets are CU relative. for (const auto &TheU : CUs) { TheU->setDebugInfoOffset(SecOffset); // CU-relative offset is reset to 0 here. unsigned Offset = sizeof(int32_t) + // Length of Unit Info TheU->getHeaderSize(); // Unit-specific headers // EndOffset here is CU-relative, after laying out // all of the CU DIE. unsigned EndOffset = computeSizeAndOffset(TheU->getUnitDie(), Offset); SecOffset += EndOffset; } } // Compute the size and offset of a DIE. The offset is relative to start of the // CU. It returns the offset after laying out the DIE. unsigned DwarfFile::computeSizeAndOffset(DIE &Die, unsigned Offset) { // Record the abbreviation. assignAbbrevNumber(Die.getAbbrev()); // Get the abbreviation for this DIE. const DIEAbbrev &Abbrev = Die.getAbbrev(); // Set DIE offset Die.setOffset(Offset); // Start the size with the size of abbreviation code. Offset += getULEB128Size(Die.getAbbrevNumber()); const SmallVectorImpl &Values = Die.getValues(); const SmallVectorImpl &AbbrevData = Abbrev.getData(); // Size the DIE attribute values. for (unsigned i = 0, N = Values.size(); i < N; ++i) // Size attribute value. Offset += Values[i]->SizeOf(Asm, AbbrevData[i].getForm()); // Get the children. const auto &Children = Die.getChildren(); // Size the DIE children if any. if (!Children.empty()) { assert(Abbrev.hasChildren() && "Children flag not set"); for (auto &Child : Children) Offset = computeSizeAndOffset(*Child, Offset); // End of children marker. Offset += sizeof(int8_t); } Die.setSize(Offset - Die.getOffset()); return Offset; } void DwarfFile::emitAbbrevs(const MCSection *Section) { // Check to see if it is worth the effort. if (!Abbreviations.empty()) { // Start the debug abbrev section. Asm->OutStreamer.SwitchSection(Section); // For each abbrevation. for (const DIEAbbrev *Abbrev : Abbreviations) { // Emit the abbrevations code (base 1 index.) Asm->EmitULEB128(Abbrev->getNumber(), "Abbreviation Code"); // Emit the abbreviations data. Abbrev->Emit(Asm); } // Mark end of abbreviations. Asm->EmitULEB128(0, "EOM(3)"); } } // Emit strings into a string section. void DwarfFile::emitStrings(const MCSection *StrSection, const MCSection *OffsetSection) { StrPool.emit(*Asm, StrSection, OffsetSection); } void DwarfFile::addScopeVariable(LexicalScope *LS, DbgVariable *Var) { SmallVectorImpl &Vars = ScopeVariables[LS]; DIVariable DV = Var->getVariable(); // Variables with positive arg numbers are parameters. if (unsigned ArgNum = DV.getArgNumber()) { // Keep all parameters in order at the start of the variable list to ensure // function types are correct (no out-of-order parameters) // // This could be improved by only doing it for optimized builds (unoptimized // builds have the right order to begin with), searching from the back (this // would catch the unoptimized case quickly), or doing a binary search // rather than linear search. auto I = Vars.begin(); while (I != Vars.end()) { unsigned CurNum = (*I)->getVariable().getArgNumber(); // A local (non-parameter) variable has been found, insert immediately // before it. if (CurNum == 0) break; // A later indexed parameter has been found, insert immediately before it. if (CurNum > ArgNum) break; // FIXME: There are still some cases where two inlined functions are // conflated together (two calls to the same function at the same // location (eg: via a macro, or without column info, etc)) and then // their arguments are conflated as well. assert((LS->getParent() || CurNum != ArgNum) && "Duplicate argument for top level (non-inlined) function"); ++I; } Vars.insert(I, Var); return; } Vars.push_back(Var); } }