//===-- llvm/CodeGen/DwarfUnit.h - Dwarf Compile Unit ---*- C++ -*--===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file contains support for writing dwarf compile unit. // //===----------------------------------------------------------------------===// #ifndef CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H #define CODEGEN_ASMPRINTER_DWARFCOMPILEUNIT_H #include "DIE.h" #include "DwarfDebug.h" #include "llvm/ADT/DenseMap.h" #include "llvm/ADT/Optional.h" #include "llvm/ADT/StringMap.h" #include "llvm/CodeGen/AsmPrinter.h" #include "llvm/IR/DIBuilder.h" #include "llvm/IR/DebugInfo.h" #include "llvm/MC/MCExpr.h" #include "llvm/MC/MCSection.h" #include "llvm/MC/MCDwarf.h" namespace llvm { class MachineLocation; class MachineOperand; class ConstantInt; class ConstantFP; class DbgVariable; class DwarfCompileUnit; // Data structure to hold a range for range lists. class RangeSpan { public: RangeSpan(MCSymbol *S, MCSymbol *E) : Start(S), End(E) {} const MCSymbol *getStart() const { return Start; } const MCSymbol *getEnd() const { return End; } void setEnd(const MCSymbol *E) { End = E; } private: const MCSymbol *Start, *End; }; class RangeSpanList { private: // Index for locating within the debug_range section this particular span. MCSymbol *RangeSym; // List of ranges. SmallVector Ranges; public: RangeSpanList(MCSymbol *Sym) : RangeSym(Sym) {} MCSymbol *getSym() const { return RangeSym; } const SmallVectorImpl &getRanges() const { return Ranges; } void addRange(RangeSpan Range) { Ranges.push_back(Range); } }; enum AbstractOrInlined { AOI_None, AOI_Inlined, AOI_Abstract }; //===----------------------------------------------------------------------===// /// Unit - This dwarf writer support class manages information associated /// with a source file. class DwarfUnit { protected: /// UniqueID - a numeric ID unique among all CUs in the module unsigned UniqueID; /// Node - MDNode for the compile unit. DICompileUnit CUNode; /// Unit debug information entry. DIE UnitDie; /// Offset of the UnitDie from beginning of debug info section. unsigned DebugInfoOffset; /// Asm - Target of Dwarf emission. AsmPrinter *Asm; // Holders for some common dwarf information. DwarfDebug *DD; DwarfFile *DU; /// IndexTyDie - An anonymous type for index type. Owned by UnitDie. DIE *IndexTyDie; /// MDNodeToDieMap - Tracks the mapping of unit level debug information /// variables to debug information entries. DenseMap MDNodeToDieMap; /// MDNodeToDIEEntryMap - Tracks the mapping of unit level debug information /// descriptors to debug information entries using a DIEEntry proxy. DenseMap MDNodeToDIEEntryMap; /// GlobalNames - A map of globally visible named entities for this unit. StringMap GlobalNames; /// GlobalTypes - A map of globally visible types for this unit. StringMap GlobalTypes; /// DIEBlocks - A list of all the DIEBlocks in use. std::vector DIEBlocks; /// DIELocs - A list of all the DIELocs in use. std::vector DIELocs; /// ContainingTypeMap - This map is used to keep track of subprogram DIEs that /// need DW_AT_containing_type attribute. This attribute points to a DIE that /// corresponds to the MDNode mapped with the subprogram DIE. DenseMap ContainingTypeMap; // List of ranges for a given compile unit. SmallVector CURanges; // List of range lists for a given compile unit, separate from the ranges for // the CU itself. SmallVector CURangeLists; // DIEValueAllocator - All DIEValues are allocated through this allocator. BumpPtrAllocator DIEValueAllocator; // DIEIntegerOne - A preallocated DIEValue because 1 is used frequently. DIEInteger *DIEIntegerOne; /// The section this unit will be emitted in. const MCSection *Section; /// A label at the start of the non-dwo section related to this unit. MCSymbol *SectionSym; /// The start of the unit within its section. MCSymbol *LabelBegin; /// The end of the unit within its section. MCSymbol *LabelEnd; /// Skeleton unit associated with this unit. DwarfUnit *Skeleton; DwarfUnit(unsigned UID, dwarf::Tag, DICompileUnit CU, AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU); public: virtual ~DwarfUnit(); /// Set the skeleton unit associated with this unit. void setSkeleton(DwarfUnit &Skel) { Skeleton = &Skel; } /// Get the skeleton unit associated with this unit. DwarfUnit *getSkeleton() const { return Skeleton; } /// Pass in the SectionSym even though we could recreate it in every compile /// unit (type units will have actually distinct symbols once they're in /// comdat sections). void initSection(const MCSection *Section, MCSymbol *SectionSym) { assert(!this->Section); this->Section = Section; this->SectionSym = SectionSym; this->LabelBegin = Asm->GetTempSymbol(Section->getLabelBeginName(), getUniqueID()); this->LabelEnd = Asm->GetTempSymbol(Section->getLabelEndName(), getUniqueID()); } const MCSection *getSection() const { assert(Section); return Section; } /// If there's a skeleton then return the section symbol for the skeleton /// unit, otherwise return the section symbol for this unit. MCSymbol *getLocalSectionSym() const { if (Skeleton) return Skeleton->getSectionSym(); return getSectionSym(); } MCSymbol *getSectionSym() const { assert(Section); return SectionSym; } /// If there's a skeleton then return the begin label for the skeleton unit, /// otherwise return the local label for this unit. MCSymbol *getLocalLabelBegin() const { if (Skeleton) return Skeleton->getLabelBegin(); return getLabelBegin(); } MCSymbol *getLabelBegin() const { assert(Section); return LabelBegin; } MCSymbol *getLabelEnd() const { assert(Section); return LabelEnd; } // Accessors. unsigned getUniqueID() const { return UniqueID; } uint16_t getLanguage() const { return CUNode.getLanguage(); } DICompileUnit getCUNode() const { return CUNode; } DIE &getUnitDie() { return UnitDie; } const StringMap &getGlobalNames() const { return GlobalNames; } const StringMap &getGlobalTypes() const { return GlobalTypes; } unsigned getDebugInfoOffset() const { return DebugInfoOffset; } void setDebugInfoOffset(unsigned DbgInfoOff) { DebugInfoOffset = DbgInfoOff; } /// hasContent - Return true if this compile unit has something to write out. bool hasContent() const { return !UnitDie.getChildren().empty(); } /// addRange - Add an address range to the list of ranges for this unit. void addRange(RangeSpan Range); /// getRanges - Get the list of ranges for this unit. const SmallVectorImpl &getRanges() const { return CURanges; } SmallVectorImpl &getRanges() { return CURanges; } /// addRangeList - Add an address range list to the list of range lists. void addRangeList(RangeSpanList Ranges) { CURangeLists.push_back(Ranges); } /// getRangeLists - Get the vector of range lists. const SmallVectorImpl &getRangeLists() const { return CURangeLists; } SmallVectorImpl &getRangeLists() { return CURangeLists; } /// getParentContextString - Get a string containing the language specific /// context for a global name. std::string getParentContextString(DIScope Context) const; /// addGlobalName - Add a new global entity to the compile unit. /// void addGlobalName(StringRef Name, DIE &Die, DIScope Context); /// addAccelNamespace - Add a new name to the namespace accelerator table. void addAccelNamespace(StringRef Name, const DIE &Die); /// getDIE - Returns the debug information entry map slot for the /// specified debug variable. We delegate the request to DwarfDebug /// when the MDNode can be part of the type system, since DIEs for /// the type system can be shared across CUs and the mappings are /// kept in DwarfDebug. DIE *getDIE(DIDescriptor D) const; /// getDIELoc - Returns a fresh newly allocated DIELoc. DIELoc *getDIELoc() { return new (DIEValueAllocator) DIELoc(); } /// insertDIE - Insert DIE into the map. We delegate the request to DwarfDebug /// when the MDNode can be part of the type system, since DIEs for /// the type system can be shared across CUs and the mappings are /// kept in DwarfDebug. void insertDIE(DIDescriptor Desc, DIE *D); /// addFlag - Add a flag that is true to the DIE. void addFlag(DIE &Die, dwarf::Attribute Attribute); /// addUInt - Add an unsigned integer attribute data and value. void addUInt(DIE &Die, dwarf::Attribute Attribute, Optional Form, uint64_t Integer); void addUInt(DIE &Block, dwarf::Form Form, uint64_t Integer); /// addSInt - Add an signed integer attribute data and value. void addSInt(DIE &Die, dwarf::Attribute Attribute, Optional Form, int64_t Integer); void addSInt(DIELoc &Die, Optional Form, int64_t Integer); /// addString - Add a string attribute data and value. void addString(DIE &Die, dwarf::Attribute Attribute, const StringRef Str); /// addLocalString - Add a string attribute data and value. void addLocalString(DIE &Die, dwarf::Attribute Attribute, const StringRef Str); /// addExpr - Add a Dwarf expression attribute data and value. void addExpr(DIELoc &Die, dwarf::Form Form, const MCExpr *Expr); /// addLabel - Add a Dwarf label attribute data and value. void addLabel(DIE &Die, dwarf::Attribute Attribute, dwarf::Form Form, const MCSymbol *Label); void addLabel(DIELoc &Die, dwarf::Form Form, const MCSymbol *Label); /// addLocationList - Add a Dwarf loclistptr attribute data and value. void addLocationList(DIE &Die, dwarf::Attribute Attribute, unsigned Index); /// addSectionLabel - Add a Dwarf section label attribute data and value. /// void addSectionLabel(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Label); /// addSectionOffset - Add an offset into a section attribute data and value. /// void addSectionOffset(DIE &Die, dwarf::Attribute Attribute, uint64_t Integer); /// addOpAddress - Add a dwarf op address data and value using the /// form given and an op of either DW_FORM_addr or DW_FORM_GNU_addr_index. void addOpAddress(DIELoc &Die, const MCSymbol *Label); /// addSectionDelta - Add a label delta attribute data and value. void addSectionDelta(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Hi, const MCSymbol *Lo); /// addLabelDelta - Add a label delta attribute data and value. void addLabelDelta(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Hi, const MCSymbol *Lo); /// addDIEEntry - Add a DIE attribute data and value. void addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIE &Entry); /// addDIEEntry - Add a DIE attribute data and value. void addDIEEntry(DIE &Die, dwarf::Attribute Attribute, DIEEntry *Entry); void addDIETypeSignature(DIE &Die, const DwarfTypeUnit &Type); /// addBlock - Add block data. void addBlock(DIE &Die, dwarf::Attribute Attribute, DIELoc *Block); /// addBlock - Add block data. void addBlock(DIE &Die, dwarf::Attribute Attribute, DIEBlock *Block); /// addSourceLine - Add location information to specified debug information /// entry. void addSourceLine(DIE &Die, unsigned Line, StringRef File, StringRef Directory); void addSourceLine(DIE &Die, DIVariable V); void addSourceLine(DIE &Die, DIGlobalVariable G); void addSourceLine(DIE &Die, DISubprogram SP); void addSourceLine(DIE &Die, DIType Ty); void addSourceLine(DIE &Die, DINameSpace NS); void addSourceLine(DIE &Die, DIObjCProperty Ty); /// addAddress - Add an address attribute to a die based on the location /// provided. void addAddress(DIE &Die, dwarf::Attribute Attribute, const MachineLocation &Location, bool Indirect = false); /// addConstantValue - Add constant value entry in variable DIE. void addConstantValue(DIE &Die, const MachineOperand &MO, DIType Ty); void addConstantValue(DIE &Die, const ConstantInt *CI, bool Unsigned); void addConstantValue(DIE &Die, const APInt &Val, bool Unsigned); /// addConstantFPValue - Add constant value entry in variable DIE. void addConstantFPValue(DIE &Die, const MachineOperand &MO); void addConstantFPValue(DIE &Die, const ConstantFP *CFP); /// addTemplateParams - Add template parameters in buffer. void addTemplateParams(DIE &Buffer, DIArray TParams); /// addRegisterOp - Add register operand. void addRegisterOp(DIELoc &TheDie, unsigned Reg); /// addRegisterOffset - Add register offset. void addRegisterOffset(DIELoc &TheDie, unsigned Reg, int64_t Offset); /// addComplexAddress - Start with the address based on the location provided, /// and generate the DWARF information necessary to find the actual variable /// (navigating the extra location information encoded in the type) based on /// the starting location. Add the DWARF information to the die. void addComplexAddress(const DbgVariable &DV, DIE &Die, dwarf::Attribute Attribute, const MachineLocation &Location); // FIXME: Should be reformulated in terms of addComplexAddress. /// addBlockByrefAddress - Start with the address based on the location /// provided, and generate the DWARF information necessary to find the /// actual Block variable (navigating the Block struct) based on the /// starting location. Add the DWARF information to the die. Obsolete, /// please use addComplexAddress instead. void addBlockByrefAddress(const DbgVariable &DV, DIE &Die, dwarf::Attribute Attribute, const MachineLocation &Location); /// addVariableAddress - Add DW_AT_location attribute for a /// DbgVariable based on provided MachineLocation. void addVariableAddress(const DbgVariable &DV, DIE &Die, MachineLocation Location); /// addType - Add a new type attribute to the specified entity. This takes /// and attribute parameter because DW_AT_friend attributes are also /// type references. void addType(DIE &Entity, DIType Ty, dwarf::Attribute Attribute = dwarf::DW_AT_type); /// getOrCreateNameSpace - Create a DIE for DINameSpace. DIE *getOrCreateNameSpace(DINameSpace NS); /// getOrCreateSubprogramDIE - Create new DIE using SP. DIE *getOrCreateSubprogramDIE(DISubprogram SP); /// getOrCreateTypeDIE - Find existing DIE or create new DIE for the /// given DIType. DIE *getOrCreateTypeDIE(const MDNode *N); /// getOrCreateContextDIE - Get context owner's DIE. DIE *createTypeDIE(DICompositeType Ty); /// getOrCreateContextDIE - Get context owner's DIE. DIE *getOrCreateContextDIE(DIScope Context); /// constructContainingTypeDIEs - Construct DIEs for types that contain /// vtables. void constructContainingTypeDIEs(); /// constructVariableDIE - Construct a DIE for the given DbgVariable. std::unique_ptr constructVariableDIE(DbgVariable &DV, AbstractOrInlined AbsIn = AOI_None); /// constructSubprogramArguments - Construct function argument DIEs. void constructSubprogramArguments(DIE &Buffer, DIArray Args); /// Create a DIE with the given Tag, add the DIE to its parent, and /// call insertDIE if MD is not null. DIE &createAndAddDIE(unsigned Tag, DIE &Parent, DIDescriptor N = DIDescriptor()); /// Compute the size of a header for this unit, not including the initial /// length field. virtual unsigned getHeaderSize() const { return sizeof(int16_t) + // DWARF version number sizeof(int32_t) + // Offset Into Abbrev. Section sizeof(int8_t); // Pointer Size (in bytes) } /// Emit the header for this unit, not including the initial length field. virtual void emitHeader(const MCSymbol *ASectionSym) const; virtual DwarfCompileUnit &getCU() = 0; /// constructTypeDIE - Construct type DIE from DICompositeType. void constructTypeDIE(DIE &Buffer, DICompositeType CTy); protected: /// getOrCreateStaticMemberDIE - Create new static data member DIE. DIE *getOrCreateStaticMemberDIE(DIDerivedType DT); /// Look up the source ID with the given directory and source file names. If /// none currently exists, create a new ID and insert it in the line table. virtual unsigned getOrCreateSourceID(StringRef File, StringRef Directory) = 0; private: /// \brief Construct a DIE for the given DbgVariable without initializing the /// DbgVariable's DIE reference. std::unique_ptr constructVariableDIEImpl(const DbgVariable &DV, AbstractOrInlined AbsIn); /// constructTypeDIE - Construct basic type die from DIBasicType. void constructTypeDIE(DIE &Buffer, DIBasicType BTy); /// constructTypeDIE - Construct derived type die from DIDerivedType. void constructTypeDIE(DIE &Buffer, DIDerivedType DTy); /// constructSubrangeDIE - Construct subrange DIE from DISubrange. void constructSubrangeDIE(DIE &Buffer, DISubrange SR, DIE *IndexTy); /// constructArrayTypeDIE - Construct array type DIE from DICompositeType. void constructArrayTypeDIE(DIE &Buffer, DICompositeType CTy); /// constructEnumTypeDIE - Construct enum type DIE from DIEnumerator. void constructEnumTypeDIE(DIE &Buffer, DICompositeType CTy); /// constructMemberDIE - Construct member DIE from DIDerivedType. void constructMemberDIE(DIE &Buffer, DIDerivedType DT); /// constructTemplateTypeParameterDIE - Construct new DIE for the given /// DITemplateTypeParameter. void constructTemplateTypeParameterDIE(DIE &Buffer, DITemplateTypeParameter TP); /// constructTemplateValueParameterDIE - Construct new DIE for the given /// DITemplateValueParameter. void constructTemplateValueParameterDIE(DIE &Buffer, DITemplateValueParameter TVP); /// getLowerBoundDefault - Return the default lower bound for an array. If the /// DWARF version doesn't handle the language, return -1. int64_t getDefaultLowerBound() const; /// getDIEEntry - Returns the debug information entry for the specified /// debug variable. DIEEntry *getDIEEntry(const MDNode *N) const { return MDNodeToDIEEntryMap.lookup(N); } /// insertDIEEntry - Insert debug information entry into the map. void insertDIEEntry(const MDNode *N, DIEEntry *E) { MDNodeToDIEEntryMap.insert(std::make_pair(N, E)); } // getIndexTyDie - Get an anonymous type for index type. DIE *getIndexTyDie() { return IndexTyDie; } // setIndexTyDie - Set D as anonymous type for index which can be reused // later. void setIndexTyDie(DIE *D) { IndexTyDie = D; } /// createDIEEntry - Creates a new DIEEntry to be a proxy for a debug /// information entry. DIEEntry *createDIEEntry(DIE &Entry); /// resolve - Look in the DwarfDebug map for the MDNode that /// corresponds to the reference. template T resolve(DIRef Ref) const { return DD->resolve(Ref); } /// If this is a named finished type then include it in the list of types for /// the accelerator tables. void updateAcceleratorTables(DIScope Context, DIType Ty, const DIE &TyDIE); }; class DwarfCompileUnit : public DwarfUnit { /// The attribute index of DW_AT_stmt_list in the compile unit DIE, avoiding /// the need to search for it in applyStmtList. unsigned stmtListIndex; public: DwarfCompileUnit(unsigned UID, DICompileUnit Node, AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU); void initStmtList(MCSymbol *DwarfLineSectionSym); /// Apply the DW_AT_stmt_list from this compile unit to the specified DIE. void applyStmtList(DIE &D); /// createGlobalVariableDIE - create global variable DIE. void createGlobalVariableDIE(DIGlobalVariable GV); /// addLabelAddress - Add a dwarf label attribute data and value using /// either DW_FORM_addr or DW_FORM_GNU_addr_index. void addLabelAddress(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Label); /// addLocalLabelAddress - Add a dwarf label attribute data and value using /// DW_FORM_addr only. void addLocalLabelAddress(DIE &Die, dwarf::Attribute Attribute, const MCSymbol *Label); DwarfCompileUnit &getCU() override { return *this; } unsigned getOrCreateSourceID(StringRef FileName, StringRef DirName) override; }; class DwarfTypeUnit : public DwarfUnit { private: uint64_t TypeSignature; const DIE *Ty; DwarfCompileUnit &CU; MCDwarfDwoLineTable *SplitLineTable; public: DwarfTypeUnit(unsigned UID, DwarfCompileUnit &CU, AsmPrinter *A, DwarfDebug *DW, DwarfFile *DWU, MCDwarfDwoLineTable *SplitLineTable = nullptr); void setTypeSignature(uint64_t Signature) { TypeSignature = Signature; } uint64_t getTypeSignature() const { return TypeSignature; } void setType(const DIE *Ty) { this->Ty = Ty; } /// Emit the header for this unit, not including the initial length field. void emitHeader(const MCSymbol *ASectionSym) const override; unsigned getHeaderSize() const override { return DwarfUnit::getHeaderSize() + sizeof(uint64_t) + // Type Signature sizeof(uint32_t); // Type DIE Offset } void initSection(const MCSection *Section); DwarfCompileUnit &getCU() override { return CU; } protected: unsigned getOrCreateSourceID(StringRef File, StringRef Directory) override; }; } // end llvm namespace #endif