//===-- EHStreamer.h - Exception Handling Directive Streamer ---*- C++ -*--===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file contains support for writing exception info into assembly files. // //===----------------------------------------------------------------------===// #ifndef LLVM_LIB_CODEGEN_ASMPRINTER_EHSTREAMER_H #define LLVM_LIB_CODEGEN_ASMPRINTER_EHSTREAMER_H #include "AsmPrinterHandler.h" #include "llvm/ADT/DenseMap.h" namespace llvm { struct LandingPadInfo; class MachineModuleInfo; class MachineInstr; class MachineFunction; class AsmPrinter; template class SmallVectorImpl; /// Emits exception handling directives. class EHStreamer : public AsmPrinterHandler { protected: /// Target of directive emission. AsmPrinter *Asm; /// Collected machine module information. MachineModuleInfo *MMI; /// How many leading type ids two landing pads have in common. static unsigned sharedTypeIDs(const LandingPadInfo *L, const LandingPadInfo *R); /// Structure holding a try-range and the associated landing pad. struct PadRange { // The index of the landing pad. unsigned PadIndex; // The index of the begin and end labels in the landing pad's label lists. unsigned RangeIndex; }; typedef DenseMap RangeMapType; /// Structure describing an entry in the actions table. struct ActionEntry { int ValueForTypeID; // The value to write - may not be equal to the type id. int NextAction; unsigned Previous; }; /// Structure describing an entry in the call-site table. struct CallSiteEntry { // The 'try-range' is BeginLabel .. EndLabel. MCSymbol *BeginLabel; // zero indicates the start of the function. MCSymbol *EndLabel; // zero indicates the end of the function. // The landing pad starts at PadLabel. MCSymbol *PadLabel; // zero indicates that there is no landing pad. unsigned Action; }; /// Compute the actions table and gather the first action index for each /// landing pad site. unsigned computeActionsTable(const SmallVectorImpl&LPs, SmallVectorImpl &Actions, SmallVectorImpl &FirstActions); /// Return `true' if this is a call to a function marked `nounwind'. Return /// `false' otherwise. bool callToNoUnwindFunction(const MachineInstr *MI); /// Compute the call-site table. The entry for an invoke has a try-range /// containing the call, a non-zero landing pad and an appropriate action. /// The entry for an ordinary call has a try-range containing the call and /// zero for the landing pad and the action. Calls marked 'nounwind' have /// no entry and must not be contained in the try-range of any entry - they /// form gaps in the table. Entries must be ordered by try-range address. void computeCallSiteTable(SmallVectorImpl &CallSites, const RangeMapType &PadMap, const SmallVectorImpl &LPs, const SmallVectorImpl &FirstActions); /// Emit landing pads and actions. /// /// The general organization of the table is complex, but the basic concepts /// are easy. First there is a header which describes the location and /// organization of the three components that follow. /// 1. The landing pad site information describes the range of code covered /// by the try. In our case it's an accumulation of the ranges covered /// by the invokes in the try. There is also a reference to the landing /// pad that handles the exception once processed. Finally an index into /// the actions table. /// 2. The action table, in our case, is composed of pairs of type ids /// and next action offset. Starting with the action index from the /// landing pad site, each type Id is checked for a match to the current /// exception. If it matches then the exception and type id are passed /// on to the landing pad. Otherwise the next action is looked up. This /// chain is terminated with a next action of zero. If no type id is /// found the frame is unwound and handling continues. /// 3. Type id table contains references to all the C++ typeinfo for all /// catches in the function. This tables is reversed indexed base 1. void emitExceptionTable(); virtual void emitTypeInfos(unsigned TTypeEncoding); public: EHStreamer(AsmPrinter *A); virtual ~EHStreamer(); /// Emit all exception information that should come after the content. void endModule() override; /// Gather pre-function exception information. Assumes being emitted /// immediately after the function entry point. void beginFunction(const MachineFunction *MF) override; /// Gather and emit post-function exception information. void endFunction(const MachineFunction *) override; // Unused. void setSymbolSize(const MCSymbol *Sym, uint64_t Size) override {} void beginInstruction(const MachineInstr *MI) override {} void endInstruction() override {} }; } #endif