//===-- CallingConvLower.cpp - Calling Conventions ------------------------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the CCState class, used for lowering and implementing // calling conventions. // //===----------------------------------------------------------------------===// #include "llvm/CodeGen/CallingConvLower.h" #include "llvm/CodeGen/MachineFrameInfo.h" #include "llvm/IR/DataLayout.h" #include "llvm/Support/Debug.h" #include "llvm/Support/ErrorHandling.h" #include "llvm/Support/raw_ostream.h" #include "llvm/Target/TargetLowering.h" #include "llvm/Target/TargetMachine.h" #include "llvm/Target/TargetRegisterInfo.h" #include "llvm/Target/TargetSubtargetInfo.h" using namespace llvm; CCState::CCState(CallingConv::ID CC, bool isVarArg, MachineFunction &mf, SmallVectorImpl &locs, LLVMContext &C) : CallingConv(CC), IsVarArg(isVarArg), MF(mf), TRI(*MF.getSubtarget().getRegisterInfo()), Locs(locs), Context(C), CallOrPrologue(Unknown) { // No stack is used. StackOffset = 0; clearByValRegsInfo(); UsedRegs.resize((TRI.getNumRegs()+31)/32); } // HandleByVal - Allocate space on the stack large enough to pass an argument // by value. The size and alignment information of the argument is encoded in // its parameter attribute. void CCState::HandleByVal(unsigned ValNo, MVT ValVT, MVT LocVT, CCValAssign::LocInfo LocInfo, int MinSize, int MinAlign, ISD::ArgFlagsTy ArgFlags) { unsigned Align = ArgFlags.getByValAlign(); unsigned Size = ArgFlags.getByValSize(); if (MinSize > (int)Size) Size = MinSize; if (MinAlign > (int)Align) Align = MinAlign; MF.getFrameInfo()->ensureMaxAlignment(Align); MF.getSubtarget().getTargetLowering()->HandleByVal(this, Size, Align); Size = unsigned(RoundUpToAlignment(Size, MinAlign)); unsigned Offset = AllocateStack(Size, Align); addLoc(CCValAssign::getMem(ValNo, ValVT, Offset, LocVT, LocInfo)); } /// MarkAllocated - Mark a register and all of its aliases as allocated. void CCState::MarkAllocated(unsigned Reg) { for (MCRegAliasIterator AI(Reg, &TRI, true); AI.isValid(); ++AI) UsedRegs[*AI/32] |= 1 << (*AI&31); } /// AnalyzeFormalArguments - Analyze an array of argument values, /// incorporating info about the formals into this state. void CCState::AnalyzeFormalArguments(const SmallVectorImpl &Ins, CCAssignFn Fn) { unsigned NumArgs = Ins.size(); for (unsigned i = 0; i != NumArgs; ++i) { MVT ArgVT = Ins[i].VT; ISD::ArgFlagsTy ArgFlags = Ins[i].Flags; if (Fn(i, ArgVT, ArgVT, CCValAssign::Full, ArgFlags, *this)) { #ifndef NDEBUG dbgs() << "Formal argument #" << i << " has unhandled type " << EVT(ArgVT).getEVTString() << '\n'; #endif llvm_unreachable(nullptr); } } } /// CheckReturn - Analyze the return values of a function, returning true if /// the return can be performed without sret-demotion, and false otherwise. bool CCState::CheckReturn(const SmallVectorImpl &Outs, CCAssignFn Fn) { // Determine which register each value should be copied into. for (unsigned i = 0, e = Outs.size(); i != e; ++i) { MVT VT = Outs[i].VT; ISD::ArgFlagsTy ArgFlags = Outs[i].Flags; if (Fn(i, VT, VT, CCValAssign::Full, ArgFlags, *this)) return false; } return true; } /// AnalyzeReturn - Analyze the returned values of a return, /// incorporating info about the result values into this state. void CCState::AnalyzeReturn(const SmallVectorImpl &Outs, CCAssignFn Fn) { // Determine which register each value should be copied into. for (unsigned i = 0, e = Outs.size(); i != e; ++i) { MVT VT = Outs[i].VT; ISD::ArgFlagsTy ArgFlags = Outs[i].Flags; if (Fn(i, VT, VT, CCValAssign::Full, ArgFlags, *this)) { #ifndef NDEBUG dbgs() << "Return operand #" << i << " has unhandled type " << EVT(VT).getEVTString() << '\n'; #endif llvm_unreachable(nullptr); } } } /// AnalyzeCallOperands - Analyze the outgoing arguments to a call, /// incorporating info about the passed values into this state. void CCState::AnalyzeCallOperands(const SmallVectorImpl &Outs, CCAssignFn Fn) { unsigned NumOps = Outs.size(); for (unsigned i = 0; i != NumOps; ++i) { MVT ArgVT = Outs[i].VT; ISD::ArgFlagsTy ArgFlags = Outs[i].Flags; if (Fn(i, ArgVT, ArgVT, CCValAssign::Full, ArgFlags, *this)) { #ifndef NDEBUG dbgs() << "Call operand #" << i << " has unhandled type " << EVT(ArgVT).getEVTString() << '\n'; #endif llvm_unreachable(nullptr); } } } /// AnalyzeCallOperands - Same as above except it takes vectors of types /// and argument flags. void CCState::AnalyzeCallOperands(SmallVectorImpl &ArgVTs, SmallVectorImpl &Flags, CCAssignFn Fn) { unsigned NumOps = ArgVTs.size(); for (unsigned i = 0; i != NumOps; ++i) { MVT ArgVT = ArgVTs[i]; ISD::ArgFlagsTy ArgFlags = Flags[i]; if (Fn(i, ArgVT, ArgVT, CCValAssign::Full, ArgFlags, *this)) { #ifndef NDEBUG dbgs() << "Call operand #" << i << " has unhandled type " << EVT(ArgVT).getEVTString() << '\n'; #endif llvm_unreachable(nullptr); } } } /// AnalyzeCallResult - Analyze the return values of a call, /// incorporating info about the passed values into this state. void CCState::AnalyzeCallResult(const SmallVectorImpl &Ins, CCAssignFn Fn) { for (unsigned i = 0, e = Ins.size(); i != e; ++i) { MVT VT = Ins[i].VT; ISD::ArgFlagsTy Flags = Ins[i].Flags; if (Fn(i, VT, VT, CCValAssign::Full, Flags, *this)) { #ifndef NDEBUG dbgs() << "Call result #" << i << " has unhandled type " << EVT(VT).getEVTString() << '\n'; #endif llvm_unreachable(nullptr); } } } /// AnalyzeCallResult - Same as above except it's specialized for calls which /// produce a single value. void CCState::AnalyzeCallResult(MVT VT, CCAssignFn Fn) { if (Fn(0, VT, VT, CCValAssign::Full, ISD::ArgFlagsTy(), *this)) { #ifndef NDEBUG dbgs() << "Call result has unhandled type " << EVT(VT).getEVTString() << '\n'; #endif llvm_unreachable(nullptr); } }