//===--- LivePhysRegs.cpp - Live Physical Register Set --------------------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the LivePhysRegs utility for tracking liveness of // physical registers across machine instructions in forward or backward order. // A more detailed description can be found in the corresponding header file. // //===----------------------------------------------------------------------===// #include "llvm/CodeGen/LivePhysRegs.h" #include "llvm/CodeGen/MachineInstrBundle.h" #include "llvm/Support/Debug.h" using namespace llvm; /// \brief Remove all registers from the set that get clobbered by the register /// mask. void LivePhysRegs::removeRegsInMask(const MachineOperand &MO) { SparseSet::iterator LRI = LiveRegs.begin(); while (LRI != LiveRegs.end()) { if (MO.clobbersPhysReg(*LRI)) LRI = LiveRegs.erase(LRI); else ++LRI; } } /// Simulates liveness when stepping backwards over an instruction(bundle): /// Remove Defs, add uses. This is the recommended way of calculating liveness. void LivePhysRegs::stepBackward(const MachineInstr &MI) { // Remove defined registers and regmask kills from the set. for (ConstMIBundleOperands O(&MI); O.isValid(); ++O) { if (O->isReg()) { if (!O->isDef()) continue; unsigned Reg = O->getReg(); if (Reg == 0) continue; removeReg(Reg); } else if (O->isRegMask()) removeRegsInMask(*O); } // Add uses to the set. for (ConstMIBundleOperands O(&MI); O.isValid(); ++O) { if (!O->isReg() || !O->readsReg() || O->isUndef()) continue; unsigned Reg = O->getReg(); if (Reg == 0) continue; addReg(Reg); } } /// Simulates liveness when stepping forward over an instruction(bundle): Remove /// killed-uses, add defs. This is the not recommended way, because it depends /// on accurate kill flags. If possible use stepBackwards() instead of this /// function. void LivePhysRegs::stepForward(const MachineInstr &MI) { SmallVector Defs; // Remove killed registers from the set. for (ConstMIBundleOperands O(&MI); O.isValid(); ++O) { if (O->isReg()) { unsigned Reg = O->getReg(); if (Reg == 0) continue; if (O->isDef()) { if (!O->isDead()) Defs.push_back(Reg); } else { if (!O->isKill()) continue; assert(O->isUse()); removeReg(Reg); } } else if (O->isRegMask()) removeRegsInMask(*O); } // Add defs to the set. for (unsigned i = 0, e = Defs.size(); i != e; ++i) addReg(Defs[i]); } /// Prin the currently live registers to OS. void LivePhysRegs::print(raw_ostream &OS) const { OS << "Live Registers:"; if (!TRI) { OS << " (uninitialized)\n"; return; } if (empty()) { OS << " (empty)\n"; return; } for (const_iterator I = begin(), E = end(); I != E; ++I) OS << " " << PrintReg(*I, TRI); OS << "\n"; } /// Dumps the currently live registers to the debug output. void LivePhysRegs::dump() const { #if !defined(NDEBUG) || defined(LLVM_ENABLE_DUMP) dbgs() << " " << *this; #endif }