//===-- llvm/CodeGen/PseudoSourceValue.cpp ----------------------*- C++ -*-===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the PseudoSourceValue class. // //===----------------------------------------------------------------------===// #include "llvm/CodeGen/PseudoSourceValue.h" #include "llvm/CodeGen/MachineFrameInfo.h" #include "llvm/IR/DerivedTypes.h" #include "llvm/IR/LLVMContext.h" #include "llvm/Support/ErrorHandling.h" #include "llvm/Support/ManagedStatic.h" #include "llvm/Support/Mutex.h" #include "llvm/Support/raw_ostream.h" #include using namespace llvm; namespace { struct PSVGlobalsTy { // PseudoSourceValues are immutable so don't need locking. const PseudoSourceValue PSVs[4]; sys::Mutex Lock; // Guards FSValues, but not the values inside it. std::map FSValues; PSVGlobalsTy() : PSVs() {} ~PSVGlobalsTy() { for (std::map::iterator I = FSValues.begin(), E = FSValues.end(); I != E; ++I) { delete I->second; } } }; static ManagedStatic PSVGlobals; } // anonymous namespace const PseudoSourceValue *PseudoSourceValue::getStack() { return &PSVGlobals->PSVs[0]; } const PseudoSourceValue *PseudoSourceValue::getGOT() { return &PSVGlobals->PSVs[1]; } const PseudoSourceValue *PseudoSourceValue::getJumpTable() { return &PSVGlobals->PSVs[2]; } const PseudoSourceValue *PseudoSourceValue::getConstantPool() { return &PSVGlobals->PSVs[3]; } static const char *const PSVNames[] = { "Stack", "GOT", "JumpTable", "ConstantPool" }; PseudoSourceValue::PseudoSourceValue(bool isFixed) : isFixed(isFixed) {} PseudoSourceValue::~PseudoSourceValue() {} void PseudoSourceValue::printCustom(raw_ostream &O) const { O << PSVNames[this - PSVGlobals->PSVs]; } const PseudoSourceValue *PseudoSourceValue::getFixedStack(int FI) { PSVGlobalsTy &PG = *PSVGlobals; sys::ScopedLock locked(PG.Lock); const PseudoSourceValue *&V = PG.FSValues[FI]; if (!V) V = new FixedStackPseudoSourceValue(FI); return V; } bool PseudoSourceValue::isConstant(const MachineFrameInfo *) const { if (this == getStack()) return false; if (this == getGOT() || this == getConstantPool() || this == getJumpTable()) return true; llvm_unreachable("Unknown PseudoSourceValue!"); } bool PseudoSourceValue::isAliased(const MachineFrameInfo *MFI) const { if (this == getStack() || this == getGOT() || this == getConstantPool() || this == getJumpTable()) return false; llvm_unreachable("Unknown PseudoSourceValue!"); } bool PseudoSourceValue::mayAlias(const MachineFrameInfo *MFI) const { if (this == getGOT() || this == getConstantPool() || this == getJumpTable()) return false; return true; } bool FixedStackPseudoSourceValue::isConstant(const MachineFrameInfo *MFI) const{ return MFI && MFI->isImmutableObjectIndex(FI); } bool FixedStackPseudoSourceValue::isAliased(const MachineFrameInfo *MFI) const { // Negative frame indices are used for special things that don't // appear in LLVM IR. Non-negative indices may be used for things // like static allocas. if (!MFI) return FI >= 0; // Spill slots should not alias others. return !MFI->isFixedObjectIndex(FI) && !MFI->isSpillSlotObjectIndex(FI); } bool FixedStackPseudoSourceValue::mayAlias(const MachineFrameInfo *MFI) const { if (!MFI) return true; // Spill slots will not alias any LLVM IR value. return !MFI->isSpillSlotObjectIndex(FI); } void FixedStackPseudoSourceValue::printCustom(raw_ostream &OS) const { OS << "FixedStack" << FI; }