//===-- llvm/CodeGen/SDNodeDbgValue.h - SelectionDAG dbg_value --*- C++ -*-===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file declares the SDDbgValue class. // //===----------------------------------------------------------------------===// #ifndef LLVM_CODEGEN_SDNODEDBGVALUE_H #define LLVM_CODEGEN_SDNODEDBGVALUE_H #include "llvm/ADT/SmallVector.h" #include "llvm/Support/DebugLoc.h" namespace llvm { class MDNode; class SDNode; class Value; /// SDDbgValue - Holds the information from a dbg_value node through SDISel. /// We do not use SDValue here to avoid including its header. class SDDbgValue { public: enum DbgValueKind { SDNODE = 0, // value is the result of an expression CONST = 1, // value is a constant FRAMEIX = 2 // value is contents of a stack location }; private: enum DbgValueKind kind; union { struct { SDNode *Node; // valid for expressions unsigned ResNo; // valid for expressions } s; Value *Const; // valid for constants unsigned FrameIx; // valid for stack objects } u; MDNode *mdPtr; uint64_t Offset; DebugLoc DL; unsigned Order; public: // Constructor for non-constants. SDDbgValue(MDNode *mdP, SDNode *N, unsigned R, uint64_t off, DebugLoc dl, unsigned O) : mdPtr(mdP), Offset(off), DL(dl), Order(O) { kind = SDNODE; u.s.Node = N; u.s.ResNo = R; } // Constructor for constants. SDDbgValue(MDNode *mdP, Value *C, uint64_t off, DebugLoc dl, unsigned O) : mdPtr(mdP), Offset(off), DL(dl), Order(O) { kind = CONST; u.Const = C; } // Constructor for frame indices. SDDbgValue(MDNode *mdP, unsigned FI, uint64_t off, DebugLoc dl, unsigned O) : mdPtr(mdP), Offset(off), DL(dl), Order(O) { kind = FRAMEIX; u.FrameIx = FI; } // Returns the kind. DbgValueKind getKind() { return kind; } // Returns the MDNode pointer. MDNode *getMDPtr() { return mdPtr; } // Returns the SDNode* for a register ref SDNode *getSDNode() { assert (kind==SDNODE); return u.s.Node; } // Returns the ResNo for a register ref unsigned getResNo() { assert (kind==SDNODE); return u.s.ResNo; } // Returns the Value* for a constant Value *getConst() { assert (kind==CONST); return u.Const; } // Returns the FrameIx for a stack object unsigned getFrameIx() { assert (kind==FRAMEIX); return u.FrameIx; } // Returns the offset. uint64_t getOffset() { return Offset; } // Returns the DebugLoc. DebugLoc getDebugLoc() { return DL; } // Returns the SDNodeOrder. This is the order of the preceding node in the // input. unsigned getOrder() { return Order; } }; } // end llvm namespace #endif