//===-- StackColoring.cpp -------------------------------------------------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This pass implements the stack-coloring optimization that looks for // lifetime markers machine instructions (LIFESTART_BEGIN and LIFESTART_END), // which represent the possible lifetime of stack slots. It attempts to // merge disjoint stack slots and reduce the used stack space. // NOTE: This pass is not StackSlotColoring, which optimizes spill slots. // // TODO: In the future we plan to improve stack coloring in the following ways: // 1. Allow merging multiple small slots into a single larger slot at different // offsets. // 2. Merge this pass with StackSlotColoring and allow merging of allocas with // spill slots. // //===----------------------------------------------------------------------===// #define DEBUG_TYPE "stackcoloring" #include "llvm/CodeGen/Passes.h" #include "llvm/ADT/BitVector.h" #include "llvm/ADT/DepthFirstIterator.h" #include "llvm/ADT/PostOrderIterator.h" #include "llvm/ADT/SetVector.h" #include "llvm/ADT/SmallPtrSet.h" #include "llvm/ADT/SparseSet.h" #include "llvm/ADT/Statistic.h" #include "llvm/Analysis/Dominators.h" #include "llvm/Analysis/ValueTracking.h" #include "llvm/CodeGen/LiveInterval.h" #include "llvm/CodeGen/MachineBasicBlock.h" #include "llvm/CodeGen/MachineBranchProbabilityInfo.h" #include "llvm/CodeGen/MachineDominators.h" #include "llvm/CodeGen/MachineFrameInfo.h" #include "llvm/CodeGen/MachineFunctionPass.h" #include "llvm/CodeGen/MachineLoopInfo.h" #include "llvm/CodeGen/MachineMemOperand.h" #include "llvm/CodeGen/MachineModuleInfo.h" #include "llvm/CodeGen/MachineRegisterInfo.h" #include "llvm/CodeGen/PseudoSourceValue.h" #include "llvm/CodeGen/SlotIndexes.h" #include "llvm/DebugInfo.h" #include "llvm/IR/Function.h" #include "llvm/IR/Instructions.h" #include "llvm/IR/Module.h" #include "llvm/MC/MCInstrItineraries.h" #include "llvm/Support/CommandLine.h" #include "llvm/Support/Debug.h" #include "llvm/Support/raw_ostream.h" #include "llvm/Target/TargetInstrInfo.h" #include "llvm/Target/TargetRegisterInfo.h" using namespace llvm; static cl::opt DisableColoring("no-stack-coloring", cl::init(false), cl::Hidden, cl::desc("Disable stack coloring")); /// The user may write code that uses allocas outside of the declared lifetime /// zone. This can happen when the user returns a reference to a local /// data-structure. We can detect these cases and decide not to optimize the /// code. If this flag is enabled, we try to save the user. static cl::opt ProtectFromEscapedAllocas("protect-from-escaped-allocas", cl::init(false), cl::Hidden, cl::desc("Do not optimize lifetime zones that " "are broken")); STATISTIC(NumMarkerSeen, "Number of lifetime markers found."); STATISTIC(StackSpaceSaved, "Number of bytes saved due to merging slots."); STATISTIC(StackSlotMerged, "Number of stack slot merged."); STATISTIC(EscapedAllocas, "Number of allocas that escaped the lifetime region"); //===----------------------------------------------------------------------===// // StackColoring Pass //===----------------------------------------------------------------------===// namespace { /// StackColoring - A machine pass for merging disjoint stack allocations, /// marked by the LIFETIME_START and LIFETIME_END pseudo instructions. class StackColoring : public MachineFunctionPass { MachineFrameInfo *MFI; MachineFunction *MF; /// A class representing liveness information for a single basic block. /// Each bit in the BitVector represents the liveness property /// for a different stack slot. struct BlockLifetimeInfo { /// Which slots BEGINs in each basic block. BitVector Begin; /// Which slots ENDs in each basic block. BitVector End; /// Which slots are marked as LIVE_IN, coming into each basic block. BitVector LiveIn; /// Which slots are marked as LIVE_OUT, coming out of each basic block. BitVector LiveOut; }; /// Maps active slots (per bit) for each basic block. typedef DenseMap LivenessMap; LivenessMap BlockLiveness; /// Maps serial numbers to basic blocks. DenseMap BasicBlocks; /// Maps basic blocks to a serial number. SmallVector BasicBlockNumbering; /// Maps liveness intervals for each slot. SmallVector Intervals; /// VNInfo is used for the construction of LiveIntervals. VNInfo::Allocator VNInfoAllocator; /// SlotIndex analysis object. SlotIndexes *Indexes; /// The list of lifetime markers found. These markers are to be removed /// once the coloring is done. SmallVector Markers; /// SlotSizeSorter - A Sort utility for arranging stack slots according /// to their size. struct SlotSizeSorter { MachineFrameInfo *MFI; SlotSizeSorter(MachineFrameInfo *mfi) : MFI(mfi) { } bool operator()(int LHS, int RHS) { // We use -1 to denote a uninteresting slot. Place these slots at the end. if (LHS == -1) return false; if (RHS == -1) return true; // Sort according to size. return MFI->getObjectSize(LHS) > MFI->getObjectSize(RHS); } }; public: static char ID; StackColoring() : MachineFunctionPass(ID) { initializeStackColoringPass(*PassRegistry::getPassRegistry()); } void getAnalysisUsage(AnalysisUsage &AU) const; bool runOnMachineFunction(MachineFunction &MF); private: /// Debug. void dump() const; /// Removes all of the lifetime marker instructions from the function. /// \returns true if any markers were removed. bool removeAllMarkers(); /// Scan the machine function and find all of the lifetime markers. /// Record the findings in the BEGIN and END vectors. /// \returns the number of markers found. unsigned collectMarkers(unsigned NumSlot); /// Perform the dataflow calculation and calculate the lifetime for each of /// the slots, based on the BEGIN/END vectors. Set the LifetimeLIVE_IN and /// LifetimeLIVE_OUT maps that represent which stack slots are live coming /// in and out blocks. void calculateLocalLiveness(); /// Construct the LiveIntervals for the slots. void calculateLiveIntervals(unsigned NumSlots); /// Go over the machine function and change instructions which use stack /// slots to use the joint slots. void remapInstructions(DenseMap &SlotRemap); /// The input program may contain instructions which are not inside lifetime /// markers. This can happen due to a bug in the compiler or due to a bug in /// user code (for example, returning a reference to a local variable). /// This procedure checks all of the instructions in the function and /// invalidates lifetime ranges which do not contain all of the instructions /// which access that frame slot. void removeInvalidSlotRanges(); /// Map entries which point to other entries to their destination. /// A->B->C becomes A->C. void expungeSlotMap(DenseMap &SlotRemap, unsigned NumSlots); }; } // end anonymous namespace char StackColoring::ID = 0; char &llvm::StackColoringID = StackColoring::ID; INITIALIZE_PASS_BEGIN(StackColoring, "stack-coloring", "Merge disjoint stack slots", false, false) INITIALIZE_PASS_DEPENDENCY(MachineDominatorTree) INITIALIZE_PASS_DEPENDENCY(SlotIndexes) INITIALIZE_PASS_END(StackColoring, "stack-coloring", "Merge disjoint stack slots", false, false) void StackColoring::getAnalysisUsage(AnalysisUsage &AU) const { AU.addRequired(); AU.addPreserved(); AU.addRequired(); MachineFunctionPass::getAnalysisUsage(AU); } void StackColoring::dump() const { for (df_iterator FI = df_begin(MF), FE = df_end(MF); FI != FE; ++FI) { DEBUG(dbgs()<<"Inspecting block #"<getName()<<"]\n"); LivenessMap::const_iterator BI = BlockLiveness.find(*FI); assert(BI != BlockLiveness.end() && "Block not found"); const BlockLifetimeInfo &BlockInfo = BI->second; DEBUG(dbgs()<<"BEGIN : {"); for (unsigned i=0; i < BlockInfo.Begin.size(); ++i) DEBUG(dbgs()< FI = df_begin(MF), FE = df_end(MF); FI != FE; ++FI) { // Assign a serial number to this basic block. BasicBlocks[*FI] = BasicBlockNumbering.size(); BasicBlockNumbering.push_back(*FI); // Keep a reference to avoid repeated lookups. BlockLifetimeInfo &BlockInfo = BlockLiveness[*FI]; BlockInfo.Begin.resize(NumSlot); BlockInfo.End.resize(NumSlot); for (MachineBasicBlock::iterator BI = (*FI)->begin(), BE = (*FI)->end(); BI != BE; ++BI) { if (BI->getOpcode() != TargetOpcode::LIFETIME_START && BI->getOpcode() != TargetOpcode::LIFETIME_END) continue; Markers.push_back(BI); bool IsStart = BI->getOpcode() == TargetOpcode::LIFETIME_START; const MachineOperand &MI = BI->getOperand(0); unsigned Slot = MI.getIndex(); MarkersFound++; const AllocaInst *Allocation = MFI->getObjectAllocation(Slot); if (Allocation) { DEBUG(dbgs()<<"Found a lifetime marker for slot #"<getName()<<"\n"); } if (IsStart) { BlockInfo.Begin.set(Slot); } else { if (BlockInfo.Begin.test(Slot)) { // Allocas that start and end within a single block are handled // specially when computing the LiveIntervals to avoid pessimizing // the liveness propagation. BlockInfo.Begin.reset(Slot); } else { BlockInfo.End.set(Slot); } } } } // Update statistics. NumMarkerSeen += MarkersFound; return MarkersFound; } void StackColoring::calculateLocalLiveness() { // Perform a standard reverse dataflow computation to solve for // global liveness. The BEGIN set here is equivalent to KILL in the standard // formulation, and END is equivalent to GEN. The result of this computation // is a map from blocks to bitvectors where the bitvectors represent which // allocas are live in/out of that block. SmallPtrSet BBSet(BasicBlockNumbering.begin(), BasicBlockNumbering.end()); unsigned NumSSMIters = 0; bool changed = true; while (changed) { changed = false; ++NumSSMIters; SmallPtrSet NextBBSet; for (SmallVectorImpl::iterator PI = BasicBlockNumbering.begin(), PE = BasicBlockNumbering.end(); PI != PE; ++PI) { const MachineBasicBlock *BB = *PI; if (!BBSet.count(BB)) continue; // Use an iterator to avoid repeated lookups. LivenessMap::iterator BI = BlockLiveness.find(BB); assert(BI != BlockLiveness.end() && "Block not found"); BlockLifetimeInfo &BlockInfo = BI->second; BitVector LocalLiveIn; BitVector LocalLiveOut; // Forward propagation from begins to ends. for (MachineBasicBlock::const_pred_iterator PI = BB->pred_begin(), PE = BB->pred_end(); PI != PE; ++PI) { LivenessMap::const_iterator I = BlockLiveness.find(*PI); assert(I != BlockLiveness.end() && "Predecessor not found"); LocalLiveIn |= I->second.LiveOut; } LocalLiveIn |= BlockInfo.End; LocalLiveIn.reset(BlockInfo.Begin); // Reverse propagation from ends to begins. for (MachineBasicBlock::const_succ_iterator SI = BB->succ_begin(), SE = BB->succ_end(); SI != SE; ++SI) { LivenessMap::const_iterator I = BlockLiveness.find(*SI); assert(I != BlockLiveness.end() && "Successor not found"); LocalLiveOut |= I->second.LiveIn; } LocalLiveOut |= BlockInfo.Begin; LocalLiveOut.reset(BlockInfo.End); LocalLiveIn |= LocalLiveOut; LocalLiveOut |= LocalLiveIn; // After adopting the live bits, we need to turn-off the bits which // are de-activated in this block. LocalLiveOut.reset(BlockInfo.End); LocalLiveIn.reset(BlockInfo.Begin); // If we have both BEGIN and END markers in the same basic block then // we know that the BEGIN marker comes after the END, because we already // handle the case where the BEGIN comes before the END when collecting // the markers (and building the BEGIN/END vectore). // Want to enable the LIVE_IN and LIVE_OUT of slots that have both // BEGIN and END because it means that the value lives before and after // this basic block. BitVector LocalEndBegin = BlockInfo.End; LocalEndBegin &= BlockInfo.Begin; LocalLiveIn |= LocalEndBegin; LocalLiveOut |= LocalEndBegin; if (LocalLiveIn.test(BlockInfo.LiveIn)) { changed = true; BlockInfo.LiveIn |= LocalLiveIn; for (MachineBasicBlock::const_pred_iterator PI = BB->pred_begin(), PE = BB->pred_end(); PI != PE; ++PI) NextBBSet.insert(*PI); } if (LocalLiveOut.test(BlockInfo.LiveOut)) { changed = true; BlockInfo.LiveOut |= LocalLiveOut; for (MachineBasicBlock::const_succ_iterator SI = BB->succ_begin(), SE = BB->succ_end(); SI != SE; ++SI) NextBBSet.insert(*SI); } } BBSet = NextBBSet; }// while changed. } void StackColoring::calculateLiveIntervals(unsigned NumSlots) { SmallVector Starts; SmallVector Finishes; // For each block, find which slots are active within this block // and update the live intervals. for (MachineFunction::iterator MBB = MF->begin(), MBBe = MF->end(); MBB != MBBe; ++MBB) { Starts.clear(); Starts.resize(NumSlots); Finishes.clear(); Finishes.resize(NumSlots); // Create the interval for the basic blocks with lifetime markers in them. for (SmallVectorImpl::const_iterator it = Markers.begin(), e = Markers.end(); it != e; ++it) { const MachineInstr *MI = *it; if (MI->getParent() != MBB) continue; assert((MI->getOpcode() == TargetOpcode::LIFETIME_START || MI->getOpcode() == TargetOpcode::LIFETIME_END) && "Invalid Lifetime marker"); bool IsStart = MI->getOpcode() == TargetOpcode::LIFETIME_START; const MachineOperand &Mo = MI->getOperand(0); int Slot = Mo.getIndex(); assert(Slot >= 0 && "Invalid slot"); SlotIndex ThisIndex = Indexes->getInstructionIndex(MI); if (IsStart) { if (!Starts[Slot].isValid() || Starts[Slot] > ThisIndex) Starts[Slot] = ThisIndex; } else { if (!Finishes[Slot].isValid() || Finishes[Slot] < ThisIndex) Finishes[Slot] = ThisIndex; } } // Create the interval of the blocks that we previously found to be 'alive'. BlockLifetimeInfo &MBBLiveness = BlockLiveness[MBB]; for (int pos = MBBLiveness.LiveIn.find_first(); pos != -1; pos = MBBLiveness.LiveIn.find_next(pos)) { Starts[pos] = Indexes->getMBBStartIdx(MBB); } for (int pos = MBBLiveness.LiveOut.find_first(); pos != -1; pos = MBBLiveness.LiveOut.find_next(pos)) { Finishes[pos] = Indexes->getMBBEndIdx(MBB); } for (unsigned i = 0; i < NumSlots; ++i) { assert(Starts[i].isValid() == Finishes[i].isValid() && "Unmatched range"); if (!Starts[i].isValid()) continue; assert(Starts[i] && Finishes[i] && "Invalid interval"); VNInfo *ValNum = Intervals[i]->getValNumInfo(0); SlotIndex S = Starts[i]; SlotIndex F = Finishes[i]; if (S < F) { // We have a single consecutive region. Intervals[i]->addSegment(LiveInterval::Segment(S, F, ValNum)); } else { // We have two non consecutive regions. This happens when // LIFETIME_START appears after the LIFETIME_END marker. SlotIndex NewStart = Indexes->getMBBStartIdx(MBB); SlotIndex NewFin = Indexes->getMBBEndIdx(MBB); Intervals[i]->addSegment(LiveInterval::Segment(NewStart, F, ValNum)); Intervals[i]->addSegment(LiveInterval::Segment(S, NewFin, ValNum)); } } } } bool StackColoring::removeAllMarkers() { unsigned Count = 0; for (unsigned i = 0; i < Markers.size(); ++i) { Markers[i]->eraseFromParent(); Count++; } Markers.clear(); DEBUG(dbgs()<<"Removed "< &SlotRemap) { unsigned FixedInstr = 0; unsigned FixedMemOp = 0; unsigned FixedDbg = 0; MachineModuleInfo *MMI = &MF->getMMI(); // Remap debug information that refers to stack slots. MachineModuleInfo::VariableDbgInfoMapTy &VMap = MMI->getVariableDbgInfo(); for (MachineModuleInfo::VariableDbgInfoMapTy::iterator VI = VMap.begin(), VE = VMap.end(); VI != VE; ++VI) { const MDNode *Var = VI->first; if (!Var) continue; std::pair &VP = VI->second; if (SlotRemap.count(VP.first)) { DEBUG(dbgs()<<"Remapping debug info for ["<getName()<<"].\n"); VP.first = SlotRemap[VP.first]; FixedDbg++; } } // Keep a list of *allocas* which need to be remapped. DenseMap Allocas; for (DenseMap::const_iterator it = SlotRemap.begin(), e = SlotRemap.end(); it != e; ++it) { const AllocaInst *From = MFI->getObjectAllocation(it->first); const AllocaInst *To = MFI->getObjectAllocation(it->second); assert(To && From && "Invalid allocation object"); Allocas[From] = To; } // Remap all instructions to the new stack slots. MachineFunction::iterator BB, BBE; MachineBasicBlock::iterator I, IE; for (BB = MF->begin(), BBE = MF->end(); BB != BBE; ++BB) for (I = BB->begin(), IE = BB->end(); I != IE; ++I) { // Skip lifetime markers. We'll remove them soon. if (I->getOpcode() == TargetOpcode::LIFETIME_START || I->getOpcode() == TargetOpcode::LIFETIME_END) continue; // Update the MachineMemOperand to use the new alloca. for (MachineInstr::mmo_iterator MM = I->memoperands_begin(), E = I->memoperands_end(); MM != E; ++MM) { MachineMemOperand *MMO = *MM; const Value *V = MMO->getValue(); if (!V) continue; const PseudoSourceValue *PSV = dyn_cast(V); if (PSV && PSV->isConstant(MFI)) continue; // Climb up and find the original alloca. V = GetUnderlyingObject(V); // If we did not find one, or if the one that we found is not in our // map, then move on. if (!V || !isa(V)) { // Clear mem operand since we don't know for sure that it doesn't // alias a merged alloca. MMO->setValue(0); continue; } const AllocaInst *AI= cast(V); if (!Allocas.count(AI)) continue; MMO->setValue(Allocas[AI]); FixedMemOp++; } // Update all of the machine instruction operands. for (unsigned i = 0 ; i < I->getNumOperands(); ++i) { MachineOperand &MO = I->getOperand(i); if (!MO.isFI()) continue; int FromSlot = MO.getIndex(); // Don't touch arguments. if (FromSlot<0) continue; // Only look at mapped slots. if (!SlotRemap.count(FromSlot)) continue; // In a debug build, check that the instruction that we are modifying is // inside the expected live range. If the instruction is not inside // the calculated range then it means that the alloca usage moved // outside of the lifetime markers, or that the user has a bug. // NOTE: Alloca address calculations which happen outside the lifetime // zone are are okay, despite the fact that we don't have a good way // for validating all of the usages of the calculation. #ifndef NDEBUG bool TouchesMemory = I->mayLoad() || I->mayStore(); // If we *don't* protect the user from escaped allocas, don't bother // validating the instructions. if (!I->isDebugValue() && TouchesMemory && ProtectFromEscapedAllocas) { SlotIndex Index = Indexes->getInstructionIndex(I); LiveInterval *Interval = Intervals[FromSlot]; assert(Interval->find(Index) != Interval->end() && "Found instruction usage outside of live range."); } #endif // Fix the machine instructions. int ToSlot = SlotRemap[FromSlot]; MO.setIndex(ToSlot); FixedInstr++; } } DEBUG(dbgs()<<"Fixed "<begin(), BBE = MF->end(); BB != BBE; ++BB) for (I = BB->begin(), IE = BB->end(); I != IE; ++I) { if (I->getOpcode() == TargetOpcode::LIFETIME_START || I->getOpcode() == TargetOpcode::LIFETIME_END || I->isDebugValue()) continue; // Some intervals are suspicious! In some cases we find address // calculations outside of the lifetime zone, but not actual memory // read or write. Memory accesses outside of the lifetime zone are a clear // violation, but address calculations are okay. This can happen when // GEPs are hoisted outside of the lifetime zone. // So, in here we only check instructions which can read or write memory. if (!I->mayLoad() && !I->mayStore()) continue; // Check all of the machine operands. for (unsigned i = 0 ; i < I->getNumOperands(); ++i) { const MachineOperand &MO = I->getOperand(i); if (!MO.isFI()) continue; int Slot = MO.getIndex(); if (Slot<0) continue; if (Intervals[Slot]->empty()) continue; // Check that the used slot is inside the calculated lifetime range. // If it is not, warn about it and invalidate the range. LiveInterval *Interval = Intervals[Slot]; SlotIndex Index = Indexes->getInstructionIndex(I); if (Interval->find(Index) == Interval->end()) { Intervals[Slot]->clear(); DEBUG(dbgs()<<"Invalidating range #"< &SlotRemap, unsigned NumSlots) { // Expunge slot remap map. for (unsigned i=0; i < NumSlots; ++i) { // If we are remapping i if (SlotRemap.count(i)) { int Target = SlotRemap[i]; // As long as our target is mapped to something else, follow it. while (SlotRemap.count(Target)) { Target = SlotRemap[Target]; SlotRemap[i] = Target; } } } } bool StackColoring::runOnMachineFunction(MachineFunction &Func) { DEBUG(dbgs() << "********** Stack Coloring **********\n" << "********** Function: " << ((const Value*)Func.getFunction())->getName() << '\n'); MF = &Func; MFI = MF->getFrameInfo(); Indexes = &getAnalysis(); BlockLiveness.clear(); BasicBlocks.clear(); BasicBlockNumbering.clear(); Markers.clear(); Intervals.clear(); VNInfoAllocator.Reset(); unsigned NumSlots = MFI->getObjectIndexEnd(); // If there are no stack slots then there are no markers to remove. if (!NumSlots) return false; SmallVector SortedSlots; SortedSlots.reserve(NumSlots); Intervals.reserve(NumSlots); unsigned NumMarkers = collectMarkers(NumSlots); unsigned TotalSize = 0; DEBUG(dbgs()<<"Found "<getObjectIndexEnd(); ++i) { DEBUG(dbgs()<<"Slot #"<getObjectSize(i)<<" bytes.\n"); TotalSize += MFI->getObjectSize(i); } DEBUG(dbgs()<<"Total Stack size: "<getNextValue(Indexes->getZeroIndex(), VNInfoAllocator); SortedSlots.push_back(i); } // Calculate the liveness of each block. calculateLocalLiveness(); // Propagate the liveness information. calculateLiveIntervals(NumSlots); // Search for allocas which are used outside of the declared lifetime // markers. if (ProtectFromEscapedAllocas) removeInvalidSlotRanges(); // Maps old slots to new slots. DenseMap SlotRemap; unsigned RemovedSlots = 0; unsigned ReducedSize = 0; // Do not bother looking at empty intervals. for (unsigned I = 0; I < NumSlots; ++I) { if (Intervals[SortedSlots[I]]->empty()) SortedSlots[I] = -1; } // This is a simple greedy algorithm for merging allocas. First, sort the // slots, placing the largest slots first. Next, perform an n^2 scan and look // for disjoint slots. When you find disjoint slots, merge the samller one // into the bigger one and update the live interval. Remove the small alloca // and continue. // Sort the slots according to their size. Place unused slots at the end. // Use stable sort to guarantee deterministic code generation. std::stable_sort(SortedSlots.begin(), SortedSlots.end(), SlotSizeSorter(MFI)); bool Changed = true; while (Changed) { Changed = false; for (unsigned I = 0; I < NumSlots; ++I) { if (SortedSlots[I] == -1) continue; for (unsigned J=I+1; J < NumSlots; ++J) { if (SortedSlots[J] == -1) continue; int FirstSlot = SortedSlots[I]; int SecondSlot = SortedSlots[J]; LiveInterval *First = Intervals[FirstSlot]; LiveInterval *Second = Intervals[SecondSlot]; assert (!First->empty() && !Second->empty() && "Found an empty range"); // Merge disjoint slots. if (!First->overlaps(*Second)) { Changed = true; First->MergeSegmentsInAsValue(*Second, First->getValNumInfo(0)); SlotRemap[SecondSlot] = FirstSlot; SortedSlots[J] = -1; DEBUG(dbgs()<<"Merging #"<getObjectAlignment(FirstSlot), MFI->getObjectAlignment(SecondSlot)); assert(MFI->getObjectSize(FirstSlot) >= MFI->getObjectSize(SecondSlot) && "Merging a small object into a larger one"); RemovedSlots+=1; ReducedSize += MFI->getObjectSize(SecondSlot); MFI->setObjectAlignment(FirstSlot, MaxAlignment); MFI->RemoveStackObject(SecondSlot); } } } }// While changed. // Record statistics. StackSpaceSaved += ReducedSize; StackSlotMerged += RemovedSlots; DEBUG(dbgs()<<"Merge "<