//===-- StackMapLivenessAnalysis.cpp - StackMap live Out Analysis ----------===// // // The LLVM Compiler Infrastructure // // This file is distributed under the University of Illinois Open Source // License. See LICENSE.TXT for details. // //===----------------------------------------------------------------------===// // // This file implements the StackMap Liveness analysis pass. The pass calculates // the liveness for each basic block in a function and attaches the register // live-out information to a stackmap or patchpoint intrinsic if present. // //===----------------------------------------------------------------------===// #include "llvm/ADT/Statistic.h" #include "llvm/CodeGen/MachineFrameInfo.h" #include "llvm/CodeGen/MachineFunction.h" #include "llvm/CodeGen/MachineFunctionAnalysis.h" #include "llvm/CodeGen/Passes.h" #include "llvm/CodeGen/StackMapLivenessAnalysis.h" #include "llvm/Support/CommandLine.h" #include "llvm/Support/Debug.h" using namespace llvm; #define DEBUG_TYPE "stackmaps" namespace llvm { cl::opt EnableStackMapLiveness("enable-stackmap-liveness", cl::Hidden, cl::desc("Enable StackMap Liveness Analysis Pass")); cl::opt EnablePatchPointLiveness("enable-patchpoint-liveness", cl::Hidden, cl::desc("Enable PatchPoint Liveness Analysis Pass")); } STATISTIC(NumStackMapFuncVisited, "Number of functions visited"); STATISTIC(NumStackMapFuncSkipped, "Number of functions skipped"); STATISTIC(NumBBsVisited, "Number of basic blocks visited"); STATISTIC(NumBBsHaveNoStackmap, "Number of basic blocks with no stackmap"); STATISTIC(NumStackMaps, "Number of StackMaps visited"); char StackMapLiveness::ID = 0; char &llvm::StackMapLivenessID = StackMapLiveness::ID; INITIALIZE_PASS(StackMapLiveness, "stackmap-liveness", "StackMap Liveness Analysis", false, false) /// Default construct and initialize the pass. StackMapLiveness::StackMapLiveness() : MachineFunctionPass(ID) { initializeStackMapLivenessPass(*PassRegistry::getPassRegistry()); } /// Tell the pass manager which passes we depend on and what information we /// preserve. void StackMapLiveness::getAnalysisUsage(AnalysisUsage &AU) const { // We preserve all information. AU.setPreservesAll(); AU.setPreservesCFG(); // Default dependencie for all MachineFunction passes. AU.addRequired(); } /// Calculate the liveness information for the given machine function. bool StackMapLiveness::runOnMachineFunction(MachineFunction &_MF) { DEBUG(dbgs() << "********** COMPUTING STACKMAP LIVENESS: " << _MF.getName() << " **********\n"); MF = &_MF; TRI = MF->getTarget().getRegisterInfo(); ++NumStackMapFuncVisited; // Skip this function if there are no stackmaps or patchpoints to process. if (!((MF->getFrameInfo()->hasStackMap() && EnableStackMapLiveness) || (MF->getFrameInfo()->hasPatchPoint() && EnablePatchPointLiveness))) { ++NumStackMapFuncSkipped; return false; } return calculateLiveness(); } /// Performs the actual liveness calculation for the function. bool StackMapLiveness::calculateLiveness() { bool HasChanged = false; // For all basic blocks in the function. for (MachineFunction::iterator MBBI = MF->begin(), MBBE = MF->end(); MBBI != MBBE; ++MBBI) { DEBUG(dbgs() << "****** BB " << MBBI->getName() << " ******\n"); LiveRegs.init(TRI); LiveRegs.addLiveOuts(MBBI); bool HasStackMap = false; // Reverse iterate over all instructions and add the current live register // set to an instruction if we encounter a stackmap or patchpoint // instruction. for (MachineBasicBlock::reverse_iterator I = MBBI->rbegin(), E = MBBI->rend(); I != E; ++I) { int Opc = I->getOpcode(); if ((EnableStackMapLiveness && (Opc == TargetOpcode::STACKMAP)) || (EnablePatchPointLiveness && (Opc == TargetOpcode::PATCHPOINT))) { addLiveOutSetToMI(*I); HasChanged = true; HasStackMap = true; ++NumStackMaps; } DEBUG(dbgs() << " " << LiveRegs << " " << *I); LiveRegs.stepBackward(*I); } ++NumBBsVisited; if (!HasStackMap) ++NumBBsHaveNoStackmap; } return HasChanged; } /// Add the current register live set to the instruction. void StackMapLiveness::addLiveOutSetToMI(MachineInstr &MI) { uint32_t *Mask = createRegisterMask(); MachineOperand MO = MachineOperand::CreateRegLiveOut(Mask); MI.addOperand(*MF, MO); } /// Create a register mask and initialize it with the registers from the /// register live set. uint32_t *StackMapLiveness::createRegisterMask() const { // The mask is owned and cleaned up by the Machine Function. uint32_t *Mask = MF->allocateRegisterMask(TRI->getNumRegs()); for (LivePhysRegs::const_iterator RI = LiveRegs.begin(), RE = LiveRegs.end(); RI != RE; ++RI) Mask[*RI / 32] |= 1U << (*RI % 32); return Mask; }